1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
|
/**
* @file servo.h
* @brief Implements a generic clock servo interface.
* @note Copyright (C) 2011 Richard Cochran <richardcochran@gmail.com>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 2 of the License, or
* (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License along
* with this program; if not, write to the Free Software Foundation, Inc.,
* 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
*/
#ifndef HAVE_SERVO_H
#define HAVE_SERVO_H
#include <stdint.h>
struct config;
/** Opaque type */
struct servo;
/**
* Defines the available servo cores
*/
enum servo_type {
CLOCK_SERVO_PI,
CLOCK_SERVO_LINREG,
CLOCK_SERVO_NTPSHM,
CLOCK_SERVO_NULLF,
};
/**
* Defines the caller visible states of a clock servo.
*/
enum servo_state {
/**
* The servo is not yet ready to track the master clock.
*/
SERVO_UNLOCKED,
/**
* The is ready to track and requests a clock jump to
* immediately correct the estimated offset.
*/
SERVO_JUMP,
/**
* The servo is tracking the master clock.
*/
SERVO_LOCKED,
};
/**
* Create a new instance of a clock servo.
* @param type The type of the servo to create.
* @param fadj The clock's current adjustment in parts per billion.
* @param max_ppb The absolute maxinum adjustment allowed by the clock
* in parts per billion. The clock servo will clamp its
* output according to this limit.
* @param sw_ts Indicates that software time stamping will be used,
* and the servo should use more aggressive filtering.
* @return A pointer to a new servo on success, NULL otherwise.
*/
struct servo *servo_create(struct config *cfg, enum servo_type type,
int fadj, int max_ppb, int sw_ts);
/**
* Destroy an instance of a clock servo.
* @param servo Pointer to a servo obtained via @ref servo_create().
*/
void servo_destroy(struct servo *servo);
/**
* Feed a sample into a clock servo.
* @param servo Pointer to a servo obtained via @ref servo_create().
* @param offset The estimated clock offset in nanoseconds.
* @param local_ts The local time stamp of the sample in nanoseconds.
* @param weight The weight of the sample, larger if more reliable,
* 1.0 is the maximum value.
* @param state Returns the servo's state.
* @return The clock adjustment in parts per billion.
*/
double servo_sample(struct servo *servo,
int64_t offset,
uint64_t local_ts,
double weight,
enum servo_state *state);
/**
* Inform a clock servo about the master's sync interval.
* @param servo Pointer to a servo obtained via @ref servo_create().
* @param interval The sync interval in seconds.
*/
void servo_sync_interval(struct servo *servo, double interval);
/**
* Reset a clock servo.
* @param servo Pointer to a servo obtained via @ref servo_create().
*/
void servo_reset(struct servo *servo);
/**
* Obtain ratio between master's frequency and current servo frequency.
* @param servo Pointer to a servo obtained via @ref servo_create().
* @return The rate ratio, 1.0 is returned when not known.
*/
double servo_rate_ratio(struct servo *servo);
/**
* Inform a clock servo about upcoming leap second.
* @param servo Pointer to a servo obtained via @ref servo_create().
* @param leap +1 when leap second will be inserted, -1 when leap second
* will be deleted, 0 when it passed.
*/
void servo_leap(struct servo *servo, int leap);
#endif
|