diff options
author | Jason Reeder | 2015-10-16 16:58:36 -0500 |
---|---|---|
committer | Jason Reeder | 2015-10-16 16:58:36 -0500 |
commit | c550c2e3ed65bd4c881b3afae09dc18c666c5a13 (patch) | |
tree | 827d9cf0639e04c16e8f8ee0b4958aa753c829db | |
parent | cfd75be8de951e246b087e5e96085a8cfc650883 (diff) | |
download | pru-software-support-package-c550c2e3ed65bd4c881b3afae09dc18c666c5a13.tar.gz pru-software-support-package-c550c2e3ed65bd4c881b3afae09dc18c666c5a13.tar.xz pru-software-support-package-c550c2e3ed65bd4c881b3afae09dc18c666c5a13.zip |
Updating the ReadMe files
Signed-off-by: Jason Reeder <jreeder@ti.com>
-rwxr-xr-x | ReadMe.txt | 14 | ||||
-rwxr-xr-x | examples/am335x/ReadMe.txt | 49 | ||||
-rwxr-xr-x | examples/am437x/ReadMe.txt (renamed from examples/ReadMe.txt) | 23 | ||||
-rwxr-xr-x | examples/am572x/ReadMe.txt | 45 | ||||
-rwxr-xr-x | labs/ReadMe.txt | 4 |
5 files changed, 115 insertions, 20 deletions
@@ -25,12 +25,12 @@ WHAT's INCLUDED? | |||
25 | 25 | ||
26 | DIRECTORY CONTENTS | 26 | DIRECTORY CONTENTS |
27 | --------- -------- | 27 | --------- -------- |
28 | examples Basic PRU examples | 28 | examples Basic PRU examples |
29 | include PRU firmware header files | 29 | include PRU firmware header files |
30 | labs Source code for step-by-step labs | 30 | labs Source code for step-by-step labs |
31 | lib PRU library files and library source files | 31 | lib PRU library files and library source files |
32 | patches Linux kernel patches to enable PRU support | 32 | patches Linux kernel patches to enable PRU support |
33 | pru_cape Demo software for the BeagleBone PRU Cape | 33 | pru_cape Demo software for the BeagleBone PRU Cape |
34 | 34 | ||
35 | 35 | ||
36 | 36 | ||
@@ -41,5 +41,5 @@ ADDITIONAL RESOURCES | |||
41 | PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS | 41 | PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS |
42 | PRU Training Slides – http://www.ti.com/sitarabootcamp | 42 | PRU Training Slides – http://www.ti.com/sitarabootcamp |
43 | PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE | 43 | PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE |
44 | Support – http://e2e.ti.com | 44 | Support – http://e2e.ti.com |
45 | 45 | ||
diff --git a/examples/am335x/ReadMe.txt b/examples/am335x/ReadMe.txt new file mode 100755 index 0000000..6ac0152 --- /dev/null +++ b/examples/am335x/ReadMe.txt | |||
@@ -0,0 +1,49 @@ | |||
1 | Programmable Real-time Unit (PRU) Software Support Package | ||
2 | ------------------------------------------------------------ | ||
3 | ============================================================ | ||
4 | EXAMPLES | ||
5 | ============================================================ | ||
6 | |||
7 | DESCRIPTION | ||
8 | |||
9 | This directory provides basic "building block" examples for the PRU. Each | ||
10 | example demonstrates a particular feature of the PRU. The concepts shown in | ||
11 | these examples can be combined to create PRU applications. Hence, they are | ||
12 | considered "building blocks." | ||
13 | |||
14 | |||
15 | |||
16 | WHAT EXAMPLES ARE INCLUDED? | ||
17 | |||
18 | The following examples are included in this directory. | ||
19 | |||
20 | EXAMPLE | ||
21 | --------- | ||
22 | PRU_access_const_table | ||
23 | PRU_ARMtoPRU_Interrupt | ||
24 | PRU_Direct_Connect0 | ||
25 | PRU_Direct_Connect1 | ||
26 | PRU_Halt | ||
27 | PRU_edmaConfig | ||
28 | PRU_gpioToggle | ||
29 | PRU_Hardware_UART | ||
30 | PRU_IEP | ||
31 | PRU_MAC_Multiply_Accum | ||
32 | PRU_mem1DTransfer | ||
33 | PRU_PRUtoARM_Interrupt | ||
34 | PRU_RPMsg_Echo_Interrupt0 | ||
35 | PRU_RPMsg_Echo_Interrupt1 | ||
36 | PRU_RPMsg_Echo_Polling0 | ||
37 | PRU_RPMsg_Echo_Polling1 | ||
38 | |||
39 | |||
40 | |||
41 | ADDITIONAL RESOURCES | ||
42 | |||
43 | For more information about the PRU, visit: | ||
44 | |||
45 | PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS | ||
46 | PRU Training Slides – http://www.ti.com/sitarabootcamp | ||
47 | PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE | ||
48 | Support – http://e2e.ti.com | ||
49 | |||
diff --git a/examples/ReadMe.txt b/examples/am437x/ReadMe.txt index 5abab6e..27308a2 100755 --- a/examples/ReadMe.txt +++ b/examples/am437x/ReadMe.txt | |||
@@ -6,23 +6,24 @@ Programmable Real-time Unit (PRU) Software Support Package | |||
6 | 6 | ||
7 | DESCRIPTION | 7 | DESCRIPTION |
8 | 8 | ||
9 | This directory provides basic "building block" examples for the PRU. Each | 9 | This directory provides basic "building block" examples for the PRU. Each |
10 | example demonstrates a particular feature of the PRU. The concepts shown in | 10 | example demonstrates a particular feature of the PRU. The concepts shown in |
11 | these examples can be combined to create PRU applications. Hence, they are | 11 | these examples can be combined to create PRU applications. Hence, they are |
12 | considered "building blocks." | 12 | considered "building blocks." |
13 | 13 | ||
14 | 14 | ||
15 | 15 | ||
16 | WHAT EXAMPLES ARE INCLUDED? | 16 | WHAT EXAMPLES ARE INCLUDED? |
17 | 17 | ||
18 | The following examples are included in this directory. | 18 | The following examples are included in this directory. |
19 | 19 | ||
20 | EXAMPLE | 20 | EXAMPLE |
21 | --------- | 21 | --------- |
22 | PRU_access_const_table | 22 | PRU_access_const_table |
23 | PRU_ARMtoPRU_Interrupt | 23 | PRU_ARMtoPRU_Interrupt |
24 | PRU_Direct_Connect0 | 24 | PRU_Direct_Connect0 |
25 | PRU_Direct_Connect1 | 25 | PRU_Direct_Connect1 |
26 | PRU_Halt | ||
26 | PRU_edmaConfig | 27 | PRU_edmaConfig |
27 | PRU_gpioToggle | 28 | PRU_gpioToggle |
28 | PRU_Hardware_UART | 29 | PRU_Hardware_UART |
@@ -39,10 +40,10 @@ WHAT EXAMPLES ARE INCLUDED? | |||
39 | 40 | ||
40 | ADDITIONAL RESOURCES | 41 | ADDITIONAL RESOURCES |
41 | 42 | ||
42 | For more information about the PRU, visit: | 43 | For more information about the PRU, visit: |
43 | 44 | ||
44 | PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS | 45 | PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS |
45 | PRU Training Slides – http://www.ti.com/sitarabootcamp | 46 | PRU Training Slides – http://www.ti.com/sitarabootcamp |
46 | PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE | 47 | PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE |
47 | Support – http://e2e.ti.com | 48 | Support – http://e2e.ti.com |
48 | 49 | ||
diff --git a/examples/am572x/ReadMe.txt b/examples/am572x/ReadMe.txt new file mode 100755 index 0000000..8f28a6d --- /dev/null +++ b/examples/am572x/ReadMe.txt | |||
@@ -0,0 +1,45 @@ | |||
1 | Programmable Real-time Unit (PRU) Software Support Package | ||
2 | ------------------------------------------------------------ | ||
3 | ============================================================ | ||
4 | EXAMPLES | ||
5 | ============================================================ | ||
6 | |||
7 | DESCRIPTION | ||
8 | |||
9 | This directory provides basic "building block" examples for the PRU. Each | ||
10 | example demonstrates a particular feature of the PRU. The concepts shown in | ||
11 | these examples can be combined to create PRU applications. Hence, they are | ||
12 | considered "building blocks." | ||
13 | |||
14 | |||
15 | |||
16 | WHAT EXAMPLES ARE INCLUDED? | ||
17 | |||
18 | The following examples are included in this directory. | ||
19 | |||
20 | EXAMPLE | ||
21 | --------- | ||
22 | PRU_Direct_Connect0 | ||
23 | PRU_Direct_Connect1 | ||
24 | PRU_Halt | ||
25 | PRU_MAC_Multiply_Accum | ||
26 | PRU_RPMsg_Echo_Interrupt1_0 | ||
27 | PRU_RPMsg_Echo_Interrupt1_1 | ||
28 | PRU_RPMsg_Echo_Interrupt2_0 | ||
29 | PRU_RPMsg_Echo_Interrupt2_1 | ||
30 | PRU_RPMsg_Echo_Polling1_0 | ||
31 | PRU_RPMsg_Echo_Polling1_1 | ||
32 | PRU_RPMsg_Echo_Polling2_0 | ||
33 | PRU_RPMsg_Echo_Polling2_1 | ||
34 | |||
35 | |||
36 | |||
37 | ADDITIONAL RESOURCES | ||
38 | |||
39 | For more information about the PRU, visit: | ||
40 | |||
41 | PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS | ||
42 | PRU Training Slides – http://www.ti.com/sitarabootcamp | ||
43 | PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE | ||
44 | Support – http://e2e.ti.com | ||
45 | |||
diff --git a/labs/ReadMe.txt b/labs/ReadMe.txt index fca6bf5..7b9071c 100755 --- a/labs/ReadMe.txt +++ b/labs/ReadMe.txt | |||
@@ -30,10 +30,10 @@ WHAT LABS ARE INCLUDED? | |||
30 | 30 | ||
31 | ADDITIONAL RESOURCES | 31 | ADDITIONAL RESOURCES |
32 | 32 | ||
33 | For more information about the PRU, visit: | 33 | For more information about the PRU, visit: |
34 | 34 | ||
35 | PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS | 35 | PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS |
36 | PRU Training Slides – http://www.ti.com/sitarabootcamp | 36 | PRU Training Slides – http://www.ti.com/sitarabootcamp |
37 | PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE | 37 | PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE |
38 | Support – http://e2e.ti.com | 38 | Support – http://e2e.ti.com |
39 | 39 | ||