diff options
author | Jason Reeder | 2016-03-15 13:28:01 -0500 |
---|---|---|
committer | Jason Reeder | 2016-03-15 13:28:01 -0500 |
commit | 32396e60e4c0628d065e85afcedfacfd2c6ca2cd (patch) | |
tree | a2bd4392099c51ea5a9cdc0252492256225ca6db /labs | |
parent | 6f42b6006ba7a98c7ad9075424b8f77e8d531ab0 (diff) | |
download | pru-software-support-package-32396e60e4c0628d065e85afcedfacfd2c6ca2cd.tar.gz pru-software-support-package-32396e60e4c0628d065e85afcedfacfd2c6ca2cd.tar.xz pru-software-support-package-32396e60e4c0628d065e85afcedfacfd2c6ca2cd.zip |
Removing code that causes compiler warnings
There were several places where a halt instruction was being
used after a while(1) loop. These halt instructions have
been removed.
There were also two instances where a 32 bit pointer was
getting used as an 8 bit pointer which caused a compiler
warning. This has been corrected.
Signed-off-by: Jason Reeder <jreeder@ti.com>
Diffstat (limited to 'labs')
-rwxr-xr-x | labs/lab_2/button_led_0.c | 3 | ||||
-rwxr-xr-x | labs/lab_2/button_led_1.c | 3 | ||||
-rwxr-xr-x | labs/lab_2/solution/button_led_0/button_led_0.c | 3 | ||||
-rwxr-xr-x | labs/lab_2/solution/button_led_1/button_led_1.c | 3 | ||||
-rwxr-xr-x | labs/lab_4/solution/button_led_0/button_led_0.c | 3 | ||||
-rwxr-xr-x | labs/lab_4/solution/button_led_1/button_led_1.c | 3 |
6 files changed, 0 insertions, 18 deletions
diff --git a/labs/lab_2/button_led_0.c b/labs/lab_2/button_led_0.c index 9babaf7..a98f134 100755 --- a/labs/lab_2/button_led_0.c +++ b/labs/lab_2/button_led_0.c | |||
@@ -95,8 +95,5 @@ void main(){ | |||
95 | /* TODO: Trigger interrupt - see #defines */ | 95 | /* TODO: Trigger interrupt - see #defines */ |
96 | } | 96 | } |
97 | } | 97 | } |
98 | |||
99 | /* Halt the PRU core - shouldn't get here */ | ||
100 | __halt(); | ||
101 | } | 98 | } |
102 | 99 | ||
diff --git a/labs/lab_2/button_led_1.c b/labs/lab_2/button_led_1.c index bd5b0a9..9575c12 100755 --- a/labs/lab_2/button_led_1.c +++ b/labs/lab_2/button_led_1.c | |||
@@ -59,8 +59,5 @@ void main(){ | |||
59 | CT_INTC.SICR = /*TODO: Clear event 16*/; | 59 | CT_INTC.SICR = /*TODO: Clear event 16*/; |
60 | } | 60 | } |
61 | } | 61 | } |
62 | |||
63 | /* Halt the PRU core - shouldn't get here */ | ||
64 | __halt(); | ||
65 | } | 62 | } |
66 | 63 | ||
diff --git a/labs/lab_2/solution/button_led_0/button_led_0.c b/labs/lab_2/solution/button_led_0/button_led_0.c index 5407a47..8de1b5c 100755 --- a/labs/lab_2/solution/button_led_0/button_led_0.c +++ b/labs/lab_2/solution/button_led_0/button_led_0.c | |||
@@ -99,8 +99,5 @@ void main(){ | |||
99 | PRU0_PRU1_TRIGGER; | 99 | PRU0_PRU1_TRIGGER; |
100 | } | 100 | } |
101 | } | 101 | } |
102 | |||
103 | /* Halt the PRU core - shouldn't get here */ | ||
104 | __halt(); | ||
105 | } | 102 | } |
106 | 103 | ||
diff --git a/labs/lab_2/solution/button_led_1/button_led_1.c b/labs/lab_2/solution/button_led_1/button_led_1.c index 9b1bbb0..f4d7883 100755 --- a/labs/lab_2/solution/button_led_1/button_led_1.c +++ b/labs/lab_2/solution/button_led_1/button_led_1.c | |||
@@ -63,8 +63,5 @@ void main(){ | |||
63 | __delay_cycles(5); | 63 | __delay_cycles(5); |
64 | } | 64 | } |
65 | } | 65 | } |
66 | |||
67 | /* Halt the PRU core - shouldn't get here */ | ||
68 | __halt(); | ||
69 | } | 66 | } |
70 | 67 | ||
diff --git a/labs/lab_4/solution/button_led_0/button_led_0.c b/labs/lab_4/solution/button_led_0/button_led_0.c index 58ad514..3183984 100755 --- a/labs/lab_4/solution/button_led_0/button_led_0.c +++ b/labs/lab_4/solution/button_led_0/button_led_0.c | |||
@@ -100,8 +100,5 @@ void main(){ | |||
100 | PRU0_PRU1_TRIGGER; | 100 | PRU0_PRU1_TRIGGER; |
101 | } | 101 | } |
102 | } | 102 | } |
103 | |||
104 | /* Halt the PRU core - shouldn't get here */ | ||
105 | __halt(); | ||
106 | } | 103 | } |
107 | 104 | ||
diff --git a/labs/lab_4/solution/button_led_1/button_led_1.c b/labs/lab_4/solution/button_led_1/button_led_1.c index ce99987..c7859b9 100755 --- a/labs/lab_4/solution/button_led_1/button_led_1.c +++ b/labs/lab_4/solution/button_led_1/button_led_1.c | |||
@@ -64,8 +64,5 @@ void main(){ | |||
64 | __delay_cycles(5); | 64 | __delay_cycles(5); |
65 | } | 65 | } |
66 | } | 66 | } |
67 | |||
68 | /* Halt the PRU core - shouldn't get here */ | ||
69 | __halt(); | ||
70 | } | 67 | } |
71 | 68 | ||