aboutsummaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* examples: add TRM links to READMEsNick Saulnier2020-04-304-0/+4
* examples/am65x: Update the examples for AM65x SR2.0Suman Anna2020-04-2219-85/+625
* examples/am65x: Update labels in linker command filesSuman Anna2020-04-2212-291/+291
* examples/am65x: Cleanup Halt and MAC_Multiply_Accum MakefilesSuman Anna2020-04-224-36/+36
* am65x examples: add ReadMeNick Saulnier2019-12-091-0/+59
* PRU_gpioToggle: toggle all GPO pins by defaultNick Saulnier2019-12-092-4/+6
* Examples: J721E: Add Halt examplesv5.5.0Suman Anna2019-09-0616-1/+1460
* Examples: J721E: Add RPMsg examples for J721E SoCsSuman Anna2019-09-0618-1/+2017
* Examples: Use FW_RSC_ADDR_ANY for vring device addressesSuman Anna2019-08-0219-38/+38
* examples/am335x: update commentsNick Saulnier2019-02-064-0/+23
* examples/am335x/PRU_ADC_onChip: bug fixesv5.4.0Nick Saulnier2018-11-273-5/+13
* examples/am335x: rename PRU_ADC to PRU_ADC_onChipv5.3.0Nick Saulnier2018-09-108-1/+1
* labs: Lab_0, Lab_5 cleanupNick Saulnier2018-08-281-0/+0
* examples: fixed datesNick Saulnier2018-08-2658-73/+73
* examples, labs: Linux kernel 4.14 Resource TableNick Saulnier2018-08-2627-73/+73
* examples/am65x: re-updated linker command filesNick Saulnier2018-08-2612-228/+204
* RPMsg: Add RPMSG_MESSAGE_SIZENick Saulnier2018-08-2620-37/+21
* examples/am65x: updated linker command filesNick Saulnier2018-08-1212-150/+174
* examples/am65x: added Halt, MAC_Multiply_AccumNick Saulnier2018-08-1221-1/+2026
* examples/am65x: updated RPMsg examplesNick Saulnier2018-08-124-8/+8
* examples: Update RPMsg payload message lengthv5.2.1Nick Saulnier2018-07-2414-28/+56
* examples/am335x: Add PRU_ADC exampleNick Saulnier2018-07-247-0/+967
* examples: Bug fixes for EMCR addrNick Saulnier2018-07-242-2/+2
* examples: Update DDR len in Linkr Cmd FilesNick Saulnier2018-07-2444-44/+44
* Examples: AM65x: Add RPMsg examples for AM65x SoCsv5.2.0Suman Anna2018-06-2718-1/+2021
* Make it more clear that CCS is not needed to build fwsv5.0.1Jason Reeder2016-09-0744-176/+572
* [WIP] Updating makefiles using scriptJason Reeder2016-09-0644-308/+396
* Correcting capitalization in RPMsg example commentsJason Reeder2016-07-2214-22/+22
* Remove SYSCFG accesses from AM437x PRUSS0 codeJason Reeder2016-07-222-4/+14
* Examples: Update Readme filesSuman Anna2016-07-114-14/+0
* Indentation and comment fixes in RPMsg codeJason Reeder2016-06-2314-101/+101
* Improve the abstraction of RPMsg lib and examplesJason Reeder2016-06-2314-84/+28
* Further line ending and trailing whitespace cleanupJason Reeder2016-06-204-196/+196
* Add includes and examples for k2g (66AK2G02)Jason Reeder2016-05-2035-1/+2969
* Convert RPMsg examples from mailboxes to interruptsJason Reeder2016-05-2093-5940/+249
* Reformat code and remove whitespace errorsAndrew F. Davis2016-05-09140-6962/+7008
* Remove exacutable bit from file permissions for code filesAndrew F. Davis2016-05-09233-0/+0
* PRUSS0 enablement patch update to latest SDKJason Reeder2016-04-281-75/+2350
* Differentiate between AM572x silicon revisionsv4.0.2Jason Reeder2016-03-1624-286/+286
* Removing code that causes compiler warningsJason Reeder2016-03-154-8/+2
* Ability to use PRUSS0 instead of PRUSS1 on AM437xJason Reeder2016-01-2855-944/+1948
* Moving PRU_SHAREDMEM to PAGE 2 in the linker filesJason Reeder2016-01-2742-0/+84
* Updating the ReadMe filesJason Reeder2015-10-163-11/+106
* Putting a halt example into each device folderJason Reeder2015-10-1430-3/+1529
* Removing AM571x examples from this releaseJason Reeder2015-10-14101-6999/+1
* Adding example for the AM57xx devicesJason Reeder2015-10-1456-2/+3382
* Updating the CCS build configurationsJason Reeder2015-10-1430-2168/+2228
* Added a status check in the RPMsg examplesJason Reeder2015-10-1424-172/+436
* Adding RPMsg examples for AM571x and AM572xJason Reeder2015-10-13147-3/+10409
* Copy examples into device-specific foldersJason Reeder2015-10-13273-1050/+9406