aboutsummaryrefslogtreecommitdiffstats
path: root/labs
Commit message (Expand)AuthorAgeFilesLines
* labs: update AM65x linker command filesHEADv5.7.0masterNick Saulnier2020-04-309-282/+298
* labs: fix makefiles for Labsv5.6.0Nick Saulnier2019-12-1620-36/+80
* labs: Add the PRU Getting Started LabsNick Saulnier2019-12-09239-379/+8081
* Labs: Use FW_RSC_ADDR_ANY for vring device addressesNick Saulnier2019-08-026-12/+12
* labs: Lab_0, Lab_5 cleanupNick Saulnier2018-08-285-10/+23
* examples: fixed datesNick Saulnier2018-08-2612-17/+13
* examples, labs: Linux kernel 4.14 Resource TableNick Saulnier2018-08-2652-470/+2995
* RPMsg: Add RPMSG_MESSAGE_SIZENick Saulnier2018-08-262-4/+4
* labs: add lab_0Nick Saulnier2018-08-2626-0/+2098
* Mimic the StarterWare PRU cape demo on Linux consolev5.1.0Jason Reeder2016-11-151-2/+1
* Fixed an ECAP interrupt issue in the TempSensor demoJason Reeder2016-11-151-0/+1
* Make it more clear that CCS is not needed to build fwsv5.0.1Jason Reeder2016-09-0710-40/+130
* [WIP] Updating makefiles using scriptJason Reeder2016-09-0610-70/+90
* Correcting capitalization in RPMsg example commentsJason Reeder2016-07-222-4/+4
* Remove the hex utility step from lab projectsJason Reeder2016-06-245-45/+23
* Indentation and comment fixes in RPMsg codeJason Reeder2016-06-232-17/+17
* Improve the abstraction of RPMsg lib and examplesJason Reeder2016-06-232-12/+4
* Further line ending and trailing whitespace cleanupJason Reeder2016-06-201-38/+38
* Convert RPMsg examples from mailboxes to interruptsJason Reeder2016-05-204-75/+74
* Reformat code and remove whitespace errorsAndrew F. Davis2016-05-0939-1859/+1883
* Remove exacutable bit from file permissions for code filesAndrew F. Davis2016-05-0971-0/+0
* Removing code that causes compiler warningsJason Reeder2016-03-156-18/+0
* Adding PAGE 2 to the hex utility input filesJason Reeder2016-01-272-4/+8
* Moving PRU_SHAREDMEM to PAGE 2 in the linker filesJason Reeder2016-01-2712-2/+26
* Modifying CCS build configurationsv4.0.0Jason Reeder2015-10-161-0/+4
* Updating the ReadMe filesJason Reeder2015-10-161-2/+2
* Added a status check in the RPMsg examplesJason Reeder2015-10-142-18/+40
* Update the labs/cape examples include folderJason Reeder2015-10-1324-18/+46
* Updating the BSD License header in the source codeJason Reeder2015-08-1326-700/+772
* Changing the copyright date to 2015Jason Reeder2015-08-1034-32/+92
* Adding the license at the top of the RPMsg filesJason Reeder2015-08-102-0/+60
* Increasing number of buffers in vrings to 16Jason Reeder2015-08-092-4/+4
* Adding a shell script to toggle LEDs to lab 6Jason Reeder2015-08-091-0/+16
* Added comments to the user space RPMsg echo exampleJason Reeder2015-08-091-1/+13
* Making RPMsg channel name comment more descriptiveJason Reeder2015-08-092-2/+7
* Adding a user space rpmsg_pru echo exampleJason Reeder2015-08-091-0/+43
* Adding a __halt() example to lab_5Jason Reeder2015-08-0910-2/+498
* Updating ReadMe.txt filesJason Reeder2015-08-091-1/+3
* Adding the RPMsg LED example as lab 6Jason Reeder2015-08-068-0/+493
* Adding an RPMsg Echo example as lab 5Jason Reeder2015-08-068-0/+531
* Updating CCS build settings for projectsJason Reeder2015-08-0618-528/+645
* Removing the usage of 16-bit bit fieldsJason Reeder2015-08-061-7/+7
* Updating empty resource table headersJason Reeder2015-08-064-140/+36
* Removing constant table structure instantiationsJason Reeder2015-08-069-35/+0
* Correct the CT memory lengths in the linker fileJason Reeder2015-08-069-191/+195
* Adding/Updating MakefilesJason Reeder2015-08-0610-0/+799
* Removing generated lab files from trackingJason Reeder2015-08-0679-24897/+0
* Updated the temp sensor applicationJason Reeder2015-06-302-9/+11
* Update CCS projects for resource table changev2.0.0mwatkins2015-04-308-191/+191
* Update empty Resource Table header filesmwatkins2015-04-302-38/+4