aboutsummaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* RPMsg: Add RPMSG_MESSAGE_SIZENick Saulnier2018-08-261-2/+2
* pru_demo: update fw path in StarterWare MakefileJason Reeder2018-01-021-8/+8
* Mimic the StarterWare PRU cape demo on Linux consolev5.1.0Jason Reeder2016-11-1546-26/+786
* Fixed an ECAP interrupt issue in the TempSensor demoJason Reeder2016-11-151-0/+1
* Update the BeagleBoneBlack PRU cape dtsi fileJason Reeder2016-11-141-6/+11
* Fix incorrect pinout in PRU cape dtsi filesJason Reeder2016-11-142-2/+2
* Make it more clear that CCS is not needed to build fwsv5.0.1Jason Reeder2016-09-078-32/+104
* [WIP] Updating makefiles using scriptJason Reeder2016-09-068-68/+76
* Correcting capitalization in RPMsg example commentsJason Reeder2016-07-221-2/+2
* Add hex utility output to the PRU_RPMsg_LED0 fimwareJason Reeder2016-07-113-8/+46
* Indentation and comment fixes in RPMsg codeJason Reeder2016-06-231-10/+10
* Improve the abstraction of RPMsg lib and examplesJason Reeder2016-06-231-6/+2
* Further line ending and trailing whitespace cleanupJason Reeder2016-06-2010-554/+553
* Convert RPMsg examples from mailboxes to interruptsJason Reeder2016-05-202-24/+51
* Reformat code and remove whitespace errorsAndrew F. Davis2016-05-0941-3188/+3192
* Remove exacutable bit from file permissions for code filesAndrew F. Davis2016-05-0982-0/+0
* Removing code that causes compiler warningsJason Reeder2016-03-154-27/+4
* Adding PAGE 2 to the hex utility input filesJason Reeder2016-01-277-14/+28
* Moving PRU_SHAREDMEM to PAGE 2 in the linker filesJason Reeder2016-01-278-2/+18
* Correcting a typo in the BBB PRU cape dtsi fileJason Reeder2015-11-171-1/+1
* Refer to hdmi and sound node using absolute pathJason Reeder2015-11-161-5/+9
* Modifying CCS build configurationsv4.0.0Jason Reeder2015-10-162-2/+2
* Added a status check in the RPMsg examplesJason Reeder2015-10-141-9/+20
* Update the labs/cape examples include folderJason Reeder2015-10-1319-19/+39
* Updating the BSD License header in the source codeJason Reeder2015-08-1327-814/+815
* Changing the copyright date to 2015Jason Reeder2015-08-1039-39/+39
* Adding the license at the top of the RPMsg filesJason Reeder2015-08-101-0/+30
* Increasing number of buffers in vrings to 16Jason Reeder2015-08-091-2/+2
* Making RPMsg channel name comment more descriptiveJason Reeder2015-08-091-1/+1
* Configure FCR.DMAMODE1=1 per TRMBrad Griffis2015-08-071-1/+1
* Remove unnecessary clearing of FIFOBrad Griffis2015-08-071-4/+0
* Null terminate messages for easier printingBrad Griffis2015-08-071-12/+9
* Simplify new line formattingBrad Griffis2015-08-071-12/+3
* Remove unused variables and typedefsBrad Griffis2015-08-071-23/+0
* Updating CCS build settings for projectsJason Reeder2015-08-0620-553/+644
* Updating the pru_demo project build methodsJason Reeder2015-08-069-113/+777
* Removing the usage of 16-bit bit fieldsJason Reeder2015-08-061-7/+7
* Updating empty resource table headersJason Reeder2015-08-067-140/+0
* Correct the CT memory lengths in the linker fileJason Reeder2015-08-068-164/+164
* Adding/Updating MakefilesJason Reeder2015-08-0610-37/+390
* Removing generated lab files from trackingJason Reeder2015-08-0613-6798/+0
* Adding 'make' build capabilities to all projectsJason Reeder2015-07-319-0/+590
* Add a .gitignore at the toplevel and remove othersJason Reeder2015-07-311-4/+0
* Update examples to use new header constant defsJason Reeder2015-07-098-34/+10
* Removing generated files from the pru-fw directoryJason Reeder2015-07-0971-25150/+0
* Adding an RPMsg LED example for PRU0Jason Reeder2015-07-088-0/+489
* Changing the time interval back to 3 secondsJason Reeder2015-07-071-1/+1
* Adding a .gitignore file to the pru_fw directoryJason Reeder2015-06-301-0/+4
* Updated the temp sensor applicationJason Reeder2015-06-306-24/+28
* Update CCS projects for resource table changev2.0.0mwatkins2015-04-3043-521/+521