From 3a77d6ad63bd82b1202986a5ab3fac589af68558 Mon Sep 17 00:00:00 2001 From: Jason Reeder Date: Mon, 20 Jun 2016 12:54:32 -0500 Subject: Further line ending and trailing whitespace cleanup Signed-off-by: Jason Reeder --- ReadMe.txt | 48 ++++++++++++++++++++++++------------------------ 1 file changed, 24 insertions(+), 24 deletions(-) (limited to 'ReadMe.txt') diff --git a/ReadMe.txt b/ReadMe.txt index 90c4d51..93801c0 100644 --- a/ReadMe.txt +++ b/ReadMe.txt @@ -1,24 +1,24 @@ -Programmable Real-time Unit (PRU) Software Support Package release 5.0 - - -DESCRIPTION - - The PRU Software Support Package is an add-on package that provides a framework - and examples for developing software for the Programmable Real-time Unit - sub-system and Industrial Communication Sub-System (PRU-ICSS) in the supported - TI processors. The PRU-ICSS achieves deterministic, real-time processing, direct - access to I/Os and meets ultra-low-latency requirements. - - This software package contains example PRU firmware code as well as application - loader code for the host OS. The examples demonstrate the PRU capabilities to - interact with and control the system and its resources. - - For more details about the PRU, visit - +Programmable Real-time Unit (PRU) Software Support Package release 5.0 + + +DESCRIPTION + + The PRU Software Support Package is an add-on package that provides a framework + and examples for developing software for the Programmable Real-time Unit + sub-system and Industrial Communication Sub-System (PRU-ICSS) in the supported + TI processors. The PRU-ICSS achieves deterministic, real-time processing, direct + access to I/Os and meets ultra-low-latency requirements. + + This software package contains example PRU firmware code as well as application + loader code for the host OS. The examples demonstrate the PRU capabilities to + interact with and control the system and its resources. + + For more details about the PRU, visit + http://processors.wiki.ti.com/index.php/PRU-ICSS - - - + + + WHAT's INCLUDED? This package includes the following resources: @@ -37,8 +37,8 @@ ADDITIONAL RESOURCES For more information about the PRU, visit: - PRU-ICSS Wiki – http://processors.wiki.ti.com/index.php/PRU-ICSS - PRU Training Slides – http://www.ti.com/sitarabootcamp - PRU Evaluation Hardware – http://www.ti.com/tool/PRUCAPE - Support – http://e2e.ti.com + PRU-ICSS Wiki - http://processors.wiki.ti.com/index.php/PRU-ICSS + PRU Training Slides - http://www.ti.com/sitarabootcamp + PRU Evaluation Hardware - http://www.ti.com/tool/PRUCAPE + Support - http://e2e.ti.com -- cgit v1.2.3-54-g00ecf