blob: b1b9271f06ee81633ed25012fbd9bbea5cc2d578 (
plain) (
blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
|
# PRU_CGT environment variable must point to the TI PRU code gen tools directory. E.g.:
#(Desktop Linux) export PRU_CGT=/path/to/pru/code/gen/tools/ti-cgt-pru_2.1.2
#(Windows) set PRU_CGT=C:/path/to/pru/code/gen/tools/ti-cgt-pru_2.1.2
#(ARM Linux*) export PRU_CGT=/usr/share/ti/cgt-pru
#
# *ARM Linux also needs to create a symbolic link to the /usr/bin/ directory in
# order to use the same Makefile
#(ARM Linux) ln -s /usr/bin/ /usr/share/ti/cgt-pru/bin
ifndef PRU_CGT
define ERROR_BODY
*******************************************************************************
PRU_CGT environment variable is not set. Examples given:
(Desktop Linux) export PRU_CGT=/path/to/pru/code/gen/tools/ti-cgt-pru_2.1.2
(Windows) set PRU_CGT=C:/path/to/pru/code/gen/tools/ti-cgt-pru_2.1.2
(ARM Linux*) export PRU_CGT=/usr/share/ti/cgt-pru
*ARM Linux also needs to create a symbolic link to the /usr/bin/ directory in
order to use the same Makefile
(ARM Linux) ln -s /usr/bin/ /usr/share/ti/cgt-pru/bin
*******************************************************************************
endef
$(error $(ERROR_BODY))
endif
MKFILE_PATH := $(abspath $(lastword $(MAKEFILE_LIST)))
CURRENT_DIR := $(notdir $(patsubst %/,%,$(dir $(MKFILE_PATH))))
PROJ_NAME=$(CURRENT_DIR)
LINKER_COMMAND_FILE=./AM335x_PRU.cmd
LIBS=--library=../../../lib/rpmsg_lib.lib
INCLUDE=--include_path=../../../include --include_path=../../../include/am335x
STACK_SIZE=0x100
HEAP_SIZE=0x100
GEN_DIR=gen
#Common compiler and linker flags (Defined in 'PRU Optimizing C/C++ Compiler User's Guide)
CFLAGS=-v3 -O2 --display_error_number --endian=little --hardware_mac=on --obj_directory=$(GEN_DIR) --pp_directory=$(GEN_DIR) -ppd -ppa
#Linker flags (Defined in 'PRU Optimizing C/C++ Compiler User's Guide)
LFLAGS=--reread_libs --warn_sections --stack_size=$(STACK_SIZE) --heap_size=$(HEAP_SIZE)
TARGET=$(GEN_DIR)/$(PROJ_NAME).out
MAP=$(GEN_DIR)/$(PROJ_NAME).map
SOURCES=$(wildcard *.c)
#Using .object instead of .obj in order to not conflict with the CCS build process
OBJECTS=$(patsubst %,$(GEN_DIR)/%,$(SOURCES:.c=.object))
all: printStart $(TARGET) printEnd
printStart:
@echo ''
@echo '************************************************************'
@echo 'Building project: $(PROJ_NAME)'
printEnd:
@echo ''
@echo 'Output files can be found in the "$(GEN_DIR)" directory'
@echo ''
@echo 'Finished building project: $(PROJ_NAME)'
@echo '************************************************************'
@echo ''
# Invokes the linker (-z flag) to make the .out file
$(TARGET): $(OBJECTS) $(LINKER_COMMAND_FILE)
@echo ''
@echo 'Building target: $@'
@echo 'Invoking: PRU Linker'
$(PRU_CGT)/bin/clpru $(CFLAGS) -z -i$(PRU_CGT)/lib -i$(PRU_CGT)/include $(LFLAGS) -o $(TARGET) $(OBJECTS) -m$(MAP) $(LINKER_COMMAND_FILE) --library=libc.a $(LIBS)
@echo 'Finished building target: $@'
# Invokes the compiler on all c files in the directory to create the object files
$(GEN_DIR)/%.object: %.c
@mkdir -p $(GEN_DIR)
@echo ''
@echo 'Building file: $<'
@echo 'Invoking: PRU Compiler'
$(PRU_CGT)/bin/clpru --include_path=$(PRU_CGT)/include $(INCLUDE) $(CFLAGS) -fe $@ $<
.PHONY: all clean
# Remove the $(GEN_DIR) directory
clean:
@echo ''
@echo '************************************************************'
@echo 'Cleaning project: $(PROJ_NAME)'
@echo ''
@echo 'Removing files in the "$(GEN_DIR)" directory'
@rm -rf $(GEN_DIR)
@echo ''
@echo 'Finished cleaning project: $(PROJ_NAME)'
@echo '************************************************************'
@echo ''
# Includes the dependencies that the compiler creates (-ppd and -ppa flags)
-include $(OBJECTS:%.object=%.pp)
|