/* SPDX-License-Identifier: GPL-2.0 */
/*
* Discontiguous memory support, Kanoj Sarcar, SGI, Nov 1999
*/
#ifndef _LINUX_BOOTMEM_H
#define _LINUX_BOOTMEM_H
#include <linux/mmzone.h>
#include <linux/mm_types.h>
#include <asm/dma.h>
#include <asm/processor.h>
/*
* simple boot-time physical memory area allocator.
*/
extern unsigned long max_low_pfn;
extern unsigned long min_low_pfn;
/*
* highest page
*/
extern unsigned long max_pfn;
/*
* highest possible page
*/
extern unsigned long long max_possible_pfn;
#ifndef CONFIG_NO_BOOTMEM
/**
* struct bootmem_data - per-node information used by the bootmem allocator
* @node_min_pfn: the starting physical address of the node's memory
* @node_low_pfn: the end physical address of the directly addressable memory
* @node_bootmem_map: is a bitmap pointer - the bits represent all physical
* memory pages (including holes) on the node.
* @last_end_off: the offset within the page of the end of the last allocation;
* if 0, the page used is full
* @hint_idx: the PFN of the page used with the last allocation;
* together with using this with the @last_end_offset field,
* a test can be made to see if allocations can be merged
* with the page used for the last allocation rather than
* using up a full new page.
* @list: list entry in the linked list ordered by the memory addresses
*/
typedef struct bootmem_data {
unsigned long node_min_pfn;
unsigned long node_low_pfn;
void *node_bootmem_map;
unsigned long last_end_off;
unsigned long hint_idx;
struct list_head list;
} bootmem_data_t;
extern bootmem_data_t bootmem_node_data[];
#endif
extern unsigned long bootmem_bootmap_pages(unsigned long);
extern unsigned long init_bootmem_node(pg_data_t *pgdat,
unsigned long freepfn,
unsigned long startpfn,
unsigned long endpfn);
extern unsigned long init_bootmem(unsigned long addr, unsigned long memend);
extern unsigned long free_all_bootmem(void);
extern void reset_node_managed_pages(pg_data_t *pgdat);
extern void reset_all_zones_managed_pages(void);
extern void free_bootmem_node(pg_data_t *pgdat,
unsigned long addr,
unsigned long size);
extern void free_bootmem(unsigned long physaddr, unsigned long size);
extern void free_bootmem_late(unsigned long physaddr, unsigned long size);
/*
* Flags for reserve_bootmem (also if CONFIG_HAVE_ARCH_BOOTMEM_NODE,
* the architecture-specific code should honor this).
*
* If flags is BOOTMEM_DEFAULT, then the return value is always 0 (success).
* If flags contains BOOTMEM_EXCLUSIVE, then -EBUSY is returned if the memory
* already was reserved.
*/
#define BOOTMEM_DEFAULT 0
#define BOOTMEM_EXCLUSIVE (1<<0)
extern int reserve_bootmem(unsigned long addr,
unsigned long size,
int flags);
extern int reserve_bootmem_node(pg_data_t *pgdat,
unsigned long physaddr,
unsigned long size,
int flags);
extern void *__alloc_bootmem(unsigned long size,
unsigned long align,
unsigned long goal);
extern void *__alloc_bootmem_nopanic(unsigned long size,
unsigned long align,
unsigned long goal) __malloc;
extern void *__alloc_bootmem_node(pg_data_t *pgdat,
unsigned long size,
unsigned long align,
unsigned long goal) __malloc;
void *__alloc_bootmem_node_high(pg_data_t *pgdat,
unsigned long size,
unsigned long align,
unsigned long goal) __malloc;
extern void *__alloc_bootmem_node_nopanic(pg_data_t *pgdat,
unsigned long size,
unsigned long align,
unsigned long goal) __malloc;
void *___alloc_bootmem_node_nopanic(pg_data_t *pgdat,
unsigned long size,
unsigned long align,
unsigned long goal,
unsigned long limit) __malloc;
extern void *__alloc_bootmem_low(unsigned long size,
unsigned long align,
unsigned long goal) __malloc;
void *__alloc_bootmem_low_nopanic(unsigned long size,
unsigned long align,
unsigned long goal) __malloc;
extern void *__alloc_bootmem_low_node(pg_data_t *pgdat,
unsigned long size,
unsigned long align,
unsigned long goal) __malloc;
#ifdef CONFIG_NO_BOOTMEM
/* We are using top down, so it is safe to use 0 here */
#define BOOTMEM_LOW_LIMIT 0
#else
#define BOOTMEM_LOW_LIMIT __pa(MAX_DMA_ADDRESS)
#endif
#ifndef ARCH_LOW_ADDRESS_LIMIT
#define ARCH_LOW_ADDRESS_LIMIT 0xffffffffUL
#endif
#define alloc_bootmem(x) \
__alloc_bootmem(x, SMP_CACHE_BYTES, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_align(x, align) \
__alloc_bootmem(x, align, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_nopanic(x) \
__alloc_bootmem_nopanic(x, SMP_CACHE_BYTES, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_pages(x) \
__alloc_bootmem(x, PAGE_SIZE, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_pages_nopanic(x) \
__alloc_bootmem_nopanic(x, PAGE_SIZE, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_node(pgdat, x) \
__alloc_bootmem_node(pgdat, x, SMP_CACHE_BYTES, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_node_nopanic(pgdat, x) \
__alloc_bootmem_node_nopanic(pgdat, x, SMP_CACHE_BYTES, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_pages_node(pgdat, x) \
__alloc_bootmem_node(pgdat, x, PAGE_SIZE, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_pages_node_nopanic(pgdat, x) \
__alloc_bootmem_node_nopanic(pgdat, x, PAGE_SIZE, BOOTMEM_LOW_LIMIT)
#define alloc_bootmem_low(x) \
__alloc_bootmem_low(x, SMP_CACHE_BYTES, 0)
#define alloc_bootmem_low_pages_nopanic(x) \
__alloc_bootmem_low_nopanic(x, PAGE_SIZE, 0)
#define alloc_bootmem_low_pages(x) \
__alloc_bootmem_low(x, PAGE_SIZE, 0)
#define alloc_bootmem_low_pages_node(pgdat, x) \
__alloc_bootmem_low_node(pgdat, x, PAGE_SIZE, 0)
#if defined(CONFIG_HAVE_MEMBLOCK) && defined(CONFIG_NO_BOOTMEM)
/* FIXME: use MEMBLOCK_ALLOC_* variants here */
#define BOOTMEM_ALLOC_ACCESSIBLE 0
#define BOOTMEM_ALLOC_ANYWHERE (~(phys_addr_t)0)
/* FIXME: Move to memblock.h at a point where we remove nobootmem.c */
void *memblock_virt_alloc_try_nid_raw(phys_addr_t size, phys_addr_t align,
phys_addr_t min_addr,
phys_addr_t max_addr, int nid);
void *memblock_virt_alloc_try_nid_nopanic(phys_addr_t size,
phys_addr_t align, phys_addr_t min_addr,
phys_addr_t max_addr, int nid);
void *memblock_virt_alloc_try_nid(phys_addr_t size, phys_addr_t align,
phys_addr_t min_addr, phys_addr_t max_addr, int nid);
void __memblock_free_early(phys_addr_t base, phys_addr_t size);
void __memblock_free_late(phys_addr_t base, phys_addr_t size);
static inline void * __init memblock_virt_alloc(
phys_addr_t size, phys_addr_t align)
{
return memblock_virt_alloc_try_nid(size, align, BOOTMEM_LOW_LIMIT,
BOOTMEM_ALLOC_ACCESSIBLE,
NUMA_NO_NODE);
}
static inline void * __init memblock_virt_alloc_raw(
phys_addr_t size, phys_addr_t align)
{
return memblock_virt_alloc_try_nid_raw(size, align, BOOTMEM_LOW_LIMIT,
BOOTMEM_ALLOC_ACCESSIBLE,
NUMA_NO_NODE);
}
static inline void * __init memblock_virt_alloc_nopanic(
phys_addr_t size, phys_addr_t align)
{
return memblock_virt_alloc_try_nid_nopanic(size, align,
BOOTMEM_LOW_LIMIT,
BOOTMEM_ALLOC_ACCESSIBLE,
NUMA_NO_NODE);
}
static inline void * __init memblock_virt_alloc_low(
phys_addr_t size, phys_addr_t align)
{
return memblock_virt_alloc_try_nid(size, align,
BOOTMEM_LOW_LIMIT,
ARCH_LOW_ADDRESS_LIMIT,
NUMA_NO_NODE);
}
static inline void * __init memblock_virt_alloc_low_nopanic(
phys_addr_t size, phys_addr_t align)
{
return memblock_virt_alloc_try_nid_nopanic(size, align,
BOOTMEM_LOW_LIMIT,
ARCH_LOW_ADDRESS_LIMIT,
NUMA_NO_NODE);
}
static inline void * __init memblock_virt_alloc_from_nopanic(
phys_addr_t size, phys_addr_t align, phys_addr_t min_addr)
{
return memblock_virt_alloc_try_nid_nopanic(size, align, min_addr,
BOOTMEM_ALLOC_ACCESSIBLE,
NUMA_NO_NODE);
}
static inline void * __init memblock_virt_alloc_node(
phys_addr_t size, int nid)
{
return memblock_virt_alloc_try_nid(size, 0, BOOTMEM_LOW_LIMIT,
BOOTMEM_ALLOC_ACCESSIBLE, nid);
}
static inline void * __init memblock_virt_alloc_node_nopanic(
phys_addr_t size, int nid)
{
return memblock_virt_alloc_try_nid_nopanic(size, 0, BOOTMEM_LOW_LIMIT,
BOOTMEM_ALLOC_ACCESSIBLE,
nid);
}
static inline void __init memblock_free_early(
phys_addr_t base, phys_addr_t size)
{
__memblock_free_early(base, size);
}
static inline void __init memblock_free_early_nid(
phys_addr_t base, phys_addr_t size, int nid)
{
__memblock_free_early(base, size);
}
static inline void __init memblock_free_late(
phys_addr_t base, phys_addr_t size)
{
__memblock_free_late(base, size);
}
#else
#define BOOTMEM_ALLOC_ACCESSIBLE 0
/* Fall back to all the existing bootmem APIs */
static inline void * __init memblock_virt_alloc(
phys_addr_t size, phys_addr_t align)
{
if (!align)
align = SMP_CACHE_BYTES;
return __alloc_bootmem(size, align, BOOTMEM_LOW_LIMIT);
}
static inline void * __init memblock_virt_alloc_raw(
phys_addr_t size, phys_addr_t align)
{
if (!align)
align = SMP_CACHE_BYTES;
return __alloc_bootmem_nopanic(size, align, BOOTMEM_LOW_LIMIT);
}
static inline void * __init memblock_virt_alloc_nopanic(
phys_addr_t size, phys_addr_t align)
{
if (!align)
align = SMP_CACHE_BYTES;
return __alloc_bootmem_nopanic(size, align, BOOTMEM_LOW_LIMIT);
}
static inline void * __init memblock_virt_alloc_low(
phys_addr_t size, phys_addr_t align)
{
if (!align)
align = SMP_CACHE_BYTES;
return __alloc_bootmem_low(size, align, 0);
}
static inline void * __init memblock_virt_alloc_low_nopanic(
phys_addr_t size, phys_addr_t align)
{
if (!align)
align = SMP_CACHE_BYTES;
return __alloc_bootmem_low_nopanic(size, align, 0);
}
static inline void * __init memblock_virt_alloc_from_nopanic(
phys_addr_t size, phys_addr_t align, phys_addr_t min_addr)
{
return __alloc_bootmem_nopanic(size, align, min_addr);
}
static inline void * __init memblock_virt_alloc_node(
phys_addr_t size, int nid)
{
return __alloc_bootmem_node(NODE_DATA(nid), size, SMP_CACHE_BYTES,
BOOTMEM_LOW_LIMIT);
}
static inline void * __init memblock_virt_alloc_node_nopanic(
phys_addr_t size, int nid)
{
return __alloc_bootmem_node_nopanic(NODE_DATA(nid), size,
SMP_CACHE_BYTES,
BOOTMEM_LOW_LIMIT);
}
static inline void * __init memblock_virt_alloc_try_nid(phys_addr_t size,
phys_addr_t align, phys_addr_t min_addr, phys_addr_t max_addr, int nid)
{
return __alloc_bootmem_node_high(NODE_DATA(nid), size, align,
min_addr);
}
static inline void * __init memblock_virt_alloc_try_nid_raw(
phys_addr_t size, phys_addr_t align,
phys_addr_t min_addr, phys_addr_t max_addr, int nid)
{
return ___alloc_bootmem_node_nopanic(NODE_DATA(nid), size, align,
min_addr, max_addr);
}
static inline void * __init memblock_virt_alloc_try_nid_nopanic(
phys_addr_t size, phys_addr_t align,
phys_addr_t min_addr, phys_addr_t max_addr, int nid)
{
return ___alloc_bootmem_node_nopanic(NODE_DATA(nid), size, align,
min_addr, max_addr);
}
static inline void __init memblock_free_early(
phys_addr_t base, phys_addr_t size)
{
free_bootmem(base, size);
}
static inline void __init memblock_free_early_nid(
phys_addr_t base, phys_addr_t size, int nid)
{
free_bootmem_node(NODE_DATA(nid), base, size);
}
static inline void __init memblock_free_late(
phys_addr_t base, phys_addr_t size)
{
free_bootmem_late(base, size);
}
#endif /* defined(CONFIG_HAVE_MEMBLOCK) && defined(CONFIG_NO_BOOTMEM) */
extern void *alloc_large_system_hash(const char *tablename,
unsigned long bucketsize,
unsigned long numentries,
int scale,
int flags,
unsigned int *_hash_shift,
unsigned int *_hash_mask,
unsigned long low_limit,
unsigned long high_limit);
#define HASH_EARLY 0x00000001 /* Allocating during early boot? */
#define HASH_SMALL 0x00000002 /* sub-page allocation allowed, min
* shift passed via *_hash_shift */
#define HASH_ZERO 0x00000004 /* Zero allocated hash table */
/* Only NUMA needs hash distribution. 64bit NUMA architectures have
* sufficient vmalloc space.
*/
#ifdef CONFIG_NUMA
#define HASHDIST_DEFAULT IS_ENABLED(CONFIG_64BIT)
extern int hashdist; /* Distribute hashes across NUMA nodes? */
#else
#define hashdist (0)
#endif
#endif /* _LINUX_BOOTMEM_H */