aboutsummaryrefslogblamecommitdiffstats
blob: fe7a22dd133b5a3c62833fd2539668d99f20b6f8 (plain) (tree)





















                                                                       

                         
                        
















                                                                                

                                                                               


                                                                               























                                                                           

                                                              
 




                                                                       

                       

                                                             



                                          
                                     





                                                                                
                    

 























                                                                                 





                                                                         








                                                                         
                                
/*
 * bvec iterator
 *
 * Copyright (C) 2001 Ming Lei <ming.lei@canonical.com>
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 *
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public Licens
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-
 */
#ifndef __LINUX_BVEC_ITER_H
#define __LINUX_BVEC_ITER_H

#include <linux/kernel.h>
#include <linux/bug.h>
#include <linux/errno.h>

/*
 * was unsigned short, but we might as well be ready for > 64kB I/O pages
 */
struct bio_vec {
	struct page	*bv_page;
	unsigned int	bv_len;
	unsigned int	bv_offset;
};

struct bvec_iter {
	sector_t		bi_sector;	/* device address in 512 byte
						   sectors */
	unsigned int		bi_size;	/* residual I/O count */

	unsigned int		bi_idx;		/* current index into bvl_vec */

	unsigned int            bi_done;	/* number of bytes completed */

	unsigned int            bi_bvec_done;	/* number of bytes completed in
						   current bvec */
};

/*
 * various member access, note that bio_data should of course not be used
 * on highmem page vectors
 */
#define __bvec_iter_bvec(bvec, iter)	(&(bvec)[(iter).bi_idx])

#define bvec_iter_page(bvec, iter)				\
	(__bvec_iter_bvec((bvec), (iter))->bv_page)

#define bvec_iter_len(bvec, iter)				\
	min((iter).bi_size,					\
	    __bvec_iter_bvec((bvec), (iter))->bv_len - (iter).bi_bvec_done)

#define bvec_iter_offset(bvec, iter)				\
	(__bvec_iter_bvec((bvec), (iter))->bv_offset + (iter).bi_bvec_done)

#define bvec_iter_bvec(bvec, iter)				\
((struct bio_vec) {						\
	.bv_page	= bvec_iter_page((bvec), (iter)),	\
	.bv_len		= bvec_iter_len((bvec), (iter)),	\
	.bv_offset	= bvec_iter_offset((bvec), (iter)),	\
})

static inline bool bvec_iter_advance(const struct bio_vec *bv,
		struct bvec_iter *iter, unsigned bytes)
{
	if (WARN_ONCE(bytes > iter->bi_size,
		     "Attempted to advance past end of bvec iter\n")) {
		iter->bi_size = 0;
		return false;
	}

	while (bytes) {
		unsigned iter_len = bvec_iter_len(bv, *iter);
		unsigned len = min(bytes, iter_len);

		bytes -= len;
		iter->bi_size -= len;
		iter->bi_bvec_done += len;
		iter->bi_done += len;

		if (iter->bi_bvec_done == __bvec_iter_bvec(bv, *iter)->bv_len) {
			iter->bi_bvec_done = 0;
			iter->bi_idx++;
		}
	}
	return true;
}

static inline bool bvec_iter_rewind(const struct bio_vec *bv,
				     struct bvec_iter *iter,
				     unsigned int bytes)
{
	while (bytes) {
		unsigned len = min(bytes, iter->bi_bvec_done);

		if (iter->bi_bvec_done == 0) {
			if (WARN_ONCE(iter->bi_idx == 0,
				      "Attempted to rewind iter beyond "
				      "bvec's boundaries\n")) {
				return false;
			}
			iter->bi_idx--;
			iter->bi_bvec_done = __bvec_iter_bvec(bv, *iter)->bv_len;
			continue;
		}
		bytes -= len;
		iter->bi_size += len;
		iter->bi_bvec_done -= len;
	}
	return true;
}

#define for_each_bvec(bvl, bio_vec, iter, start)			\
	for (iter = (start);						\
	     (iter).bi_size &&						\
		((bvl = bvec_iter_bvec((bio_vec), (iter))), 1);	\
	     bvec_iter_advance((bio_vec), &(iter), (bvl).bv_len))

/* for iterating one bio from start to end */
#define BVEC_ITER_ALL_INIT (struct bvec_iter)				\
{									\
	.bi_sector	= 0,						\
	.bi_size	= UINT_MAX,					\
	.bi_idx		= 0,						\
	.bi_bvec_done	= 0,						\
}

#endif /* __LINUX_BVEC_ITER_H */