aboutsummaryrefslogblamecommitdiffstats
blob: 218df7f4d3e1df69fda1bab3ee88bbe901eb2194 (plain) (tree)
1
2
3
4
5
6
7
8
9
                                      







                                                                
  
                                                        
              



                     


                           
                             
 
              
                   
                       
 

                                                                     
                                                                                
                          

  
                                
                                        

                            
 
                                                  
                                                   
                                              
                                                         

                                                                             
 

                                                               
 

                                                                     
 





                                                                             

                                                                                    

                                                                       
 



                                                                       
                         
                                            

                                                      
      
 


                                                                           
   





                                                                       
 
                 
                               
                             
                                           

                                        
 
                        
                                 
 







                                              
                       
                                  

                         



                                    
                                    
                                           

                                      
                                     
                               
 





                                              
                                                           
                                                     








                                                                  
 
                          




                                              
                                      
                                

                                                          
                                 
 
                                               
 

                                     




                                                                     





                                 


                                   

                                          


                                                   


                                                   

                                      








                                                      
                                        
                                               
                                         

                                                         
                                                  
                                                         
                                                   

      
                          
/* SPDX-License-Identifier: GPL-2.0 */
/*
 * include/linux/cpu.h - generic cpu definition
 *
 * This is mainly for topological representation. We define the 
 * basic 'struct cpu' here, which can be embedded in per-arch 
 * definitions of processors.
 *
 * Basic handling of the devices is done in drivers/base/cpu.c
 *
 * CPUs are exported via sysfs in the devices/system/cpu
 * directory. 
 */
#ifndef _LINUX_CPU_H_
#define _LINUX_CPU_H_

#include <linux/node.h>
#include <linux/compiler.h>
#include <linux/cpumask.h>
#include <linux/cpuhotplug.h>

struct device;
struct device_node;
struct attribute_group;

struct cpu {
	int node_id;		/* The node which contains the CPU */
	int hotpluggable;	/* creates sysfs control file if hotpluggable */
	struct device dev;
};

extern void boot_cpu_init(void);
extern void boot_cpu_hotplug_init(void);
extern void cpu_init(void);
extern void trap_init(void);

extern int register_cpu(struct cpu *cpu, int num);
extern struct device *get_cpu_device(unsigned cpu);
extern bool cpu_is_hotpluggable(unsigned cpu);
extern bool arch_match_cpu_phys_id(int cpu, u64 phys_id);
extern bool arch_find_n_match_cpu_physical_id(struct device_node *cpun,
					      int cpu, unsigned int *thread);

extern int cpu_add_dev_attr(struct device_attribute *attr);
extern void cpu_remove_dev_attr(struct device_attribute *attr);

extern int cpu_add_dev_attr_group(struct attribute_group *attrs);
extern void cpu_remove_dev_attr_group(struct attribute_group *attrs);

extern ssize_t cpu_show_meltdown(struct device *dev,
				 struct device_attribute *attr, char *buf);
extern ssize_t cpu_show_spectre_v1(struct device *dev,
				   struct device_attribute *attr, char *buf);
extern ssize_t cpu_show_spectre_v2(struct device *dev,
				   struct device_attribute *attr, char *buf);
extern ssize_t cpu_show_spec_store_bypass(struct device *dev,
					  struct device_attribute *attr, char *buf);
extern ssize_t cpu_show_l1tf(struct device *dev,
			     struct device_attribute *attr, char *buf);

extern __printf(4, 5)
struct device *cpu_device_create(struct device *parent, void *drvdata,
				 const struct attribute_group **groups,
				 const char *fmt, ...);
#ifdef CONFIG_HOTPLUG_CPU
extern void unregister_cpu(struct cpu *cpu);
extern ssize_t arch_cpu_probe(const char *, size_t);
extern ssize_t arch_cpu_release(const char *, size_t);
#endif

/*
 * These states are not related to the core CPU hotplug mechanism. They are
 * used by various (sub)architectures to track internal state
 */
#define CPU_ONLINE		0x0002 /* CPU is up */
#define CPU_UP_PREPARE		0x0003 /* CPU coming up */
#define CPU_DEAD		0x0007 /* CPU dead */
#define CPU_DEAD_FROZEN		0x0008 /* CPU timed out on unplug */
#define CPU_POST_DEAD		0x0009 /* CPU successfully unplugged */
#define CPU_BROKEN		0x000B /* CPU did not die properly */

#ifdef CONFIG_SMP
extern bool cpuhp_tasks_frozen;
int cpu_up(unsigned int cpu);
void notify_cpu_starting(unsigned int cpu);
extern void cpu_maps_update_begin(void);
extern void cpu_maps_update_done(void);

#else	/* CONFIG_SMP */
#define cpuhp_tasks_frozen	0

static inline void cpu_maps_update_begin(void)
{
}

static inline void cpu_maps_update_done(void)
{
}

#endif /* CONFIG_SMP */
extern struct bus_type cpu_subsys;

#ifdef CONFIG_HOTPLUG_CPU
extern void cpus_write_lock(void);
extern void cpus_write_unlock(void);
extern void cpus_read_lock(void);
extern void cpus_read_unlock(void);
extern int  cpus_read_trylock(void);
extern void lockdep_assert_cpus_held(void);
extern void cpu_hotplug_disable(void);
extern void cpu_hotplug_enable(void);
void clear_tasks_mm_cpumask(int cpu);
int cpu_down(unsigned int cpu);

#else /* CONFIG_HOTPLUG_CPU */

static inline void cpus_write_lock(void) { }
static inline void cpus_write_unlock(void) { }
static inline void cpus_read_lock(void) { }
static inline void cpus_read_unlock(void) { }
static inline int  cpus_read_trylock(void) { return true; }
static inline void lockdep_assert_cpus_held(void) { }
static inline void cpu_hotplug_disable(void) { }
static inline void cpu_hotplug_enable(void) { }
#endif	/* !CONFIG_HOTPLUG_CPU */

/* Wrappers which go away once all code is converted */
static inline void cpu_hotplug_begin(void) { cpus_write_lock(); }
static inline void cpu_hotplug_done(void) { cpus_write_unlock(); }
static inline void get_online_cpus(void) { cpus_read_lock(); }
static inline void put_online_cpus(void) { cpus_read_unlock(); }

#ifdef CONFIG_PM_SLEEP_SMP
extern int freeze_secondary_cpus(int primary);
static inline int disable_nonboot_cpus(void)
{
	return freeze_secondary_cpus(0);
}
extern void enable_nonboot_cpus(void);
#else /* !CONFIG_PM_SLEEP_SMP */
static inline int disable_nonboot_cpus(void) { return 0; }
static inline void enable_nonboot_cpus(void) {}
#endif /* !CONFIG_PM_SLEEP_SMP */

void cpu_startup_entry(enum cpuhp_state state);

void cpu_idle_poll_ctrl(bool enable);

/* Attach to any functions which should be considered cpuidle. */
#define __cpuidle	__attribute__((__section__(".cpuidle.text")))

bool cpu_in_idle(unsigned long pc);

void arch_cpu_idle(void);
void arch_cpu_idle_prepare(void);
void arch_cpu_idle_enter(void);
void arch_cpu_idle_exit(void);
void arch_cpu_idle_dead(void);

int cpu_report_state(int cpu);
int cpu_check_up_prepare(int cpu);
void cpu_set_state_online(int cpu);
void play_idle(unsigned long duration_ms);

#ifdef CONFIG_HOTPLUG_CPU
bool cpu_wait_death(unsigned int cpu, int seconds);
bool cpu_report_death(void);
void cpuhp_report_idle_dead(void);
#else
static inline void cpuhp_report_idle_dead(void) { }
#endif /* #ifdef CONFIG_HOTPLUG_CPU */

enum cpuhp_smt_control {
	CPU_SMT_ENABLED,
	CPU_SMT_DISABLED,
	CPU_SMT_FORCE_DISABLED,
	CPU_SMT_NOT_SUPPORTED,
};

#if defined(CONFIG_SMP) && defined(CONFIG_HOTPLUG_SMT)
extern enum cpuhp_smt_control cpu_smt_control;
extern void cpu_smt_disable(bool force);
extern void cpu_smt_check_topology_early(void);
extern void cpu_smt_check_topology(void);
#else
# define cpu_smt_control		(CPU_SMT_ENABLED)
static inline void cpu_smt_disable(bool force) { }
static inline void cpu_smt_check_topology_early(void) { }
static inline void cpu_smt_check_topology(void) { }
#endif

#endif /* _LINUX_CPU_H_ */