aboutsummaryrefslogblamecommitdiffstats
blob: 0d3037419bc782c6c0d6883cd2207dfad2bd1773 (plain) (tree)
1
2
3
4
5
6
7
8
9
                                      





                          
             
             
             
                   
                
 


                                                    
























                                                                            

          




















                                                             










                                                                      












                                                              

          










                                                               





                                             


                                                 









                                       







                                              
                             

          


                                                                       
                                                               

                                                                            

                                                                        
                                                              
  
                                                                        
                            
  


                                                                               
                                                                              


                                                                               



                                                                            
  



                                                                              






                                                                                 




                                                                           











                                                                             


                                                                        





                                                            

                                                                      



                                                                                


                                                            
                                                    






                                                                                

  

                                                                         


                                                                               


                                                                                









                                                                               
                             
/* SPDX-License-Identifier: GPL-2.0 */
#ifndef LINUX_EXPORTFS_H
#define LINUX_EXPORTFS_H 1

#include <linux/types.h>

struct dentry;
struct iattr;
struct inode;
struct iomap;
struct super_block;
struct vfsmount;

/* limit the handle size to NFSv4 handle size now */
#define MAX_HANDLE_SZ 128

/*
 * The fileid_type identifies how the file within the filesystem is encoded.
 * In theory this is freely set and parsed by the filesystem, but we try to
 * stick to conventions so we can share some generic code and don't confuse
 * sniffers like ethereal/wireshark.
 *
 * The filesystem must not use the value '0' or '0xff'.
 */
enum fid_type {
	/*
	 * The root, or export point, of the filesystem.
	 * (Never actually passed down to the filesystem.
	 */
	FILEID_ROOT = 0,

	/*
	 * 32bit inode number, 32 bit generation number.
	 */
	FILEID_INO32_GEN = 1,

	/*
	 * 32bit inode number, 32 bit generation number,
	 * 32 bit parent directory inode number.
	 */
	FILEID_INO32_GEN_PARENT = 2,

	/*
	 * 64 bit object ID, 64 bit root object ID,
	 * 32 bit generation number.
	 */
	FILEID_BTRFS_WITHOUT_PARENT = 0x4d,

	/*
	 * 64 bit object ID, 64 bit root object ID,
	 * 32 bit generation number,
	 * 64 bit parent object ID, 32 bit parent generation.
	 */
	FILEID_BTRFS_WITH_PARENT = 0x4e,

	/*
	 * 64 bit object ID, 64 bit root object ID,
	 * 32 bit generation number,
	 * 64 bit parent object ID, 32 bit parent generation,
	 * 64 bit parent root object ID.
	 */
	FILEID_BTRFS_WITH_PARENT_ROOT = 0x4f,

	/*
	 * 32 bit block number, 16 bit partition reference,
	 * 16 bit unused, 32 bit generation number.
	 */
	FILEID_UDF_WITHOUT_PARENT = 0x51,

	/*
	 * 32 bit block number, 16 bit partition reference,
	 * 16 bit unused, 32 bit generation number,
	 * 32 bit parent block number, 32 bit parent generation number
	 */
	FILEID_UDF_WITH_PARENT = 0x52,

	/*
	 * 64 bit checkpoint number, 64 bit inode number,
	 * 32 bit generation number.
	 */
	FILEID_NILFS_WITHOUT_PARENT = 0x61,

	/*
	 * 64 bit checkpoint number, 64 bit inode number,
	 * 32 bit generation number, 32 bit parent generation.
	 * 64 bit parent inode number.
	 */
	FILEID_NILFS_WITH_PARENT = 0x62,

	/*
	 * 32 bit generation number, 40 bit i_pos.
	 */
	FILEID_FAT_WITHOUT_PARENT = 0x71,

	/*
	 * 32 bit generation number, 40 bit i_pos,
	 * 32 bit parent generation number, 40 bit parent i_pos
	 */
	FILEID_FAT_WITH_PARENT = 0x72,

	/*
	 * 128 bit child FID (struct lu_fid)
	 * 128 bit parent FID (struct lu_fid)
	 */
	FILEID_LUSTRE = 0x97,

	/*
	 * Filesystems must not use 0xff file ID.
	 */
	FILEID_INVALID = 0xff,
};

struct fid {
	union {
		struct {
			u32 ino;
			u32 gen;
			u32 parent_ino;
			u32 parent_gen;
		} i32;
 		struct {
 			u32 block;
 			u16 partref;
 			u16 parent_partref;
 			u32 generation;
 			u32 parent_block;
 			u32 parent_generation;
 		} udf;
		__u32 raw[0];
	};
};

/**
 * struct export_operations - for nfsd to communicate with file systems
 * @encode_fh:      encode a file handle fragment from a dentry
 * @fh_to_dentry:   find the implied object and get a dentry for it
 * @fh_to_parent:   find the implied object's parent and get a dentry for it
 * @get_name:       find the name for a given inode in a given directory
 * @get_parent:     find the parent of a given directory
 * @commit_metadata: commit metadata changes to stable storage
 *
 * See Documentation/filesystems/nfs/Exporting for details on how to use
 * this interface correctly.
 *
 * encode_fh:
 *    @encode_fh should store in the file handle fragment @fh (using at most
 *    @max_len bytes) information that can be used by @decode_fh to recover the
 *    file referred to by the &struct dentry @de.  If the @connectable flag is
 *    set, the encode_fh() should store sufficient information so that a good
 *    attempt can be made to find not only the file but also it's place in the
 *    filesystem.   This typically means storing a reference to de->d_parent in
 *    the filehandle fragment.  encode_fh() should return the fileid_type on
 *    success and on error returns 255 (if the space needed to encode fh is
 *    greater than @max_len*4 bytes). On error @max_len contains the minimum
 *    size(in 4 byte unit) needed to encode the file handle.
 *
 * fh_to_dentry:
 *    @fh_to_dentry is given a &struct super_block (@sb) and a file handle
 *    fragment (@fh, @fh_len). It should return a &struct dentry which refers
 *    to the same file that the file handle fragment refers to.  If it cannot,
 *    it should return a %NULL pointer if the file cannot be found, or an
 *    %ERR_PTR error code of %ENOMEM if a memory allocation failure occurred.
 *    Any other error code is treated like %NULL, and will cause an %ESTALE error
 *    for callers of exportfs_decode_fh().
 *    Any suitable dentry can be returned including, if necessary, a new dentry
 *    created with d_alloc_root.  The caller can then find any other extant
 *    dentries by following the d_alias links.
 *
 * fh_to_parent:
 *    Same as @fh_to_dentry, except that it returns a pointer to the parent
 *    dentry if it was encoded into the filehandle fragment by @encode_fh.
 *
 * get_name:
 *    @get_name should find a name for the given @child in the given @parent
 *    directory.  The name should be stored in the @name (with the
 *    understanding that it is already pointing to a a %NAME_MAX+1 sized
 *    buffer.   get_name() should return %0 on success, a negative error code
 *    or error.  @get_name will be called without @parent->i_mutex held.
 *
 * get_parent:
 *    @get_parent should find the parent directory for the given @child which
 *    is also a directory.  In the event that it cannot be found, or storage
 *    space cannot be allocated, a %ERR_PTR should be returned.
 *
 * commit_metadata:
 *    @commit_metadata should commit metadata changes to stable storage.
 *
 * Locking rules:
 *    get_parent is called with child->d_inode->i_mutex down
 *    get_name is not (which is possibly inconsistent)
 */

struct export_operations {
	int (*encode_fh)(struct inode *inode, __u32 *fh, int *max_len,
			struct inode *parent);
	struct dentry * (*fh_to_dentry)(struct super_block *sb, struct fid *fid,
			int fh_len, int fh_type);
	struct dentry * (*fh_to_parent)(struct super_block *sb, struct fid *fid,
			int fh_len, int fh_type);
	int (*get_name)(struct dentry *parent, char *name,
			struct dentry *child);
	struct dentry * (*get_parent)(struct dentry *child);
	int (*commit_metadata)(struct inode *inode);

	int (*get_uuid)(struct super_block *sb, u8 *buf, u32 *len, u64 *offset);
	int (*map_blocks)(struct inode *inode, loff_t offset,
			  u64 len, struct iomap *iomap,
			  bool write, u32 *device_generation);
	int (*commit_blocks)(struct inode *inode, struct iomap *iomaps,
			     int nr_iomaps, struct iattr *iattr);
};

extern int exportfs_encode_inode_fh(struct inode *inode, struct fid *fid,
				    int *max_len, struct inode *parent);
extern int exportfs_encode_fh(struct dentry *dentry, struct fid *fid,
	int *max_len, int connectable);
extern struct dentry *exportfs_decode_fh(struct vfsmount *mnt, struct fid *fid,
	int fh_len, int fileid_type, int (*acceptable)(void *, struct dentry *),
	void *context);

/*
 * Generic helpers for filesystems.
 */
extern struct dentry *generic_fh_to_dentry(struct super_block *sb,
	struct fid *fid, int fh_len, int fh_type,
	struct inode *(*get_inode) (struct super_block *sb, u64 ino, u32 gen));
extern struct dentry *generic_fh_to_parent(struct super_block *sb,
	struct fid *fid, int fh_len, int fh_type,
	struct inode *(*get_inode) (struct super_block *sb, u64 ino, u32 gen));

#endif /* LINUX_EXPORTFS_H */