aboutsummaryrefslogblamecommitdiffstats
blob: 7f033b1ea5680e392efd082fbc8cdf0f91b926ac (plain) (tree)
1
2
3
4
5
6
7
  
                                        
                                                                    
  


                                               















                                                                       
   



                          
                         
 
  








                                                                     

                                                        
                                 
 


                                 
 






                                                                      



                                                                  
   





                                                                       
                                                                     
                                                                
 








                                                                            
 




                                                                                  
                                                          
                                                                  






                                      
 
  
                                                          






















                                                          



                                      




                                        

                                         
                                         
                                         

                                         
                                         











                                                                               










                                           

                                           
                                           











                                                                              
                  
 
                             
  
                                                                     
                                                              
   
                                                                      
 
  
                                                              


                                                             

                                                                          
                                                                    



                                                                        

                                                                    

  


                                                                           



                                                                            
   
                                                                             
                                                           
                                                                               
                                                           





                                                                         
 










                                                                   
  
                                                                               
   
                                                                         
                                                                             

                                                                        
 
                                                  

                                                                 
                         
                                                                            



                 
                                                                               

                                                                      


                 
 
                                                                         
                                                                   



                 
                                                                   
                                                                           




                                                                     
                                                                           



                 










                                                                         

                                                                               
                                

 




                                                                                   
                                                                               
                                          
 
                                
 
                          
 











                                                                                

                                                                                
 
                       
 
 
                                                                                  
 
                       
 
                               
/*
 * External Connector (extcon) framework
 * - linux/include/linux/extcon.h for extcon consumer device driver.
 *
 * Copyright (C) 2015 Samsung Electronics
 * Author: Chanwoo Choi <cw00.choi@samsung.com>
 *
 * Copyright (C) 2012 Samsung Electronics
 * Author: Donggeun Kim <dg77.kim@samsung.com>
 * Author: MyungJoo Ham <myungjoo.ham@samsung.com>
 *
 * based on switch class driver
 * Copyright (C) 2008 Google, Inc.
 * Author: Mike Lockwood <lockwood@android.com>
 *
 * This software is licensed under the terms of the GNU General Public
 * License version 2, as published by the Free Software Foundation, and
 * may be copied, distributed, and modified under those terms.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 */

#ifndef __LINUX_EXTCON_H__
#define __LINUX_EXTCON_H__

#include <linux/device.h>

/*
 * Define the type of supported external connectors
 */
#define EXTCON_TYPE_USB		BIT(0)	/* USB connector */
#define EXTCON_TYPE_CHG		BIT(1)	/* Charger connector */
#define EXTCON_TYPE_JACK	BIT(2)	/* Jack connector */
#define EXTCON_TYPE_DISP	BIT(3)	/* Display connector */
#define EXTCON_TYPE_MISC	BIT(4)	/* Miscellaneous connector */

/*
 * Define the unique id of supported external connectors
 */
#define EXTCON_NONE		0

/* USB external connector */
#define EXTCON_USB		1
#define EXTCON_USB_HOST		2

/*
 * Charging external connector
 *
 * When one SDP charger connector was reported, we should also report
 * the USB connector, which means EXTCON_CHG_USB_SDP should always
 * appear together with EXTCON_USB. The same as ACA charger connector,
 * EXTCON_CHG_USB_ACA would normally appear with EXTCON_USB_HOST.
 *
 * The EXTCON_CHG_USB_SLOW connector can provide at least 500mA of
 * current at 5V. The EXTCON_CHG_USB_FAST connector can provide at
 * least 1A of current at 5V.
 */
#define EXTCON_CHG_USB_SDP	5	/* Standard Downstream Port */
#define EXTCON_CHG_USB_DCP	6	/* Dedicated Charging Port */
#define EXTCON_CHG_USB_CDP	7	/* Charging Downstream Port */
#define EXTCON_CHG_USB_ACA	8	/* Accessory Charger Adapter */
#define EXTCON_CHG_USB_FAST	9
#define EXTCON_CHG_USB_SLOW	10
#define EXTCON_CHG_WPT		11	/* Wireless Power Transfer */
#define EXTCON_CHG_USB_PD	12	/* USB Power Delivery */

/* Jack external connector */
#define EXTCON_JACK_MICROPHONE	20
#define EXTCON_JACK_HEADPHONE	21
#define EXTCON_JACK_LINE_IN	22
#define EXTCON_JACK_LINE_OUT	23
#define EXTCON_JACK_VIDEO_IN	24
#define EXTCON_JACK_VIDEO_OUT	25
#define EXTCON_JACK_SPDIF_IN	26	/* Sony Philips Digital InterFace */
#define EXTCON_JACK_SPDIF_OUT	27

/* Display external connector */
#define EXTCON_DISP_HDMI	40	/* High-Definition Multimedia Interface */
#define EXTCON_DISP_MHL		41	/* Mobile High-Definition Link */
#define EXTCON_DISP_DVI		42	/* Digital Visual Interface */
#define EXTCON_DISP_VGA		43	/* Video Graphics Array */
#define EXTCON_DISP_DP		44	/* Display Port */
#define EXTCON_DISP_HMD		45	/* Head-Mounted Display */

/* Miscellaneous external connector */
#define EXTCON_DOCK		60
#define EXTCON_JIG		61
#define EXTCON_MECHANICAL	62

#define EXTCON_NUM		63

/*
 * Define the properties of supported external connectors.
 *
 * When adding the new extcon property, they *must* have
 * the type/value/default information. Also, you *have to*
 * modify the EXTCON_PROP_[type]_START/END definitions
 * which mean the range of the supported properties
 * for each extcon type.
 *
 * The naming style of property
 * : EXTCON_PROP_[type]_[property name]
 *
 * EXTCON_PROP_USB_[property name]	: USB property
 * EXTCON_PROP_CHG_[property name]	: Charger property
 * EXTCON_PROP_JACK_[property name]	: Jack property
 * EXTCON_PROP_DISP_[property name]	: Display property
 */

/*
 * Properties of EXTCON_TYPE_USB.
 *
 * - EXTCON_PROP_USB_VBUS
 * @type:	integer (intval)
 * @value:	0 (low) or 1 (high)
 * @default:	0 (low)
 * - EXTCON_PROP_USB_TYPEC_POLARITY
 * @type:	integer (intval)
 * @value:	0 (normal) or 1 (flip)
 * @default:	0 (normal)
 * - EXTCON_PROP_USB_SS (SuperSpeed)
 * @type:       integer (intval)
 * @value:      0 (USB/USB2) or 1 (USB3)
 * @default:    0 (USB/USB2)
 *
 */
#define EXTCON_PROP_USB_VBUS		0
#define EXTCON_PROP_USB_TYPEC_POLARITY	1
#define EXTCON_PROP_USB_SS		2

#define EXTCON_PROP_USB_MIN		0
#define EXTCON_PROP_USB_MAX		2
#define EXTCON_PROP_USB_CNT	(EXTCON_PROP_USB_MAX - EXTCON_PROP_USB_MIN + 1)

/* Properties of EXTCON_TYPE_CHG. */
#define EXTCON_PROP_CHG_MIN		50
#define EXTCON_PROP_CHG_MAX		50
#define EXTCON_PROP_CHG_CNT	(EXTCON_PROP_CHG_MAX - EXTCON_PROP_CHG_MIN + 1)

/* Properties of EXTCON_TYPE_JACK. */
#define EXTCON_PROP_JACK_MIN		100
#define EXTCON_PROP_JACK_MAX		100
#define EXTCON_PROP_JACK_CNT (EXTCON_PROP_JACK_MAX - EXTCON_PROP_JACK_MIN + 1)

/*
 * Properties of EXTCON_TYPE_DISP.
 *
 * - EXTCON_PROP_DISP_HPD (Hot Plug Detect)
 * @type:       integer (intval)
 * @value:      0 (no hpd) or 1 (hpd)
 * @default:    0 (no hpd)
 *
 */
#define EXTCON_PROP_DISP_HPD		150

/* Properties of EXTCON_TYPE_DISP. */
#define EXTCON_PROP_DISP_MIN		150
#define EXTCON_PROP_DISP_MAX		151
#define EXTCON_PROP_DISP_CNT (EXTCON_PROP_DISP_MAX - EXTCON_PROP_DISP_MIN + 1)

/*
 * Define the type of property's value.
 *
 * Define the property's value as union type. Because each property
 * would need the different data type to store it.
 */
union extcon_property_value {
	int intval;	/* type : integer (intval) */
};

struct extcon_dev;

#if IS_ENABLED(CONFIG_EXTCON)
/*
 * Following APIs get the connected state of each external connector.
 * The 'id' argument indicates the defined external connector.
 */
extern int extcon_get_state(struct extcon_dev *edev, unsigned int id);

/*
 * Following APIs get the property of each external connector.
 * The 'id' argument indicates the defined external connector
 * and the 'prop' indicates the extcon property.
 *
 * And extcon_get_property_capability() get the capability of the property
 * for each external connector. They are used to get the capability of the
 * property of each external connector based on the id and property.
 */
extern int extcon_get_property(struct extcon_dev *edev, unsigned int id,
				unsigned int prop,
				union extcon_property_value *prop_val);
extern int extcon_get_property_capability(struct extcon_dev *edev,
				unsigned int id, unsigned int prop);

/*
 * Following APIs register the notifier block in order to detect
 * the change of both state and property value for each external connector.
 *
 * extcon_register_notifier(*edev, id, *nb) : Register a notifier block
 *			for specific external connector of the extcon.
 * extcon_register_notifier_all(*edev, *nb) : Register a notifier block
 *			for all supported external connectors of the extcon.
 */
extern int extcon_register_notifier(struct extcon_dev *edev, unsigned int id,
				struct notifier_block *nb);
extern int extcon_unregister_notifier(struct extcon_dev *edev, unsigned int id,
				struct notifier_block *nb);
extern int devm_extcon_register_notifier(struct device *dev,
				struct extcon_dev *edev, unsigned int id,
				struct notifier_block *nb);
extern void devm_extcon_unregister_notifier(struct device *dev,
				struct extcon_dev *edev, unsigned int id,
				struct notifier_block *nb);

extern int extcon_register_notifier_all(struct extcon_dev *edev,
				struct notifier_block *nb);
extern int extcon_unregister_notifier_all(struct extcon_dev *edev,
				struct notifier_block *nb);
extern int devm_extcon_register_notifier_all(struct device *dev,
				struct extcon_dev *edev,
				struct notifier_block *nb);
extern void devm_extcon_unregister_notifier_all(struct device *dev,
				struct extcon_dev *edev,
				struct notifier_block *nb);

/*
 * Following APIs get the extcon_dev from devicetree or by through extcon name.
 */
extern struct extcon_dev *extcon_get_extcon_dev(const char *extcon_name);
extern struct extcon_dev *extcon_find_edev_by_node(struct device_node *node);
extern struct extcon_dev *extcon_get_edev_by_phandle(struct device *dev,
						     int index);

/* Following API get the name of extcon device. */
extern const char *extcon_get_edev_name(struct extcon_dev *edev);

#else /* CONFIG_EXTCON */
static inline int extcon_get_state(struct extcon_dev *edev, unsigned int id)
{
	return 0;
}

static inline int extcon_get_property(struct extcon_dev *edev, unsigned int id,
				unsigned int prop,
				union extcon_property_value *prop_val)
{
	return 0;
}

static inline int extcon_get_property_capability(struct extcon_dev *edev,
				unsigned int id, unsigned int prop)
{
	return 0;
}

static inline int extcon_register_notifier(struct extcon_dev *edev,
				unsigned int id, struct notifier_block *nb)
{
	return 0;
}

static inline int extcon_unregister_notifier(struct extcon_dev *edev,
				unsigned int id, struct notifier_block *nb)
{
	return 0;
}

static inline int devm_extcon_register_notifier(struct device *dev,
				struct extcon_dev *edev, unsigned int id,
				struct notifier_block *nb)
{
	return -ENOSYS;
}

static inline  void devm_extcon_unregister_notifier(struct device *dev,
				struct extcon_dev *edev, unsigned int id,
				struct notifier_block *nb) { }

static inline struct extcon_dev *extcon_get_extcon_dev(const char *extcon_name)
{
	return ERR_PTR(-ENODEV);
}

static inline struct extcon_dev *extcon_find_edev_by_node(struct device_node *node)
{
	return ERR_PTR(-ENODEV);
}

static inline struct extcon_dev *extcon_get_edev_by_phandle(struct device *dev,
				int index)
{
	return ERR_PTR(-ENODEV);
}
#endif /* CONFIG_EXTCON */

/*
 * Following structure and API are deprecated. EXTCON remains the function
 * definition to prevent the build break.
 */
struct extcon_specific_cable_nb {
       struct notifier_block *user_nb;
       int cable_index;
       struct extcon_dev *edev;
       unsigned long previous_value;
};

static inline int extcon_register_interest(struct extcon_specific_cable_nb *obj,
				const char *extcon_name, const char *cable_name,
				struct notifier_block *nb)
{
	return -EINVAL;
}

static inline int extcon_unregister_interest(struct extcon_specific_cable_nb *obj)
{
	return -EINVAL;
}
#endif /* __LINUX_EXTCON_H__ */