aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* ARM: dts: am572x-idk-common: Add CMA pools and enable IPU & DSP rprocsSuman Anna2019-03-041-0/+54
| | | | | | | | | | | | | | | | | | | | | | The CMA reserved memory nodes have been added for all the IPU and DSP remoteproc devices in the am572x-idk-common.dtsi file that is common to both the AM572x and AM574x IDK boards. These nodes are assigned to the respective rproc device nodes, and all the IPU and DSP remote processors are enabled. The current CMA pools and sizes are defined statically for each device. The addresses chosen are the same as the respective processors on the AM57xx EVM board to maintain firmware compatibility between the two boards. The CMA pools and sizes are defined using 64-bit values to support LPAE. The starting addresses are fixed to meet current dependencies on the remote processor firmwares, and this will go away when the remote-side code has been improved to gather this information runtime during its initialization. An associated pair of the rproc node and its CMA node can be disabled later on if there is no use-case defined to use that remote processor. Signed-off-by: Suman Anna <s-anna@ti.com>
* ARM: dts: dra7-ipu-dsp-common: Move mailboxes into common filesSuman Anna2019-03-041-20/+1
| | | | | | | | | | | | | | | | | | | | | The System Mailboxes 5 and 6 and their corresponding child sub-mailbox (IPC 3.x) nodes are enabled in each of the DRA7xx and AM57xx board dts files individually at present. These mailboxes enable the Remote Processor Messaging (RPMsg) communication stack between the MPU host processor and each of the IPU1, IPU2, DSP1 and DSP2 remote processors. Move these nodes into two common dtsi files - dra7-ipu-dsp-common and dra74-ipu-dsp-common files, which are then included in various board dts files. These files can be used to add all the common configuration properties (except memory data) required by remote processor nodes. The memory pools and the remote processor nodes themselves are to be enabled in the actual board dts files. The first file is to used by platforms using DRA72x/DRA71x/AM571x/AM570x SoCs, and the second file is to be used by platforms using DRA74x/DRA76x/AM572x/AM574x SoCs. The second file includes the first file and contains additional data only applicable for DSP2 remote processor. Signed-off-by: Suman Anna <s-anna@ti.com>
* ARM: dts: am57xx-idk: Enable dual role for USB2 portRoger Quadros2018-07-031-4/+0
| | | | | | | | | | Dual-role support was added in v4.12. We should be using it for USB2 port on the am57xx-idk. Cc: <stable@vger.kernel.org> [4.16+] Reported-by: Bin Liu <b-liu@ti.com> Signed-off-by: Roger Quadros <rogerq@ti.com> Signed-off-by: Tony Lindgren <tony@atomide.com>
* ARM: dts: am57xx: Add support for am574x-idkLokesh Vutla2017-12-211-0/+100
am574x-idk is similar to am572x-idk with am574x SoC. So create a common file for both evms and include SoC dtsi as needed. Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> Signed-off-by: Tony Lindgren <tony@atomide.com>