| Commit message (Collapse) | Author | Age | Files | Lines |
|\
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
rproc-linux-4.19.y
Merge in the updated iommu feature branch into remoteproc tree to
pull in the suspend/resume support in the OMAP IOMMU driver. The
following are the main changes:
- improvements in the OMAP iommu to perform the enabling &
disabling of the IOMMU from within the runtime pm callbacks
- system suspend/resume support through late dev_pm_ops
- two new API that needs to be invoked from the OMAP remoteproc
driver to runtime suspend/resume the IOMMU
- locked TLB save & restore logic
- add needed pdata quirks to all supported IOMMUs
Suspend/resume support in the OMAP mailbox driver is already supported
in baseline upstream kernel.
* 'iommu-linux-4.19.y' of git://git.ti.com/rpmsg/iommu:
iommu/omap: introduce new API for runtime suspend/resume control
iommu/omap: Add system suspend/resume support
iommu/omap: add logic to save/restore locked TLBs
iommu/omap: streamline enable/disable through runtime pm callbacks
ARM: OMAP2+: add pdata-quirks for OMAP3 ISP IOMMU
ARM: OMAP2+: Add iommu pdata-quirks for DRA7 DSP EDMA MMUs
ARM: OMAP2+: plug in device_enable/idle ops for IOMMUs
iommu/omap: add pdata ops for omap_device_enable/idle
Signed-off-by: Suman Anna <s-anna@ti.com>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Add two new platform data ops to allow the OMAP iommu driver to
be able to invoke the omap_device_enable and omap_device_idle
from within the driver. These are being added to streamline the
sequence between managing the hard reset lines and the clocks
during the suspend path, as the default device pm_domain callback
sequences in omap_device layer are not conducive for the OMAP
IOMMU driver.
This could have been done by expanding the existing pdata ops
for reset management (like in the OMAP remoteproc driver), but
this was chosen to avoid adding additional code in the separate
file in the mach-omap2 layer.
Signed-off-by: Suman Anna <s-anna@ti.com>
|
|\|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
rproc-linux-4.19.y
Merge in the updated iommu feature branch into remoteproc tree to
pull in the necessary support to fix the DRA7 IPU1 boot issue and
couple of DRA7 DSP idle issues with HW_AUTO setting. The DSP idle
status is achieved across all the DSPs and boards only with the
fix for errata i879.
* 'iommu-linux-4.19.y' of git://git.ti.com/rpmsg/iommu:
ARM: OMAP2+: Add workaround for DRA7 DSP MStandby errata i879
ARM: OMAP2+: Extend DRA7 IPU1 MMU pdata quirks to DSP MDMA MMUs
ARM: OMAP2+: Use separate IOMMU pdata to fix DRA7 IPU1 boot
iommu/omap: Fix boot issue on remoteprocs with AMMU/Unicache
Signed-off-by: Suman Anna <s-anna@ti.com>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Support has been added to the OMAP IOMMU driver to fix a boot hang
issue on OMAP remoteprocs with AMMU/Unicache, caused by an improper
AMMU/Unicache state upon initial deassertion of the processor reset.
The issue is described in detail in the next three paragraphs.
All the Cortex M3/M4 IPU processor subsystems in OMAP SoCs have a
AMMU/Unicache IP that dictates the memory attributes for addresses
seen by the processor cores. The AMMU/Unicache is configured/enabled
by the SCACHE_CONFIG.BYPASS bit - a value of 1 enables the cache and
mandates all addresses accessed by M3/M4 be defined in the AMMU. This
bit is not programmable from the host processor. The M3/M4 boot
sequence starts out with the AMMU/Unicache in disabled state, and
SYS/BIOS programs the AMMU regions and enables the Unicache during
one of its initial boot steps. This SCACHE_CONFIG.BYPASS bit is
however enabled by default whenever a RET reset is applied to the IP,
irrespective of whether it was previously enabled or not. The AMMU
registers lose their context whenever this reset is applied. The reset
is effective as long as the MMU portion of the subsystem is enabled
and clocked. This behavior is common to all the IPU and DSP subsystems
that have an AMMU/Unicache.
The IPU boot sequence involves enabling and programming the MMU, and
loading the processor and releasing the reset(s) for the processor.
The PM setup code currently sets the target state for most of the
power domains to RET. The L2 MMU can be enabled, programmed and
accessed properly just fine with the domain in hardware supervised
mode, while the power domain goes through a RET->ON->RET transition
during the programming sequence. However, the ON->RET transition
asserts a RET reset, and the SCACHE_CONFIG.BYPASS bit gets auto-set.
An AMMU fault is thrown immediately when the M3/M4 core's reset is
released since the first instruction address itself will not be
defined in any valid AMMU regions. The ON->RET transition happens
automatically on the power domain after enabling the iommu due to
the hardware supervised mode.
This patch adds and invokes the .set_pwrdm_constraint pdata ops, if
present, during the OMAP IOMMU enable and disable functions to resolve
the above boot hang issue. The ops will allow to invoke a mach-omap2
layer API pwrdm_set_next_pwrst() in a multi-arch kernel environment.
The ops also returns the current power domain state while enforcing
the constraint so that the driver can store it and use it to set back
the power domain state while releasing the constraint. The pdata ops
implementation restricts the target power domain to ON during enable,
and back to the original power domain state during disable, and thereby
eliminating the conditions for the boot issue. The implementation is
effective only when the original power domain state is either RET or
OFF, and is a no-op when it is ON or INACTIVE.
The .set_pwrdm_constraint ops need to be plugged in pdata-quirks
for the affected remote processors to be able to boot properly.
Note that the current issue is seen only on kernels with the affected
power domains programmed to enter RET. For eg., IPU1 on DRA7xx is in a
separate domain and is susceptible to this bug, while the IPU2 subsystem
is within CORE power domain, and CORE RET is not supported on this SoC.
IPUs on OMAP4 and OMAP5 are also susceptible since they are in CORE power
domain, and CORE RET is a valid power target on these SoCs.
Signed-off-by: Suman Anna <s-anna@ti.com>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
The omap_rproc_reserve_cma() function is not defined at the moment.
This prototype was to be used to define a function to declare a
remoteproc device-specific CMA pool.
The remoteproc devices will be defined through DT going forward. A
device specific CMA pool will be defined under the reserved-memory
node, and will be associated with the appropriate remoteproc device
node. This function prototype will no longer be needed and has
therefore been cleaned up.
Signed-off-by: Suman Anna <s-anna@ti.com>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
The following fields: .name, .oh_name, .oh_name_opt, .mbox_name,
.firmware, .ops and .set_bootaddr, are removed from the platform data,
as these are no longer needed after the addition of DT support to the
OMAP remoteproc driver.
The .name field was used to give a name to the remoteproc, and this
is replaced with the device name. The .ops field was never used by
the OMAP remoteproc driver. The .mbox_name was used to define the
sub-mailbox node used for communication with the remote processor,
and is retrieved using the 'mboxes' property in the DT node. The
.firmware field is encoded directly in the OMAP remoteproc driver and
is retrieved using driver match data. The .set_bootaddr ops was used
for using a OMAP Control Module API to configure the boot address for
the processor, and is now implemented within the driver using a
syscon property.
The .oh_name field is used to define the primary hwmod for the processor
node, and is represented using the 'ti,hwmods' property in the DT node.
The .oh_name_opt field was primarily defined to identify the hwmod for
the second cpu in a dual Cortex-M3/M4 IPU processor sub-system. This
hwmod entry is no longer defined usually, but rather a single hwmod
representing both the processors in the IPU sub-system is defined.
A single firmware image (either in SMP-mode or a combined image for
non-SMP mode) is used, with both the resets released together always
as part of the device management. Any power management and recovery
aspects require that both the processors be managed as one entity due
to the presence of shared MMU and unicache within the IPU sub-system.
The OMAP remoteproc platform data structure is eventually expected
to be removed completely once the other dependencies with the
mach-omap layer are met.
Signed-off-by: Suman Anna <s-anna@ti.com>
|
| |
| |
| |
| |
| |
| |
| | |
Use the appropriate SPDX license identifiers in various OMAP remoteproc
source files and drop the previous boilerplate license text.
Signed-off-by: Suman Anna <s-anna@ti.com>
|
|/
|
|
|
|
|
|
|
|
|
|
|
| |
The PRUSS can have a PRCM reset line associated with the IP on
some OMAP architecture based SoCs. The reset needs to be programmed
properly before accessing any of the internal registers in the PRUSS.
This functionality is achieved through the omap_device layer, which
is not exposed outside of mach-omap2 layer. Define a platform data
structure for PRUSS so that this API can be invoked through platform
data ops from the driver.
Signed-off-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Roger Quadros <rogerq@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
fix the sysfs shunt resistor read access: return the shunt resistor
value, not the calibration register contents.
update email address
Signed-off-by: Lothar Felten <lothar.felten@gmail.com>
Signed-off-by: Guenter Roeck <linux@roeck-us.net>
|
|\
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
git://git.kernel.org/pub/scm/linux/kernel/git/joro/iommu
Pull IOMMU updates from Joerg Roedel:
- PASID table handling updates for the Intel VT-d driver. It implements
a global PASID space now so that applications usings multiple devices
will just have one PASID.
- A new config option to make iommu passthroug mode the default.
- New sysfs attribute for iommu groups to export the type of the
default domain.
- A debugfs interface (for debug only) usable by IOMMU drivers to
export internals to user-space.
- R-Car Gen3 SoCs support for the ipmmu-vmsa driver
- The ARM-SMMU now aborts transactions from unknown devices and devices
not attached to any domain.
- Various cleanups and smaller fixes all over the place.
* tag 'iommu-updates-v4.19' of git://git.kernel.org/pub/scm/linux/kernel/git/joro/iommu: (42 commits)
iommu/omap: Fix cache flushes on L2 table entries
iommu: Remove the ->map_sg indirection
iommu/arm-smmu-v3: Abort all transactions if SMMU is enabled in kdump kernel
iommu/arm-smmu-v3: Prevent any devices access to memory without registration
iommu/ipmmu-vmsa: Don't register as BUS IOMMU if machine doesn't have IPMMU-VMSA
iommu/ipmmu-vmsa: Clarify supported platforms
iommu/ipmmu-vmsa: Fix allocation in atomic context
iommu: Add config option to set passthrough as default
iommu: Add sysfs attribyte for domain type
iommu/arm-smmu-v3: sync the OVACKFLG to PRIQ consumer register
iommu/arm-smmu: Error out only if not enough context interrupts
iommu/io-pgtable-arm-v7s: Abort allocation when table address overflows the PTE
iommu/io-pgtable-arm: Fix pgtable allocation in selftest
iommu/vt-d: Remove the obsolete per iommu pasid tables
iommu/vt-d: Apply per pci device pasid table in SVA
iommu/vt-d: Allocate and free pasid table
iommu/vt-d: Per PCI device pasid table interfaces
iommu/vt-d: Add for_each_device_domain() helper
iommu/vt-d: Move device_domain_info to header
iommu/vt-d: Apply global PASID in SVA
...
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
include/linux/platform_data/sh_ipmmu.h is unused since commit
ae50dc4874c5 ("iommu/shmobile: Remove unused Renesas IPMMU/IPMMUI")
Let's remove it.
Signed-off-by: Corentin Labbe <clabbe@baylibre.com>
Reviewed-by: Geert Uytterhoeven <geert+renesas@glider.be>
Reviewed-by: Simon Horman <horms+renesas@verge.net.au>
Signed-off-by: Joerg Roedel <jroedel@suse.de>
|
| |
| |
| |
| |
| |
| |
| | |
The old @sunsite.dk address is no longer active, so update the references.
Signed-off-by: Peter Korsgaard <peter@korsgaard.com>
Signed-off-by: Wolfram Sang <wsa@the-dreams.de>
|
|\ \
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc
Pull ARM SoC driver updates from Olof Johansson:
"Some of the larger changes this merge window:
- Removal of drivers for Exynos5440, a Samsung SoC that never saw
widespread use.
- Uniphier support for USB3 and SPI reset handling
- Syste control and SRAM drivers and bindings for Allwinner platforms
- Qualcomm AOSS (Always-on subsystem) reset controller drivers
- Raspberry Pi hwmon driver for voltage
- Mediatek pwrap (pmic) support for MT6797 SoC"
* tag 'armsoc-drivers' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc: (52 commits)
drivers/firmware: psci_checker: stash and use topology_core_cpumask for hotplug tests
soc: fsl: cleanup Kconfig menu
soc: fsl: dpio: Convert DPIO documentation to .rst
staging: fsl-mc: Remove remaining files
staging: fsl-mc: Move DPIO from staging to drivers/soc/fsl
staging: fsl-dpaa2: eth: move generic FD defines to DPIO
soc: fsl: qe: gpio: Add qe_gpio_set_multiple
usb: host: exynos: Remove support for Exynos5440
clk: samsung: Remove support for Exynos5440
soc: sunxi: Add the A13, A23 and H3 system control compatibles
reset: uniphier: add reset control support for SPI
cpufreq: exynos: Remove support for Exynos5440
ata: ahci-platform: Remove support for Exynos5440
soc: imx6qp: Use GENPD_FLAG_ALWAYS_ON for PU errata
soc: mediatek: pwrap: add mt6351 driver for mt6797 SoCs
soc: mediatek: pwrap: add pwrap driver for mt6797 SoCs
soc: mediatek: pwrap: fix cipher init setting error
dt-bindings: pwrap: mediatek: add pwrap support for MT6797
reset: uniphier: add USB3 core reset control
dt-bindings: reset: uniphier: add USB3 core reset support
...
|
| |/
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
The dra76x MCAN generic interconnect module has a its own
format for the bits in the control registers.
Therefore add a new module type, new regbits and new capabilities
specific to the MCAN module.
Acked-by: Rob Herring <robh@kernel.org>
CC: Tony Lindgren <tony@atomide.com>
Signed-off-by: Faiz Abbas <faiz_abbas@ti.com>
Signed-off-by: Tony Lindgren <tony@atomide.com>
|
|\ \
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc
Pull ARM 32-bit SoC platform updates from Olof Johansson:
"Most of the SoC updates in this cycle are cleanups and moves to more
modern infrastructure:
- Davinci was moved to common clock framework
- OMAP1-based Amstrad E3 "Superphone" saw a bunch of cleanups to the
keyboard interface (bitbanged AT keyboard via GPIO).
- Removal of some stale code for Renesas platforms
- Power management improvements for i.MX6LL"
* tag 'armsoc-soc' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc: (112 commits)
ARM: uniphier: select RESET_CONTROLLER
arm64: uniphier: select RESET_CONTROLLER
ARM: uniphier: remove empty Makefile
ARM: exynos: Clear global variable on init error path
ARM: exynos: Remove outdated maintainer information
ARM: shmobile: Always enable ARCH_TIMER on SoCs with A7 and/or A15
ARM: shmobile: r8a7779: hide unused r8a7779_platform_cpu_kill
soc: r9a06g032: don't build SMP files for non-SMP config
ARM: shmobile: Add the R9A06G032 SMP enabler driver
ARM: at91: pm: configure wakeup sources for ULP1 mode
ARM: at91: pm: add PMC fast startup registers defines
ARM: at91: pm: Add ULP1 mode support
ARM: at91: pm: Use ULP0 naming instead of slow clock
ARM: hisi: handle of_iomap and fix missing of_node_put
ARM: hisi: check of_iomap and fix missing of_node_put
ARM: hisi: fix error handling and missing of_node_put
ARM: mx5: Set the DBGEN bit in ARM_GPC register
ARM: imx51: Configure M4IF to avoid visual artifacts
ARM: imx: call imx6sx_cpuidle_init() conditionally for 6sll
ARM: imx: fix i.MX6SLL build
...
|
| |\ \
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
This is the pxa changes for 4.19 cycle :
- the pxa architecture is ported to dma slavemap
- some minor AC97 fixes
- some minor board fixes
* tag 'pxa-for-4.19-v2' of https://github.com/rjarzmik/linux:
net: smc91x: remove the dmaengine compat need
net: smc911x: remove the dmaengine compat need
ARM: pxa: zylonite: use the new ac97 bus support
ARM: pxa: add the missing AC97 clocks
ARM: pxa: mioa701 convert to the new AC97 bus
ARM: pxa: hx4700: fix the usb client
ARM: pxa: change SSP DMA channels allocation
ARM: pxa: remove the DMA IO resources
dmaengine: pxa: document pxad_param
ata: pata_pxa: remove the dmaengine compat need
mtd: rawnand: marvell: remove the dmaengine compat need
media: pxa_camera: remove the dmaengine compat need
mmc: pxamci: remove the dmaengine compat need
dmaengine: pxa: add a default requestor policy
ARM: pxa: add dma slave map
dmaengine: pxa: use a dma slave map
Signed-off-by: Olof Johansson <olof@lixom.net>
|
| |\ \ \
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/tmlind/linux-omap into next/soc
SoC updates for omaps for v4.19 merge window
These changes are mostly PM related changes for am335x and
am437x to support RTC only suspend mode. Some of the clock
and driver related chances are still pending so it's not
yet fully functional.
Also included is a change for PM debug sysfs entry to use
DEFINE_SHOW_ATTRIBUTE.
* tag 'omap-for-v4.19/soc-signed' of git://git.kernel.org/pub/scm/linux/kernel/git/tmlind/linux-omap:
ARM: OMAP2+: sleep33/43xx: Add RTC-Mode support
ARM: OMAP2+: sleep33/43xx: Make sleep actions configurable
ARM: OMAP2+: reuse DEFINE_SHOW_ATTRIBUTE() macro
ARM: hwmod: RTC: Don't assume lock/unlock will be called with irq enabled
Signed-off-by: Olof Johansson <olof@lixom.net>
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
Add support for RTC mode to low level suspend code. This includes
providing the rtc base address for the assembly code to configuring the
PMIC_PWR_EN line late in suspend to enter RTC+DDR mode.
Note: This patch also fold in left out space parameter for
am33xx_emif_sram_table and am43xx_emif_sram_table
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
Signed-off-by: Tony Lindgren <tony@atomide.com>
|
| | | |/
| | |/|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Add an argument to the sleep33xx and sleep43xx code to allow us to set
flags to determine which portions of the code get called in order to use
the same code for multiple power saving modes. This patch allows us to
decide whether or not we flush and disable caches, save EMIF context,
put the memory into self refresh and disable the EMIF, and/or invoke
the wkup_m3 when entering into WFI.
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
Signed-off-by: Tero Kristo <t-kristo@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
Signed-off-by: Tony Lindgren <tony@atomide.com>
|
| |\ \ \
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/tmlind/linux-omap into next/soc
SoC updates for omap1 for v4.19 merge window
Mostly a series by Janusz Krzysztofik to clean up the
GPIO and input handling for ams-delta. Because of the
platform data changes, we decided that it's best to
merge the related input changes also via the arm-soc
tree so Dmitry Torokhov has acked the input changes.
Also included is a change to constify gpio_leds from
Arvind Yadav.
* tag 'omap-for-v4.19/omap1-v2-signed' of git://git.kernel.org/pub/scm/linux/kernel/git/tmlind/linux-omap:
ARM: OMAP1: ams-delta: move late devices back to init_machine
Input: ams_delta_serio: Get FIQ buffer from platform_data
Input: ams_delta_serio: use IRQ resource
ARM: OMAP1: Get rid of <mach/ams-delta-fiq.h>
ARM: OMAP1: ams-delta FIQ: Keep serio input GPIOs requested
ARM: OMAP1: ams-delta FIQ: don't use static GPIO numbers
ARM: OMAP1: ams-delta: Hog "keybrd_dataout" GPIO pin
Input: ams_delta_serio: Replace power GPIO with regulator
Input: ams_delta_serio: use private structure
Input: ams_delta_serio: convert to platform driver
ARM: OMAP1: ams-delta: drop GPIO lookup table for serio device
ARM: OMAP1: ams-delta: assign LED GPIO numbers from descriptors
ARM: OMAP1: ams-delta: refactor late_init()
ARM: OMAP1: constify gpio_led
Signed-off-by: Olof Johansson <olof@lixom.net>
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
Instead of exporting the FIQ buffer symbol to be used in
ams-delta-serio driver, pass it to the driver as platform_data.
Signed-off-by: Janusz Krzysztofik <jmkrzyszt@gmail.com>
Acked-by: Dmitry Torokhov <dmitry.torokhov@gmail.com>
Signed-off-by: Tony Lindgren <tony@atomide.com>
|
| | |/ /
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Split the header file into two parts and move them to directories where
they belong.
Information on internal structure of FIQ buffer is moved to
<linux/platform_data/ams-delta-fiq.h> for ams-delta-serio driver use.
Other information used by ams-delta board init file and FIQ code is
made local to mach-omap1 root directory.
Signed-off-by: Janusz Krzysztofik <jmkrzyszt@gmail.com>
Acked-by: Dmitry Torokhov <dmitry.torokhov@gmail.com>
Signed-off-by: Tony Lindgren <tony@atomide.com>
|
| |/ /
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
All users now register platform devices using the ti-aemif driver.
Remove the handcrafted aemif API.
Signed-off-by: Bartosz Golaszewski <bgolaszewski@baylibre.com>
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
|
|\ \ \
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/jikos/hid
Pull HID updates from Jiri Kosina:
- touch_max detection improvements and quirk handling fixes in wacom
driver from Jason Gerecke and Ping Cheng
- Palm rejection from Dmitry Torokhov and _dial support from Benjamin
Tissoires for hid-multitouch driver
- Low voltage support for i2c-hid driver from Stephen Boyd
- Guitar-Hero support from Nicolas Adenis-Lamarre
- other assorted small fixes and device ID additions
* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/jikos/hid: (40 commits)
HID: intel_ish-hid: tx_buf memory leak on probe/remove
HID: intel-ish-hid: Prevent loading of driver on Mehlow
HID: cougar: Add support for the Cougar 500k Gaming Keyboard
HID: cougar: make compare_device_paths reusable
HID: intel-ish-hid: remove redundant variable num_frags
HID: multitouch: handle palm for touchscreens
HID: multitouch: touchscreens also use confidence reports
HID: multitouch: report MT_TOOL_PALM for non-confident touches
HID: microsoft: support the Surface Dial
HID: core: do not upper bound the collection stack
HID: input: enable Totem on the Dell Canvas 27
HID: multitouch: remove one copy of values
HID: multitouch: ditch mt_report_id
HID: multitouch: store a per application quirks value
HID: multitouch: Store per collection multitouch data
HID: multitouch: make sure the static list of class is not changed
input: add MT_TOOL_DIAL
HID: elan: Add support for touchpad on the Toshiba Click Mini L9W
HID: elan: Add USB-id for HP x2 10-n000nd touchpad
HID: elan: Add a flag for selecting if the touchpad has a LED
...
|
| |\ \ \
| | |/ /
| |/| |
| | | | |
Low voltage support for i2c-hid
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Some wacom w9013 devices have a vddl supply for "low valtage"
requirements. Add support in this driver to turn on this low voltage
supply. We can also drop a handful of error messages because the
regulator core is already printing an error when bulk regulators fail to
enable or disable.
Cc: Benjamin Tissoires <benjamin.tissoires@redhat.com>
Cc: Hans de Goede <hdegoede@redhat.com>
Cc: Andy Shevchenko <andriy.shevchenko@linux.intel.com>
Cc: Dmitry Torokhov <dtor@chromium.org>
Cc: Doug Anderson <dianders@chromium.org>
Acked-by: Rob Herring <robh@kernel.org>
Cc: <devicetree@vger.kernel.org>
Signed-off-by: Stephen Boyd <swboyd@chromium.org>
Acked-by: Benjamin Tissoires <benjamin.tissoires@redhat.com>
Signed-off-by: Jiri Kosina <jkosina@suse.cz>
|
|\ \ \ \
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
Pull MMC updates from Ulf Hansson:
"Updates for MMC for v4.19.
MMC core:
- Add some fine-grained hooks to further support HS400 tuning
- Improve error path for bus width setting for HS400es
- Use a common method when checking R1 status
MMC host:
- renesas_sdhi: Add r8a77990 support
- renesas_sdhi: Add eMMC HS400 mode support
- tmio/renesas_sdhi: Improve tuning/clock management
- tmio: Add eMMC HS400 mode support
- sunxi: Add support for 3.3V eMMC DDR mode
- mmci: Initial support to manage variant specific callbacks
- sdhci: Don't try 3.3V I/O voltage if not supported
- sdhci-pci-dwc-mshc: Add driver to support Synopsys dwc mshc SDHCI PCI
- sdhci-of-dwcmshc: Add driver to support Synopsys DWC MSHC SDHCI
- sdhci-msm: Add support for new version sdcc V5
- sdhci-pci-o2micro: Add support for O2 eMMC HS200 mode
- sdhci-pci-o2micro: Add support for O2 hardware tuning
- sdhci-pci-o2micro: Add MSI interrupt support for O2 SD host
- sdhci-pci: Add support for Intel ICP
- sdhci-tegra: Prevent ACMD23 and HS200 mode on Tegra 3
- sdhci-tegra: Fix eMMC DDR52 mode
- sdhci-tegra: Improve clock management
- dw_mmc-rockchip: Document compatible string for px30
- sdhci-esdhc-imx: Add support for 3.3V eMMC DDR mode
- sdhci-of-esdhc: Set proper DMA mask for ls104x chips
- sdhci-of-esdhc: Improve clock management
- sdhci-of-arasan: Add a quirk to manage unstable clocks
- dw_mmc-exynos: Address potential external abort during system resume
- pxamci: Add support for common MMC DT bindings
- pxamci: Several cleanups and improvements
- pxamci: Merge immutable branch for pxa to switch to DMA slave maps"
* tag 'mmc-v4.19' of git://git.kernel.org/pub/scm/linux/kernel/git/ulfh/mmc: (56 commits)
mmc: core: improve reasonableness of bus width setting for HS400es
mmc: tmio: remove unneeded variable in tmio_mmc_start_command()
mmc: renesas_sdhi: Fix sampling clock position selecting
mmc: tmio: Fix tuning flow
mmc: sunxi: remove output of virtual base address
dt-bindings: mmc: rockchip-dw-mshc: add description for px30
mmc: renesas_sdhi: Add r8a77990 support
mmc: sunxi: allow 3.3V DDR when DDR is available
mmc: mmci: Add and implement a ->dma_setup() callback for qcom dml
mmc: mmci: Initial support to manage variant specific callbacks
mmc: tegra: Force correct divider calculation on DDR50/52
mmc: sdhci: Add MSI interrupt support for O2 SD host
mmc: sdhci: Add support for O2 hardware tuning
mmc: sdhci: Export sdhci tuning function symbol
mmc: sdhci: Change O2 Host HS200 mode clock frequency to 200MHz
mmc: sdhci: Add support for O2 eMMC HS200 mode
mmc: tegra: Add and use tegra_sdhci_get_max_clock()
mmc: sdhci-esdhc-imx: fix indent
mmc: sdhci-esdhc-imx: disable clocks before changing frequency
mmc: tegra: prevent ACMD23 on Tegra 3
...
|
| | |_|/
| |/| |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
The field support_vsel is currently only used in the device tree
case. Get rid of it. No change in behavior.
Signed-off-by: Stefan Agner <stefan@agner.ch>
Signed-off-by: Ulf Hansson <ulf.hansson@linaro.org>
|
|\ \ \ \
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/linusw/linux-gpio
Pull GPIO updates from Linus Walleij:
"This is the bulk of GPIO changes for the v4.19 kernel cycle.
I don't know if anything in particular stands out. Maybe the Aspeed
coprocessor thing from Benji: Aspeed is doing baseboard management
chips (BMC's) for servers etc.
These Aspeed's are ARM processors that exist inside (I guess) Intel
servers, and they are moving forward to using mainline Linux in those.
This is one of the pieces of the puzzle to achive that. They are doing
OpenBMC, it's pretty cool: https://lwn.net/Articles/683320/
Summary:
Core changes:
- Add a new API for explicitly naming GPIO consumers, when needed.
- Don't let userspace set values on input lines. While we do not
think anyone would do this crazy thing we better plug the hole
before someone uses it and think it's a nifty feature.
- Avoid calling chip->request() for unused GPIOs.
New drivers/subdrivers:
- The Mediatek MT7621 is supported which is a big win for OpenWRT and
similar router distributions using this chip, as it seems every
major router manufacturer on the planet has made products using
this chip: https://wikidevi.com/wiki/MediaTek_MT7621
- The Tegra 194 is now supported.
- The IT87 driver now supports IT8786E and IT8718F super-IO chips.
- Add support for Rockchip RK3328 in the syscon GPIO driver.
Driver changes:
- Handle the get/set_multiple() properly on MMIO chips with inverted
direction registers. We didn't have this problem until a new chip
appear that has get/set registers AND inverted direction bits, OK
now we handle it.
- A patch series making more error codes percolate upward properly
for different errors on gpiochip_lock_as_irq().
- Get/set multiple for the OMAP driver, accelerating these multiple
line operations if possible.
- A coprocessor interface for the Aspeed driver. Sometimes a few GPIO
lines need to be grabbed by a co-processor for doing automated
tasks, sometimes they are available as GPIO lines. By adding an
explicit API in this driver we make it possible for the two line
consumers to coexist. (This work was made available on the
ib-aspeed branch, which may be appearing in other pull requests.)
- Implemented .get_direction() and open drain in the SCH311x driver.
- Continuing cleanup of included headers in GPIO drivers"
* tag 'gpio-v4.19-1' of git://git.kernel.org/pub/scm/linux/kernel/git/linusw/linux-gpio: (80 commits)
gpio: it87: Add support for IT8613
gpio: it87: add support for IT8718F Super I/O.
gpiolib: Avoid calling chip->request() for unused gpios
gpio: tegra: Include the right header
gpio: mmio: Fix up inverted direction registers
gpio: xilinx: Use the right include
gpio: timberdale: Include the right header
gpio: tb10x: Use the right include
gpiolib: Fix of_node inconsistency
gpio: vr41xx: Bail out on gpiochip_lock_as_irq() error
gpio: uniphier: Bail out on gpiochip_lock_as_irq() error
gpio: xgene-sb: Don't shadow error code of gpiochip_lock_as_irq()
gpio: em: Don't shadow error code of gpiochip_lock_as_irq()
gpio: dwapb: Don't shadow error code of gpiochip_lock_as_irq()
gpio: bcm-kona: Don't shadow error code of gpiochip_lock_as_irq()
gpiolib: Don't shadow error code of gpiochip_lock_as_irq()
gpio: syscon: rockchip: add GRF GPIO support for rk3328
gpio: omap: Add get/set_multiple() callbacks
gpio: pxa: remove set but not used variable 'gpio_offset'
gpio-it87: add support for IT8786E Super I/O
...
|
| | |/ /
| |/| |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Currently the driver assumes that the interrupts are continuous
and does platform_get_irq only once and assumes the rest are continuous,
instead call platform_get_irq for all the interrupts and store them
in an array for later use.
Signed-off-by: Keerthy <j-keerthy@ti.com>
Reviewed-by: Grygorii Strashko <grygorii.strashko@ti.com>
Signed-off-by: Linus Walleij <linus.walleij@linaro.org>
|
|\ \ \ \
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/mchehab/linux-media
Pull media updates from Mauro Carvalho Chehab:
- new Socionext MN88443x ISDB-S/T demodulator driver: mn88443x
- new sensor drivers: ak7375, ov2680 and rj54n1cb0c
- an old soc-camera sensor driver converted to the V4L2 framework:
mt9v111
- a new Voice-Coil Motor (VCM) driver: dw9807-vcm
- some cleanups at cx25821, removing legacy unused code
- some improvements at ddbridge driver
- new platform driver: vicodec
- some DVB API cleanups, removing ioctls and compat code for old
out-of-tree drivers that were never merged upstream
- improvements at DVB core to support frontents that support both
Satellite and non-satellite delivery systems
- got rid of the unused VIDIOC_RESERVED V4L2 ioctl
- some cleanups/improvements at gl861 ISDB driver
- several improvements on ov772x, ov7670 and ov5640, imx274, ov5645,
and smiapp sensor drivers
- fixes at em28xx to support dual TS devices
- some cleanups at V4L2/VB2 locking logic
- some API improvements at media controller
- some cec core and drivers improvements
- some uvcvideo improvements
- some improvements at platform drivers: stm32-dcmi, rcar-vin, coda,
reneseas-ceu, imx, vsp1, venus, camss
- lots of other cleanups and fixes
* tag 'media/v4.19-1' of git://git.kernel.org/pub/scm/linux/kernel/git/mchehab/linux-media: (406 commits)
Revert "media: vivid: shut up warnings due to a non-trivial logic"
siano: get rid of an unused return code for debugfs register
media: isp: fix a warning about a wrong struct initializer
media: radio-wl1273: fix return code for the polling routine
media: s3c-camif: fix return code for the polling routine
media: saa7164: fix return codes for the polling routine
media: exynos-gsc: fix return code if mutex was interrupted
media: mt9v111: Fix build error with no VIDEO_V4L2_SUBDEV_API
media: xc4000: get rid of uneeded casts
media: drxj: get rid of uneeded casts
media: tuner-xc2028: don't use casts for printing sizes
media: cleanup fall-through comments
media: vivid: shut up warnings due to a non-trivial logic
media: rtl28xxu: be sure that it won't go past the array size
media: mt9v111: avoid going past the buffer
media: vsp1_dl: add a description for cmdpool field
media: sta2x11: add a missing parameter description
media: v4l2-mem2mem: add descriptions to MC fields
media: i2c: fix warning in Aptina MT9V111
media: imx: shut up a false positive warning
...
|
| |/ / /
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
The include/linux/platform_data/media/sii9234.h header file is unused,
let's remove it.
Signed-off-by: Corentin Labbe <clabbe@baylibre.com>
Signed-off-by: Mauro Carvalho Chehab <mchehab+samsung@kernel.org>
|
|\ \ \ \
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
Pull networking updates from David Miller:
"Highlights:
- Gustavo A. R. Silva keeps working on the implicit switch fallthru
changes.
- Support 802.11ax High-Efficiency wireless in cfg80211 et al, From
Luca Coelho.
- Re-enable ASPM in r8169, from Kai-Heng Feng.
- Add virtual XFRM interfaces, which avoids all of the limitations of
existing IPSEC tunnels. From Steffen Klassert.
- Convert GRO over to use a hash table, so that when we have many
flows active we don't traverse a long list during accumluation.
- Many new self tests for routing, TC, tunnels, etc. Too many
contributors to mention them all, but I'm really happy to keep
seeing this stuff.
- Hardware timestamping support for dpaa_eth/fsl-fman from Yangbo Lu.
- Lots of cleanups and fixes in L2TP code from Guillaume Nault.
- Add IPSEC offload support to netdevsim, from Shannon Nelson.
- Add support for slotting with non-uniform distribution to netem
packet scheduler, from Yousuk Seung.
- Add UDP GSO support to mlx5e, from Boris Pismenny.
- Support offloading of Team LAG in NFP, from John Hurley.
- Allow to configure TX queue selection based upon RX queue, from
Amritha Nambiar.
- Support ethtool ring size configuration in aquantia, from Anton
Mikaev.
- Support DSCP and flowlabel per-transport in SCTP, from Xin Long.
- Support list based batching and stack traversal of SKBs, this is
very exciting work. From Edward Cree.
- Busyloop optimizations in vhost_net, from Toshiaki Makita.
- Introduce the ETF qdisc, which allows time based transmissions. IGB
can offload this in hardware. From Vinicius Costa Gomes.
- Add parameter support to devlink, from Moshe Shemesh.
- Several multiplication and division optimizations for BPF JIT in
nfp driver, from Jiong Wang.
- Lots of prepatory work to make more of the packet scheduler layer
lockless, when possible, from Vlad Buslov.
- Add ACK filter and NAT awareness to sch_cake packet scheduler, from
Toke Høiland-Jørgensen.
- Support regions and region snapshots in devlink, from Alex Vesker.
- Allow to attach XDP programs to both HW and SW at the same time on
a given device, with initial support in nfp. From Jakub Kicinski.
- Add TLS RX offload and support in mlx5, from Ilya Lesokhin.
- Use PHYLIB in r8169 driver, from Heiner Kallweit.
- All sorts of changes to support Spectrum 2 in mlxsw driver, from
Ido Schimmel.
- PTP support in mv88e6xxx DSA driver, from Andrew Lunn.
- Make TCP_USER_TIMEOUT socket option more accurate, from Jon
Maxwell.
- Support for templates in packet scheduler classifier, from Jiri
Pirko.
- IPV6 support in RDS, from Ka-Cheong Poon.
- Native tproxy support in nf_tables, from Máté Eckl.
- Maintain IP fragment queue in an rbtree, but optimize properly for
in-order frags. From Peter Oskolkov.
- Improvde handling of ACKs on hole repairs, from Yuchung Cheng"
* git://git.kernel.org/pub/scm/linux/kernel/git/davem/net-next: (1996 commits)
bpf: test: fix spelling mistake "REUSEEPORT" -> "REUSEPORT"
hv/netvsc: Fix NULL dereference at single queue mode fallback
net: filter: mark expected switch fall-through
xen-netfront: fix warn message as irq device name has '/'
cxgb4: Add new T5 PCI device ids 0x50af and 0x50b0
net: dsa: mv88e6xxx: missing unlock on error path
rds: fix building with IPV6=m
inet/connection_sock: prefer _THIS_IP_ to current_text_addr
net: dsa: mv88e6xxx: bitwise vs logical bug
net: sock_diag: Fix spectre v1 gadget in __sock_diag_cmd()
ieee802154: hwsim: using right kind of iteration
net: hns3: Add vlan filter setting by ethtool command -K
net: hns3: Set tx ring' tc info when netdev is up
net: hns3: Remove tx ring BD len register in hns3_enet
net: hns3: Fix desc num set to default when setting channel
net: hns3: Fix for phy link issue when using marvell phy driver
net: hns3: Fix for information of phydev lost problem when down/up
net: hns3: Fix for command format parsing error in hclge_is_all_function_id_zero
net: hns3: Add support for serdes loopback selftest
bnxt_en: take coredump_record structure off stack
...
|
| |/ / /
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Nothing in tree use this header which seems a remains of a staging
driver.
This patch remove it.
Signed-off-by: Corentin Labbe <clabbe@baylibre.com>
Reviewed-by: Sebastian Reichel <sebastian.reichel@collabora.co.uk>
Signed-off-by: Marcel Holtmann <marcel@holtmann.org>
|
|\ \ \ \
| | |/ /
| |/| |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound
Pull sound updates from Takashi Iwai:
"It's been busy summer weeks and hence lots of changes, partly for a
few new drivers and partly for a wide range of fixes.
Here are highlights:
ALSA Core:
- Fix rawmidi buffer management, code cleanup / refactoring
- Fix the SG-buffer page handling with incorrect fallback size
- Fix the stall at virmidi trigger callback with a large buffer; also
offloading and code-refactoring along with it
- Various ALSA sequencer code cleanups
ASoC:
- Deploy the standard snd_pcm_stop_xrun() helper in several drivers
- Support for providing name prefixes to generic component nodes
- Quite a few fixes for DPCM as it gains a bit wider use and more
robust testing
- Generalization of the DIO2125 support to a simple amplifier driver
- Accessory detection support for the audio graph card
- DT support for PXA AC'97 devices
- Quirks for a number of new x86 systems
- Support for AM Logic Meson, Everest ES7154, Intel systems with
RT5682, Qualcomm QDSP6 and WCD9335, Realtek RT5682 and TI TAS5707
HD-audio:
- Code refactoring in HD-audio ext codec codes to drop own classes;
preliminary works for the upcoming legacy codec support
- Generalized DRM audio component for the upcoming radeon / amdgpu
support
- Unification of mic mute-LED and GPIO support for various codecs
- Further improvement of CA0132 codec support including Recon3D
- Proper vga_switcheroo handling for AMD i-GPU
- Update of model list in documentation
- Fixups for another HP Spectre x360, Conexant codecs, power-save
blacklist update
USB-audio:
- Fix the invalid sample rate setup with external clock
- Support of UAC3 selector units and processing units
- Basic UAC3 power-domain support
- Support for Encore mDSD and Thesycon-based DSD devices
- Preparation for future complete callback changes
Firewire:
- Add support for MOTU Traveler
Misc:
- The endianess notation fixes in various drivers
- Add fall-through comment in lots of drivers
- Various sparse warning fixes, e.g. about PCM format types"
* tag 'sound-4.19-rc1' of git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound: (529 commits)
ASoC: adav80x: mark expected switch fall-through
ASoC: da7219: Add delays to capture path to remove DC offset noise
ALSA: usb-audio: Mark expected switch fall-through
ALSA: mixart: Mark expected switch fall-through
ALSA: opl3: Mark expected switch fall-through
ALSA: hda/ca0132 - Add exit commands for Recon3D
ALSA: hda/ca0132 - Change mixer controls for Recon3D
ALSA: hda/ca0132 - Add Recon3D input and output select commands
ALSA: hda/ca0132 - Add DSP setup defaults for Recon3D
ALSA: hda/ca0132 - Add Recon3D startup functions and setup
ALSA: hda/ca0132 - Add bool variable to enable/disable pci region2 mmio
ALSA: hda/ca0132 - Add Recon3D pincfg
ALSA: hda/ca0132 - Add quirk ID and enum for Recon3D
ALSA: hda/ca0132 - Add alt_functions unsolicited response
ALSA: hda/ca0132 - Clean up ca0132_init function.
ALSA: hda/ca0132 - Create mmio gpio function to make code clearer
ASoC: wm_adsp: Make DSP name configurable by codec driver
ASoC: wm_adsp: Declare firmware controls from codec driver
ASoC: max98373: Added software reset register to readable registers
ASoC: wm_adsp: Correct DSP pointer for preloader control
...
|
| |/ /
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
In order to remove the specific knowledge of the dma mapping from PXA
drivers, add a default slave map for pxa architectures.
This won't impact MMP architecture, but is aimed only at all PXA boards.
This is the first step, and once all drivers are converted,
pxad_filter_fn() will be made static, and the DMA resources removed from
device.c.
Signed-off-by: Robert Jarzmik <robert.jarzmik@free.fr>
Reported-by: Arnd Bergmann <arnd@arndb.de>
Acked-by: Vinod Koul <vkoul@kernel.org>
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
This way we will be able to compile the jz4740_nand driver when
COMPILE_TEST=y.
Signed-off-by: Boris Brezillon <boris.brezillon@bootlin.com>
Acked-by: Paul Burton <paul.burton@mips.com>
Signed-off-by: Miquel Raynal <miquel.raynal@bootlin.com>
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
This way we will be able to compile the ndfmc driver when
COMPILE_TEST=y.
Signed-off-by: Boris Brezillon <boris.brezillon@bootlin.com>
Acked-by: Paul Burton <paul.burton@mips.com>
Signed-off-by: Miquel Raynal <miquel.raynal@bootlin.com>
|
|/ /
| |
| |
| |
| |
| |
| |
| | |
None of the boards seem to overload the ->dev_ready() hook, just drop
this field from orion_nand_data.
Signed-off-by: Boris Brezillon <boris.brezillon@bootlin.com>
Signed-off-by: Miquel Raynal <miquel.raynal@bootlin.com>
|
|\ \
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Pull documentation fixes from Mauro Carvalho Chehab:
"This solves a series of broken links for files under Documentation,
and improves a script meant to detect such broken links (see
scripts/documentation-file-ref-check).
The changes on this series are:
- can.rst: fix a footnote reference;
- crypto_engine.rst: Fix two parsing warnings;
- Fix a lot of broken references to Documentation/*;
- improve the scripts/documentation-file-ref-check script, in order
to help detecting/fixing broken references, preventing
false-positives.
After this patch series, only 33 broken references to doc files are
detected by scripts/documentation-file-ref-check"
* tag 'docs-broken-links' of git://linuxtv.org/mchehab/experimental: (26 commits)
fix a series of Documentation/ broken file name references
Documentation: rstFlatTable.py: fix a broken reference
ABI: sysfs-devices-system-cpu: remove a broken reference
devicetree: fix a series of wrong file references
devicetree: fix name of pinctrl-bindings.txt
devicetree: fix some bindings file names
MAINTAINERS: fix location of DT npcm files
MAINTAINERS: fix location of some display DT bindings
kernel-parameters.txt: fix pointers to sound parameters
bindings: nvmem/zii: Fix location of nvmem.txt
docs: Fix more broken references
scripts/documentation-file-ref-check: check tools/*/Documentation
scripts/documentation-file-ref-check: get rid of false-positives
scripts/documentation-file-ref-check: hint: dash or underline
scripts/documentation-file-ref-check: add a fix logic for DT
scripts/documentation-file-ref-check: accept more wildcards at filenames
scripts/documentation-file-ref-check: fix help message
media: max2175: fix location of driver's companion documentation
media: v4l: fix broken video4linux docs locations
media: dvb: point to the location of the old README.dvb-usb file
...
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
As files move around, their previous links break. Fix the
references for them.
Acked-by: Andy Shevchenko <andy.shevchenko@gmail.com>
Signed-off-by: Mauro Carvalho Chehab <mchehab+samsung@kernel.org>
Acked-by: Jonathan Corbet <corbet@lwn.net>
|
|\ \ \
| |/ /
|/| |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Pull fbdev updates from Bartlomiej Zolnierkiewicz:
"There is nothing really major here, few small fixes, some cleanups and
dead drivers removal:
- mark omapfb drivers as orphans in MAINTAINERS file (Tomi Valkeinen)
- add missing module license tags to omap/omapfb driver (Arnd
Bergmann)
- add missing GPIOLIB dependendy to omap2/omapfb driver (Arnd
Bergmann)
- convert savagefb, aty128fb & radeonfb drivers to use msleep & co.
(Jia-Ju Bai)
- allow COMPILE_TEST build for viafb driver (media part was reviewed
by media subsystem Maintainer)
- remove unused MERAM support from sh_mobile_lcdcfb and shmob-drm
drivers (drm parts were acked by shmob-drm driver Maintainer)
- remove unused auo_k190xfb drivers
- misc cleanups (Souptick Joarder, Wolfram Sang, Markus Elfring, Andy
Shevchenko, Colin Ian King)"
* tag 'fbdev-v4.18' of git://github.com/bzolnier/linux: (26 commits)
fb_omap2: add gpiolib dependency
video/omap: add module license tags
MAINTAINERS: make omapfb orphan
video: fbdev: pxafb: match_string() conversion fixup
video: fbdev: nvidia: fix spelling mistake: "scaleing" -> "scaling"
video: fbdev: fix spelling mistake: "frambuffer" -> "framebuffer"
video: fbdev: pxafb: Convert to use match_string() helper
video: fbdev: via: allow COMPILE_TEST build
video: fbdev: remove unused sh_mobile_meram driver
drm: shmobile: remove unused MERAM support
video: fbdev: sh_mobile_lcdcfb: remove unused MERAM support
video: fbdev: remove unused auo_k190xfb drivers
video: omap: Improve a size determination in omapfb_do_probe()
video: sm501fb: Improve a size determination in sm501fb_probe()
video: fbdev-MMP: Improve a size determination in path_init()
video: fbdev-MMP: Delete an error message for a failed memory allocation in two functions
video: auo_k190x: Delete an error message for a failed memory allocation in auok190x_common_probe()
video: sh_mobile_lcdcfb: Delete an error message for a failed memory allocation in two functions
video: sh_mobile_meram: Delete an error message for a failed memory allocation in sh_mobile_meram_probe()
video: fbdev: sh_mobile_meram: Drop SUPERH platform dependency
...
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Since commit a521422ea4ae ("ARM: shmobile: mackerel: Remove Legacy C
board code") MERAM functionality is unused. Remove it.
Reviewed-by: Simon Horman <horms+renesas@verge.net.au>
Cc: Geert Uytterhoeven <geert+renesas@glider.be>
Acked-by: Laurent Pinchart <laurent.pinchart@ideasonboard.com>
Acked-by: Daniel Vetter <daniel@ffwll.ch>
Signed-off-by: Bartlomiej Zolnierkiewicz <b.zolnierkie@samsung.com>
|
|\ \ \
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
git://git.infradead.org/linux-platform-drivers-x86
Pull x86 platform driver updates from Darren Hart:
"Several incremental improvements including new keycodes, new models,
new quirks, and related documentation. Adds LED platform driver
activation for Mellanox systems. Some minor optimizations and
cleanups. Includes several bug fixes, message silencing, mostly minor
Automated summary:
acer-wmi:
- add another KEY_POWER keycode
apple-gmux:
- fix gmux_get_client_id()'s return type
asus-laptop:
- Simplify getting .drvdata
asus-wireless:
- Fix format specifier
dell-laptop:
- Fix keyboard backlight timeout on XPS 13 9370
dell-smbios:
- Match on www.dell.com in OEM strings too
dell-wmi:
- Ignore new rfkill and fn-lock events
- Set correct keycode for Fn + left arrow
fujitsu-laptop:
- Simplify soft key handling
ideapad-laptop:
- Add E42-80 to no_hw_rfkill
- Add fn-lock setting
- Add MIIX 720-12IKB to no_hw_rfkill
lib/string_helpers:
- Add missed declaration of struct task_struct
intel_scu_ipc:
- Replace mdelay with usleep_range in intel_scu_ipc_i2c_cntrl
mlx-platform:
- Add LED platform driver activation
platform/mellanox:
- Add new ODM system types to mlx-platform
- mlxreg-hotplug: add extra cycle for hotplug work queue
- mlxreg-hotplug: Document fixes for hotplug private data
platform_data/mlxreg:
- Document fixes for hotplug device
silead_dmi:
- Add entry for Chuwi Hi8 tablet touchscreen
- Add touchscreen info for the Onda V891w tablet
- Add info for the PoV mobii TAB-P800W (v2.0)
- Add touchscreen info for the Jumper EZpad 6 Pro
thinkpad_acpi:
- silence false-positive-prone pr_warn
- do not report thermal sensor state for tablet mode switch
- silence HKEY 0x6032, 0x60f0, 0x6030"
* tag 'platform-drivers-x86-v4.18-1' of git://git.infradead.org/linux-platform-drivers-x86: (30 commits)
platform/x86: silead_dmi: Add entry for Chuwi Hi8 tablet touchscreen
platform/x86: dell-laptop: Fix keyboard backlight timeout on XPS 13 9370
platform/x86: dell-wmi: Ignore new rfkill and fn-lock events
platform/x86: mlx-platform: Add LED platform driver activation
platform/mellanox: Add new ODM system types to mlx-platform
platform/mellanox: mlxreg-hotplug: add extra cycle for hotplug work queue
platform/x86: ideapad-laptop: Add E42-80 to no_hw_rfkill
platform/x86: silead_dmi: Add touchscreen info for the Onda V891w tablet
platform/x86: silead_dmi: Add info for the PoV mobii TAB-P800W (v2.0)
platform/x86: silead_dmi: Add touchscreen info for the Jumper EZpad 6 Pro
platform/x86: asus-wireless: Fix format specifier
platform/x86: asus-wmi: Fix NULL pointer dereference
platform/x86: dell-wmi: Set correct keycode for Fn + left arrow
platform/x86: acer-wmi: add another KEY_POWER keycode
platform/x86: ideapad-laptop: Add fn-lock setting
platform/x86: ideapad-laptop: Add MIIX 720-12IKB to no_hw_rfkill
lib/string_helpers: Add missed declaration of struct task_struct
platform/x86: DELL_WMI use depends on instead of select for DELL_SMBIOS
platform/mellanox: mlxreg-hotplug: Document fixes for hotplug private data
platform_data/mlxreg: Document fixes for hotplug device
...
|
| |/ /
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Remove redunadant description of label in struct mlxreg_hotplug_device.
Change location of access_mode in struct mlxreg_hotplug_device.
Signed-off-by: Vadim Pasternak <vadimp@mellanox.com>
Signed-off-by: Darren Hart (VMware) <dvhart@infradead.org>
|
|\ \ \
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/wsa/linux
Pull i2c updates from Wolfram Sang:
- mainly feature additions to drivers (stm32f7, qup, xlp9xx, mlxcpld, ...)
- conversion to use the i2c_8bit_addr_from_msg macro consistently
- move includes to platform_data
- core updates to allow the (still in review) I3C subsystem to connect
- and the regular share of smaller driver updates
* 'i2c/for-4.18' of git://git.kernel.org/pub/scm/linux/kernel/git/wsa/linux: (68 commits)
i2c: qup: fix building without CONFIG_ACPI
i2c: tegra: Remove suspend-resume
i2c: imx-lpi2c: Switch to SPDX identifier
i2c: mxs: Switch to SPDX identifier
i2c: busses: make use of i2c_8bit_addr_from_msg
i2c: algos: make use of i2c_8bit_addr_from_msg
i2c: rcar: document R8A77980 bindings
i2c: qup: Add command-line parameter to override SCL frequency
i2c: qup: Correct duty cycle for FM and FM+
i2c: qup: Add support for Fast Mode Plus
i2c: qup: add probe path for Centriq ACPI devices
i2c: robotfuzz-osif: drop pointless test
i2c: robotfuzz-osif: remove pointless local variable
i2c: rk3x: Don't print visible virtual mapping MMIO address
i2c: opal: don't check number of messages in the driver
i2c: ibm_iic: don't check number of messages in the driver
i2c: imx: Switch to SPDX identifier
i2c: mux: pca954x: merge calls to of_match_device and of_device_get_match_data
i2c: mux: demux-pinctrl: use proper parent device for demux adapter
i2c: mux: improve error message for failed symlink
...
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
This header only contains platform_data. Move it to the proper directory.
Signed-off-by: Wolfram Sang <wsa@the-dreams.de>
Acked-by: Lee Jones <lee.jones@linaro.org>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
This header only contains platform_data. Move it to the proper directory.
Signed-off-by: Wolfram Sang <wsa@the-dreams.de>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
This header only contains platform_data. Move it to the proper directory.
Signed-off-by: Wolfram Sang <wsa@the-dreams.de>
Acked-by: Tony Lindgren <tony@atomide.com>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
This header only contains platform_data. Move it to the proper directory.
Signed-off-by: Wolfram Sang <wsa@the-dreams.de>
Acked-by: Lee Jones <lee.jones@linaro.org>
|