/* SPDX-License-Identifier: GPL-2.0 */ /* * Filesystem access notification for Linux * * Copyright (C) 2008 Red Hat, Inc., Eric Paris */ #ifndef __LINUX_FSNOTIFY_BACKEND_H #define __LINUX_FSNOTIFY_BACKEND_H #ifdef __KERNEL__ #include /* inotify uses this */ #include /* struct inode */ #include #include /* struct path */ #include #include #include #include #include /* * IN_* from inotfy.h lines up EXACTLY with FS_*, this is so we can easily * convert between them. dnotify only needs conversion at watch creation * so no perf loss there. fanotify isn't defined yet, so it can use the * wholes if it needs more events. */ #define FS_ACCESS 0x00000001 /* File was accessed */ #define FS_MODIFY 0x00000002 /* File was modified */ #define FS_ATTRIB 0x00000004 /* Metadata changed */ #define FS_CLOSE_WRITE 0x00000008 /* Writtable file was closed */ #define FS_CLOSE_NOWRITE 0x00000010 /* Unwrittable file closed */ #define FS_OPEN 0x00000020 /* File was opened */ #define FS_MOVED_FROM 0x00000040 /* File was moved from X */ #define FS_MOVED_TO 0x00000080 /* File was moved to Y */ #define FS_CREATE 0x00000100 /* Subfile was created */ #define FS_DELETE 0x00000200 /* Subfile was deleted */ #define FS_DELETE_SELF 0x00000400 /* Self was deleted */ #define FS_MOVE_SELF 0x00000800 /* Self was moved */ #define FS_UNMOUNT 0x00002000 /* inode on umount fs */ #define FS_Q_OVERFLOW 0x00004000 /* Event queued overflowed */ #define FS_IN_IGNORED 0x00008000 /* last inotify event here */ #define FS_OPEN_PERM 0x00010000 /* open event in an permission hook */ #define FS_ACCESS_PERM 0x00020000 /* access event in a permissions hook */ #define FS_EXCL_UNLINK 0x04000000 /* do not send events if object is unlinked */ #define FS_ISDIR 0x40000000 /* event occurred against dir */ #define FS_IN_ONESHOT 0x80000000 /* only send event once */ #define FS_DN_RENAME 0x10000000 /* file renamed */ #define FS_DN_MULTISHOT 0x20000000 /* dnotify multishot */ /* This inode cares about things that happen to its children. Always set for * dnotify and inotify. */ #define FS_EVENT_ON_CHILD 0x08000000 /* This is a list of all events that may get sent to a parernt based on fs event * happening to inodes inside that directory */ #define FS_EVENTS_POSS_ON_CHILD (FS_ACCESS | FS_MODIFY | FS_ATTRIB |\ FS_CLOSE_WRITE | FS_CLOSE_NOWRITE | FS_OPEN |\ FS_MOVED_FROM | FS_MOVED_TO | FS_CREATE |\ FS_DELETE | FS_OPEN_PERM | FS_ACCESS_PERM) #define FS_MOVE (FS_MOVED_FROM | FS_MOVED_TO) #define ALL_FSNOTIFY_PERM_EVENTS (FS_OPEN_PERM | FS_ACCESS_PERM) #define ALL_FSNOTIFY_EVENTS (FS_ACCESS | FS_MODIFY | FS_ATTRIB | \ FS_CLOSE_WRITE | FS_CLOSE_NOWRITE | FS_OPEN | \ FS_MOVED_FROM | FS_MOVED_TO | FS_CREATE | \ FS_DELETE | FS_DELETE_SELF | FS_MOVE_SELF | \ FS_UNMOUNT | FS_Q_OVERFLOW | FS_IN_IGNORED | \ FS_OPEN_PERM | FS_ACCESS_PERM | FS_EXCL_UNLINK | \ FS_ISDIR | FS_IN_ONESHOT | FS_DN_RENAME | \ FS_DN_MULTISHOT | FS_EVENT_ON_CHILD) struct fsnotify_group; struct fsnotify_event; struct fsnotify_mark; struct fsnotify_event_private_data; struct fsnotify_fname; struct fsnotify_iter_info; struct mem_cgroup; /* * Each group much define these ops. The fsnotify infrastructure will call * these operations for each relevant group. * * handle_event - main call for a group to handle an fs event * free_group_priv - called when a group refcnt hits 0 to clean up the private union * freeing_mark - called when a mark is being destroyed for some reason. The group * MUST be holding a reference on each mark and that reference must be * dropped in this function. inotify uses this function to send * userspace messages that marks have been removed. */ struct fsnotify_ops { int (*handle_event)(struct fsnotify_group *group, struct inode *inode, u32 mask, const void *data, int data_type, const unsigned char *file_name, u32 cookie, struct fsnotify_iter_info *iter_info); void (*free_group_priv)(struct fsnotify_group *group); void (*freeing_mark)(struct fsnotify_mark *mark, struct fsnotify_group *group); void (*free_event)(struct fsnotify_event *event); /* called on final put+free to free memory */ void (*free_mark)(struct fsnotify_mark *mark); }; /* * all of the information about the original object we want to now send to * a group. If you want to carry more info from the accessing task to the * listener this structure is where you need to be adding fields. */ struct fsnotify_event { struct list_head list; /* inode may ONLY be dereferenced during handle_event(). */ struct inode *inode; /* either the inode the event happened to or its parent */ u32 mask; /* the type of access, bitwise OR for FS_* event types */ }; /* * A group is a "thing" that wants to receive notification about filesystem * events. The mask holds the subset of event types this group cares about. * refcnt on a group is up to the implementor and at any moment if it goes 0 * everything will be cleaned up. */ struct fsnotify_group { const struct fsnotify_ops *ops; /* how this group handles things */ /* * How the refcnt is used is up to each group. When the refcnt hits 0 * fsnotify will clean up all of the resources associated with this group. * As an example, the dnotify group will always have a refcnt=1 and that * will never change. Inotify, on the other hand, has a group per * inotify_init() and the refcnt will hit 0 only when that fd has been * closed. */ refcount_t refcnt; /* things with interest in this group */ /* needed to send notification to userspace */ spinlock_t notification_lock; /* protect the notification_list */ struct list_head notification_list; /* list of event_holder this group needs to send to userspace */ wait_queue_head_t notification_waitq; /* read() on the notification file blocks on this waitq */ unsigned int q_len; /* events on the queue */ unsigned int max_events; /* maximum events allowed on the list */ /* * Valid fsnotify group priorities. Events are send in order from highest * priority to lowest priority. We default to the lowest priority. */ #define FS_PRIO_0 0 /* normal notifiers, no permissions */ #define FS_PRIO_1 1 /* fanotify content based access control */ #define FS_PRIO_2 2 /* fanotify pre-content access */ unsigned int priority; bool shutdown; /* group is being shut down, don't queue more events */ /* stores all fastpath marks assoc with this group so they can be cleaned on unregister */ struct mutex mark_mutex; /* protect marks_list */ atomic_t num_marks; /* 1 for each mark and 1 for not being * past the point of no return when freeing * a group */ atomic_t user_waits; /* Number of tasks waiting for user * response */ struct list_head marks_list; /* all inode marks for this group */ struct fasync_struct *fsn_fa; /* async notification */ struct fsnotify_event *overflow_event; /* Event we queue when the * notification list is too * full */ struct mem_cgroup *memcg; /* memcg to charge allocations */ /* groups can define private fields here or use the void *private */ union { void *private; #ifdef CONFIG_INOTIFY_USER struct inotify_group_private_data { spinlock_t idr_lock; struct idr idr; struct ucounts *ucounts; } inotify_data; #endif #ifdef CONFIG_FANOTIFY struct fanotify_group_private_data { /* allows a group to block waiting for a userspace response */ struct list_head access_list; wait_queue_head_t access_waitq; int f_flags; unsigned int max_marks; struct user_struct *user; bool audit; } fanotify_data; #endif /* CONFIG_FANOTIFY */ }; }; /* when calling fsnotify tell it if the data is a path or inode */ #define FSNOTIFY_EVENT_NONE 0 #define FSNOTIFY_EVENT_PATH 1 #define FSNOTIFY_EVENT_INODE 2 enum fsnotify_obj_type { FSNOTIFY_OBJ_TYPE_INODE, FSNOTIFY_OBJ_TYPE_VFSMOUNT, FSNOTIFY_OBJ_TYPE_COUNT, FSNOTIFY_OBJ_TYPE_DETACHED = FSNOTIFY_OBJ_TYPE_COUNT }; #define FSNOTIFY_OBJ_TYPE_INODE_FL (1U << FSNOTIFY_OBJ_TYPE_INODE) #define FSNOTIFY_OBJ_TYPE_VFSMOUNT_FL (1U << FSNOTIFY_OBJ_TYPE_VFSMOUNT) #define FSNOTIFY_OBJ_ALL_TYPES_MASK ((1U << FSNOTIFY_OBJ_TYPE_COUNT) - 1) static inline bool fsnotify_valid_obj_type(unsigned int type) { return (type < FSNOTIFY_OBJ_TYPE_COUNT); } struct fsnotify_iter_info { struct fsnotify_mark *marks[FSNOTIFY_OBJ_TYPE_COUNT]; unsigned int report_mask; int srcu_idx; }; static inline bool fsnotify_iter_should_report_type( struct fsnotify_iter_info *iter_info, int type) { return (iter_info->report_mask & (1U << type)); } static inline void fsnotify_iter_set_report_type( struct fsnotify_iter_info *iter_info, int type) { iter_info->report_mask |= (1U << type); } static inline void fsnotify_iter_set_report_type_mark( struct fsnotify_iter_info *iter_info, int type, struct fsnotify_mark *mark) { iter_info->marks[type] = mark; iter_info->report_mask |= (1U << type); } #define FSNOTIFY_ITER_FUNCS(name, NAME) \ static inline struct fsnotify_mark *fsnotify_iter_##name##_mark( \ struct fsnotify_iter_info *iter_info) \ { \ return (iter_info->report_mask & FSNOTIFY_OBJ_TYPE_##NAME##_FL) ? \ iter_info->marks[FSNOTIFY_OBJ_TYPE_##NAME] : NULL; \ } FSNOTIFY_ITER_FUNCS(inode, INODE) FSNOTIFY_ITER_FUNCS(vfsmount, VFSMOUNT) #define fsnotify_foreach_obj_type(type) \ for (type = 0; type < FSNOTIFY_OBJ_TYPE_COUNT; type++) /* * fsnotify_connp_t is what we embed in objects which connector can be attached * to. fsnotify_connp_t * is how we refer from connector back to object. */ struct fsnotify_mark_connector; typedef struct fsnotify_mark_connector __rcu *fsnotify_connp_t; /* * Inode / vfsmount point to this structure which tracks all marks attached to * the inode / vfsmount. The reference to inode / vfsmount is held by this * structure. We destroy this structure when there are no more marks attached * to it. The structure is protected by fsnotify_mark_srcu. */ struct fsnotify_mark_connector { spinlock_t lock; unsigned int type; /* Type of object [lock] */ union { /* Object pointer [lock] */ fsnotify_connp_t *obj; /* Used listing heads to free after srcu period expires */ struct fsnotify_mark_connector *destroy_next; }; struct hlist_head list; }; /* * A mark is simply an object attached to an in core inode which allows an * fsnotify listener to indicate they are either no longer interested in events * of a type matching mask or only interested in those events. * * These are flushed when an inode is evicted from core and may be flushed * when the inode is modified (as seen by fsnotify_access). Some fsnotify * users (such as dnotify) will flush these when the open fd is closed and not * at inode eviction or modification. * * Text in brackets is showing the lock(s) protecting modifications of a * particular entry. obj_lock means either inode->i_lock or * mnt->mnt_root->d_lock depending on the mark type. */ struct fsnotify_mark { /* Mask this mark is for [mark->lock, group->mark_mutex] */ __u32 mask; /* We hold one for presence in g_list. Also one ref for each 'thing' * in kernel that found and may be using this mark. */ refcount_t refcnt; /* Group this mark is for. Set on mark creation, stable until last ref * is dropped */ struct fsnotify_group *group; /* List of marks by group->marks_list. Also reused for queueing * mark into destroy_list when it's waiting for the end of SRCU period * before it can be freed. [group->mark_mutex] */ struct list_head g_list; /* Protects inode / mnt pointers, flags, masks */ spinlock_t lock; /* List of marks for inode / vfsmount [connector->lock, mark ref] */ struct hlist_node obj_list; /* Head of list of marks for an object [mark ref] */ struct fsnotify_mark_connector *connector; /* Events types to ignore [mark->lock, group->mark_mutex] */ __u32 ignored_mask; #define FSNOTIFY_MARK_FLAG_IGNORED_SURV_MODIFY 0x01 #define FSNOTIFY_MARK_FLAG_ALIVE 0x02 #define FSNOTIFY_MARK_FLAG_ATTACHED 0x04 unsigned int flags; /* flags [mark->lock] */ }; #ifdef CONFIG_FSNOTIFY /* called from the vfs helpers */ /* main fsnotify call to send events */ extern int fsnotify(struct inode *to_tell, __u32 mask, const void *data, int data_is, const unsigned char *name, u32 cookie); extern int __fsnotify_parent(const struct path *path, struct dentry *dentry, __u32 mask); extern void __fsnotify_inode_delete(struct inode *inode); extern void __fsnotify_vfsmount_delete(struct vfsmount *mnt); extern u32 fsnotify_get_cookie(void); static inline int fsnotify_inode_watches_children(struct inode *inode) { /* FS_EVENT_ON_CHILD is set if the inode may care */ if (!(inode->i_fsnotify_mask & FS_EVENT_ON_CHILD)) return 0; /* this inode might care about child events, does it care about the * specific set of events that can happen on a child? */ return inode->i_fsnotify_mask & FS_EVENTS_POSS_ON_CHILD; } /* * Update the dentry with a flag indicating the interest of its parent to receive * filesystem events when those events happens to this dentry->d_inode. */ static inline void fsnotify_update_flags(struct dentry *dentry) { assert_spin_locked(&dentry->d_lock); /* * Serialisation of setting PARENT_WATCHED on the dentries is provided * by d_lock. If inotify_inode_watched changes after we have taken * d_lock, the following __fsnotify_update_child_dentry_flags call will * find our entry, so it will spin until we complete here, and update * us with the new state. */ if (fsnotify_inode_watches_children(dentry->d_parent->d_inode)) dentry->d_flags |= DCACHE_FSNOTIFY_PARENT_WATCHED; else dentry->d_flags &= ~DCACHE_FSNOTIFY_PARENT_WATCHED; } /* called from fsnotify listeners, such as fanotify or dnotify */ /* create a new group */ extern struct fsnotify_group *fsnotify_alloc_group(const struct fsnotify_ops *ops); /* get reference to a group */ extern void fsnotify_get_group(struct fsnotify_group *group); /* drop reference on a group from fsnotify_alloc_group */ extern void fsnotify_put_group(struct fsnotify_group *group); /* group destruction begins, stop queuing new events */ extern void fsnotify_group_stop_queueing(struct fsnotify_group *group); /* destroy group */ extern void fsnotify_destroy_group(struct fsnotify_group *group); /* fasync handler function */ extern int fsnotify_fasync(int fd, struct file *file, int on); /* Free event from memory */ extern void fsnotify_destroy_event(struct fsnotify_group *group, struct fsnotify_event *event); /* attach the event to the group notification queue */ extern int fsnotify_add_event(struct fsnotify_group *group, struct fsnotify_event *event, int (*merge)(struct list_head *, struct fsnotify_event *)); /* Queue overflow event to a notification group */ static inline void fsnotify_queue_overflow(struct fsnotify_group *group) { fsnotify_add_event(group, group->overflow_event, NULL); } /* true if the group notification queue is empty */ extern bool fsnotify_notify_queue_is_empty(struct fsnotify_group *group); /* return, but do not dequeue the first event on the notification queue */ extern struct fsnotify_event *fsnotify_peek_first_event(struct fsnotify_group *group); /* return AND dequeue the first event on the notification queue */ extern struct fsnotify_event *fsnotify_remove_first_event(struct fsnotify_group *group); /* functions used to manipulate the marks attached to inodes */ /* Get mask of events for a list of marks */ extern __u32 fsnotify_conn_mask(struct fsnotify_mark_connector *conn); /* Calculate mask of events for a list of marks */ extern void fsnotify_recalc_mask(struct fsnotify_mark_connector *conn); extern void fsnotify_init_mark(struct fsnotify_mark *mark, struct fsnotify_group *group); /* Find mark belonging to given group in the list of marks */ extern struct fsnotify_mark *fsnotify_find_mark(fsnotify_connp_t *connp, struct fsnotify_group *group); /* attach the mark to the object */ extern int fsnotify_add_mark(struct fsnotify_mark *mark, fsnotify_connp_t *connp, unsigned int type, int allow_dups); extern int fsnotify_add_mark_locked(struct fsnotify_mark *mark, fsnotify_connp_t *connp, unsigned int type, int allow_dups); /* attach the mark to the inode */ static inline int fsnotify_add_inode_mark(struct fsnotify_mark *mark, struct inode *inode, int allow_dups) { return fsnotify_add_mark(mark, &inode->i_fsnotify_marks, FSNOTIFY_OBJ_TYPE_INODE, allow_dups); } static inline int fsnotify_add_inode_mark_locked(struct fsnotify_mark *mark, struct inode *inode, int allow_dups) { return fsnotify_add_mark_locked(mark, &inode->i_fsnotify_marks, FSNOTIFY_OBJ_TYPE_INODE, allow_dups); } /* given a group and a mark, flag mark to be freed when all references are dropped */ extern void fsnotify_destroy_mark(struct fsnotify_mark *mark, struct fsnotify_group *group); /* detach mark from inode / mount list, group list, drop inode reference */ extern void fsnotify_detach_mark(struct fsnotify_mark *mark); /* free mark */ extern void fsnotify_free_mark(struct fsnotify_mark *mark); /* run all the marks in a group, and clear all of the marks attached to given object type */ extern void fsnotify_clear_marks_by_group(struct fsnotify_group *group, unsigned int type); /* run all the marks in a group, and clear all of the vfsmount marks */ static inline void fsnotify_clear_vfsmount_marks_by_group(struct fsnotify_group *group) { fsnotify_clear_marks_by_group(group, FSNOTIFY_OBJ_TYPE_VFSMOUNT_FL); } /* run all the marks in a group, and clear all of the inode marks */ static inline void fsnotify_clear_inode_marks_by_group(struct fsnotify_group *group) { fsnotify_clear_marks_by_group(group, FSNOTIFY_OBJ_TYPE_INODE_FL); } extern void fsnotify_get_mark(struct fsnotify_mark *mark); extern void fsnotify_put_mark(struct fsnotify_mark *mark); extern void fsnotify_unmount_inodes(struct super_block *sb); extern void fsnotify_finish_user_wait(struct fsnotify_iter_info *iter_info); extern bool fsnotify_prepare_user_wait(struct fsnotify_iter_info *iter_info); /* put here because inotify does some weird stuff when destroying watches */ extern void fsnotify_init_event(struct fsnotify_event *event, struct inode *to_tell, u32 mask); #else static inline int fsnotify(struct inode *to_tell, __u32 mask, const void *data, int data_is, const unsigned char *name, u32 cookie) { return 0; } static inline int __fsnotify_parent(const struct path *path, struct dentry *dentry, __u32 mask) { return 0; } static inline void __fsnotify_inode_delete(struct inode *inode) {} static inline void __fsnotify_vfsmount_delete(struct vfsmount *mnt) {} static inline void fsnotify_update_flags(struct dentry *dentry) {} static inline u32 fsnotify_get_cookie(void) { return 0; } static inline void fsnotify_unmount_inodes(struct super_block *sb) {} #endif /* CONFIG_FSNOTIFY */ #endif /* __KERNEL __ */ #endif /* __LINUX_FSNOTIFY_BACKEND_H */