/* Definitions for key type implementations * * Copyright (C) 2007 Red Hat, Inc. All Rights Reserved. * Written by David Howells (dhowells@redhat.com) * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public Licence * as published by the Free Software Foundation; either version * 2 of the Licence, or (at your option) any later version. */ #ifndef _LINUX_KEY_TYPE_H #define _LINUX_KEY_TYPE_H #include #include #ifdef CONFIG_KEYS /* * key under-construction record * - passed to the request_key actor if supplied */ struct key_construction { struct key *key; /* key being constructed */ struct key *authkey;/* authorisation for key being constructed */ }; /* * Pre-parsed payload, used by key add, update and instantiate. * * This struct will be cleared and data and datalen will be set with the data * and length parameters from the caller and quotalen will be set from * def_datalen from the key type. Then if the preparse() op is provided by the * key type, that will be called. Then the struct will be passed to the * instantiate() or the update() op. * * If the preparse() op is given, the free_preparse() op will be called to * clear the contents. */ struct key_preparsed_payload { char *description; /* Proposed key description (or NULL) */ union key_payload payload; /* Proposed payload */ const void *data; /* Raw data */ size_t datalen; /* Raw datalen */ size_t quotalen; /* Quota length for proposed payload */ time64_t expiry; /* Expiry time of key */ } __randomize_layout; typedef int (*request_key_actor_t)(struct key_construction *key, const char *op, void *aux); /* * Preparsed matching criterion. */ struct key_match_data { /* Comparison function, defaults to exact description match, but can be * overridden by type->match_preparse(). Should return true if a match * is found and false if not. */ bool (*cmp)(const struct key *key, const struct key_match_data *match_data); const void *raw_data; /* Raw match data */ void *preparsed; /* For ->match_preparse() to stash stuff */ unsigned lookup_type; /* Type of lookup for this search. */ #define KEYRING_SEARCH_LOOKUP_DIRECT 0x0000 /* Direct lookup by description. */ #define KEYRING_SEARCH_LOOKUP_ITERATE 0x0001 /* Iterative search. */ }; /* * kernel managed key type definition */ struct key_type { /* name of the type */ const char *name; /* default payload length for quota precalculation (optional) * - this can be used instead of calling key_payload_reserve(), that * function only needs to be called if the real datalen is different */ size_t def_datalen; /* vet a description */ int (*vet_description)(const char *description); /* Preparse the data blob from userspace that is to be the payload, * generating a proposed description and payload that will be handed to * the instantiate() and update() ops. */ int (*preparse)(struct key_preparsed_payload *prep); /* Free a preparse data structure. */ void (*free_preparse)(struct key_preparsed_payload *prep); /* instantiate a key of this type * - this method should call key_payload_reserve() to determine if the * user's quota will hold the payload */ int (*instantiate)(struct key *key, struct key_preparsed_payload *prep); /* update a key of this type (optional) * - this method should call key_payload_reserve() to recalculate the * quota consumption * - the key must be locked against read when modifying */ int (*update)(struct key *key, struct key_preparsed_payload *prep); /* Preparse the data supplied to ->match() (optional). The * data to be preparsed can be found in match_data->raw_data. * The lookup type can also be set by this function. */ int (*match_preparse)(struct key_match_data *match_data); /* Free preparsed match data (optional). This should be supplied it * ->match_preparse() is supplied. */ void (*match_free)(struct key_match_data *match_data); /* clear some of the data from a key on revokation (optional) * - the key's semaphore will be write-locked by the caller */ void (*revoke)(struct key *key); /* clear the data from a key (optional) */ void (*destroy)(struct key *key); /* describe a key */ void (*describe)(const struct key *key, struct seq_file *p); /* read a key's data (optional) * - permission checks will be done by the caller * - the key's semaphore will be readlocked by the caller * - should return the amount of data that could be read, no matter how * much is copied into the buffer * - shouldn't do the copy if the buffer is NULL */ long (*read)(const struct key *key, char __user *buffer, size_t buflen); /* handle request_key() for this type instead of invoking * /sbin/request-key (optional) * - key is the key to instantiate * - authkey is the authority to assume when instantiating this key * - op is the operation to be done, usually "create" * - the call must not return until the instantiation process has run * its course */ request_key_actor_t request_key; /* Look up a keyring access restriction (optional) * * - NULL is a valid return value (meaning the requested restriction * is known but will never block addition of a key) * - should return -EINVAL if the restriction is unknown */ struct key_restriction *(*lookup_restriction)(const char *params); /* internal fields */ struct list_head link; /* link in types list */ struct lock_class_key lock_class; /* key->sem lock class */ } __randomize_layout; extern struct key_type key_type_keyring; extern int register_key_type(struct key_type *ktype); extern void unregister_key_type(struct key_type *ktype); extern int key_payload_reserve(struct key *key, size_t datalen); extern int key_instantiate_and_link(struct key *key, const void *data, size_t datalen, struct key *keyring, struct key *instkey); extern int key_reject_and_link(struct key *key, unsigned timeout, unsigned error, struct key *keyring, struct key *instkey); extern void complete_request_key(struct key_construction *cons, int error); static inline int key_negate_and_link(struct key *key, unsigned timeout, struct key *keyring, struct key *instkey) { return key_reject_and_link(key, timeout, ENOKEY, keyring, instkey); } extern int generic_key_instantiate(struct key *key, struct key_preparsed_payload *prep); #endif /* CONFIG_KEYS */ #endif /* _LINUX_KEY_TYPE_H */