/* * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301, USA. * */ #ifndef __KVM_TYPES_H__ #define __KVM_TYPES_H__ struct kvm; struct kvm_async_pf; struct kvm_device_ops; struct kvm_interrupt; struct kvm_irq_routing_table; struct kvm_memory_slot; struct kvm_one_reg; struct kvm_run; struct kvm_userspace_memory_region; struct kvm_vcpu; struct kvm_vcpu_init; struct kvm_memslots; enum kvm_mr_change; #include /* * Address types: * * gva - guest virtual address * gpa - guest physical address * gfn - guest frame number * hva - host virtual address * hpa - host physical address * hfn - host frame number */ typedef unsigned long gva_t; typedef u64 gpa_t; typedef u64 gfn_t; typedef unsigned long hva_t; typedef u64 hpa_t; typedef u64 hfn_t; typedef hfn_t kvm_pfn_t; struct gfn_to_hva_cache { u64 generation; gpa_t gpa; unsigned long hva; unsigned long len; struct kvm_memory_slot *memslot; }; #endif /* __KVM_TYPES_H__ */