/* * Driver model for leds and led triggers * * Copyright (C) 2005 John Lenz * Copyright (C) 2005 Richard Purdie * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * */ #ifndef __LINUX_LEDS_H_INCLUDED #define __LINUX_LEDS_H_INCLUDED #include #include #include #include #include #include #include #include struct device; /* * LED Core */ enum led_brightness { LED_OFF = 0, LED_ON = 1, LED_HALF = 127, LED_FULL = 255, }; struct led_classdev { const char *name; enum led_brightness brightness; enum led_brightness max_brightness; int flags; /* Lower 16 bits reflect status */ #define LED_SUSPENDED BIT(0) #define LED_UNREGISTERING BIT(1) /* Upper 16 bits reflect control information */ #define LED_CORE_SUSPENDRESUME BIT(16) #define LED_SYSFS_DISABLE BIT(17) #define LED_DEV_CAP_FLASH BIT(18) #define LED_HW_PLUGGABLE BIT(19) #define LED_PANIC_INDICATOR BIT(20) #define LED_BRIGHT_HW_CHANGED BIT(21) #define LED_RETAIN_AT_SHUTDOWN BIT(22) /* set_brightness_work / blink_timer flags, atomic, private. */ unsigned long work_flags; #define LED_BLINK_SW 0 #define LED_BLINK_ONESHOT 1 #define LED_BLINK_ONESHOT_STOP 2 #define LED_BLINK_INVERT 3 #define LED_BLINK_BRIGHTNESS_CHANGE 4 #define LED_BLINK_DISABLE 5 /* Set LED brightness level * Must not sleep. Use brightness_set_blocking for drivers * that can sleep while setting brightness. */ void (*brightness_set)(struct led_classdev *led_cdev, enum led_brightness brightness); /* * Set LED brightness level immediately - it can block the caller for * the time required for accessing a LED device register. */ int (*brightness_set_blocking)(struct led_classdev *led_cdev, enum led_brightness brightness); /* Get LED brightness level */ enum led_brightness (*brightness_get)(struct led_classdev *led_cdev); /* * Activate hardware accelerated blink, delays are in milliseconds * and if both are zero then a sensible default should be chosen. * The call should adjust the timings in that case and if it can't * match the values specified exactly. * Deactivate blinking again when the brightness is set to LED_OFF * via the brightness_set() callback. */ int (*blink_set)(struct led_classdev *led_cdev, unsigned long *delay_on, unsigned long *delay_off); struct device *dev; const struct attribute_group **groups; struct list_head node; /* LED Device list */ const char *default_trigger; /* Trigger to use */ unsigned long blink_delay_on, blink_delay_off; struct timer_list blink_timer; int blink_brightness; int new_blink_brightness; void (*flash_resume)(struct led_classdev *led_cdev); struct work_struct set_brightness_work; int delayed_set_value; #ifdef CONFIG_LEDS_TRIGGERS /* Protects the trigger data below */ struct rw_semaphore trigger_lock; struct led_trigger *trigger; struct list_head trig_list; void *trigger_data; /* true if activated - deactivate routine uses it to do cleanup */ bool activated; #endif #ifdef CONFIG_LEDS_BRIGHTNESS_HW_CHANGED int brightness_hw_changed; struct kernfs_node *brightness_hw_changed_kn; #endif /* Ensures consistent access to the LED Flash Class device */ struct mutex led_access; }; extern int of_led_classdev_register(struct device *parent, struct device_node *np, struct led_classdev *led_cdev); #define led_classdev_register(parent, led_cdev) \ of_led_classdev_register(parent, NULL, led_cdev) extern int devm_of_led_classdev_register(struct device *parent, struct device_node *np, struct led_classdev *led_cdev); #define devm_led_classdev_register(parent, led_cdev) \ devm_of_led_classdev_register(parent, NULL, led_cdev) extern void led_classdev_unregister(struct led_classdev *led_cdev); extern void devm_led_classdev_unregister(struct device *parent, struct led_classdev *led_cdev); extern void led_classdev_suspend(struct led_classdev *led_cdev); extern void led_classdev_resume(struct led_classdev *led_cdev); /** * led_blink_set - set blinking with software fallback * @led_cdev: the LED to start blinking * @delay_on: the time it should be on (in ms) * @delay_off: the time it should ble off (in ms) * * This function makes the LED blink, attempting to use the * hardware acceleration if possible, but falling back to * software blinking if there is no hardware blinking or if * the LED refuses the passed values. * * Note that if software blinking is active, simply calling * led_cdev->brightness_set() will not stop the blinking, * use led_classdev_brightness_set() instead. */ extern void led_blink_set(struct led_classdev *led_cdev, unsigned long *delay_on, unsigned long *delay_off); /** * led_blink_set_oneshot - do a oneshot software blink * @led_cdev: the LED to start blinking * @delay_on: the time it should be on (in ms) * @delay_off: the time it should ble off (in ms) * @invert: blink off, then on, leaving the led on * * This function makes the LED blink one time for delay_on + * delay_off time, ignoring the request if another one-shot * blink is already in progress. * * If invert is set, led blinks for delay_off first, then for * delay_on and leave the led on after the on-off cycle. */ extern void led_blink_set_oneshot(struct led_classdev *led_cdev, unsigned long *delay_on, unsigned long *delay_off, int invert); /** * led_set_brightness - set LED brightness * @led_cdev: the LED to set * @brightness: the brightness to set it to * * Set an LED's brightness, and, if necessary, cancel the * software blink timer that implements blinking when the * hardware doesn't. This function is guaranteed not to sleep. */ extern void led_set_brightness(struct led_classdev *led_cdev, enum led_brightness brightness); /** * led_set_brightness_sync - set LED brightness synchronously * @led_cdev: the LED to set * @brightness: the brightness to set it to * * Set an LED's brightness immediately. This function will block * the caller for the time required for accessing device registers, * and it can sleep. * * Returns: 0 on success or negative error value on failure */ extern int led_set_brightness_sync(struct led_classdev *led_cdev, enum led_brightness value); /** * led_update_brightness - update LED brightness * @led_cdev: the LED to query * * Get an LED's current brightness and update led_cdev->brightness * member with the obtained value. * * Returns: 0 on success or negative error value on failure */ extern int led_update_brightness(struct led_classdev *led_cdev); /** * led_sysfs_disable - disable LED sysfs interface * @led_cdev: the LED to set * * Disable the led_cdev's sysfs interface. */ extern void led_sysfs_disable(struct led_classdev *led_cdev); /** * led_sysfs_enable - enable LED sysfs interface * @led_cdev: the LED to set * * Enable the led_cdev's sysfs interface. */ extern void led_sysfs_enable(struct led_classdev *led_cdev); /** * led_sysfs_is_disabled - check if LED sysfs interface is disabled * @led_cdev: the LED to query * * Returns: true if the led_cdev's sysfs interface is disabled. */ static inline bool led_sysfs_is_disabled(struct led_classdev *led_cdev) { return led_cdev->flags & LED_SYSFS_DISABLE; } /* * LED Triggers */ /* Registration functions for simple triggers */ #define DEFINE_LED_TRIGGER(x) static struct led_trigger *x; #define DEFINE_LED_TRIGGER_GLOBAL(x) struct led_trigger *x; #ifdef CONFIG_LEDS_TRIGGERS #define TRIG_NAME_MAX 50 struct led_trigger { /* Trigger Properties */ const char *name; int (*activate)(struct led_classdev *led_cdev); void (*deactivate)(struct led_classdev *led_cdev); /* LEDs under control by this trigger (for simple triggers) */ rwlock_t leddev_list_lock; struct list_head led_cdevs; /* Link to next registered trigger */ struct list_head next_trig; const struct attribute_group **groups; }; /* * Currently the attributes in struct led_trigger::groups are added directly to * the LED device. As this might change in the future, the following * macros abstract getting the LED device and its trigger_data from the dev * parameter passed to the attribute accessor functions. */ #define led_trigger_get_led(dev) ((struct led_classdev *)dev_get_drvdata((dev))) #define led_trigger_get_drvdata(dev) (led_get_trigger_data(led_trigger_get_led(dev))) ssize_t led_trigger_store(struct device *dev, struct device_attribute *attr, const char *buf, size_t count); ssize_t led_trigger_show(struct device *dev, struct device_attribute *attr, char *buf); /* Registration functions for complex triggers */ extern int led_trigger_register(struct led_trigger *trigger); extern void led_trigger_unregister(struct led_trigger *trigger); extern int devm_led_trigger_register(struct device *dev, struct led_trigger *trigger); extern void led_trigger_register_simple(const char *name, struct led_trigger **trigger); extern void led_trigger_unregister_simple(struct led_trigger *trigger); extern void led_trigger_event(struct led_trigger *trigger, enum led_brightness event); extern void led_trigger_blink(struct led_trigger *trigger, unsigned long *delay_on, unsigned long *delay_off); extern void led_trigger_blink_oneshot(struct led_trigger *trigger, unsigned long *delay_on, unsigned long *delay_off, int invert); extern void led_trigger_set_default(struct led_classdev *led_cdev); extern int led_trigger_set(struct led_classdev *led_cdev, struct led_trigger *trigger); extern void led_trigger_remove(struct led_classdev *led_cdev); static inline void led_set_trigger_data(struct led_classdev *led_cdev, void *trigger_data) { led_cdev->trigger_data = trigger_data; } static inline void *led_get_trigger_data(struct led_classdev *led_cdev) { return led_cdev->trigger_data; } /** * led_trigger_rename_static - rename a trigger * @name: the new trigger name * @trig: the LED trigger to rename * * Change a LED trigger name by copying the string passed in * name into current trigger name, which MUST be large * enough for the new string. * * Note that name must NOT point to the same string used * during LED registration, as that could lead to races. * * This is meant to be used on triggers with statically * allocated name. */ extern void led_trigger_rename_static(const char *name, struct led_trigger *trig); #define module_led_trigger(__led_trigger) \ module_driver(__led_trigger, led_trigger_register, \ led_trigger_unregister) #else /* Trigger has no members */ struct led_trigger {}; /* Trigger inline empty functions */ static inline void led_trigger_register_simple(const char *name, struct led_trigger **trigger) {} static inline void led_trigger_unregister_simple(struct led_trigger *trigger) {} static inline void led_trigger_event(struct led_trigger *trigger, enum led_brightness event) {} static inline void led_trigger_blink(struct led_trigger *trigger, unsigned long *delay_on, unsigned long *delay_off) {} static inline void led_trigger_blink_oneshot(struct led_trigger *trigger, unsigned long *delay_on, unsigned long *delay_off, int invert) {} static inline void led_trigger_set_default(struct led_classdev *led_cdev) {} static inline int led_trigger_set(struct led_classdev *led_cdev, struct led_trigger *trigger) { return 0; } static inline void led_trigger_remove(struct led_classdev *led_cdev) {} static inline void led_set_trigger_data(struct led_classdev *led_cdev) {} static inline void *led_get_trigger_data(struct led_classdev *led_cdev) { return NULL; } #endif /* CONFIG_LEDS_TRIGGERS */ /* Trigger specific functions */ #ifdef CONFIG_LEDS_TRIGGER_DISK extern void ledtrig_disk_activity(bool write); #else static inline void ledtrig_disk_activity(bool write) {} #endif #ifdef CONFIG_LEDS_TRIGGER_MTD extern void ledtrig_mtd_activity(void); #else static inline void ledtrig_mtd_activity(void) {} #endif #if defined(CONFIG_LEDS_TRIGGER_CAMERA) || defined(CONFIG_LEDS_TRIGGER_CAMERA_MODULE) extern void ledtrig_flash_ctrl(bool on); extern void ledtrig_torch_ctrl(bool on); #else static inline void ledtrig_flash_ctrl(bool on) {} static inline void ledtrig_torch_ctrl(bool on) {} #endif /* * Generic LED platform data for describing LED names and default triggers. */ struct led_info { const char *name; const char *default_trigger; int flags; }; struct led_platform_data { int num_leds; struct led_info *leds; }; struct gpio_desc; typedef int (*gpio_blink_set_t)(struct gpio_desc *desc, int state, unsigned long *delay_on, unsigned long *delay_off); /* For the leds-gpio driver */ struct gpio_led { const char *name; const char *default_trigger; unsigned gpio; unsigned active_low : 1; unsigned retain_state_suspended : 1; unsigned panic_indicator : 1; unsigned default_state : 2; unsigned retain_state_shutdown : 1; /* default_state should be one of LEDS_GPIO_DEFSTATE_(ON|OFF|KEEP) */ struct gpio_desc *gpiod; }; #define LEDS_GPIO_DEFSTATE_OFF 0 #define LEDS_GPIO_DEFSTATE_ON 1 #define LEDS_GPIO_DEFSTATE_KEEP 2 struct gpio_led_platform_data { int num_leds; const struct gpio_led *leds; #define GPIO_LED_NO_BLINK_LOW 0 /* No blink GPIO state low */ #define GPIO_LED_NO_BLINK_HIGH 1 /* No blink GPIO state high */ #define GPIO_LED_BLINK 2 /* Please, blink */ gpio_blink_set_t gpio_blink_set; }; #ifdef CONFIG_NEW_LEDS struct platform_device *gpio_led_register_device( int id, const struct gpio_led_platform_data *pdata); #else static inline struct platform_device *gpio_led_register_device( int id, const struct gpio_led_platform_data *pdata) { return 0; } #endif enum cpu_led_event { CPU_LED_IDLE_START, /* CPU enters idle */ CPU_LED_IDLE_END, /* CPU idle ends */ CPU_LED_START, /* Machine starts, especially resume */ CPU_LED_STOP, /* Machine stops, especially suspend */ CPU_LED_HALTED, /* Machine shutdown */ }; #ifdef CONFIG_LEDS_TRIGGER_CPU extern void ledtrig_cpu(enum cpu_led_event evt); #else static inline void ledtrig_cpu(enum cpu_led_event evt) { return; } #endif #ifdef CONFIG_LEDS_BRIGHTNESS_HW_CHANGED extern void led_classdev_notify_brightness_hw_changed( struct led_classdev *led_cdev, enum led_brightness brightness); #else static inline void led_classdev_notify_brightness_hw_changed( struct led_classdev *led_cdev, enum led_brightness brightness) { } #endif #endif /* __LINUX_LEDS_H_INCLUDED */