/* SPDX-License-Identifier: GPL-2.0 */ /* * Copyright (c) 2013 Red Hat, Inc. and Parallels Inc. All rights reserved. * Authors: David Chinner and Glauber Costa * * Generic LRU infrastructure */ #ifndef _LRU_LIST_H #define _LRU_LIST_H #include #include #include struct mem_cgroup; /* list_lru_walk_cb has to always return one of those */ enum lru_status { LRU_REMOVED, /* item removed from list */ LRU_REMOVED_RETRY, /* item removed, but lock has been dropped and reacquired */ LRU_ROTATE, /* item referenced, give another pass */ LRU_SKIP, /* item cannot be locked, skip */ LRU_RETRY, /* item not freeable. May drop the lock internally, but has to return locked. */ }; struct list_lru_one { struct list_head list; /* may become negative during memcg reparenting */ long nr_items; }; struct list_lru_memcg { struct rcu_head rcu; /* array of per cgroup lists, indexed by memcg_cache_id */ struct list_lru_one *lru[0]; }; struct list_lru_node { /* protects all lists on the node, including per cgroup */ spinlock_t lock; /* global list, used for the root cgroup in cgroup aware lrus */ struct list_lru_one lru; #ifdef CONFIG_MEMCG_KMEM /* for cgroup aware lrus points to per cgroup lists, otherwise NULL */ struct list_lru_memcg __rcu *memcg_lrus; #endif long nr_items; } ____cacheline_aligned_in_smp; struct list_lru { struct list_lru_node *node; #ifdef CONFIG_MEMCG_KMEM struct list_head list; int shrinker_id; #endif }; void list_lru_destroy(struct list_lru *lru); int __list_lru_init(struct list_lru *lru, bool memcg_aware, struct lock_class_key *key, struct shrinker *shrinker); #define list_lru_init(lru) \ __list_lru_init((lru), false, NULL, NULL) #define list_lru_init_key(lru, key) \ __list_lru_init((lru), false, (key), NULL) #define list_lru_init_memcg(lru, shrinker) \ __list_lru_init((lru), true, NULL, shrinker) int memcg_update_all_list_lrus(int num_memcgs); void memcg_drain_all_list_lrus(int src_idx, struct mem_cgroup *dst_memcg); /** * list_lru_add: add an element to the lru list's tail * @list_lru: the lru pointer * @item: the item to be added. * * If the element is already part of a list, this function returns doing * nothing. Therefore the caller does not need to keep state about whether or * not the element already belongs in the list and is allowed to lazy update * it. Note however that this is valid for *a* list, not *this* list. If * the caller organize itself in a way that elements can be in more than * one type of list, it is up to the caller to fully remove the item from * the previous list (with list_lru_del() for instance) before moving it * to @list_lru * * Return value: true if the list was updated, false otherwise */ bool list_lru_add(struct list_lru *lru, struct list_head *item); /** * list_lru_del: delete an element to the lru list * @list_lru: the lru pointer * @item: the item to be deleted. * * This function works analogously as list_lru_add in terms of list * manipulation. The comments about an element already pertaining to * a list are also valid for list_lru_del. * * Return value: true if the list was updated, false otherwise */ bool list_lru_del(struct list_lru *lru, struct list_head *item); /** * list_lru_count_one: return the number of objects currently held by @lru * @lru: the lru pointer. * @nid: the node id to count from. * @memcg: the cgroup to count from. * * Always return a non-negative number, 0 for empty lists. There is no * guarantee that the list is not updated while the count is being computed. * Callers that want such a guarantee need to provide an outer lock. */ unsigned long list_lru_count_one(struct list_lru *lru, int nid, struct mem_cgroup *memcg); unsigned long list_lru_count_node(struct list_lru *lru, int nid); static inline unsigned long list_lru_shrink_count(struct list_lru *lru, struct shrink_control *sc) { return list_lru_count_one(lru, sc->nid, sc->memcg); } static inline unsigned long list_lru_count(struct list_lru *lru) { long count = 0; int nid; for_each_node_state(nid, N_NORMAL_MEMORY) count += list_lru_count_node(lru, nid); return count; } void list_lru_isolate(struct list_lru_one *list, struct list_head *item); void list_lru_isolate_move(struct list_lru_one *list, struct list_head *item, struct list_head *head); typedef enum lru_status (*list_lru_walk_cb)(struct list_head *item, struct list_lru_one *list, spinlock_t *lock, void *cb_arg); /** * list_lru_walk_one: walk a list_lru, isolating and disposing freeable items. * @lru: the lru pointer. * @nid: the node id to scan from. * @memcg: the cgroup to scan from. * @isolate: callback function that is resposible for deciding what to do with * the item currently being scanned * @cb_arg: opaque type that will be passed to @isolate * @nr_to_walk: how many items to scan. * * This function will scan all elements in a particular list_lru, calling the * @isolate callback for each of those items, along with the current list * spinlock and a caller-provided opaque. The @isolate callback can choose to * drop the lock internally, but *must* return with the lock held. The callback * will return an enum lru_status telling the list_lru infrastructure what to * do with the object being scanned. * * Please note that nr_to_walk does not mean how many objects will be freed, * just how many objects will be scanned. * * Return value: the number of objects effectively removed from the LRU. */ unsigned long list_lru_walk_one(struct list_lru *lru, int nid, struct mem_cgroup *memcg, list_lru_walk_cb isolate, void *cb_arg, unsigned long *nr_to_walk); /** * list_lru_walk_one_irq: walk a list_lru, isolating and disposing freeable items. * @lru: the lru pointer. * @nid: the node id to scan from. * @memcg: the cgroup to scan from. * @isolate: callback function that is resposible for deciding what to do with * the item currently being scanned * @cb_arg: opaque type that will be passed to @isolate * @nr_to_walk: how many items to scan. * * Same as @list_lru_walk_one except that the spinlock is acquired with * spin_lock_irq(). */ unsigned long list_lru_walk_one_irq(struct list_lru *lru, int nid, struct mem_cgroup *memcg, list_lru_walk_cb isolate, void *cb_arg, unsigned long *nr_to_walk); unsigned long list_lru_walk_node(struct list_lru *lru, int nid, list_lru_walk_cb isolate, void *cb_arg, unsigned long *nr_to_walk); static inline unsigned long list_lru_shrink_walk(struct list_lru *lru, struct shrink_control *sc, list_lru_walk_cb isolate, void *cb_arg) { return list_lru_walk_one(lru, sc->nid, sc->memcg, isolate, cb_arg, &sc->nr_to_scan); } static inline unsigned long list_lru_shrink_walk_irq(struct list_lru *lru, struct shrink_control *sc, list_lru_walk_cb isolate, void *cb_arg) { return list_lru_walk_one_irq(lru, sc->nid, sc->memcg, isolate, cb_arg, &sc->nr_to_scan); } static inline unsigned long list_lru_walk(struct list_lru *lru, list_lru_walk_cb isolate, void *cb_arg, unsigned long nr_to_walk) { long isolated = 0; int nid; for_each_node_state(nid, N_NORMAL_MEMORY) { isolated += list_lru_walk_node(lru, nid, isolate, cb_arg, &nr_to_walk); if (nr_to_walk <= 0) break; } return isolated; } #endif /* _LRU_LIST_H */