/* SPDX-License-Identifier: GPL-2.0 */ /* * linux/mii.h: definitions for MII-compatible transceivers * Originally drivers/net/sunhme.h. * * Copyright (C) 1996, 1999, 2001 David S. Miller (davem@redhat.com) */ #ifndef __LINUX_MII_H__ #define __LINUX_MII_H__ #include #include struct ethtool_cmd; struct mii_if_info { int phy_id; int advertising; int phy_id_mask; int reg_num_mask; unsigned int full_duplex : 1; /* is full duplex? */ unsigned int force_media : 1; /* is autoneg. disabled? */ unsigned int supports_gmii : 1; /* are GMII registers supported? */ struct net_device *dev; int (*mdio_read) (struct net_device *dev, int phy_id, int location); void (*mdio_write) (struct net_device *dev, int phy_id, int location, int val); }; extern int mii_link_ok (struct mii_if_info *mii); extern int mii_nway_restart (struct mii_if_info *mii); extern int mii_ethtool_gset(struct mii_if_info *mii, struct ethtool_cmd *ecmd); extern void mii_ethtool_get_link_ksettings( struct mii_if_info *mii, struct ethtool_link_ksettings *cmd); extern int mii_ethtool_sset(struct mii_if_info *mii, struct ethtool_cmd *ecmd); extern int mii_ethtool_set_link_ksettings( struct mii_if_info *mii, const struct ethtool_link_ksettings *cmd); extern int mii_check_gmii_support(struct mii_if_info *mii); extern void mii_check_link (struct mii_if_info *mii); extern unsigned int mii_check_media (struct mii_if_info *mii, unsigned int ok_to_print, unsigned int init_media); extern int generic_mii_ioctl(struct mii_if_info *mii_if, struct mii_ioctl_data *mii_data, int cmd, unsigned int *duplex_changed); static inline struct mii_ioctl_data *if_mii(struct ifreq *rq) { return (struct mii_ioctl_data *) &rq->ifr_ifru; } /** * mii_nway_result * @negotiated: value of MII ANAR and'd with ANLPAR * * Given a set of MII abilities, check each bit and returns the * currently supported media, in the priority order defined by * IEEE 802.3u. We use LPA_xxx constants but note this is not the * value of LPA solely, as described above. * * The one exception to IEEE 802.3u is that 100baseT4 is placed * between 100T-full and 100T-half. If your phy does not support * 100T4 this is fine. If your phy places 100T4 elsewhere in the * priority order, you will need to roll your own function. */ static inline unsigned int mii_nway_result (unsigned int negotiated) { unsigned int ret; if (negotiated & LPA_100FULL) ret = LPA_100FULL; else if (negotiated & LPA_100BASE4) ret = LPA_100BASE4; else if (negotiated & LPA_100HALF) ret = LPA_100HALF; else if (negotiated & LPA_10FULL) ret = LPA_10FULL; else ret = LPA_10HALF; return ret; } /** * mii_duplex * @duplex_lock: Non-zero if duplex is locked at full * @negotiated: value of MII ANAR and'd with ANLPAR * * A small helper function for a common case. Returns one * if the media is operating or locked at full duplex, and * returns zero otherwise. */ static inline unsigned int mii_duplex (unsigned int duplex_lock, unsigned int negotiated) { if (duplex_lock) return 1; if (mii_nway_result(negotiated) & LPA_DUPLEX) return 1; return 0; } /** * ethtool_adv_to_mii_adv_t * @ethadv: the ethtool advertisement settings * * A small helper function that translates ethtool advertisement * settings to phy autonegotiation advertisements for the * MII_ADVERTISE register. */ static inline u32 ethtool_adv_to_mii_adv_t(u32 ethadv) { u32 result = 0; if (ethadv & ADVERTISED_10baseT_Half) result |= ADVERTISE_10HALF; if (ethadv & ADVERTISED_10baseT_Full) result |= ADVERTISE_10FULL; if (ethadv & ADVERTISED_100baseT_Half) result |= ADVERTISE_100HALF; if (ethadv & ADVERTISED_100baseT_Full) result |= ADVERTISE_100FULL; if (ethadv & ADVERTISED_Pause) result |= ADVERTISE_PAUSE_CAP; if (ethadv & ADVERTISED_Asym_Pause) result |= ADVERTISE_PAUSE_ASYM; return result; } /** * mii_adv_to_ethtool_adv_t * @adv: value of the MII_ADVERTISE register * * A small helper function that translates MII_ADVERTISE bits * to ethtool advertisement settings. */ static inline u32 mii_adv_to_ethtool_adv_t(u32 adv) { u32 result = 0; if (adv & ADVERTISE_10HALF) result |= ADVERTISED_10baseT_Half; if (adv & ADVERTISE_10FULL) result |= ADVERTISED_10baseT_Full; if (adv & ADVERTISE_100HALF) result |= ADVERTISED_100baseT_Half; if (adv & ADVERTISE_100FULL) result |= ADVERTISED_100baseT_Full; if (adv & ADVERTISE_PAUSE_CAP) result |= ADVERTISED_Pause; if (adv & ADVERTISE_PAUSE_ASYM) result |= ADVERTISED_Asym_Pause; return result; } /** * ethtool_adv_to_mii_ctrl1000_t * @ethadv: the ethtool advertisement settings * * A small helper function that translates ethtool advertisement * settings to phy autonegotiation advertisements for the * MII_CTRL1000 register when in 1000T mode. */ static inline u32 ethtool_adv_to_mii_ctrl1000_t(u32 ethadv) { u32 result = 0; if (ethadv & ADVERTISED_1000baseT_Half) result |= ADVERTISE_1000HALF; if (ethadv & ADVERTISED_1000baseT_Full) result |= ADVERTISE_1000FULL; return result; } /** * mii_ctrl1000_to_ethtool_adv_t * @adv: value of the MII_CTRL1000 register * * A small helper function that translates MII_CTRL1000 * bits, when in 1000Base-T mode, to ethtool * advertisement settings. */ static inline u32 mii_ctrl1000_to_ethtool_adv_t(u32 adv) { u32 result = 0; if (adv & ADVERTISE_1000HALF) result |= ADVERTISED_1000baseT_Half; if (adv & ADVERTISE_1000FULL) result |= ADVERTISED_1000baseT_Full; return result; } /** * mii_lpa_to_ethtool_lpa_t * @adv: value of the MII_LPA register * * A small helper function that translates MII_LPA * bits, when in 1000Base-T mode, to ethtool * LP advertisement settings. */ static inline u32 mii_lpa_to_ethtool_lpa_t(u32 lpa) { u32 result = 0; if (lpa & LPA_LPACK) result |= ADVERTISED_Autoneg; return result | mii_adv_to_ethtool_adv_t(lpa); } /** * mii_stat1000_to_ethtool_lpa_t * @adv: value of the MII_STAT1000 register * * A small helper function that translates MII_STAT1000 * bits, when in 1000Base-T mode, to ethtool * advertisement settings. */ static inline u32 mii_stat1000_to_ethtool_lpa_t(u32 lpa) { u32 result = 0; if (lpa & LPA_1000HALF) result |= ADVERTISED_1000baseT_Half; if (lpa & LPA_1000FULL) result |= ADVERTISED_1000baseT_Full; return result; } /** * ethtool_adv_to_mii_adv_x * @ethadv: the ethtool advertisement settings * * A small helper function that translates ethtool advertisement * settings to phy autonegotiation advertisements for the * MII_CTRL1000 register when in 1000Base-X mode. */ static inline u32 ethtool_adv_to_mii_adv_x(u32 ethadv) { u32 result = 0; if (ethadv & ADVERTISED_1000baseT_Half) result |= ADVERTISE_1000XHALF; if (ethadv & ADVERTISED_1000baseT_Full) result |= ADVERTISE_1000XFULL; if (ethadv & ADVERTISED_Pause) result |= ADVERTISE_1000XPAUSE; if (ethadv & ADVERTISED_Asym_Pause) result |= ADVERTISE_1000XPSE_ASYM; return result; } /** * mii_adv_to_ethtool_adv_x * @adv: value of the MII_CTRL1000 register * * A small helper function that translates MII_CTRL1000 * bits, when in 1000Base-X mode, to ethtool * advertisement settings. */ static inline u32 mii_adv_to_ethtool_adv_x(u32 adv) { u32 result = 0; if (adv & ADVERTISE_1000XHALF) result |= ADVERTISED_1000baseT_Half; if (adv & ADVERTISE_1000XFULL) result |= ADVERTISED_1000baseT_Full; if (adv & ADVERTISE_1000XPAUSE) result |= ADVERTISED_Pause; if (adv & ADVERTISE_1000XPSE_ASYM) result |= ADVERTISED_Asym_Pause; return result; } /** * mii_lpa_to_ethtool_lpa_x * @adv: value of the MII_LPA register * * A small helper function that translates MII_LPA * bits, when in 1000Base-X mode, to ethtool * LP advertisement settings. */ static inline u32 mii_lpa_to_ethtool_lpa_x(u32 lpa) { u32 result = 0; if (lpa & LPA_LPACK) result |= ADVERTISED_Autoneg; return result | mii_adv_to_ethtool_adv_x(lpa); } /** * mii_advertise_flowctrl - get flow control advertisement flags * @cap: Flow control capabilities (FLOW_CTRL_RX, FLOW_CTRL_TX or both) */ static inline u16 mii_advertise_flowctrl(int cap) { u16 adv = 0; if (cap & FLOW_CTRL_RX) adv = ADVERTISE_PAUSE_CAP | ADVERTISE_PAUSE_ASYM; if (cap & FLOW_CTRL_TX) adv ^= ADVERTISE_PAUSE_ASYM; return adv; } /** * mii_resolve_flowctrl_fdx * @lcladv: value of MII ADVERTISE register * @rmtadv: value of MII LPA register * * Resolve full duplex flow control as per IEEE 802.3-2005 table 28B-3 */ static inline u8 mii_resolve_flowctrl_fdx(u16 lcladv, u16 rmtadv) { u8 cap = 0; if (lcladv & rmtadv & ADVERTISE_PAUSE_CAP) { cap = FLOW_CTRL_TX | FLOW_CTRL_RX; } else if (lcladv & rmtadv & ADVERTISE_PAUSE_ASYM) { if (lcladv & ADVERTISE_PAUSE_CAP) cap = FLOW_CTRL_RX; else if (rmtadv & ADVERTISE_PAUSE_CAP) cap = FLOW_CTRL_TX; } return cap; } #endif /* __LINUX_MII_H__ */