/* SPDX-License-Identifier: GPL-2.0 */ #ifndef _LINUX_SHRINKER_H #define _LINUX_SHRINKER_H /* * This struct is used to pass information from page reclaim to the shrinkers. * We consolidate the values for easier extention later. * * The 'gfpmask' refers to the allocation we are currently trying to * fulfil. */ struct shrink_control { gfp_t gfp_mask; /* current node being shrunk (for NUMA aware shrinkers) */ int nid; /* * How many objects scan_objects should scan and try to reclaim. * This is reset before every call, so it is safe for callees * to modify. */ unsigned long nr_to_scan; /* * How many objects did scan_objects process? * This defaults to nr_to_scan before every call, but the callee * should track its actual progress. */ unsigned long nr_scanned; /* current memcg being shrunk (for memcg aware shrinkers) */ struct mem_cgroup *memcg; }; #define SHRINK_STOP (~0UL) #define SHRINK_EMPTY (~0UL - 1) /* * A callback you can register to apply pressure to ageable caches. * * @count_objects should return the number of freeable items in the cache. If * there are no objects to free, it should return SHRINK_EMPTY, while 0 is * returned in cases of the number of freeable items cannot be determined * or shrinker should skip this cache for this time (e.g., their number * is below shrinkable limit). No deadlock checks should be done during the * count callback - the shrinker relies on aggregating scan counts that couldn't * be executed due to potential deadlocks to be run at a later call when the * deadlock condition is no longer pending. * * @scan_objects will only be called if @count_objects returned a non-zero * value for the number of freeable objects. The callout should scan the cache * and attempt to free items from the cache. It should then return the number * of objects freed during the scan, or SHRINK_STOP if progress cannot be made * due to potential deadlocks. If SHRINK_STOP is returned, then no further * attempts to call the @scan_objects will be made from the current reclaim * context. * * @flags determine the shrinker abilities, like numa awareness */ struct shrinker { unsigned long (*count_objects)(struct shrinker *, struct shrink_control *sc); unsigned long (*scan_objects)(struct shrinker *, struct shrink_control *sc); long batch; /* reclaim batch size, 0 = default */ int seeks; /* seeks to recreate an obj */ unsigned flags; /* These are for internal use */ struct list_head list; #ifdef CONFIG_MEMCG_KMEM /* ID in shrinker_idr */ int id; #endif /* objs pending delete, per node */ atomic_long_t *nr_deferred; }; #define DEFAULT_SEEKS 2 /* A good number if you don't know better. */ /* Flags */ #define SHRINKER_NUMA_AWARE (1 << 0) #define SHRINKER_MEMCG_AWARE (1 << 1) extern int prealloc_shrinker(struct shrinker *shrinker); extern void register_shrinker_prepared(struct shrinker *shrinker); extern int register_shrinker(struct shrinker *shrinker); extern void unregister_shrinker(struct shrinker *shrinker); extern void free_prealloced_shrinker(struct shrinker *shrinker); #endif