/* SPDX-License-Identifier: GPL-2.0 */ /* * thermal.h ($Revision: 0 $) * * Copyright (C) 2008 Intel Corp * Copyright (C) 2008 Zhang Rui * Copyright (C) 2008 Sujith Thomas */ #ifndef __THERMAL_H__ #define __THERMAL_H__ #include #include #include #include #include #include #define THERMAL_TRIPS_NONE -1 #define THERMAL_MAX_TRIPS 12 /* invalid cooling state */ #define THERMAL_CSTATE_INVALID -1UL /* No upper/lower limit requirement */ #define THERMAL_NO_LIMIT ((u32)~0) /* Default weight of a bound cooling device */ #define THERMAL_WEIGHT_DEFAULT 0 /* use value, which < 0K, to indicate an invalid/uninitialized temperature */ #define THERMAL_TEMP_INVALID -274000 /* Unit conversion macros */ #define DECI_KELVIN_TO_CELSIUS(t) ({ \ long _t = (t); \ ((_t-2732 >= 0) ? (_t-2732+5)/10 : (_t-2732-5)/10); \ }) #define CELSIUS_TO_DECI_KELVIN(t) ((t)*10+2732) #define DECI_KELVIN_TO_MILLICELSIUS_WITH_OFFSET(t, off) (((t) - (off)) * 100) #define DECI_KELVIN_TO_MILLICELSIUS(t) DECI_KELVIN_TO_MILLICELSIUS_WITH_OFFSET(t, 2732) #define MILLICELSIUS_TO_DECI_KELVIN_WITH_OFFSET(t, off) (((t) / 100) + (off)) #define MILLICELSIUS_TO_DECI_KELVIN(t) MILLICELSIUS_TO_DECI_KELVIN_WITH_OFFSET(t, 2732) /* Default Thermal Governor */ #if defined(CONFIG_THERMAL_DEFAULT_GOV_STEP_WISE) #define DEFAULT_THERMAL_GOVERNOR "step_wise" #elif defined(CONFIG_THERMAL_DEFAULT_GOV_FAIR_SHARE) #define DEFAULT_THERMAL_GOVERNOR "fair_share" #elif defined(CONFIG_THERMAL_DEFAULT_GOV_USER_SPACE) #define DEFAULT_THERMAL_GOVERNOR "user_space" #elif defined(CONFIG_THERMAL_DEFAULT_GOV_POWER_ALLOCATOR) #define DEFAULT_THERMAL_GOVERNOR "power_allocator" #endif struct thermal_zone_device; struct thermal_cooling_device; struct thermal_instance; enum thermal_device_mode { THERMAL_DEVICE_DISABLED = 0, THERMAL_DEVICE_ENABLED, }; enum thermal_trip_type { THERMAL_TRIP_ACTIVE = 0, THERMAL_TRIP_PASSIVE, THERMAL_TRIP_HOT, THERMAL_TRIP_CRITICAL, }; enum thermal_trend { THERMAL_TREND_STABLE, /* temperature is stable */ THERMAL_TREND_RAISING, /* temperature is raising */ THERMAL_TREND_DROPPING, /* temperature is dropping */ THERMAL_TREND_RAISE_FULL, /* apply highest cooling action */ THERMAL_TREND_DROP_FULL, /* apply lowest cooling action */ }; /* Thermal notification reason */ enum thermal_notify_event { THERMAL_EVENT_UNSPECIFIED, /* Unspecified event */ THERMAL_EVENT_TEMP_SAMPLE, /* New Temperature sample */ THERMAL_TRIP_VIOLATED, /* TRIP Point violation */ THERMAL_TRIP_CHANGED, /* TRIP Point temperature changed */ THERMAL_DEVICE_DOWN, /* Thermal device is down */ THERMAL_DEVICE_UP, /* Thermal device is up after a down event */ THERMAL_DEVICE_POWER_CAPABILITY_CHANGED, /* power capability changed */ THERMAL_TABLE_CHANGED, /* Thermal table(s) changed */ }; struct thermal_zone_device_ops { int (*bind) (struct thermal_zone_device *, struct thermal_cooling_device *); int (*unbind) (struct thermal_zone_device *, struct thermal_cooling_device *); int (*get_temp) (struct thermal_zone_device *, int *); int (*set_trips) (struct thermal_zone_device *, int, int); int (*get_mode) (struct thermal_zone_device *, enum thermal_device_mode *); int (*set_mode) (struct thermal_zone_device *, enum thermal_device_mode); int (*get_trip_type) (struct thermal_zone_device *, int, enum thermal_trip_type *); int (*get_trip_temp) (struct thermal_zone_device *, int, int *); int (*set_trip_temp) (struct thermal_zone_device *, int, int); int (*get_trip_hyst) (struct thermal_zone_device *, int, int *); int (*set_trip_hyst) (struct thermal_zone_device *, int, int); int (*get_crit_temp) (struct thermal_zone_device *, int *); int (*set_emul_temp) (struct thermal_zone_device *, int); int (*get_trend) (struct thermal_zone_device *, int, enum thermal_trend *); int (*notify) (struct thermal_zone_device *, int, enum thermal_trip_type); }; struct thermal_cooling_device_ops { int (*get_max_state) (struct thermal_cooling_device *, unsigned long *); int (*get_cur_state) (struct thermal_cooling_device *, unsigned long *); int (*set_cur_state) (struct thermal_cooling_device *, unsigned long); int (*get_requested_power)(struct thermal_cooling_device *, struct thermal_zone_device *, u32 *); int (*state2power)(struct thermal_cooling_device *, struct thermal_zone_device *, unsigned long, u32 *); int (*power2state)(struct thermal_cooling_device *, struct thermal_zone_device *, u32, unsigned long *); }; struct thermal_cooling_device { int id; char type[THERMAL_NAME_LENGTH]; struct device device; struct device_node *np; void *devdata; void *stats; const struct thermal_cooling_device_ops *ops; bool updated; /* true if the cooling device does not need update */ struct mutex lock; /* protect thermal_instances list */ struct list_head thermal_instances; struct list_head node; }; struct thermal_attr { struct device_attribute attr; char name[THERMAL_NAME_LENGTH]; }; /** * struct thermal_zone_device - structure for a thermal zone * @id: unique id number for each thermal zone * @type: the thermal zone device type * @device: &struct device for this thermal zone * @trip_temp_attrs: attributes for trip points for sysfs: trip temperature * @trip_type_attrs: attributes for trip points for sysfs: trip type * @trip_hyst_attrs: attributes for trip points for sysfs: trip hysteresis * @devdata: private pointer for device private data * @trips: number of trip points the thermal zone supports * @trips_disabled; bitmap for disabled trips * @passive_delay: number of milliseconds to wait between polls when * performing passive cooling. * @polling_delay: number of milliseconds to wait between polls when * checking whether trip points have been crossed (0 for * interrupt driven systems) * @temperature: current temperature. This is only for core code, * drivers should use thermal_zone_get_temp() to get the * current temperature * @last_temperature: previous temperature read * @emul_temperature: emulated temperature when using CONFIG_THERMAL_EMULATION * @passive: 1 if you've crossed a passive trip point, 0 otherwise. * @prev_low_trip: the low current temperature if you've crossed a passive trip point. * @prev_high_trip: the above current temperature if you've crossed a passive trip point. * @forced_passive: If > 0, temperature at which to switch on all ACPI * processor cooling devices. Currently only used by the * step-wise governor. * @need_update: if equals 1, thermal_zone_device_update needs to be invoked. * @ops: operations this &thermal_zone_device supports * @tzp: thermal zone parameters * @governor: pointer to the governor for this thermal zone * @governor_data: private pointer for governor data * @thermal_instances: list of &struct thermal_instance of this thermal zone * @ida: &struct ida to generate unique id for this zone's cooling * devices * @lock: lock to protect thermal_instances list * @node: node in thermal_tz_list (in thermal_core.c) * @poll_queue: delayed work for polling * @notify_event: Last notification event */ struct thermal_zone_device { int id; char type[THERMAL_NAME_LENGTH]; struct device device; struct attribute_group trips_attribute_group; struct thermal_attr *trip_temp_attrs; struct thermal_attr *trip_type_attrs; struct thermal_attr *trip_hyst_attrs; void *devdata; int trips; unsigned long trips_disabled; /* bitmap for disabled trips */ int passive_delay; int polling_delay; int temperature; int last_temperature; int emul_temperature; int passive; int prev_low_trip; int prev_high_trip; unsigned int forced_passive; atomic_t need_update; struct thermal_zone_device_ops *ops; struct thermal_zone_params *tzp; struct thermal_governor *governor; void *governor_data; struct list_head thermal_instances; struct ida ida; struct mutex lock; struct list_head node; struct delayed_work poll_queue; enum thermal_notify_event notify_event; }; /** * struct thermal_governor - structure that holds thermal governor information * @name: name of the governor * @bind_to_tz: callback called when binding to a thermal zone. If it * returns 0, the governor is bound to the thermal zone, * otherwise it fails. * @unbind_from_tz: callback called when a governor is unbound from a * thermal zone. * @throttle: callback called for every trip point even if temperature is * below the trip point temperature * @governor_list: node in thermal_governor_list (in thermal_core.c) */ struct thermal_governor { char name[THERMAL_NAME_LENGTH]; int (*bind_to_tz)(struct thermal_zone_device *tz); void (*unbind_from_tz)(struct thermal_zone_device *tz); int (*throttle)(struct thermal_zone_device *tz, int trip); struct list_head governor_list; }; /* Structure that holds binding parameters for a zone */ struct thermal_bind_params { struct thermal_cooling_device *cdev; /* * This is a measure of 'how effectively these devices can * cool 'this' thermal zone. It shall be determined by * platform characterization. This value is relative to the * rest of the weights so a cooling device whose weight is * double that of another cooling device is twice as * effective. See Documentation/thermal/sysfs-api.txt for more * information. */ int weight; /* * This is a bit mask that gives the binding relation between this * thermal zone and cdev, for a particular trip point. * See Documentation/thermal/sysfs-api.txt for more information. */ int trip_mask; /* * This is an array of cooling state limits. Must have exactly * 2 * thermal_zone.number_of_trip_points. It is an array consisting * of tuples of state limits. Each trip * will be associated with one state limit tuple when binding. * A NULL pointer means * on all trips. */ unsigned long *binding_limits; int (*match) (struct thermal_zone_device *tz, struct thermal_cooling_device *cdev); }; /* Structure to define Thermal Zone parameters */ struct thermal_zone_params { char governor_name[THERMAL_NAME_LENGTH]; /* * a boolean to indicate if the thermal to hwmon sysfs interface * is required. when no_hwmon == false, a hwmon sysfs interface * will be created. when no_hwmon == true, nothing will be done */ bool no_hwmon; int num_tbps; /* Number of tbp entries */ struct thermal_bind_params *tbp; /* * Sustainable power (heat) that this thermal zone can dissipate in * mW */ u32 sustainable_power; /* * Proportional parameter of the PID controller when * overshooting (i.e., when temperature is below the target) */ s32 k_po; /* * Proportional parameter of the PID controller when * undershooting */ s32 k_pu; /* Integral parameter of the PID controller */ s32 k_i; /* Derivative parameter of the PID controller */ s32 k_d; /* threshold below which the error is no longer accumulated */ s32 integral_cutoff; /* * @slope: slope of a linear temperature adjustment curve. * Used by thermal zone drivers. */ int slope; /* * @offset: offset of a linear temperature adjustment curve. * Used by thermal zone drivers (default 0). */ int offset; }; struct thermal_genl_event { u32 orig; enum events event; }; /** * struct thermal_zone_of_device_ops - scallbacks for handling DT based zones * * Mandatory: * @get_temp: a pointer to a function that reads the sensor temperature. * * Optional: * @get_trend: a pointer to a function that reads the sensor temperature trend. * @set_trips: a pointer to a function that sets a temperature window. When * this window is left the driver must inform the thermal core via * thermal_zone_device_update. * @set_emul_temp: a pointer to a function that sets sensor emulated * temperature. * @set_trip_temp: a pointer to a function that sets the trip temperature on * hardware. */ struct thermal_zone_of_device_ops { int (*get_temp)(void *, int *); int (*get_trend)(void *, int, enum thermal_trend *); int (*set_trips)(void *, int, int); int (*set_emul_temp)(void *, int); int (*set_trip_temp)(void *, int, int); }; /** * struct thermal_trip - representation of a point in temperature domain * @np: pointer to struct device_node that this trip point was created from * @temperature: temperature value in miliCelsius * @hysteresis: relative hysteresis in miliCelsius * @type: trip point type */ struct thermal_trip { struct device_node *np; int temperature; int hysteresis; enum thermal_trip_type type; }; /* Function declarations */ #ifdef CONFIG_THERMAL_OF struct thermal_zone_device * thermal_zone_of_sensor_register(struct device *dev, int id, void *data, const struct thermal_zone_of_device_ops *ops); void thermal_zone_of_sensor_unregister(struct device *dev, struct thermal_zone_device *tz); struct thermal_zone_device *devm_thermal_zone_of_sensor_register( struct device *dev, int id, void *data, const struct thermal_zone_of_device_ops *ops); void devm_thermal_zone_of_sensor_unregister(struct device *dev, struct thermal_zone_device *tz); #else static inline struct thermal_zone_device * thermal_zone_of_sensor_register(struct device *dev, int id, void *data, const struct thermal_zone_of_device_ops *ops) { return ERR_PTR(-ENODEV); } static inline void thermal_zone_of_sensor_unregister(struct device *dev, struct thermal_zone_device *tz) { } static inline struct thermal_zone_device *devm_thermal_zone_of_sensor_register( struct device *dev, int id, void *data, const struct thermal_zone_of_device_ops *ops) { return ERR_PTR(-ENODEV); } static inline void devm_thermal_zone_of_sensor_unregister(struct device *dev, struct thermal_zone_device *tz) { } #endif #if IS_ENABLED(CONFIG_THERMAL) static inline bool cdev_is_power_actor(struct thermal_cooling_device *cdev) { return cdev->ops->get_requested_power && cdev->ops->state2power && cdev->ops->power2state; } int power_actor_get_max_power(struct thermal_cooling_device *, struct thermal_zone_device *tz, u32 *max_power); int power_actor_get_min_power(struct thermal_cooling_device *, struct thermal_zone_device *tz, u32 *min_power); int power_actor_set_power(struct thermal_cooling_device *, struct thermal_instance *, u32); struct thermal_zone_device *thermal_zone_device_register(const char *, int, int, void *, struct thermal_zone_device_ops *, struct thermal_zone_params *, int, int); void thermal_zone_device_unregister(struct thermal_zone_device *); int thermal_zone_bind_cooling_device(struct thermal_zone_device *, int, struct thermal_cooling_device *, unsigned long, unsigned long, unsigned int); int thermal_zone_unbind_cooling_device(struct thermal_zone_device *, int, struct thermal_cooling_device *); void thermal_zone_device_update(struct thermal_zone_device *, enum thermal_notify_event); void thermal_zone_set_trips(struct thermal_zone_device *); struct thermal_cooling_device *thermal_cooling_device_register(char *, void *, const struct thermal_cooling_device_ops *); struct thermal_cooling_device * thermal_of_cooling_device_register(struct device_node *np, char *, void *, const struct thermal_cooling_device_ops *); void thermal_cooling_device_unregister(struct thermal_cooling_device *); struct thermal_zone_device *thermal_zone_get_zone_by_name(const char *name); int thermal_zone_get_temp(struct thermal_zone_device *tz, int *temp); int thermal_zone_get_slope(struct thermal_zone_device *tz); int thermal_zone_get_offset(struct thermal_zone_device *tz); int get_tz_trend(struct thermal_zone_device *, int); struct thermal_instance *get_thermal_instance(struct thermal_zone_device *, struct thermal_cooling_device *, int); void thermal_cdev_update(struct thermal_cooling_device *); void thermal_notify_framework(struct thermal_zone_device *, int); #else static inline bool cdev_is_power_actor(struct thermal_cooling_device *cdev) { return false; } static inline int power_actor_get_max_power(struct thermal_cooling_device *cdev, struct thermal_zone_device *tz, u32 *max_power) { return 0; } static inline int power_actor_get_min_power(struct thermal_cooling_device *cdev, struct thermal_zone_device *tz, u32 *min_power) { return -ENODEV; } static inline int power_actor_set_power(struct thermal_cooling_device *cdev, struct thermal_instance *tz, u32 power) { return 0; } static inline struct thermal_zone_device *thermal_zone_device_register( const char *type, int trips, int mask, void *devdata, struct thermal_zone_device_ops *ops, struct thermal_zone_params *tzp, int passive_delay, int polling_delay) { return ERR_PTR(-ENODEV); } static inline void thermal_zone_device_unregister( struct thermal_zone_device *tz) { } static inline int thermal_zone_bind_cooling_device( struct thermal_zone_device *tz, int trip, struct thermal_cooling_device *cdev, unsigned long upper, unsigned long lower, unsigned int weight) { return -ENODEV; } static inline int thermal_zone_unbind_cooling_device( struct thermal_zone_device *tz, int trip, struct thermal_cooling_device *cdev) { return -ENODEV; } static inline void thermal_zone_device_update(struct thermal_zone_device *tz, enum thermal_notify_event event) { } static inline void thermal_zone_set_trips(struct thermal_zone_device *tz) { } static inline struct thermal_cooling_device * thermal_cooling_device_register(char *type, void *devdata, const struct thermal_cooling_device_ops *ops) { return ERR_PTR(-ENODEV); } static inline struct thermal_cooling_device * thermal_of_cooling_device_register(struct device_node *np, char *type, void *devdata, const struct thermal_cooling_device_ops *ops) { return ERR_PTR(-ENODEV); } static inline void thermal_cooling_device_unregister( struct thermal_cooling_device *cdev) { } static inline struct thermal_zone_device *thermal_zone_get_zone_by_name( const char *name) { return ERR_PTR(-ENODEV); } static inline int thermal_zone_get_temp( struct thermal_zone_device *tz, int *temp) { return -ENODEV; } static inline int thermal_zone_get_slope( struct thermal_zone_device *tz) { return -ENODEV; } static inline int thermal_zone_get_offset( struct thermal_zone_device *tz) { return -ENODEV; } static inline int get_tz_trend(struct thermal_zone_device *tz, int trip) { return -ENODEV; } static inline struct thermal_instance * get_thermal_instance(struct thermal_zone_device *tz, struct thermal_cooling_device *cdev, int trip) { return ERR_PTR(-ENODEV); } static inline void thermal_cdev_update(struct thermal_cooling_device *cdev) { } static inline void thermal_notify_framework(struct thermal_zone_device *tz, int trip) { } #endif /* CONFIG_THERMAL */ #if defined(CONFIG_NET) && IS_ENABLED(CONFIG_THERMAL) extern int thermal_generate_netlink_event(struct thermal_zone_device *tz, enum events event); #else static inline int thermal_generate_netlink_event(struct thermal_zone_device *tz, enum events event) { return 0; } #endif #endif /* __THERMAL_H__ */