aboutsummaryrefslogtreecommitdiffstats
blob: 681d866efb1eb858c377cae5a35806e2931a97d8 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
/* SPDX-License-Identifier: GPL-2.0 */
#ifndef __LINUX_COMPILER_H
#define __LINUX_COMPILER_H

#include <linux/compiler_types.h>

#ifndef __ASSEMBLY__

#ifdef __KERNEL__

/*
 * Note: DISABLE_BRANCH_PROFILING can be used by special lowlevel code
 * to disable branch tracing on a per file basis.
 */
#if defined(CONFIG_TRACE_BRANCH_PROFILING) \
    && !defined(DISABLE_BRANCH_PROFILING) && !defined(__CHECKER__)
void ftrace_likely_update(struct ftrace_likely_data *f, int val,
			  int expect, int is_constant);

#define likely_notrace(x)	__builtin_expect(!!(x), 1)
#define unlikely_notrace(x)	__builtin_expect(!!(x), 0)

#define __branch_check__(x, expect, is_constant) ({			\
			long ______r;					\
			static struct ftrace_likely_data		\
				__attribute__((__aligned__(4)))		\
				__attribute__((section("_ftrace_annotated_branch"))) \
				______f = {				\
				.data.func = __func__,			\
				.data.file = __FILE__,			\
				.data.line = __LINE__,			\
			};						\
			______r = __builtin_expect(!!(x), expect);	\
			ftrace_likely_update(&______f, ______r,		\
					     expect, is_constant);	\
			______r;					\
		})

/*
 * Using __builtin_constant_p(x) to ignore cases where the return
 * value is always the same.  This idea is taken from a similar patch
 * written by Daniel Walker.
 */
# ifndef likely
#  define likely(x)	(__branch_check__(x, 1, __builtin_constant_p(x)))
# endif
# ifndef unlikely
#  define unlikely(x)	(__branch_check__(x, 0, __builtin_constant_p(x)))
# endif

#ifdef CONFIG_PROFILE_ALL_BRANCHES
/*
 * "Define 'is'", Bill Clinton
 * "Define 'if'", Steven Rostedt
 */
#define if(cond, ...) __trace_if( (cond , ## __VA_ARGS__) )
#define __trace_if(cond) \
	if (__builtin_constant_p(!!(cond)) ? !!(cond) :			\
	({								\
		int ______r;						\
		static struct ftrace_branch_data			\
			__attribute__((__aligned__(4)))			\
			__attribute__((section("_ftrace_branch")))	\
			______f = {					\
				.func = __func__,			\
				.file = __FILE__,			\
				.line = __LINE__,			\
			};						\
		______r = !!(cond);					\
		______f.miss_hit[______r]++;					\
		______r;						\
	}))
#endif /* CONFIG_PROFILE_ALL_BRANCHES */

#else
# define likely(x)	__builtin_expect(!!(x), 1)
# define unlikely(x)	__builtin_expect(!!(x), 0)
#endif

/* Optimization barrier */
#ifndef barrier
# define barrier() __memory_barrier()
#endif

#ifndef barrier_data
# define barrier_data(ptr) barrier()
#endif

/* workaround for GCC PR82365 if needed */
#ifndef barrier_before_unreachable
# define barrier_before_unreachable() do { } while (0)
#endif

/* Unreachable code */
#ifdef CONFIG_STACK_VALIDATION
/*
 * These macros help objtool understand GCC code flow for unreachable code.
 * The __COUNTER__ based labels are a hack to make each instance of the macros
 * unique, to convince GCC not to merge duplicate inline asm statements.
 */
#define annotate_reachable() ({						\
	asm volatile("%c0:\n\t"						\
		     ".pushsection .discard.reachable\n\t"		\
		     ".long %c0b - .\n\t"				\
		     ".popsection\n\t" : : "i" (__COUNTER__));		\
})
#define annotate_unreachable() ({					\
	asm volatile("%c0:\n\t"						\
		     ".pushsection .discard.unreachable\n\t"		\
		     ".long %c0b - .\n\t"				\
		     ".popsection\n\t" : : "i" (__COUNTER__));		\
})
#define ASM_UNREACHABLE							\
	"999:\n\t"							\
	".pushsection .discard.unreachable\n\t"				\
	".long 999b - .\n\t"						\
	".popsection\n\t"
#else
#define annotate_reachable()
#define annotate_unreachable()
#endif

#ifndef ASM_UNREACHABLE
# define ASM_UNREACHABLE
#endif
#ifndef unreachable
# define unreachable() do { annotate_reachable(); do { } while (1); } while (0)
#endif

/*
 * KENTRY - kernel entry point
 * This can be used to annotate symbols (functions or data) that are used
 * without their linker symbol being referenced explicitly. For example,
 * interrupt vector handlers, or functions in the kernel image that are found
 * programatically.
 *
 * Not required for symbols exported with EXPORT_SYMBOL, or initcalls. Those
 * are handled in their own way (with KEEP() in linker scripts).
 *
 * KENTRY can be avoided if the symbols in question are marked as KEEP() in the
 * linker script. For example an architecture could KEEP() its entire
 * boot/exception vector code rather than annotate each function and data.
 */
#ifndef KENTRY
# define KENTRY(sym)						\
	extern typeof(sym) sym;					\
	static const unsigned long __kentry_##sym		\
	__used							\
	__attribute__((section("___kentry" "+" #sym ), used))	\
	= (unsigned long)&sym;
#endif

#ifndef RELOC_HIDE
# define RELOC_HIDE(ptr, off)					\
  ({ unsigned long __ptr;					\
     __ptr = (unsigned long) (ptr);				\
    (typeof(ptr)) (__ptr + (off)); })
#endif

#ifndef OPTIMIZER_HIDE_VAR
#define OPTIMIZER_HIDE_VAR(var) barrier()
#endif

/* Not-quite-unique ID. */
#ifndef __UNIQUE_ID
# define __UNIQUE_ID(prefix) __PASTE(__PASTE(__UNIQUE_ID_, prefix), __LINE__)
#endif

#include <uapi/linux/types.h>

#define __READ_ONCE_SIZE						\
({									\
	switch (size) {							\
	case 1: *(__u8 *)res = *(volatile __u8 *)p; break;		\
	case 2: *(__u16 *)res = *(volatile __u16 *)p; break;		\
	case 4: *(__u32 *)res = *(volatile __u32 *)p; break;		\
	case 8: *(__u64 *)res = *(volatile __u64 *)p; break;		\
	default:							\
		barrier();						\
		__builtin_memcpy((void *)res, (const void *)p, size);	\
		barrier();						\
	}								\
})

static __always_inline
void __read_once_size(const volatile void *p, void *res, int size)
{
	__READ_ONCE_SIZE;
}

#ifdef CONFIG_KASAN
/*
 * We can't declare function 'inline' because __no_sanitize_address confilcts
 * with inlining. Attempt to inline it may cause a build failure.
 * 	https://gcc.gnu.org/bugzilla/show_bug.cgi?id=67368
 * '__maybe_unused' allows us to avoid defined-but-not-used warnings.
 */
# define __no_kasan_or_inline __no_sanitize_address __maybe_unused
#else
# define __no_kasan_or_inline __always_inline
#endif

static __no_kasan_or_inline
void __read_once_size_nocheck(const volatile void *p, void *res, int size)
{
	__READ_ONCE_SIZE;
}

static __always_inline void __write_once_size(volatile void *p, void *res, int size)
{
	switch (size) {
	case 1: *(volatile __u8 *)p = *(__u8 *)res; break;
	case 2: *(volatile __u16 *)p = *(__u16 *)res; break;
	case 4: *(volatile __u32 *)p = *(__u32 *)res; break;
	case 8: *(volatile __u64 *)p = *(__u64 *)res; break;
	default:
		barrier();
		__builtin_memcpy((void *)p, (const void *)res, size);
		barrier();
	}
}

/*
 * Prevent the compiler from merging or refetching reads or writes. The
 * compiler is also forbidden from reordering successive instances of
 * READ_ONCE and WRITE_ONCE, but only when the compiler is aware of some
 * particular ordering. One way to make the compiler aware of ordering is to
 * put the two invocations of READ_ONCE or WRITE_ONCE in different C
 * statements.
 *
 * These two macros will also work on aggregate data types like structs or
 * unions. If the size of the accessed data type exceeds the word size of
 * the machine (e.g., 32 bits or 64 bits) READ_ONCE() and WRITE_ONCE() will
 * fall back to memcpy(). There's at least two memcpy()s: one for the
 * __builtin_memcpy() and then one for the macro doing the copy of variable
 * - '__u' allocated on the stack.
 *
 * Their two major use cases are: (1) Mediating communication between
 * process-level code and irq/NMI handlers, all running on the same CPU,
 * and (2) Ensuring that the compiler does not fold, spindle, or otherwise
 * mutilate accesses that either do not require ordering or that interact
 * with an explicit memory barrier or atomic instruction that provides the
 * required ordering.
 */
#include <asm/barrier.h>
#include <linux/kasan-checks.h>

#define __READ_ONCE(x, check)						\
({									\
	union { typeof(x) __val; char __c[1]; } __u;			\
	if (check)							\
		__read_once_size(&(x), __u.__c, sizeof(x));		\
	else								\
		__read_once_size_nocheck(&(x), __u.__c, sizeof(x));	\
	smp_read_barrier_depends(); /* Enforce dependency ordering from x */ \
	__u.__val;							\
})
#define READ_ONCE(x) __READ_ONCE(x, 1)

/*
 * Use READ_ONCE_NOCHECK() instead of READ_ONCE() if you need
 * to hide memory access from KASAN.
 */
#define READ_ONCE_NOCHECK(x) __READ_ONCE(x, 0)

static __no_kasan_or_inline
unsigned long read_word_at_a_time(const void *addr)
{
	kasan_check_read(addr, 1);
	return *(unsigned long *)addr;
}

#define WRITE_ONCE(x, val) \
({							\
	union { typeof(x) __val; char __c[1]; } __u =	\
		{ .__val = (__force typeof(x)) (val) }; \
	__write_once_size(&(x), __u.__c, sizeof(x));	\
	__u.__val;					\
})

#endif /* __KERNEL__ */

/*
 * Force the compiler to emit 'sym' as a symbol, so that we can reference
 * it from inline assembler. Necessary in case 'sym' could be inlined
 * otherwise, or eliminated entirely due to lack of references that are
 * visible to the compiler.
 */
#define __ADDRESSABLE(sym) \
	static void * __attribute__((section(".discard.addressable"), used)) \
		__PASTE(__addressable_##sym, __LINE__) = (void *)&sym;

/**
 * offset_to_ptr - convert a relative memory offset to an absolute pointer
 * @off:	the address of the 32-bit offset value
 */
static inline void *offset_to_ptr(const int *off)
{
	return (void *)((unsigned long)off + *off);
}

#endif /* __ASSEMBLY__ */

#ifndef __optimize
# define __optimize(level)
#endif

/* Compile time object size, -1 for unknown */
#ifndef __compiletime_object_size
# define __compiletime_object_size(obj) -1
#endif
#ifndef __compiletime_warning
# define __compiletime_warning(message)
#endif
#ifndef __compiletime_error
# define __compiletime_error(message)
/*
 * Sparse complains of variable sized arrays due to the temporary variable in
 * __compiletime_assert. Unfortunately we can't just expand it out to make
 * sparse see a constant array size without breaking compiletime_assert on old
 * versions of GCC (e.g. 4.2.4), so hide the array from sparse altogether.
 */
# ifndef __CHECKER__
#  define __compiletime_error_fallback(condition) \
	do { ((void)sizeof(char[1 - 2 * condition])); } while (0)
# endif
#endif
#ifndef __compiletime_error_fallback
# define __compiletime_error_fallback(condition) do { } while (0)
#endif

#ifdef __OPTIMIZE__
# define __compiletime_assert(condition, msg, prefix, suffix)		\
	do {								\
		int __cond = !(condition);				\
		extern void prefix ## suffix(void) __compiletime_error(msg); \
		if (__cond)						\
			prefix ## suffix();				\
		__compiletime_error_fallback(__cond);			\
	} while (0)
#else
# define __compiletime_assert(condition, msg, prefix, suffix) do { } while (0)
#endif

#define _compiletime_assert(condition, msg, prefix, suffix) \
	__compiletime_assert(condition, msg, prefix, suffix)

/**
 * compiletime_assert - break build and emit msg if condition is false
 * @condition: a compile-time constant condition to check
 * @msg:       a message to emit if condition is false
 *
 * In tradition of POSIX assert, this macro will break the build if the
 * supplied condition is *false*, emitting the supplied error message if the
 * compiler has support to do so.
 */
#define compiletime_assert(condition, msg) \
	_compiletime_assert(condition, msg, __compiletime_assert_, __LINE__)

#define compiletime_assert_atomic_type(t)				\
	compiletime_assert(__native_word(t),				\
		"Need native word sized stores/loads for atomicity.")

#endif /* __LINUX_COMPILER_H */