aboutsummaryrefslogtreecommitdiffstats
blob: 952ab97af325ea32b537cf32f32a2afd30648cdd (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
/* SPDX-License-Identifier: GPL-2.0 */
/*
 * fscrypt.h: declarations for per-file encryption
 *
 * Filesystems that implement per-file encryption include this header
 * file with the __FS_HAS_ENCRYPTION set according to whether that filesystem
 * is being built with encryption support or not.
 *
 * Copyright (C) 2015, Google, Inc.
 *
 * Written by Michael Halcrow, 2015.
 * Modified by Jaegeuk Kim, 2015.
 */
#ifndef _LINUX_FSCRYPT_H
#define _LINUX_FSCRYPT_H

#include <linux/fs.h>

#define FS_CRYPTO_BLOCK_SIZE		16

struct fscrypt_ctx;
struct fscrypt_info;

struct fscrypt_str {
	unsigned char *name;
	u32 len;
};

struct fscrypt_name {
	const struct qstr *usr_fname;
	struct fscrypt_str disk_name;
	u32 hash;
	u32 minor_hash;
	struct fscrypt_str crypto_buf;
};

#define FSTR_INIT(n, l)		{ .name = n, .len = l }
#define FSTR_TO_QSTR(f)		QSTR_INIT((f)->name, (f)->len)
#define fname_name(p)		((p)->disk_name.name)
#define fname_len(p)		((p)->disk_name.len)

/* Maximum value for the third parameter of fscrypt_operations.set_context(). */
#define FSCRYPT_SET_CONTEXT_MAX_SIZE	28

#if __FS_HAS_ENCRYPTION
#include <linux/fscrypt_supp.h>
#else
#include <linux/fscrypt_notsupp.h>
#endif

/**
 * fscrypt_require_key - require an inode's encryption key
 * @inode: the inode we need the key for
 *
 * If the inode is encrypted, set up its encryption key if not already done.
 * Then require that the key be present and return -ENOKEY otherwise.
 *
 * No locks are needed, and the key will live as long as the struct inode --- so
 * it won't go away from under you.
 *
 * Return: 0 on success, -ENOKEY if the key is missing, or another -errno code
 * if a problem occurred while setting up the encryption key.
 */
static inline int fscrypt_require_key(struct inode *inode)
{
	if (IS_ENCRYPTED(inode)) {
		int err = fscrypt_get_encryption_info(inode);

		if (err)
			return err;
		if (!fscrypt_has_encryption_key(inode))
			return -ENOKEY;
	}
	return 0;
}

/**
 * fscrypt_prepare_link - prepare to link an inode into a possibly-encrypted directory
 * @old_dentry: an existing dentry for the inode being linked
 * @dir: the target directory
 * @dentry: negative dentry for the target filename
 *
 * A new link can only be added to an encrypted directory if the directory's
 * encryption key is available --- since otherwise we'd have no way to encrypt
 * the filename.  Therefore, we first set up the directory's encryption key (if
 * not already done) and return an error if it's unavailable.
 *
 * We also verify that the link will not violate the constraint that all files
 * in an encrypted directory tree use the same encryption policy.
 *
 * Return: 0 on success, -ENOKEY if the directory's encryption key is missing,
 * -EPERM if the link would result in an inconsistent encryption policy, or
 * another -errno code.
 */
static inline int fscrypt_prepare_link(struct dentry *old_dentry,
				       struct inode *dir,
				       struct dentry *dentry)
{
	if (IS_ENCRYPTED(dir))
		return __fscrypt_prepare_link(d_inode(old_dentry), dir);
	return 0;
}

/**
 * fscrypt_prepare_rename - prepare for a rename between possibly-encrypted directories
 * @old_dir: source directory
 * @old_dentry: dentry for source file
 * @new_dir: target directory
 * @new_dentry: dentry for target location (may be negative unless exchanging)
 * @flags: rename flags (we care at least about %RENAME_EXCHANGE)
 *
 * Prepare for ->rename() where the source and/or target directories may be
 * encrypted.  A new link can only be added to an encrypted directory if the
 * directory's encryption key is available --- since otherwise we'd have no way
 * to encrypt the filename.  A rename to an existing name, on the other hand,
 * *is* cryptographically possible without the key.  However, we take the more
 * conservative approach and just forbid all no-key renames.
 *
 * We also verify that the rename will not violate the constraint that all files
 * in an encrypted directory tree use the same encryption policy.
 *
 * Return: 0 on success, -ENOKEY if an encryption key is missing, -EPERM if the
 * rename would cause inconsistent encryption policies, or another -errno code.
 */
static inline int fscrypt_prepare_rename(struct inode *old_dir,
					 struct dentry *old_dentry,
					 struct inode *new_dir,
					 struct dentry *new_dentry,
					 unsigned int flags)
{
	if (IS_ENCRYPTED(old_dir) || IS_ENCRYPTED(new_dir))
		return __fscrypt_prepare_rename(old_dir, old_dentry,
						new_dir, new_dentry, flags);
	return 0;
}

/**
 * fscrypt_prepare_lookup - prepare to lookup a name in a possibly-encrypted directory
 * @dir: directory being searched
 * @dentry: filename being looked up
 * @flags: lookup flags
 *
 * Prepare for ->lookup() in a directory which may be encrypted.  Lookups can be
 * done with or without the directory's encryption key; without the key,
 * filenames are presented in encrypted form.  Therefore, we'll try to set up
 * the directory's encryption key, but even without it the lookup can continue.
 *
 * To allow invalidating stale dentries if the directory's encryption key is
 * added later, we also install a custom ->d_revalidate() method and use the
 * DCACHE_ENCRYPTED_WITH_KEY flag to indicate whether a given dentry is a
 * plaintext name (flag set) or a ciphertext name (flag cleared).
 *
 * Return: 0 on success, -errno if a problem occurred while setting up the
 * encryption key
 */
static inline int fscrypt_prepare_lookup(struct inode *dir,
					 struct dentry *dentry,
					 unsigned int flags)
{
	if (IS_ENCRYPTED(dir))
		return __fscrypt_prepare_lookup(dir, dentry);
	return 0;
}

/**
 * fscrypt_prepare_setattr - prepare to change a possibly-encrypted inode's attributes
 * @dentry: dentry through which the inode is being changed
 * @attr: attributes to change
 *
 * Prepare for ->setattr() on a possibly-encrypted inode.  On an encrypted file,
 * most attribute changes are allowed even without the encryption key.  However,
 * without the encryption key we do have to forbid truncates.  This is needed
 * because the size being truncated to may not be a multiple of the filesystem
 * block size, and in that case we'd have to decrypt the final block, zero the
 * portion past i_size, and re-encrypt it.  (We *could* allow truncating to a
 * filesystem block boundary, but it's simpler to just forbid all truncates ---
 * and we already forbid all other contents modifications without the key.)
 *
 * Return: 0 on success, -ENOKEY if the key is missing, or another -errno code
 * if a problem occurred while setting up the encryption key.
 */
static inline int fscrypt_prepare_setattr(struct dentry *dentry,
					  struct iattr *attr)
{
	if (attr->ia_valid & ATTR_SIZE)
		return fscrypt_require_key(d_inode(dentry));
	return 0;
}

/**
 * fscrypt_prepare_symlink - prepare to create a possibly-encrypted symlink
 * @dir: directory in which the symlink is being created
 * @target: plaintext symlink target
 * @len: length of @target excluding null terminator
 * @max_len: space the filesystem has available to store the symlink target
 * @disk_link: (out) the on-disk symlink target being prepared
 *
 * This function computes the size the symlink target will require on-disk,
 * stores it in @disk_link->len, and validates it against @max_len.  An
 * encrypted symlink may be longer than the original.
 *
 * Additionally, @disk_link->name is set to @target if the symlink will be
 * unencrypted, but left NULL if the symlink will be encrypted.  For encrypted
 * symlinks, the filesystem must call fscrypt_encrypt_symlink() to create the
 * on-disk target later.  (The reason for the two-step process is that some
 * filesystems need to know the size of the symlink target before creating the
 * inode, e.g. to determine whether it will be a "fast" or "slow" symlink.)
 *
 * Return: 0 on success, -ENAMETOOLONG if the symlink target is too long,
 * -ENOKEY if the encryption key is missing, or another -errno code if a problem
 * occurred while setting up the encryption key.
 */
static inline int fscrypt_prepare_symlink(struct inode *dir,
					  const char *target,
					  unsigned int len,
					  unsigned int max_len,
					  struct fscrypt_str *disk_link)
{
	if (IS_ENCRYPTED(dir) || fscrypt_dummy_context_enabled(dir))
		return __fscrypt_prepare_symlink(dir, len, max_len, disk_link);

	disk_link->name = (unsigned char *)target;
	disk_link->len = len + 1;
	if (disk_link->len > max_len)
		return -ENAMETOOLONG;
	return 0;
}

/**
 * fscrypt_encrypt_symlink - encrypt the symlink target if needed
 * @inode: symlink inode
 * @target: plaintext symlink target
 * @len: length of @target excluding null terminator
 * @disk_link: (in/out) the on-disk symlink target being prepared
 *
 * If the symlink target needs to be encrypted, then this function encrypts it
 * into @disk_link->name.  fscrypt_prepare_symlink() must have been called
 * previously to compute @disk_link->len.  If the filesystem did not allocate a
 * buffer for @disk_link->name after calling fscrypt_prepare_link(), then one
 * will be kmalloc()'ed and the filesystem will be responsible for freeing it.
 *
 * Return: 0 on success, -errno on failure
 */
static inline int fscrypt_encrypt_symlink(struct inode *inode,
					  const char *target,
					  unsigned int len,
					  struct fscrypt_str *disk_link)
{
	if (IS_ENCRYPTED(inode))
		return __fscrypt_encrypt_symlink(inode, target, len, disk_link);
	return 0;
}

#endif	/* _LINUX_FSCRYPT_H */