aboutsummaryrefslogtreecommitdiffstats
blob: faebf0ca0686ce05bab67aa242767c8cdf098d39 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
/*
 * fwnode.h - Firmware device node object handle type definition.
 *
 * Copyright (C) 2015, Intel Corporation
 * Author: Rafael J. Wysocki <rafael.j.wysocki@intel.com>
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 */

#ifndef _LINUX_FWNODE_H_
#define _LINUX_FWNODE_H_

#include <linux/types.h>

struct fwnode_operations;
struct device;

struct fwnode_handle {
	struct fwnode_handle *secondary;
	const struct fwnode_operations *ops;
};

/**
 * struct fwnode_endpoint - Fwnode graph endpoint
 * @port: Port number
 * @id: Endpoint id
 * @local_fwnode: reference to the related fwnode
 */
struct fwnode_endpoint {
	unsigned int port;
	unsigned int id;
	const struct fwnode_handle *local_fwnode;
};

#define NR_FWNODE_REFERENCE_ARGS	8

/**
 * struct fwnode_reference_args - Fwnode reference with additional arguments
 * @fwnode:- A reference to the base fwnode
 * @nargs: Number of elements in @args array
 * @args: Integer arguments on the fwnode
 */
struct fwnode_reference_args {
	struct fwnode_handle *fwnode;
	unsigned int nargs;
	u64 args[NR_FWNODE_REFERENCE_ARGS];
};

/**
 * struct fwnode_operations - Operations for fwnode interface
 * @get: Get a reference to an fwnode.
 * @put: Put a reference to an fwnode.
 * @device_get_match_data: Return the device driver match data.
 * @property_present: Return true if a property is present.
 * @property_read_integer_array: Read an array of integer properties. Return
 *				 zero on success, a negative error code
 *				 otherwise.
 * @property_read_string_array: Read an array of string properties. Return zero
 *				on success, a negative error code otherwise.
 * @get_parent: Return the parent of an fwnode.
 * @get_next_child_node: Return the next child node in an iteration.
 * @get_named_child_node: Return a child node with a given name.
 * @get_reference_args: Return a reference pointed to by a property, with args
 * @graph_get_next_endpoint: Return an endpoint node in an iteration.
 * @graph_get_remote_endpoint: Return the remote endpoint node of a local
 *			       endpoint node.
 * @graph_get_port_parent: Return the parent node of a port node.
 * @graph_parse_endpoint: Parse endpoint for port and endpoint id.
 */
struct fwnode_operations {
	struct fwnode_handle *(*get)(struct fwnode_handle *fwnode);
	void (*put)(struct fwnode_handle *fwnode);
	bool (*device_is_available)(const struct fwnode_handle *fwnode);
	const void *(*device_get_match_data)(const struct fwnode_handle *fwnode,
					     const struct device *dev);
	bool (*property_present)(const struct fwnode_handle *fwnode,
				 const char *propname);
	int (*property_read_int_array)(const struct fwnode_handle *fwnode,
				       const char *propname,
				       unsigned int elem_size, void *val,
				       size_t nval);
	int
	(*property_read_string_array)(const struct fwnode_handle *fwnode_handle,
				      const char *propname, const char **val,
				      size_t nval);
	struct fwnode_handle *(*get_parent)(const struct fwnode_handle *fwnode);
	struct fwnode_handle *
	(*get_next_child_node)(const struct fwnode_handle *fwnode,
			       struct fwnode_handle *child);
	struct fwnode_handle *
	(*get_named_child_node)(const struct fwnode_handle *fwnode,
				const char *name);
	int (*get_reference_args)(const struct fwnode_handle *fwnode,
				  const char *prop, const char *nargs_prop,
				  unsigned int nargs, unsigned int index,
				  struct fwnode_reference_args *args);
	struct fwnode_handle *
	(*graph_get_next_endpoint)(const struct fwnode_handle *fwnode,
				   struct fwnode_handle *prev);
	struct fwnode_handle *
	(*graph_get_remote_endpoint)(const struct fwnode_handle *fwnode);
	struct fwnode_handle *
	(*graph_get_port_parent)(struct fwnode_handle *fwnode);
	int (*graph_parse_endpoint)(const struct fwnode_handle *fwnode,
				    struct fwnode_endpoint *endpoint);
};

#define fwnode_has_op(fwnode, op)				\
	((fwnode) && (fwnode)->ops && (fwnode)->ops->op)
#define fwnode_call_int_op(fwnode, op, ...)				\
	(fwnode ? (fwnode_has_op(fwnode, op) ?				\
		   (fwnode)->ops->op(fwnode, ## __VA_ARGS__) : -ENXIO) : \
	 -EINVAL)
#define fwnode_call_bool_op(fwnode, op, ...)				\
	(fwnode ? (fwnode_has_op(fwnode, op) ?				\
		   (fwnode)->ops->op(fwnode, ## __VA_ARGS__) : false) : \
	 false)
#define fwnode_call_ptr_op(fwnode, op, ...)		\
	(fwnode_has_op(fwnode, op) ?			\
	 (fwnode)->ops->op(fwnode, ## __VA_ARGS__) : NULL)
#define fwnode_call_void_op(fwnode, op, ...)				\
	do {								\
		if (fwnode_has_op(fwnode, op))				\
			(fwnode)->ops->op(fwnode, ## __VA_ARGS__);	\
	} while (false)

#endif