aboutsummaryrefslogtreecommitdiffstats
blob: c304dcdb4eac2a9117080e6a14f4e3f28d07fd56 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
/* SPDX-License-Identifier: GPL-2.0 */
#ifndef _LINUX_GETCPU_H
#define _LINUX_GETCPU_H 1

/* Cache for getcpu() to speed it up. Results might be a short time
   out of date, but will be faster.

   User programs should not refer to the contents of this structure.
   I repeat they should not refer to it. If they do they will break
   in future kernels.

   It is only a private cache for vgetcpu(). It will change in future kernels.
   The user program must store this information per thread (__thread)
   If you want 100% accurate information pass NULL instead. */
struct getcpu_cache {
	unsigned long blob[128 / sizeof(long)];
};

#endif