aboutsummaryrefslogtreecommitdiffstats
blob: 417d2c4bc60db4b80b29d1a7f78d1273b600b258 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
/* SPDX-License-Identifier: GPL-2.0 */
/*
 * Statically sized hash table implementation
 * (C) 2012  Sasha Levin <levinsasha928@gmail.com>
 */

#ifndef _LINUX_HASHTABLE_H
#define _LINUX_HASHTABLE_H

#include <linux/list.h>
#include <linux/types.h>
#include <linux/kernel.h>
#include <linux/hash.h>
#include <linux/rculist.h>

#define DEFINE_HASHTABLE(name, bits)						\
	struct hlist_head name[1 << (bits)] =					\
			{ [0 ... ((1 << (bits)) - 1)] = HLIST_HEAD_INIT }

#define DEFINE_READ_MOSTLY_HASHTABLE(name, bits)				\
	struct hlist_head name[1 << (bits)] __read_mostly =			\
			{ [0 ... ((1 << (bits)) - 1)] = HLIST_HEAD_INIT }

#define DECLARE_HASHTABLE(name, bits)                                   	\
	struct hlist_head name[1 << (bits)]

#define HASH_SIZE(name) (ARRAY_SIZE(name))
#define HASH_BITS(name) ilog2(HASH_SIZE(name))

/* Use hash_32 when possible to allow for fast 32bit hashing in 64bit kernels. */
#define hash_min(val, bits)							\
	(sizeof(val) <= 4 ? hash_32(val, bits) : hash_long(val, bits))

static inline void __hash_init(struct hlist_head *ht, unsigned int sz)
{
	unsigned int i;

	for (i = 0; i < sz; i++)
		INIT_HLIST_HEAD(&ht[i]);
}

/**
 * hash_init - initialize a hash table
 * @hashtable: hashtable to be initialized
 *
 * Calculates the size of the hashtable from the given parameter, otherwise
 * same as hash_init_size.
 *
 * This has to be a macro since HASH_BITS() will not work on pointers since
 * it calculates the size during preprocessing.
 */
#define hash_init(hashtable) __hash_init(hashtable, HASH_SIZE(hashtable))

/**
 * hash_add - add an object to a hashtable
 * @hashtable: hashtable to add to
 * @node: the &struct hlist_node of the object to be added
 * @key: the key of the object to be added
 */
#define hash_add(hashtable, node, key)						\
	hlist_add_head(node, &hashtable[hash_min(key, HASH_BITS(hashtable))])

/**
 * hash_add_rcu - add an object to a rcu enabled hashtable
 * @hashtable: hashtable to add to
 * @node: the &struct hlist_node of the object to be added
 * @key: the key of the object to be added
 */
#define hash_add_rcu(hashtable, node, key)					\
	hlist_add_head_rcu(node, &hashtable[hash_min(key, HASH_BITS(hashtable))])

/**
 * hash_hashed - check whether an object is in any hashtable
 * @node: the &struct hlist_node of the object to be checked
 */
static inline bool hash_hashed(struct hlist_node *node)
{
	return !hlist_unhashed(node);
}

static inline bool __hash_empty(struct hlist_head *ht, unsigned int sz)
{
	unsigned int i;

	for (i = 0; i < sz; i++)
		if (!hlist_empty(&ht[i]))
			return false;

	return true;
}

/**
 * hash_empty - check whether a hashtable is empty
 * @hashtable: hashtable to check
 *
 * This has to be a macro since HASH_BITS() will not work on pointers since
 * it calculates the size during preprocessing.
 */
#define hash_empty(hashtable) __hash_empty(hashtable, HASH_SIZE(hashtable))

/**
 * hash_del - remove an object from a hashtable
 * @node: &struct hlist_node of the object to remove
 */
static inline void hash_del(struct hlist_node *node)
{
	hlist_del_init(node);
}

/**
 * hash_del_rcu - remove an object from a rcu enabled hashtable
 * @node: &struct hlist_node of the object to remove
 */
static inline void hash_del_rcu(struct hlist_node *node)
{
	hlist_del_init_rcu(node);
}

/**
 * hash_for_each - iterate over a hashtable
 * @name: hashtable to iterate
 * @bkt: integer to use as bucket loop cursor
 * @obj: the type * to use as a loop cursor for each entry
 * @member: the name of the hlist_node within the struct
 */
#define hash_for_each(name, bkt, obj, member)				\
	for ((bkt) = 0, obj = NULL; obj == NULL && (bkt) < HASH_SIZE(name);\
			(bkt)++)\
		hlist_for_each_entry(obj, &name[bkt], member)

/**
 * hash_for_each_rcu - iterate over a rcu enabled hashtable
 * @name: hashtable to iterate
 * @bkt: integer to use as bucket loop cursor
 * @obj: the type * to use as a loop cursor for each entry
 * @member: the name of the hlist_node within the struct
 */
#define hash_for_each_rcu(name, bkt, obj, member)			\
	for ((bkt) = 0, obj = NULL; obj == NULL && (bkt) < HASH_SIZE(name);\
			(bkt)++)\
		hlist_for_each_entry_rcu(obj, &name[bkt], member)

/**
 * hash_for_each_safe - iterate over a hashtable safe against removal of
 * hash entry
 * @name: hashtable to iterate
 * @bkt: integer to use as bucket loop cursor
 * @tmp: a &struct used for temporary storage
 * @obj: the type * to use as a loop cursor for each entry
 * @member: the name of the hlist_node within the struct
 */
#define hash_for_each_safe(name, bkt, tmp, obj, member)			\
	for ((bkt) = 0, obj = NULL; obj == NULL && (bkt) < HASH_SIZE(name);\
			(bkt)++)\
		hlist_for_each_entry_safe(obj, tmp, &name[bkt], member)

/**
 * hash_for_each_possible - iterate over all possible objects hashing to the
 * same bucket
 * @name: hashtable to iterate
 * @obj: the type * to use as a loop cursor for each entry
 * @member: the name of the hlist_node within the struct
 * @key: the key of the objects to iterate over
 */
#define hash_for_each_possible(name, obj, member, key)			\
	hlist_for_each_entry(obj, &name[hash_min(key, HASH_BITS(name))], member)

/**
 * hash_for_each_possible_rcu - iterate over all possible objects hashing to the
 * same bucket in an rcu enabled hashtable
 * @name: hashtable to iterate
 * @obj: the type * to use as a loop cursor for each entry
 * @member: the name of the hlist_node within the struct
 * @key: the key of the objects to iterate over
 */
#define hash_for_each_possible_rcu(name, obj, member, key)		\
	hlist_for_each_entry_rcu(obj, &name[hash_min(key, HASH_BITS(name))],\
		member)

/**
 * hash_for_each_possible_rcu_notrace - iterate over all possible objects hashing
 * to the same bucket in an rcu enabled hashtable in a rcu enabled hashtable
 * @name: hashtable to iterate
 * @obj: the type * to use as a loop cursor for each entry
 * @member: the name of the hlist_node within the struct
 * @key: the key of the objects to iterate over
 *
 * This is the same as hash_for_each_possible_rcu() except that it does
 * not do any RCU debugging or tracing.
 */
#define hash_for_each_possible_rcu_notrace(name, obj, member, key) \
	hlist_for_each_entry_rcu_notrace(obj, \
		&name[hash_min(key, HASH_BITS(name))], member)

/**
 * hash_for_each_possible_safe - iterate over all possible objects hashing to the
 * same bucket safe against removals
 * @name: hashtable to iterate
 * @obj: the type * to use as a loop cursor for each entry
 * @tmp: a &struct used for temporary storage
 * @member: the name of the hlist_node within the struct
 * @key: the key of the objects to iterate over
 */
#define hash_for_each_possible_safe(name, obj, tmp, member, key)	\
	hlist_for_each_entry_safe(obj, tmp,\
		&name[hash_min(key, HASH_BITS(name))], member)


#endif