aboutsummaryrefslogtreecommitdiffstats
blob: 163b79ecd01a39fb141ae8f6052f74fc86b93210 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
/* SPDX-License-Identifier: GPL-2.0+ */
/*
 * OF helpers for the GPIO API
 *
 * Copyright (c) 2007-2008  MontaVista Software, Inc.
 *
 * Author: Anton Vorontsov <avorontsov@ru.mvista.com>
 */

#ifndef __LINUX_OF_GPIO_H
#define __LINUX_OF_GPIO_H

#include <linux/compiler.h>
#include <linux/kernel.h>
#include <linux/errno.h>
#include <linux/gpio.h>
#include <linux/of.h>

struct device_node;

/*
 * This is Linux-specific flags. By default controllers' and Linux' mapping
 * match, but GPIO controllers are free to translate their own flags to
 * Linux-specific in their .xlate callback. Though, 1:1 mapping is recommended.
 */
enum of_gpio_flags {
	OF_GPIO_ACTIVE_LOW = 0x1,
	OF_GPIO_SINGLE_ENDED = 0x2,
	OF_GPIO_OPEN_DRAIN = 0x4,
	OF_GPIO_TRANSITORY = 0x8,
};

#ifdef CONFIG_OF_GPIO

/*
 * OF GPIO chip for memory mapped banks
 */
struct of_mm_gpio_chip {
	struct gpio_chip gc;
	void (*save_regs)(struct of_mm_gpio_chip *mm_gc);
	void __iomem *regs;
};

static inline struct of_mm_gpio_chip *to_of_mm_gpio_chip(struct gpio_chip *gc)
{
	return container_of(gc, struct of_mm_gpio_chip, gc);
}

extern int of_get_named_gpio_flags(struct device_node *np,
		const char *list_name, int index, enum of_gpio_flags *flags);

extern int of_mm_gpiochip_add_data(struct device_node *np,
				   struct of_mm_gpio_chip *mm_gc,
				   void *data);
static inline int of_mm_gpiochip_add(struct device_node *np,
				     struct of_mm_gpio_chip *mm_gc)
{
	return of_mm_gpiochip_add_data(np, mm_gc, NULL);
}
extern void of_mm_gpiochip_remove(struct of_mm_gpio_chip *mm_gc);

extern int of_gpio_simple_xlate(struct gpio_chip *gc,
				const struct of_phandle_args *gpiospec,
				u32 *flags);

#else /* CONFIG_OF_GPIO */

/* Drivers may not strictly depend on the GPIO support, so let them link. */
static inline int of_get_named_gpio_flags(struct device_node *np,
		const char *list_name, int index, enum of_gpio_flags *flags)
{
	if (flags)
		*flags = 0;

	return -ENOSYS;
}

static inline int of_gpio_simple_xlate(struct gpio_chip *gc,
				       const struct of_phandle_args *gpiospec,
				       u32 *flags)
{
	return -ENOSYS;
}

#endif /* CONFIG_OF_GPIO */

/**
 * of_gpio_named_count() - Count GPIOs for a device
 * @np:		device node to count GPIOs for
 * @propname:	property name containing gpio specifier(s)
 *
 * The function returns the count of GPIOs specified for a node.
 * Note that the empty GPIO specifiers count too. Returns either
 *   Number of gpios defined in property,
 *   -EINVAL for an incorrectly formed gpios property, or
 *   -ENOENT for a missing gpios property
 *
 * Example:
 * gpios = <0
 *          &gpio1 1 2
 *          0
 *          &gpio2 3 4>;
 *
 * The above example defines four GPIOs, two of which are not specified.
 * This function will return '4'
 */
static inline int of_gpio_named_count(struct device_node *np, const char* propname)
{
	return of_count_phandle_with_args(np, propname, "#gpio-cells");
}

/**
 * of_gpio_count() - Count GPIOs for a device
 * @np:		device node to count GPIOs for
 *
 * Same as of_gpio_named_count, but hard coded to use the 'gpios' property
 */
static inline int of_gpio_count(struct device_node *np)
{
	return of_gpio_named_count(np, "gpios");
}

static inline int of_get_gpio_flags(struct device_node *np, int index,
		      enum of_gpio_flags *flags)
{
	return of_get_named_gpio_flags(np, "gpios", index, flags);
}

/**
 * of_get_named_gpio() - Get a GPIO number to use with GPIO API
 * @np:		device node to get GPIO from
 * @propname:	Name of property containing gpio specifier(s)
 * @index:	index of the GPIO
 *
 * Returns GPIO number to use with Linux generic GPIO API, or one of the errno
 * value on the error condition.
 */
static inline int of_get_named_gpio(struct device_node *np,
                                   const char *propname, int index)
{
	return of_get_named_gpio_flags(np, propname, index, NULL);
}

/**
 * of_get_gpio() - Get a GPIO number to use with GPIO API
 * @np:		device node to get GPIO from
 * @index:	index of the GPIO
 *
 * Returns GPIO number to use with Linux generic GPIO API, or one of the errno
 * value on the error condition.
 */
static inline int of_get_gpio(struct device_node *np, int index)
{
	return of_get_gpio_flags(np, index, NULL);
}

#endif /* __LINUX_OF_GPIO_H */