aboutsummaryrefslogtreecommitdiffstats
blob: 5225832bd6ff11415422470c5c25e60c1dad6821 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
/* SPDX-License-Identifier: GPL-2.0 */
#ifndef __LINUX_RTNETLINK_H
#define __LINUX_RTNETLINK_H


#include <linux/mutex.h>
#include <linux/netdevice.h>
#include <linux/wait.h>
#include <uapi/linux/rtnetlink.h>

extern int rtnetlink_send(struct sk_buff *skb, struct net *net, u32 pid, u32 group, int echo);
extern int rtnl_unicast(struct sk_buff *skb, struct net *net, u32 pid);
extern void rtnl_notify(struct sk_buff *skb, struct net *net, u32 pid,
			u32 group, struct nlmsghdr *nlh, gfp_t flags);
extern void rtnl_set_sk_err(struct net *net, u32 group, int error);
extern int rtnetlink_put_metrics(struct sk_buff *skb, u32 *metrics);
extern int rtnl_put_cacheinfo(struct sk_buff *skb, struct dst_entry *dst,
			      u32 id, long expires, u32 error);

void rtmsg_ifinfo(int type, struct net_device *dev, unsigned change, gfp_t flags);
void rtmsg_ifinfo_newnet(int type, struct net_device *dev, unsigned int change,
			 gfp_t flags, int *new_nsid, int new_ifindex);
struct sk_buff *rtmsg_ifinfo_build_skb(int type, struct net_device *dev,
				       unsigned change, u32 event,
				       gfp_t flags, int *new_nsid,
				       int new_ifindex);
void rtmsg_ifinfo_send(struct sk_buff *skb, struct net_device *dev,
		       gfp_t flags);


/* RTNL is used as a global lock for all changes to network configuration  */
extern void rtnl_lock(void);
extern void rtnl_unlock(void);
extern int rtnl_trylock(void);
extern int rtnl_is_locked(void);
extern int rtnl_lock_killable(void);

extern wait_queue_head_t netdev_unregistering_wq;
extern struct rw_semaphore pernet_ops_rwsem;
extern struct rw_semaphore net_rwsem;

#ifdef CONFIG_PROVE_LOCKING
extern bool lockdep_rtnl_is_held(void);
#else
static inline bool lockdep_rtnl_is_held(void)
{
	return true;
}
#endif /* #ifdef CONFIG_PROVE_LOCKING */

/**
 * rcu_dereference_rtnl - rcu_dereference with debug checking
 * @p: The pointer to read, prior to dereferencing
 *
 * Do an rcu_dereference(p), but check caller either holds rcu_read_lock()
 * or RTNL. Note : Please prefer rtnl_dereference() or rcu_dereference()
 */
#define rcu_dereference_rtnl(p)					\
	rcu_dereference_check(p, lockdep_rtnl_is_held())

/**
 * rcu_dereference_bh_rtnl - rcu_dereference_bh with debug checking
 * @p: The pointer to read, prior to dereference
 *
 * Do an rcu_dereference_bh(p), but check caller either holds rcu_read_lock_bh()
 * or RTNL. Note : Please prefer rtnl_dereference() or rcu_dereference_bh()
 */
#define rcu_dereference_bh_rtnl(p)				\
	rcu_dereference_bh_check(p, lockdep_rtnl_is_held())

/**
 * rtnl_dereference - fetch RCU pointer when updates are prevented by RTNL
 * @p: The pointer to read, prior to dereferencing
 *
 * Return the value of the specified RCU-protected pointer, but omit
 * the READ_ONCE(), because caller holds RTNL.
 */
#define rtnl_dereference(p)					\
	rcu_dereference_protected(p, lockdep_rtnl_is_held())

static inline struct netdev_queue *dev_ingress_queue(struct net_device *dev)
{
	return rtnl_dereference(dev->ingress_queue);
}

struct netdev_queue *dev_ingress_queue_create(struct net_device *dev);

#ifdef CONFIG_NET_INGRESS
void net_inc_ingress_queue(void);
void net_dec_ingress_queue(void);
#endif

#ifdef CONFIG_NET_EGRESS
void net_inc_egress_queue(void);
void net_dec_egress_queue(void);
#endif

void rtnetlink_init(void);
void __rtnl_unlock(void);
void rtnl_kfree_skbs(struct sk_buff *head, struct sk_buff *tail);

#define ASSERT_RTNL() \
	WARN_ONCE(!rtnl_is_locked(), \
		  "RTNL: assertion failed at %s (%d)\n", __FILE__,  __LINE__)

extern int ndo_dflt_fdb_dump(struct sk_buff *skb,
			     struct netlink_callback *cb,
			     struct net_device *dev,
			     struct net_device *filter_dev,
			     int *idx);
extern int ndo_dflt_fdb_add(struct ndmsg *ndm,
			    struct nlattr *tb[],
			    struct net_device *dev,
			    const unsigned char *addr,
			    u16 vid,
			    u16 flags);
extern int ndo_dflt_fdb_del(struct ndmsg *ndm,
			    struct nlattr *tb[],
			    struct net_device *dev,
			    const unsigned char *addr,
			    u16 vid);

extern int ndo_dflt_bridge_getlink(struct sk_buff *skb, u32 pid, u32 seq,
				   struct net_device *dev, u16 mode,
				   u32 flags, u32 mask, int nlflags,
				   u32 filter_mask,
				   int (*vlan_fill)(struct sk_buff *skb,
						    struct net_device *dev,
						    u32 filter_mask));
#endif	/* __LINUX_RTNETLINK_H */