aboutsummaryrefslogtreecommitdiffstats
blob: d1ae43c13e25940e2febed51919c171e3018ed3f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
#ifndef _LINUX_TIME32_H
#define _LINUX_TIME32_H
/*
 * These are all interfaces based on the old time_t definition
 * that overflows in 2038 on 32-bit architectures. New code
 * should use the replacements based on time64_t and timespec64.
 *
 * Any interfaces in here that become unused as we migrate
 * code to time64_t should get removed.
 */

#include <linux/time64.h>

#define TIME_T_MAX	(time_t)((1UL << ((sizeof(time_t) << 3) - 1)) - 1)

#if __BITS_PER_LONG == 64

/* timespec64 is defined as timespec here */
static inline struct timespec timespec64_to_timespec(const struct timespec64 ts64)
{
	return *(const struct timespec *)&ts64;
}

static inline struct timespec64 timespec_to_timespec64(const struct timespec ts)
{
	return *(const struct timespec64 *)&ts;
}

#else
static inline struct timespec timespec64_to_timespec(const struct timespec64 ts64)
{
	struct timespec ret;

	ret.tv_sec = (time_t)ts64.tv_sec;
	ret.tv_nsec = ts64.tv_nsec;
	return ret;
}

static inline struct timespec64 timespec_to_timespec64(const struct timespec ts)
{
	struct timespec64 ret;

	ret.tv_sec = ts.tv_sec;
	ret.tv_nsec = ts.tv_nsec;
	return ret;
}
#endif

static inline int timespec_equal(const struct timespec *a,
				 const struct timespec *b)
{
	return (a->tv_sec == b->tv_sec) && (a->tv_nsec == b->tv_nsec);
}

/*
 * lhs < rhs:  return <0
 * lhs == rhs: return 0
 * lhs > rhs:  return >0
 */
static inline int timespec_compare(const struct timespec *lhs, const struct timespec *rhs)
{
	if (lhs->tv_sec < rhs->tv_sec)
		return -1;
	if (lhs->tv_sec > rhs->tv_sec)
		return 1;
	return lhs->tv_nsec - rhs->tv_nsec;
}

extern void set_normalized_timespec(struct timespec *ts, time_t sec, s64 nsec);

static inline struct timespec timespec_add(struct timespec lhs,
						struct timespec rhs)
{
	struct timespec ts_delta;

	set_normalized_timespec(&ts_delta, lhs.tv_sec + rhs.tv_sec,
				lhs.tv_nsec + rhs.tv_nsec);
	return ts_delta;
}

/*
 * sub = lhs - rhs, in normalized form
 */
static inline struct timespec timespec_sub(struct timespec lhs,
						struct timespec rhs)
{
	struct timespec ts_delta;

	set_normalized_timespec(&ts_delta, lhs.tv_sec - rhs.tv_sec,
				lhs.tv_nsec - rhs.tv_nsec);
	return ts_delta;
}

/*
 * Returns true if the timespec is norm, false if denorm:
 */
static inline bool timespec_valid(const struct timespec *ts)
{
	/* Dates before 1970 are bogus */
	if (ts->tv_sec < 0)
		return false;
	/* Can't have more nanoseconds then a second */
	if ((unsigned long)ts->tv_nsec >= NSEC_PER_SEC)
		return false;
	return true;
}

static inline bool timespec_valid_strict(const struct timespec *ts)
{
	if (!timespec_valid(ts))
		return false;
	/* Disallow values that could overflow ktime_t */
	if ((unsigned long long)ts->tv_sec >= KTIME_SEC_MAX)
		return false;
	return true;
}

/**
 * timespec_to_ns - Convert timespec to nanoseconds
 * @ts:		pointer to the timespec variable to be converted
 *
 * Returns the scalar nanosecond representation of the timespec
 * parameter.
 */
static inline s64 timespec_to_ns(const struct timespec *ts)
{
	return ((s64) ts->tv_sec * NSEC_PER_SEC) + ts->tv_nsec;
}

/**
 * ns_to_timespec - Convert nanoseconds to timespec
 * @nsec:	the nanoseconds value to be converted
 *
 * Returns the timespec representation of the nsec parameter.
 */
extern struct timespec ns_to_timespec(const s64 nsec);

/**
 * timespec_add_ns - Adds nanoseconds to a timespec
 * @a:		pointer to timespec to be incremented
 * @ns:		unsigned nanoseconds value to be added
 *
 * This must always be inlined because its used from the x86-64 vdso,
 * which cannot call other kernel functions.
 */
static __always_inline void timespec_add_ns(struct timespec *a, u64 ns)
{
	a->tv_sec += __iter_div_u64_rem(a->tv_nsec + ns, NSEC_PER_SEC, &ns);
	a->tv_nsec = ns;
}

/**
 * time_to_tm - converts the calendar time to local broken-down time
 *
 * @totalsecs	the number of seconds elapsed since 00:00:00 on January 1, 1970,
 *		Coordinated Universal Time (UTC).
 * @offset	offset seconds adding to totalsecs.
 * @result	pointer to struct tm variable to receive broken-down time
 */
static inline void time_to_tm(time_t totalsecs, int offset, struct tm *result)
{
	time64_to_tm(totalsecs, offset, result);
}

static inline unsigned long mktime(const unsigned int year,
			const unsigned int mon, const unsigned int day,
			const unsigned int hour, const unsigned int min,
			const unsigned int sec)
{
	return mktime64(year, mon, day, hour, min, sec);
}

static inline bool timeval_valid(const struct timeval *tv)
{
	/* Dates before 1970 are bogus */
	if (tv->tv_sec < 0)
		return false;

	/* Can't have more microseconds then a second */
	if (tv->tv_usec < 0 || tv->tv_usec >= USEC_PER_SEC)
		return false;

	return true;
}

extern struct timespec timespec_trunc(struct timespec t, unsigned int gran);

/**
 * timeval_to_ns - Convert timeval to nanoseconds
 * @ts:		pointer to the timeval variable to be converted
 *
 * Returns the scalar nanosecond representation of the timeval
 * parameter.
 */
static inline s64 timeval_to_ns(const struct timeval *tv)
{
	return ((s64) tv->tv_sec * NSEC_PER_SEC) +
		tv->tv_usec * NSEC_PER_USEC;
}

/**
 * ns_to_timeval - Convert nanoseconds to timeval
 * @nsec:	the nanoseconds value to be converted
 *
 * Returns the timeval representation of the nsec parameter.
 */
extern struct timeval ns_to_timeval(const s64 nsec);
extern struct __kernel_old_timeval ns_to_kernel_old_timeval(s64 nsec);

/*
 * New aliases for compat time functions. These will be used to replace
 * the compat code so it can be shared between 32-bit and 64-bit builds
 * both of which provide compatibility with old 32-bit tasks.
 */
#define old_time32_t		compat_time_t
#define old_timeval32		compat_timeval
#define old_timespec32		compat_timespec
#define old_itimerspec32	compat_itimerspec
#define ns_to_old_timeval32	ns_to_compat_timeval
#define get_old_itimerspec32	get_compat_itimerspec64
#define put_old_itimerspec32	put_compat_itimerspec64
#define get_old_timespec32	compat_get_timespec64
#define put_old_timespec32	compat_put_timespec64

#endif