aboutsummaryrefslogtreecommitdiffstats
blob: 7acb953298a73118028ae04052fab9249529380f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
/* SPDX-License-Identifier: GPL-2.0 */
/*
 * You SHOULD NOT be including this unless you're vsyscall
 * handling code or timekeeping internal code!
 */

#ifndef _LINUX_TIMEKEEPER_INTERNAL_H
#define _LINUX_TIMEKEEPER_INTERNAL_H

#include <linux/clocksource.h>
#include <linux/jiffies.h>
#include <linux/time.h>

/**
 * struct tk_read_base - base structure for timekeeping readout
 * @clock:	Current clocksource used for timekeeping.
 * @mask:	Bitmask for two's complement subtraction of non 64bit clocks
 * @cycle_last: @clock cycle value at last update
 * @mult:	(NTP adjusted) multiplier for scaled math conversion
 * @shift:	Shift value for scaled math conversion
 * @xtime_nsec: Shifted (fractional) nano seconds offset for readout
 * @base:	ktime_t (nanoseconds) base time for readout
 * @base_real:	Nanoseconds base value for clock REALTIME readout
 *
 * This struct has size 56 byte on 64 bit. Together with a seqcount it
 * occupies a single 64byte cache line.
 *
 * The struct is separate from struct timekeeper as it is also used
 * for a fast NMI safe accessors.
 *
 * @base_real is for the fast NMI safe accessor to allow reading clock
 * realtime from any context.
 */
struct tk_read_base {
	struct clocksource	*clock;
	u64			mask;
	u64			cycle_last;
	u32			mult;
	u32			shift;
	u64			xtime_nsec;
	ktime_t			base;
	u64			base_real;
};

/**
 * struct timekeeper - Structure holding internal timekeeping values.
 * @tkr_mono:		The readout base structure for CLOCK_MONOTONIC
 * @tkr_raw:		The readout base structure for CLOCK_MONOTONIC_RAW
 * @xtime_sec:		Current CLOCK_REALTIME time in seconds
 * @ktime_sec:		Current CLOCK_MONOTONIC time in seconds
 * @wall_to_monotonic:	CLOCK_REALTIME to CLOCK_MONOTONIC offset
 * @offs_real:		Offset clock monotonic -> clock realtime
 * @offs_boot:		Offset clock monotonic -> clock boottime
 * @offs_tai:		Offset clock monotonic -> clock tai
 * @tai_offset:		The current UTC to TAI offset in seconds
 * @clock_was_set_seq:	The sequence number of clock was set events
 * @cs_was_changed_seq:	The sequence number of clocksource change events
 * @next_leap_ktime:	CLOCK_MONOTONIC time value of a pending leap-second
 * @raw_sec:		CLOCK_MONOTONIC_RAW  time in seconds
 * @cycle_interval:	Number of clock cycles in one NTP interval
 * @xtime_interval:	Number of clock shifted nano seconds in one NTP
 *			interval.
 * @xtime_remainder:	Shifted nano seconds left over when rounding
 *			@cycle_interval
 * @raw_interval:	Shifted raw nano seconds accumulated per NTP interval.
 * @ntp_error:		Difference between accumulated time and NTP time in ntp
 *			shifted nano seconds.
 * @ntp_error_shift:	Shift conversion between clock shifted nano seconds and
 *			ntp shifted nano seconds.
 * @last_warning:	Warning ratelimiter (DEBUG_TIMEKEEPING)
 * @underflow_seen:	Underflow warning flag (DEBUG_TIMEKEEPING)
 * @overflow_seen:	Overflow warning flag (DEBUG_TIMEKEEPING)
 *
 * Note: For timespec(64) based interfaces wall_to_monotonic is what
 * we need to add to xtime (or xtime corrected for sub jiffie times)
 * to get to monotonic time.  Monotonic is pegged at zero at system
 * boot time, so wall_to_monotonic will be negative, however, we will
 * ALWAYS keep the tv_nsec part positive so we can use the usual
 * normalization.
 *
 * wall_to_monotonic is moved after resume from suspend for the
 * monotonic time not to jump. We need to add total_sleep_time to
 * wall_to_monotonic to get the real boot based time offset.
 *
 * wall_to_monotonic is no longer the boot time, getboottime must be
 * used instead.
 */
struct timekeeper {
	struct tk_read_base	tkr_mono;
	struct tk_read_base	tkr_raw;
	u64			xtime_sec;
	unsigned long		ktime_sec;
	struct timespec64	wall_to_monotonic;
	ktime_t			offs_real;
	ktime_t			offs_boot;
	ktime_t			offs_tai;
	s32			tai_offset;
	unsigned int		clock_was_set_seq;
	u8			cs_was_changed_seq;
	ktime_t			next_leap_ktime;
	u64			raw_sec;

	/* The following members are for timekeeping internal use */
	u64			cycle_interval;
	u64			xtime_interval;
	s64			xtime_remainder;
	u64			raw_interval;
	/* The ntp_tick_length() value currently being used.
	 * This cached copy ensures we consistently apply the tick
	 * length for an entire tick, as ntp_tick_length may change
	 * mid-tick, and we don't want to apply that new value to
	 * the tick in progress.
	 */
	u64			ntp_tick;
	/* Difference between accumulated time and NTP time in ntp
	 * shifted nano seconds. */
	s64			ntp_error;
	u32			ntp_error_shift;
	u32			ntp_err_mult;
	/* Flag used to avoid updating NTP twice with same second */
	u32			skip_second_overflow;
#ifdef CONFIG_DEBUG_TIMEKEEPING
	long			last_warning;
	/*
	 * These simple flag variables are managed
	 * without locks, which is racy, but they are
	 * ok since we don't really care about being
	 * super precise about how many events were
	 * seen, just that a problem was observed.
	 */
	int			underflow_seen;
	int			overflow_seen;
#endif
};

#ifdef CONFIG_GENERIC_TIME_VSYSCALL

extern void update_vsyscall(struct timekeeper *tk);
extern void update_vsyscall_tz(void);

#else

static inline void update_vsyscall(struct timekeeper *tk)
{
}
static inline void update_vsyscall_tz(void)
{
}
#endif

#endif /* _LINUX_TIMEKEEPER_INTERNAL_H */