aboutsummaryrefslogtreecommitdiffstats
blob: 056da0bbda23c320f14ebe30ab565cf2eb71f5b3 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
/*
 * Copyright (c) 2020 Texas Instruments Incorporated - https://www.ti.com
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 *    Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 *    Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 *    Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
 *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
 *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
 *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
 *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
 *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
 *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
 *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
 *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
 *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 */

#ifndef __TI_RPMSG_CHAR_H__
#define __TI_RPMSG_CHAR_H__

#include <rproc_id.h>

#if defined(__cplusplus)
extern "C" {
#endif

#define RPMSG_DEV_NAME_MAXLEN	32
#define RPMSG_ADDR_ANY                  0xFFFFFFFF
#define RPMSG_RESERVED_ADDRESSES        (1024)
/*!
 * @brief Structure returned during rpmsg_char_open
 *
 * @param fd Opened file descriptor for the local rpmsg endpoint device
 * @param endpt Local Endpoint address used for receiving messages
 */
struct rpmsg_char_dev {
	int fd;
	int endpt;
};

typedef struct rpmsg_char_dev rpmsg_char_dev_t;

/*!
 *  @brief      Function to create and access a rpmsg endpoint device for a
 *              given rpmsg device
 *
 *              This function is to be used to open a communication channel
 *              in a Linux application with any rpmsg device that is bound to
 *              the Linux kernel rpmsg_chrdev driver (rpmsg_char.ko module).
 *
 *              The function returns a pointer to a rpmsg_char_dev structure
 *              with the file descriptor and local end-point address filled in
 *              and usable by an application for a given remoteproc, rpmsg
 *              device (identified by published name from remote processor) and
 *              the remote end-point address used by the rpmsg device.
 *
 *              The opened file descriptor can be used with regular file
 *              operations such as select(), read() and write() functions to
 *              wait, receive and send messages to the rpmsg device on the
 *              remote processor. The messages are received on the local
 *              end-point address.
 *
 *  @param      rproc_id remoteproc enum value identifying a remote processor.
 *                       Value is a local id used by the library
 *
 *  @param      dev_name Name of the rpmsg device name to open. Passing NULL
 *                       will use a default name "rpmsg_chrdev" for the rpmsg
 *                       devices, and identified by remote_endpt. The maximum
 *                       length for the rpmsg device name is as per the virtio
 *                       rpmsg transport, RPMSG_DEV_NAME_MAXLEN (32 bytes)
 *
 *  @param      local_endpt rpmsg local end-point address for the rpmsg device
 *                           to open. Valid value is mandatory
 *
 *  @param      remote_endpt rpmsg remote end-point address for the rpmsg device
 *                           to open. Valid value is mandatory
 *
 *  @param      eptdev_name Name used to create and identify the local endpoint
 *                          device. Needs to be unique across all the Linux
 *                          applications. The maximum length for the
 *                          eptdev_name is RPMSG_DEV_NAME_MAXLEN (32 bytes)
 *
 *  @param      flags Flags used to open the local end-point device
 *
 *  @ret        A valid pointer to a rpmsg_char_dev_t on success, NULL on
 *              failures
 *
 *  @sa         rpmsg_char_close
 */
rpmsg_char_dev_t *rpmsg_char_open(enum rproc_id id, char *dev_name,
				  int local_endpt, int remote_endpt,
				  char *eptdev_name, int flags);

/*!
 *  @brief      Function to close and delete a previously created local endpoint
 *              device with rpmsg_char_open
 *
 *              Once this function is called, any regular file operations on the
 *              underlying fd cannot be used. The pointer value is not modified
 *              within the function, but is no longer valid after a successful
 *              return.
 *
 *  @param      rcdev  Pointer to the previously created rpmsg_char_dev_t. The
 *                     handle will be unusable with any of the regular file
 *                     operation functions after a success
 *
 *  @ret        0 on success, a negative value on failure
 *
 *  @sa         rpmsg_char_open
 */
int rpmsg_char_close(rpmsg_char_dev_t *rcdev);

/*!
 *  @brief      Function to initialize the library
 *
 *              This function initializes the library after performing SoC
 *              detection and corresponding initialization. This needs to be
 *              invoked before being able to use any other function. This only
 *              needs to be invoked once in an application, there is no reference
 *              counting. The function also registers signal handlers optionally
 *              (if none are installed prior) to perform any cleanup of stale
 *              rpmsg endpoint devices during abnormal termination of
 *              applications.
 *
 *  @param      soc_name  Name of the SoC family to be used for manual detection
 *                        if kernel doesn't support a socbus device for a
 *                        particular SoC and auto detection fails. Preferred
 *                        usage is just to pass NULL
 *
 *  @ret        0 on success, 1 if already invoked previously, and a negative
 *              value on failure
 *
 *  @sa         rpmsg_char_exit
 */
int rpmsg_char_init(char *soc_name);

/*!
 *  @brief      Function to finalize the library
 *
 *              This function finalizes and performs all the de-initialization
 *              and any cleanup on the library. This is the last function that
 *              needs to be invoked after all usage is done as part of the
 *              application's cleanup. This only need to be invoked once in an
 *              application, there is no reference counting. The function also
 *              needs to be invoked in any application's signal handlers to
 *              perform the necessary cleanup of stale rpmsg endpoint devices.
 *
 *  @ret        None
 *
 *  @sa         rpmsg_char_init
 */
void rpmsg_char_exit(void);

#if defined(__cplusplus)
}
#endif

#endif /* __TI_RPMSG_CHAR_H__ */