blob: dca8a35ab24686c2b97184519bc4f1d7c5812c8a (
plain) (
tree)
|
|
#
# Freescale Kinetis KE series devices
#
source [find target/swj-dp.tcl]
if { [info exists CHIPNAME] } {
set _CHIPNAME $CHIPNAME
} else {
set _CHIPNAME ke
}
# Work-area is a space in RAM used for flash programming
# By default use 1kB
if { [info exists WORKAREASIZE] } {
set _WORKAREASIZE $WORKAREASIZE
} else {
set _WORKAREASIZE 0x400
}
if { [info exists CPUTAPID] } {
set _CPUTAPID $CPUTAPID
} else {
if { [using_jtag] } {
set _CPUTAPID 0x4ba00477
} {
set _CPUTAPID 0x2ba01477
}
}
swj_newdap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id $_CPUTAPID
set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME cortex_m -chain-position $_CHIPNAME.cpu
$_TARGETNAME configure -work-area-phys 0x20000000 -work-area-size $_WORKAREASIZE -work-area-backup 0
set _FLASHNAME $_CHIPNAME.flash
flash bank $_FLASHNAME kinetis_ke 0 0 0 0 $_TARGETNAME
adapter_khz 1000
reset_config srst_nogate
if {![using_hla]} {
# It is important that "kinetis_ke mdm check_security" is called for
# 'examine-end' event and not 'eximine-start'. Calling it in 'examine-start'
# causes "kinetis_ke mdm check_security" to fail the first time openocd
# calls it when it tries to connect after the CPU has been power-cycled.
$_CHIPNAME.cpu configure -event examine-end {
kinetis_ke mdm check_security
}
# if srst is not fitted use SYSRESETREQ to
# perform a soft reset
cortex_m reset_config sysresetreq
}
|