blob: 9cad7c492c6b2ea29a905b7dfbd48f4d439324a2 (
plain) (
tree)
|
|
# script for stm32l4x family
#
# stm32l4 devices support both JTAG and SWD transports.
#
source [find target/swj-dp.tcl]
source [find mem_helper.tcl]
if { [info exists CHIPNAME] } {
set _CHIPNAME $CHIPNAME
} else {
set _CHIPNAME stm32l4x
}
set _ENDIAN little
# Work-area is a space in RAM used for flash programming
# Smallest current target has 64kB ram, use 32kB by default to avoid surprises
if { [info exists WORKAREASIZE] } {
set _WORKAREASIZE $WORKAREASIZE
} else {
set _WORKAREASIZE 0x8000
}
#jtag scan chain
if { [info exists CPUTAPID] } {
set _CPUTAPID $CPUTAPID
} else {
if { [using_jtag] } {
# See STM Document RM0351
# Section 44.6.3 - corresponds to Cortex-M4 r0p1
set _CPUTAPID 0x4ba00477
} {
set _CPUTAPID 0x2ba01477
}
}
swj_newdap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id $_CPUTAPID
if {[using_jtag]} {
jtag newtap $_CHIPNAME bs -irlen 5
}
set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME cortex_m -endian $_ENDIAN -chain-position $_TARGETNAME
$_TARGETNAME configure -work-area-phys 0x20000000 -work-area-size $_WORKAREASIZE -work-area-backup 0
set _FLASHNAME $_CHIPNAME.flash
flash bank $_FLASHNAME stm32l4x 0 0 0 0 $_TARGETNAME
# Common knowledges tells JTAG speed should be <= F_CPU/6.
# F_CPU after reset is MSI 4MHz, so use F_JTAG = 500 kHz to stay on
# the safe side.
#
# Note that there is a pretty wide band where things are
# more or less stable, see http://openocd.zylin.com/#/c/3366/
adapter_khz 500
adapter_nsrst_delay 100
if {[using_jtag]} {
jtag_ntrst_delay 100
}
reset_config srst_nogate
if {![using_hla]} {
# if srst is not fitted use SYSRESETREQ to
# perform a soft reset
cortex_m reset_config sysresetreq
}
$_TARGETNAME configure -event reset-init {
# CPU comes out of reset with MSI_ON | MSI_RDY | MSI Range 6 (4 MHz).
# Use MSI 24 MHz clock, compliant even with VOS == 2.
# 3 WS compliant with VOS == 2 and 24 MHz.
mww 0x40022000 0x00000103 ;# FLASH_ACR = PRFTBE | 3(Latency)
mww 0x40021000 0x00000099 ;# RCC_CR = MSI_ON | MSIRGSEL| MSI Range 10
# Boost JTAG frequency
adapter_khz 4000
}
$_TARGETNAME configure -event reset-start {
# Reset clock is MSI (4 MHz)
adapter_khz 500
}
$_TARGETNAME configure -event examine-end {
# DBGMCU_CR |= DBG_STANDBY | DBG_STOP | DBG_SLEEP
mmw 0xE0042004 0x00000007 0
# Stop watchdog counters during halt
# DBGMCU_APB1_FZ |= DBG_IWDG_STOP | DBG_WWDG_STOP
mmw 0xE0042008 0x00001800 0
}
$_TARGETNAME configure -event trace-config {
# Set TRACE_IOEN; TRACE_MODE is set to async; when using sync
# change this value accordingly to configure trace pins
# assignment
mmw 0xE0042004 0x00000020 0
}
|