# Defines basic Tcl procs for OpenOCD target module proc new_target_name { } { return [target number [expr [target count] - 1 ]] } global in_process_reset set in_process_reset 0 # Catch reset recursion proc ocd_process_reset { MODE } { global in_process_reset if {$in_process_reset} { set in_process_reset 0 return -code error "'reset' can not be invoked recursively" } set in_process_reset 1 set success [expr [catch {ocd_process_reset_inner $MODE} result]==0] set in_process_reset 0 if {$success} { return $result } else { return -code error $result } } proc ocd_process_reset_inner { MODE } { set targets [target names] # If this target must be halted... set halt -1 if { 0 == [string compare $MODE halt] } { set halt 1 } if { 0 == [string compare $MODE init] } { set halt 1; } if { 0 == [string compare $MODE run ] } { set halt 0; } if { $halt < 0 } { return -code error "Invalid mode: $MODE, must be one of: halt, init, or run"; } # Target event handlers *might* change which TAPs are enabled # or disabled, so we fire all of them. But don't issue any # target "arp_*" commands, which may issue JTAG transactions, # unless we know the underlying TAP is active. # # NOTE: ARP == "Advanced Reset Process" ... "advanced" is # relative to a previous restrictive scheme foreach t $targets { # New event script. $t invoke-event reset-start } # Use TRST or TMS/TCK operations to reset all the tap controllers. # TAP reset events get reported; they might enable some taps. init_reset $MODE # Examine all targets on enabled taps. foreach t $targets { if {![using_jtag] || [jtag tapisenabled [$t cget -chain-position]]} { $t invoke-event examine-start set err [catch "$t arp_examine allow-defer"] if { $err == 0 } { $t invoke-event examine-end } } } # Assert SRST, and report the pre/post events. # Note: no target sees SRST before "pre" or after "post". foreach t $targets { $t invoke-event reset-assert-pre } foreach t $targets { # C code needs to know if we expect to 'halt' if {![using_jtag] || [jtag tapisenabled [$t cget -chain-position]]} { # TODO: Workaround for double nSRST pulse issue. The call to # init_reset above will assert and deassert nSRST. But the # steps to examine and restore debug connection only happen just # after that point. This arp_reset call will assert nSRST again # but examination will not happen again. Also, some of the events # that fire need the target scan chain to be examined. # So comment out this second nSRST assert as a quick workaround. # $t arp_reset assert $halt } } foreach t $targets { $t invoke-event reset-assert-post } # Now de-assert SRST, and report the pre/post events. # Note: no target sees !SRST before "pre" or after "post". foreach t $targets { $t invoke-event reset-deassert-pre } foreach t $targets { # Again, de-assert code needs to know if we 'halt' if {![using_jtag] || [jtag tapisenabled [$t cget -chain-position]]} { $t arp_reset deassert $halt } } foreach t $targets { $t invoke-event reset-deassert-post } # Pass 1 - Now wait for any halt (requested as part of reset # assert/deassert) to happen. Ideally it takes effect without # first executing any instructions. if { $halt } { foreach t $targets { if {[using_jtag] && ![jtag tapisenabled [$t cget -chain-position]]} { continue } # don't wait for targets where examination is deferred # they can not be halted anyway at this point if { ![$t was_examined] && [$t examine_deferred] } { continue } # Wait upto 1 second for target to halt. Why 1sec? Cause # the JTAG tap reset signal might be hooked to a slow # resistor/capacitor circuit - and it might take a while # to charge # Catch, but ignore any errors. catch { $t arp_waitstate halted 1000 } # Did we succeed? set s [$t curstate] # TODO: Workaround for targets that cannot halt while reset is # asserted. That halt during reset mechanism does not work for # all target types, yet other scripts and commands assume that # reset-halt always works. Added this bit so that failing to # halt during reset is a warning and not fatal. if { 0 != [string compare $s "halted" ] } { echo "target did not halt at reset vector" halt set s [$t curstate] } if { 0 != [string compare $s "halted" ] } { return -code error [format "TARGET: %s - Not halted" $t] } } } #Pass 2 - if needed "init" if { 0 == [string compare init $MODE] } { foreach t $targets { if {[using_jtag] && ![jtag tapisenabled [$t cget -chain-position]]} { continue } # don't wait for targets where examination is deferred # they can not be halted anyway at this point if { ![$t was_examined] && [$t examine_deferred] } { continue } set err [catch "$t arp_waitstate halted 5000"] # Did it halt? if { $err == 0 } { $t invoke-event reset-init } } } foreach t $targets { $t invoke-event reset-end } } proc using_jtag {} { set _TRANSPORT [ transport select ] expr { [ string first "jtag" $_TRANSPORT ] != -1 } } proc using_swd {} { set _TRANSPORT [ transport select ] expr { [ string first "swd" $_TRANSPORT ] != -1 } } proc using_hla {} { set _TRANSPORT [ transport select ] expr { [ string first "hla" $_TRANSPORT ] != -1 } } ######### # Temporary migration aid. May be removed starting in January 2011. proc armv4_5 params { echo "DEPRECATED! use 'arm $params' not 'armv4_5 $params'" arm $params } # Target/chain configuration scripts can either execute commands directly # or define a procedure which is executed once all configuration # scripts have completed. # # By default(classic) the config scripts will set up the target configuration proc init_targets {} { } proc set_default_target_event {t e s} { if {[$t cget -event $e] == ""} { $t configure -event $e $s } } proc init_target_events {} { set targets [target names] foreach t $targets { set_default_target_event $t gdb-flash-erase-start "reset init" set_default_target_event $t gdb-flash-write-end "reset halt" } } # Additionally board config scripts can define a procedure init_board that will be executed after init and init_targets proc init_board {} { } # deprecated target name cmds proc cortex_m3 args { echo "DEPRECATED! use 'cortex_m' not 'cortex_m3'" eval cortex_m $args } proc cortex_a8 args { echo "DEPRECATED! use 'cortex_a' not 'cortex_a8'" eval cortex_a $args }