summaryrefslogtreecommitdiffstats
blob: 6290b3a5516e2b1c4c9830faeddb84955334a7e6 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
# Defines basic Tcl procs for OpenOCD target module

proc new_target_name { } {
	return [target number [expr [target count] - 1 ]]
}

global in_process_reset
set in_process_reset 0

# Catch reset recursion
proc ocd_process_reset { MODE } {
	global in_process_reset
	if {$in_process_reset} {
		set in_process_reset 0
		return -code error "'reset' can not be invoked recursively"
	}

	set in_process_reset 1
	set success [expr [catch {ocd_process_reset_inner $MODE} result]==0]
	set in_process_reset 0

	if {$success} {
		return $result
	} else {
		return -code error $result
	}
}

proc ocd_process_reset_inner { MODE } {
	set targets [target names]

	# If this target must be halted...
	set halt -1
	if { 0 == [string compare $MODE halt] } {
		set halt 1
	}
	if { 0 == [string compare $MODE init] } {
		set halt 1;
	}
	if { 0 == [string compare $MODE run ] } {
		set halt 0;
	}
	if { $halt < 0 } {
		return -code error "Invalid mode: $MODE, must be one of: halt, init, or run";
	}

	# Target event handlers *might* change which TAPs are enabled
	# or disabled, so we fire all of them.  But don't issue any
	# target "arp_*" commands, which may issue JTAG transactions,
	# unless we know the underlying TAP is active.
	#
	# NOTE:  ARP == "Advanced Reset Process" ... "advanced" is
	# relative to a previous restrictive scheme

	foreach t $targets {
		# New event script.
		$t invoke-event reset-start
	}

	# Use TRST or TMS/TCK operations to reset all the tap controllers.
	# TAP reset events get reported; they might enable some taps.
	init_reset $MODE

	# Examine all targets on enabled taps.
	foreach t $targets {
		if {![using_jtag] || [jtag tapisenabled [$t cget -chain-position]]} {
			$t invoke-event examine-start
			set err [catch "$t arp_examine allow-defer"]
			if { $err == 0 } {
				$t invoke-event examine-end
			}
		}
	}

	# Assert SRST, and report the pre/post events.
	# Note:  no target sees SRST before "pre" or after "post".
	foreach t $targets {
		$t invoke-event reset-assert-pre
	}
	foreach t $targets {
		# C code needs to know if we expect to 'halt'
		if {![using_jtag] || [jtag tapisenabled [$t cget -chain-position]]} {
			# TODO: Workaround for double nSRST pulse issue. The call to 
			# init_reset above will assert and deassert nSRST. But the 
			# steps to examine and restore debug connection only happen just
			# after that point. This arp_reset call will assert nSRST again
			# but examination will not happen again. Also, some of the events
			# that fire need the target scan chain to be examined.
			# So comment out this second nSRST assert as a quick workaround.
			# $t arp_reset assert $halt
		}
	}
	foreach t $targets {
		$t invoke-event reset-assert-post
	}

	# Now de-assert SRST, and report the pre/post events.
	# Note:  no target sees !SRST before "pre" or after "post".
	foreach t $targets {
		$t invoke-event reset-deassert-pre
	}
	foreach t $targets {
		# Again, de-assert code needs to know if we 'halt'
		if {![using_jtag] || [jtag tapisenabled [$t cget -chain-position]]} {
			$t arp_reset deassert $halt
		}
	}
	foreach t $targets {
		$t invoke-event reset-deassert-post
	}

	# Pass 1 - Now wait for any halt (requested as part of reset
	# assert/deassert) to happen.  Ideally it takes effect without
	# first executing any instructions.
	if { $halt } {
		foreach t $targets {
			if {[using_jtag] && ![jtag tapisenabled [$t cget -chain-position]]} {
				continue
			}

			# don't wait for targets where examination is deferred
			# they can not be halted anyway at this point
			if { ![$t was_examined] && [$t examine_deferred] } {
				continue
			}

			# Wait upto 1 second for target to halt.  Why 1sec? Cause
			# the JTAG tap reset signal might be hooked to a slow
			# resistor/capacitor circuit - and it might take a while
			# to charge

			# Catch, but ignore any errors.
			catch { $t arp_waitstate halted 1000 }

			# Did we succeed?
			set s [$t curstate]

			# TODO: Workaround for targets that cannot halt while reset is
			# asserted. That halt during reset mechanism does not work for
			# all target types, yet other scripts and commands assume that
			# reset-halt always works.  Added this bit so that failing to
			# halt during reset is a warning and not fatal.
			if { 0 != [string compare $s "halted" ] } {
				echo "target did not halt at reset vector"
				halt
				set s [$t curstate]
			}

			if { 0 != [string compare $s "halted" ] } {
				return -code error [format "TARGET: %s - Not halted" $t]
			}
		}
	}

	#Pass 2 - if needed "init"
	if { 0 == [string compare init $MODE] } {
		foreach t $targets {
			if {[using_jtag] && ![jtag tapisenabled [$t cget -chain-position]]} {
				continue
			}

			# don't wait for targets where examination is deferred
			# they can not be halted anyway at this point
			if { ![$t was_examined] && [$t examine_deferred] } {
				continue
			}

			set err [catch "$t arp_waitstate halted 5000"]
			# Did it halt?
			if { $err == 0 } {
				$t invoke-event reset-init
			}
		}
	}

	foreach t $targets {
		$t invoke-event reset-end
	}
}

proc using_jtag {} {
	set _TRANSPORT [ transport select ]
	expr { [ string first "jtag" $_TRANSPORT ] != -1 }
}

proc using_swd {} {
	set _TRANSPORT [ transport select ]
	expr { [ string first "swd" $_TRANSPORT ] != -1 }
}

proc using_hla {} {
	set _TRANSPORT [ transport select ]
	expr { [ string first "hla" $_TRANSPORT ] != -1 }
}

#########

# Temporary migration aid.  May be removed starting in January 2011.
proc armv4_5 params {
	echo "DEPRECATED! use 'arm $params' not 'armv4_5 $params'"
	arm $params
}

# Target/chain configuration scripts can either execute commands directly
# or define a procedure which is executed once all configuration
# scripts have completed.
#
# By default(classic) the config scripts will set up the target configuration
proc init_targets {} {
}

proc set_default_target_event {t e s} {
	if {[$t cget -event $e] == ""} {
		$t configure -event $e $s
	}
}

proc init_target_events {} {
	set targets [target names]

	foreach t $targets {
		set_default_target_event $t gdb-flash-erase-start "reset init"
		set_default_target_event $t gdb-flash-write-end "reset halt"
	}
}

# Additionally board config scripts can define a procedure init_board that will be executed after init and init_targets
proc init_board {} {
}

# deprecated target name cmds
proc cortex_m3 args {
	echo "DEPRECATED! use 'cortex_m' not 'cortex_m3'"
	eval cortex_m $args
}

proc cortex_a8 args {
	echo "DEPRECATED! use 'cortex_a' not 'cortex_a8'"
	eval cortex_a $args
}