blob: c00dae921c49d79054691fede6f4d7450823e4e6 (
plain) (
blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
|
#
# Copyright (C) 2010-2011 by Karl Kurbjun
# Copyright (C) 2009-2011 by Øyvind Harboe
# Copyright (C) 2009 by David Brownell
# Copyright (C) 2009 by Magnus Lundin
#
# TI AM/DM37x Technical Reference Manual (Version R)
# http://www.ti.com/lit/ug/sprugn4r/sprugn4r.pdf
#
# This script is based on the AM3517 initialization. It should be considered
# preliminary since it needs more complete testing and only the basic
# operations work.
#
###############################################################################
# User modifiable parameters
###############################################################################
# This script uses the variable CHIPTYPE to determine whether this is an AM35x
# or DM37x target. If CHIPTYPE is not set it will error out.
if { [info exists CHIPTYPE] } {
if { [info exists CHIPNAME] } {
set _CHIPNAME $CHIPNAME
} else {
set _CHIPNAME $CHIPTYPE
}
switch $CHIPTYPE {
dm37x {
# Primary TAP: ICEPick-C (JTAG route controller) and boundary scan
set _JRC_TAPID "-expected-id 0x2b89102f -expected-id 0x1b89102f -expected-id 0x0b89102f"
}
am35x {
# Primary TAP: ICEPick-C (JTAG route controller) and boundary scan
set _JRC_TAPID "-expected-id 0x0b7ae02f -expected-id 0x0b86802f"
}
default {
error "ERROR: CHIPTYPE was set, but it was not set to a valid value. Acceptable values are \"dm37x\" or \"am35x\"."
}
}
} else {
error "ERROR: CHIPTYPE was not defined. Please set CHIPTYPE to \"am35x\" for the AM35x or \"dm37x\" for the DM37x series in the board configuration."
}
# Run the adapter at the fastest acceptable speed with the slowest possible
# core clock.
adapter_khz 10
###############################################################################
# JTAG setup
# The OpenOCD commands are described in the TAP Declaration section
# http://openocd.org/doc/html/TAP-Declaration.html
###############################################################################
# The AM/DM37x has an ICEPick module in it like many of TI's other devices. More
# can be read about this module in sprugn4r in chapter 27: "Debug and
# Emulation". The module is used to route the JTAG chain to the various
# subsystems in the chip.
source [find target/icepick.cfg]
# The TAP order should be described from the TDO connection in OpenOCD to the
# TDI pin. The OpenOCD FAQ describes this in more detail:
# http://openocd.org/doc/html/FAQ.html
# From SPRUGN4R CH27 the available secondary TAPs are in this order from TDO:
#
# Device | TAP number
# ---------|------------
# DAP | 3
# Sequencer| 2 Note: The sequencer is an ARM968
# DSP | 1
# D2D | 0
#
# Right now the only secondary tap enabled is the DAP so the rest are left
# undescribed.
######
# Start of Chain Description
# The Secondary TAPs all have enable functions defined for use with the ICEPick
# Only the DAP is enabled. The AM37xx does not have the Sequencer or DSP but
# the TAP numbers for ICEPick do not change.
#
# TODO: A disable function should also be added.
######
# Secondary TAP: DAP is closest to the TDO output
# The TAP enable event also needs to be described
jtag newtap $_CHIPNAME dap -irlen 4 -ircapture 0x1 -irmask 0xf -disable
jtag configure $_CHIPNAME.dap -event tap-enable \
"icepick_c_tapenable $_CHIPNAME.jrc 3"
# These taps are only present in the DM37x series.
if { $CHIPTYPE == "dm37x" } {
# Secondary TAP: Sequencer (ARM968) it is not in the chain by default
# The ICEPick can be used to enable it in the chain.
jtag newtap $_CHIPNAME arm2 -irlen 4 -ircapture 0x1 -irmask 0x0f -disable
jtag configure $_CHIPNAME.arm2 -event tap-enable \
"icepick_c_tapenable $_CHIPNAME.jrc 2"
# Secondary TAP: C64x+ DSP - it is not in the chain by default (-disable)
# The ICEPick can be used to enable it in the chain.
jtag newtap $_CHIPNAME dsp -irlen 38 -ircapture 0x25 -irmask 0x3f -disable
jtag configure $_CHIPNAME.dsp -event tap-enable \
"icepick_c_tapenable $_CHIPNAME.jrc 1"
}
# Secondary TAP: D2D it is not in the chain by default (-disable)
# The ICEPick can be used to enable it in the chain.
# This IRLEN is probably incorrect - not sure where the documentation is.
jtag newtap $_CHIPNAME d2d -irlen 4 -ircapture 0x1 -irmask 0x0f -disable
jtag configure $_CHIPNAME.d2d -event tap-enable \
"icepick_c_tapenable $_CHIPNAME.jrc 0"
# Primary TAP: ICEPick - it is closest to TDI so last in the chain
eval "jtag newtap $_CHIPNAME jrc -irlen 6 -ircapture 0x1 -irmask 0x3f $_JRC_TAPID"
######
# End of Chain Description
######
######
# Start JTAG TAP events
######
# some TCK tycles are required to activate the DEBUG power domain
jtag configure $_CHIPNAME.jrc -event post-reset "runtest 100"
# Enable the DAP TAP
jtag configure $_CHIPNAME.jrc -event setup "jtag tapenable $_CHIPNAME.dap"
######
# End JTAG TAP events
######
###############################################################################
# Target Setup:
# This section is described in the OpenOCD documentation under CPU Configuration
# http://openocd.org/doc/html/CPU-Configuration.html
###############################################################################
# Create the CPU target to be used with GDB: Cortex-A8, using DAP
set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME cortex_a -chain-position $_CHIPNAME.dap
# The DM37x has 64K of SRAM starting at address 0x4020_0000. Allow the first
# 16K to be used as a scratchpad for OpenOCD.
$_TARGETNAME configure -work-area-phys 0x40200000 -work-area-size 0x4000
######
# Start Target Reset Event Setup:
######
# Set the JTAG clock down to 10 kHz to be sure that it will work with the
# slowest possible core clock (16.8MHz/2 = 8.4MHz). It is OK to speed up
# *after* PLL and clock tree setup.
$_TARGETNAME configure -event "reset-start" { adapter_khz 10 }
# Describe the reset assert process for openocd - this is asserted with the
# ICEPick
$_TARGETNAME configure -event "reset-assert" {
global _CHIPNAME
# assert warm system reset through ICEPick
icepick_c_wreset $_CHIPNAME.jrc
}
# After the reset is asserted we need to re-initialize debugging and speed up
# the JTAG clock.
$_TARGETNAME configure -event reset-assert-post {
global _TARGETNAME
amdm37x_dbginit $_TARGETNAME
adapter_khz 1000
}
$_TARGETNAME configure -event gdb-attach {
global _TARGETNAME
amdm37x_dbginit $_TARGETNAME
echo "Halting target"
halt
}
######
# End Target Reset Event Setup:
######
###############################################################################
# Target Functions
# Add any functions needed for the target here
###############################################################################
# Run this to enable invasive debugging. This is run automatically in the
# reset sequence.
proc amdm37x_dbginit {target} {
# General Cortex-A8 debug initialisation
cortex_a dbginit
# Enable DBGEN signal. This signal is described in the ARM v7 TRM, but
# access to the signal appears to be implementation specific. TI does not
# describe this register much except a quick line that states DBGEM (sic) is
# at this address and this bit.
$target mww phys 0x5401d030 0x00002000
}
|