diff options
Diffstat (limited to 'assets/help_device.html')
-rw-r--r-- | assets/help_device.html | 36 |
1 files changed, 36 insertions, 0 deletions
diff --git a/assets/help_device.html b/assets/help_device.html new file mode 100644 index 0000000..5df5156 --- /dev/null +++ b/assets/help_device.html | |||
@@ -0,0 +1,36 @@ | |||
1 | <!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.01 Transitional//EN"> | ||
2 | <!-- ********************************************************* | ||
3 | ** File : help_device.html | ||
4 | ** Descr. : Help for device view | ||
5 | **** ****************************************************** --> | ||
6 | <html> | ||
7 | <head> | ||
8 | <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> | ||
9 | <meta HTTP-EQUIV="Pragma" CONTENT="no-cache" /> | ||
10 | <meta HTTP-EQUIV="Cache-Control" CONTENT="no-cache" /> | ||
11 | <meta HTTP-EQUIV="expires" CONTENT="0"> | ||
12 | <meta name="Author" content="Texas Instruments" /> | ||
13 | <title>BLE Device Monitor</title> | ||
14 | <link rel="stylesheet" type="text/css" href="help.css"> | ||
15 | </head> | ||
16 | |||
17 | <body> | ||
18 | <div class="main"> | ||
19 | <h1>Sensor View Help</h1> | ||
20 | <p>When the view is started a <b>Service Discovery</b> is initiated. On <b>Service Discovery</b> completion (may take a few seconds), | ||
21 | sensor images appear and data is displayed next to them. The <b>Preferences</b> tab in the options menu can be used to select <i>which</i> sensors | ||
22 | to show. Note that a maximum of four sensors may be activated per connection instance due to a limitation in Android's Bluetooth low energy stack on the number of | ||
23 | notifications.</p> | ||
24 | <p>Note that magnetometer, gyroscope and height measurement (barometer) are calibrated by tapping on the respective entry in the sensor list. The measured height shown | ||
25 | is calculated based on the difference in air pressure between the current measurement and the pressure at the moment of calibration. Measurements are always calibrated | ||
26 | on connection (but may be re-calibrated any time).</p> | ||
27 | <p>The SensorTag firmware can be upgraded OTA (Over The Air) via <b>Firmware Update</b> in the Options Menu. The application will contain images for the latest firmware, | ||
28 | but it is also possible to download custom images from Android's 'Download' directory. There are | ||
29 | two FW images for each FW revision. These are labeled <q>A</q> and <q>B</q> and differ only by the destination address in the | ||
30 | SensorTag flash. Alternative images must always be used; if the current image in flash is of type <q>A</q> the new one must of type | ||
31 | <q>B</q> and vice versa.<hr /> | ||
32 | <p class="copy">© 2013-2014 Texas Instruments</p> | ||
33 | </div> | ||
34 | </body> | ||
35 | </html> | ||
36 | |||