/*
* linux/cgroup-defs.h - basic definitions for cgroup
*
* This file provides basic type and interface. Include this file directly
* only if necessary to avoid cyclic dependencies.
*/
#ifndef _LINUX_CGROUP_DEFS_H
#define _LINUX_CGROUP_DEFS_H
#include <linux/limits.h>
#include <linux/list.h>
#include <linux/idr.h>
#include <linux/wait.h>
#include <linux/mutex.h>
#include <linux/rcupdate.h>
#include <linux/percpu-refcount.h>
#include <linux/percpu-rwsem.h>
#include <linux/workqueue.h>
#ifdef CONFIG_CGROUPS
struct cgroup;
struct cgroup_root;
struct cgroup_subsys;
struct cgroup_taskset;
struct kernfs_node;
struct kernfs_ops;
struct kernfs_open_file;
struct seq_file;
#define MAX_CGROUP_TYPE_NAMELEN 32
#define MAX_CGROUP_ROOT_NAMELEN 64
#define MAX_CFTYPE_NAME 64
/* define the enumeration of all cgroup subsystems */
#define SUBSYS(_x) _x ## _cgrp_id,
#define SUBSYS_TAG(_t) CGROUP_ ## _t, \
__unused_tag_ ## _t = CGROUP_ ## _t - 1,
enum cgroup_subsys_id {
#include <linux/cgroup_subsys.h>
CGROUP_SUBSYS_COUNT,
};
#undef SUBSYS_TAG
#undef SUBSYS
#define CGROUP_CANFORK_COUNT (CGROUP_CANFORK_END - CGROUP_CANFORK_START)
/* bits in struct cgroup_subsys_state flags field */
enum {
CSS_NO_REF = (1 << 0), /* no reference counting for this css */
CSS_ONLINE = (1 << 1), /* between ->css_online() and ->css_offline() */
CSS_RELEASED = (1 << 2), /* refcnt reached zero, released */
};
/* bits in struct cgroup flags field */
enum {
/* Control Group requires release notifications to userspace */
CGRP_NOTIFY_ON_RELEASE,
/*
* Clone the parent's configuration when creating a new child
* cpuset cgroup. For historical reasons, this option can be
* specified at mount time and thus is implemented here.
*/
CGRP_CPUSET_CLONE_CHILDREN,
};
/* cgroup_root->flags */
enum {
CGRP_ROOT_NOPREFIX = (1 << 1), /* mounted subsystems have no named prefix */
CGRP_ROOT_XATTR = (1 << 2), /* supports extended attributes */
};
/* cftype->flags */
enum {
CFTYPE_ONLY_ON_ROOT = (1 << 0), /* only create on root cgrp */
CFTYPE_NOT_ON_ROOT = (1 << 1), /* don't create on root cgrp */
CFTYPE_NO_PREFIX = (1 << 3), /* (DON'T USE FOR NEW FILES) no subsys prefix */
CFTYPE_WORLD_WRITABLE = (1 << 4), /* (DON'T USE FOR NEW FILES) S_IWUGO */
/* internal flags, do not use outside cgroup core proper */
__CFTYPE_ONLY_ON_DFL = (1 << 16), /* only on default hierarchy */
__CFTYPE_NOT_ON_DFL = (1 << 17), /* not on default hierarchy */
};
/*
* cgroup_file is the handle for a file instance created in a cgroup which
* is used, for example, to generate file changed notifications. This can
* be obtained by setting cftype->file_offset.
*/
struct cgroup_file {
/* do not access any fields from outside cgroup core */
struct kernfs_node *kn;
};
/*
* Per-subsystem/per-cgroup state maintained by the system. This is the
* fundamental structural building block that controllers deal with.
*
* Fields marked with "PI:" are public and immutable and may be accessed
* directly without synchronization.
*/
struct cgroup_subsys_state {
/* PI: the cgroup that this css is attached to */
struct cgroup *cgroup;
/* PI: the cgroup subsystem that this css is attached to */
struct cgroup_subsys *ss;
/* reference count - access via css_[try]get() and css_put() */
struct percpu_ref refcnt;
/* PI: the parent css */
struct cgroup_subsys_state *parent;
/* siblings list anchored at the parent's ->children */
struct list_head sibling;
struct list_head children;
/*
* PI: Subsys-unique ID. 0 is unused and root is always 1. The
* matching css can be looked up using css_from_id().
*/
int id;
unsigned int flags;
/*
* Monotonically increasing unique serial number which defines a
* uniform order among all csses. It's guaranteed that all
* ->children lists are in the ascending order of ->serial_nr and
* used to allow interrupting and resuming iterations.
*/
u64 serial_nr;
/*
* Incremented by online self and children. Used to guarantee that
* parents are not offlined before their children.
*/
atomic_t online_cnt;
/* percpu_ref killing and RCU release */
struct rcu_head rcu_head;
struct work_struct destroy_work;
};
/*
* A css_set is a structure holding pointers to a set of
* cgroup_subsys_state objects. This saves space in the task struct
* object and speeds up fork()/exit(), since a single inc/dec and a
* list_add()/del() can bump the reference count on the entire cgroup
* set for a task.
*/
struct css_set {
/* Reference count */
atomic_t refcount;
/*
* List running through all cgroup groups in the same hash
* slot. Protected by css_set_lock
*/
struct hlist_node hlist;
/*
* Lists running through all tasks using this cgroup group.
* mg_tasks lists tasks which belong to this cset but are in the
* process of being migrated out or in. Protected by
* css_set_rwsem, but, during migration, once tasks are moved to
* mg_tasks, it can be read safely while holding cgroup_mutex.
*/
struct list_head tasks;
struct list_head mg_tasks;
/*
* List of cgrp_cset_links pointing at cgroups referenced from this
* css_set. Protected by css_set_lock.
*/
struct list_head cgrp_links;
/* the default cgroup associated with this css_set */
struct cgroup *dfl_cgrp;
/*
* Set of subsystem states, one for each subsystem. This array is
* immutable after creation apart from the init_css_set during
* subsystem registration (at boot time).
*/
struct cgroup_subsys_state *subsys[CGROUP_SUBSYS_COUNT];
/*
* List of csets participating in the on-going migration either as
* source or destination. Protected by cgroup_mutex.
*/
struct list_head mg_preload_node;
struct list_head mg_node;
/*
* If this cset is acting as the source of migration the following
* two fields are set. mg_src_cgrp is the source cgroup of the
* on-going migration and mg_dst_cset is the destination cset the
* target tasks on this cset should be migrated to. Protected by
* cgroup_mutex.
*/
struct cgroup *mg_src_cgrp;
struct css_set *mg_dst_cset;
/*
* On the default hierarhcy, ->subsys[ssid] may point to a css
* attached to an ancestor instead of the cgroup this css_set is
* associated with. The following node is anchored at
* ->subsys[ssid]->cgroup->e_csets[ssid] and provides a way to
* iterate through all css's attached to a given cgroup.
*/
struct list_head e_cset_node[CGROUP_SUBSYS_COUNT];
/* all css_task_iters currently walking this cset */
struct list_head task_iters;
/* For RCU-protected deletion */
struct rcu_head rcu_head;
};
struct cgroup {
/* self css with NULL ->ss, points back to this cgroup */
struct cgroup_subsys_state self;
unsigned long flags; /* "unsigned long" so bitops work */
/*
* idr allocated in-hierarchy ID.
*
* ID 0 is not used, the ID of the root cgroup is always 1, and a
* new cgroup will be assigned with a smallest available ID.
*
* Allocating/Removing ID must be protected by cgroup_mutex.
*/
int id;
/*
* Each non-empty css_set associated with this cgroup contributes
* one to populated_cnt. All children with non-zero popuplated_cnt
* of their own contribute one. The count is zero iff there's no
* task in this cgroup or its subtree.
*/
int populated_cnt;
struct kernfs_node *kn; /* cgroup kernfs entry */
struct cgroup_file procs_file; /* handle for "cgroup.procs" */
struct cgroup_file events_file; /* handle for "cgroup.events" */
/*
* The bitmask of subsystems enabled on the child cgroups.
* ->subtree_control is the one configured through
* "cgroup.subtree_control" while ->child_subsys_mask is the
* effective one which may have more subsystems enabled.
* Controller knobs are made available iff it's enabled in
* ->subtree_control.
*/
unsigned int subtree_control;
unsigned int child_subsys_mask;
/* Private pointers for each registered subsystem */
struct cgroup_subsys_state __rcu *subsys[CGROUP_SUBSYS_COUNT];
struct cgroup_root *root;
/*
* List of cgrp_cset_links pointing at css_sets with tasks in this
* cgroup. Protected by css_set_lock.
*/
struct list_head cset_links;
/*
* On the default hierarchy, a css_set for a cgroup with some
* susbsys disabled will point to css's which are associated with
* the closest ancestor which has the subsys enabled. The
* following lists all css_sets which point to this cgroup's css
* for the given subsystem.
*/
struct list_head e_csets[CGROUP_SUBSYS_COUNT];
/*
* list of pidlists, up to two for each namespace (one for procs, one
* for tasks); created on demand.
*/
struct list_head pidlists;
struct mutex pidlist_mutex;
/* used to wait for offlining of csses */
wait_queue_head_t offline_waitq;
/* used to schedule release agent */
struct work_struct release_agent_work;
};
/*
* A cgroup_root represents the root of a cgroup hierarchy, and may be
* associated with a kernfs_root to form an active hierarchy. This is
* internal to cgroup core. Don't access directly from controllers.
*/
struct cgroup_root {
struct kernfs_root *kf_root;
/* The bitmask of subsystems attached to this hierarchy */
unsigned int subsys_mask;
/* Unique id for this hierarchy. */
int hierarchy_id;
/* The root cgroup. Root is destroyed on its release. */
struct cgroup cgrp;
/* Number of cgroups in the hierarchy, used only for /proc/cgroups */
atomic_t nr_cgrps;
/* A list running through the active hierarchies */
struct list_head root_list;
/* Hierarchy-specific flags */
unsigned int flags;
/* IDs for cgroups in this hierarchy */
struct idr cgroup_idr;
/* The path to use for release notifications. */
char release_agent_path[PATH_MAX];
/* The name for this hierarchy - may be empty */
char name[MAX_CGROUP_ROOT_NAMELEN];
};
/*
* struct cftype: handler definitions for cgroup control files
*
* When reading/writing to a file:
* - the cgroup to use is file->f_path.dentry->d_parent->d_fsdata
* - the 'cftype' of the file is file->f_path.dentry->d_fsdata
*/
struct cftype {
/*
* By convention, the name should begin with the name of the
* subsystem, followed by a period. Zero length string indicates
* end of cftype array.
*/
char name[MAX_CFTYPE_NAME];
unsigned long private;
/*
* The maximum length of string, excluding trailing nul, that can
* be passed to write. If < PAGE_SIZE-1, PAGE_SIZE-1 is assumed.
*/
size_t max_write_len;
/* CFTYPE_* flags */
unsigned int flags;
/*
* If non-zero, should contain the offset from the start of css to
* a struct cgroup_file field. cgroup will record the handle of
* the created file into it. The recorded handle can be used as
* long as the containing css remains accessible.
*/
unsigned int file_offset;
/*
* Fields used for internal bookkeeping. Initialized automatically
* during registration.
*/
struct cgroup_subsys *ss; /* NULL for cgroup core files */
struct list_head node; /* anchored at ss->cfts */
struct kernfs_ops *kf_ops;
/*
* read_u64() is a shortcut for the common case of returning a
* single integer. Use it in place of read()
*/
u64 (*read_u64)(struct cgroup_subsys_state *css, struct cftype *cft);
/*
* read_s64() is a signed version of read_u64()
*/
s64 (*read_s64)(struct cgroup_subsys_state *css, struct cftype *cft);
/* generic seq_file read interface */
int (*seq_show)(struct seq_file *sf, void *v);
/* optional ops, implement all or none */
void *(*seq_start)(struct seq_file *sf, loff_t *ppos);
void *(*seq_next)(struct seq_file *sf, void *v, loff_t *ppos);
void (*seq_stop)(struct seq_file *sf, void *v);
/*
* write_u64() is a shortcut for the common case of accepting
* a single integer (as parsed by simple_strtoull) from
* userspace. Use in place of write(); return 0 or error.
*/
int (*write_u64)(struct cgroup_subsys_state *css, struct cftype *cft,
u64 val);
/*
* write_s64() is a signed version of write_u64()
*/
int (*write_s64)(struct cgroup_subsys_state *css, struct cftype *cft,
s64 val);
/*
* write() is the generic write callback which maps directly to
* kernfs write operation and overrides all other operations.
* Maximum write size is determined by ->max_write_len. Use
* of_css/cft() to access the associated css and cft.
*/
ssize_t (*write)(struct kernfs_open_file *of,
char *buf, size_t nbytes, loff_t off);
#ifdef CONFIG_DEBUG_LOCK_ALLOC
struct lock_class_key lockdep_key;
#endif
};
/*
* Control Group subsystem type.
* See Documentation/cgroups/cgroups.txt for details
*/
struct cgroup_subsys {
struct cgroup_subsys_state *(*css_alloc)(struct cgroup_subsys_state *parent_css);
int (*css_online)(struct cgroup_subsys_state *css);
void (*css_offline)(struct cgroup_subsys_state *css);
void (*css_released)(struct cgroup_subsys_state *css);
void (*css_free)(struct cgroup_subsys_state *css);
void (*css_reset)(struct cgroup_subsys_state *css);
void (*css_e_css_changed)(struct cgroup_subsys_state *css);
int (*can_attach)(struct cgroup_taskset *tset);
void (*cancel_attach)(struct cgroup_taskset *tset);
void (*attach)(struct cgroup_taskset *tset);
int (*can_fork)(struct task_struct *task, void **priv_p);
void (*cancel_fork)(struct task_struct *task, void *priv);
void (*fork)(struct task_struct *task, void *priv);
void (*exit)(struct task_struct *task);
void (*free)(struct task_struct *task);
void (*bind)(struct cgroup_subsys_state *root_css);
int early_init;
/*
* If %false, this subsystem is properly hierarchical -
* configuration, resource accounting and restriction on a parent
* cgroup cover those of its children. If %true, hierarchy support
* is broken in some ways - some subsystems ignore hierarchy
* completely while others are only implemented half-way.
*
* It's now disallowed to create nested cgroups if the subsystem is
* broken and cgroup core will emit a warning message on such
* cases. Eventually, all subsystems will be made properly
* hierarchical and this will go away.
*/
bool broken_hierarchy;
bool warned_broken_hierarchy;
/* the following two fields are initialized automtically during boot */
int id;
const char *name;
/* optional, initialized automatically during boot if not set */
const char *legacy_name;
/* link to parent, protected by cgroup_lock() */
struct cgroup_root *root;
/* idr for css->id */
struct idr css_idr;
/*
* List of cftypes. Each entry is the first entry of an array
* terminated by zero length name.
*/
struct list_head cfts;
/*
* Base cftypes which are automatically registered. The two can
* point to the same array.
*/
struct cftype *dfl_cftypes; /* for the default hierarchy */
struct cftype *legacy_cftypes; /* for the legacy hierarchies */
/*
* A subsystem may depend on other subsystems. When such subsystem
* is enabled on a cgroup, the depended-upon subsystems are enabled
* together if available. Subsystems enabled due to dependency are
* not visible to userland until explicitly enabled. The following
* specifies the mask of subsystems that this one depends on.
*/
unsigned int depends_on;
};
extern struct percpu_rw_semaphore cgroup_threadgroup_rwsem;
/**
* cgroup_threadgroup_change_begin - threadgroup exclusion for cgroups
* @tsk: target task
*
* Called from threadgroup_change_begin() and allows cgroup operations to
* synchronize against threadgroup changes using a percpu_rw_semaphore.
*/
static inline void cgroup_threadgroup_change_begin(struct task_struct *tsk)
{
percpu_down_read(&cgroup_threadgroup_rwsem);
}
/**
* cgroup_threadgroup_change_end - threadgroup exclusion for cgroups
* @tsk: target task
*
* Called from threadgroup_change_end(). Counterpart of
* cgroup_threadcgroup_change_begin().
*/
static inline void cgroup_threadgroup_change_end(struct task_struct *tsk)
{
percpu_up_read(&cgroup_threadgroup_rwsem);
}
#else /* CONFIG_CGROUPS */
#define CGROUP_CANFORK_COUNT 0
#define CGROUP_SUBSYS_COUNT 0
static inline void cgroup_threadgroup_change_begin(struct task_struct *tsk) {}
static inline void cgroup_threadgroup_change_end(struct task_struct *tsk) {}
#endif /* CONFIG_CGROUPS */
#endif /* _LINUX_CGROUP_DEFS_H */