#ifndef __LINUX_DCACHE_H
#define __LINUX_DCACHE_H
#include <linux/atomic.h>
#include <linux/list.h>
#include <linux/rculist.h>
#include <linux/rculist_bl.h>
#include <linux/spinlock.h>
#include <linux/seqlock.h>
#include <linux/cache.h>
#include <linux/rcupdate.h>
#include <linux/lockref.h>
struct path;
struct vfsmount;
/*
* linux/include/linux/dcache.h
*
* Dirent cache data structures
*
* (C) Copyright 1997 Thomas Schoebel-Theuer,
* with heavy changes by Linus Torvalds
*/
#define IS_ROOT(x) ((x) == (x)->d_parent)
/* The hash is always the low bits of hash_len */
#ifdef __LITTLE_ENDIAN
#define HASH_LEN_DECLARE u32 hash; u32 len;
#define bytemask_from_count(cnt) (~(~0ul << (cnt)*8))
#else
#define HASH_LEN_DECLARE u32 len; u32 hash;
#define bytemask_from_count(cnt) (~(~0ul >> (cnt)*8))
#endif
/*
* "quick string" -- eases parameter passing, but more importantly
* saves "metadata" about the string (ie length and the hash).
*
* hash comes first so it snuggles against d_parent in the
* dentry.
*/
struct qstr {
union {
struct {
HASH_LEN_DECLARE;
};
u64 hash_len;
};
const unsigned char *name;
};
#define QSTR_INIT(n,l) { { { .len = l } }, .name = n }
#define hashlen_hash(hashlen) ((u32) (hashlen))
#define hashlen_len(hashlen) ((u32)((hashlen) >> 32))
#define hashlen_create(hash,len) (((u64)(len)<<32)|(u32)(hash))
struct dentry_stat_t {
long nr_dentry;
long nr_unused;
long age_limit; /* age in seconds */
long want_pages; /* pages requested by system */
long dummy[2];
};
extern struct dentry_stat_t dentry_stat;
/* Name hashing routines. Initial hash value */
/* Hash courtesy of the R5 hash in reiserfs modulo sign bits */
#define init_name_hash() 0
/* partial hash update function. Assume roughly 4 bits per character */
static inline unsigned long
partial_name_hash(unsigned long c, unsigned long prevhash)
{
return (prevhash + (c << 4) + (c >> 4)) * 11;
}
/*
* Finally: cut down the number of bits to a int value (and try to avoid
* losing bits)
*/
static inline unsigned long end_name_hash(unsigned long hash)
{
return (unsigned int) hash;
}
/* Compute the hash for a name string. */
extern unsigned int full_name_hash(const unsigned char *, unsigned int);
/*
* Try to keep struct dentry aligned on 64 byte cachelines (this will
* give reasonable cacheline footprint with larger lines without the
* large memory footprint increase).
*/
#ifdef CONFIG_64BIT
# define DNAME_INLINE_LEN 32 /* 192 bytes */
#else
# ifdef CONFIG_SMP
# define DNAME_INLINE_LEN 36 /* 128 bytes */
# else
# define DNAME_INLINE_LEN 40 /* 128 bytes */
# endif
#endif
#define d_lock d_lockref.lock
struct dentry {
/* RCU lookup touched fields */
unsigned int d_flags; /* protected by d_lock */
seqcount_t d_seq; /* per dentry seqlock */
struct hlist_bl_node d_hash; /* lookup hash list */
struct dentry *d_parent; /* parent directory */
struct qstr d_name;
struct inode *d_inode; /* Where the name belongs to - NULL is
* negative */
unsigned char d_iname[DNAME_INLINE_LEN]; /* small names */
/* Ref lookup also touches following */
struct lockref d_lockref; /* per-dentry lock and refcount */
const struct dentry_operations *d_op;
struct super_block *d_sb; /* The root of the dentry tree */
unsigned long d_time; /* used by d_revalidate */
void *d_fsdata; /* fs-specific data */
struct list_head d_lru; /* LRU list */
struct list_head d_child; /* child of parent list */
struct list_head d_subdirs; /* our children */
/*
* d_alias and d_rcu can share memory
*/
union {
struct hlist_node d_alias; /* inode alias list */
struct rcu_head d_rcu;
} d_u;
};
/*
* dentry->d_lock spinlock nesting subclasses:
*
* 0: normal
* 1: nested
*/
enum dentry_d_lock_class
{
DENTRY_D_LOCK_NORMAL, /* implicitly used by plain spin_lock() APIs. */
DENTRY_D_LOCK_NESTED
};
struct dentry_operations {
int (*d_revalidate)(struct dentry *, unsigned int);
int (*d_weak_revalidate)(struct dentry *, unsigned int);
int (*d_hash)(const struct dentry *, struct qstr *);
int (*d_compare)(const struct dentry *, const struct dentry *,
unsigned int, const char *, const struct qstr *);
int (*d_delete)(const struct dentry *);
void (*d_release)(struct dentry *);
void (*d_prune)(struct dentry *);
void (*d_iput)(struct dentry *, struct inode *);
char *(*d_dname)(struct dentry *, char *, int);
struct vfsmount *(*d_automount)(struct path *);
int (*d_manage)(struct dentry *, bool);
struct inode *(*d_select_inode)(struct dentry *, unsigned);
} ____cacheline_aligned;
/*
* Locking rules for dentry_operations callbacks are to be found in
* Documentation/filesystems/Locking. Keep it updated!
*
* FUrther descriptions are found in Documentation/filesystems/vfs.txt.
* Keep it updated too!
*/
/* d_flags entries */
#define DCACHE_OP_HASH 0x00000001
#define DCACHE_OP_COMPARE 0x00000002
#define DCACHE_OP_REVALIDATE 0x00000004
#define DCACHE_OP_DELETE 0x00000008
#define DCACHE_OP_PRUNE 0x00000010
#define DCACHE_DISCONNECTED 0x00000020
/* This dentry is possibly not currently connected to the dcache tree, in
* which case its parent will either be itself, or will have this flag as
* well. nfsd will not use a dentry with this bit set, but will first
* endeavour to clear the bit either by discovering that it is connected,
* or by performing lookup operations. Any filesystem which supports
* nfsd_operations MUST have a lookup function which, if it finds a
* directory inode with a DCACHE_DISCONNECTED dentry, will d_move that
* dentry into place and return that dentry rather than the passed one,
* typically using d_splice_alias. */
#define DCACHE_REFERENCED 0x00000040 /* Recently used, don't discard. */
#define DCACHE_RCUACCESS 0x00000080 /* Entry has ever been RCU-visible */
#define DCACHE_CANT_MOUNT 0x00000100
#define DCACHE_GENOCIDE 0x00000200
#define DCACHE_SHRINK_LIST 0x00000400
#define DCACHE_OP_WEAK_REVALIDATE 0x00000800
#define DCACHE_NFSFS_RENAMED 0x00001000
/* this dentry has been "silly renamed" and has to be deleted on the last
* dput() */
#define DCACHE_COOKIE 0x00002000 /* For use by dcookie subsystem */
#define DCACHE_FSNOTIFY_PARENT_WATCHED 0x00004000
/* Parent inode is watched by some fsnotify listener */
#define DCACHE_DENTRY_KILLED 0x00008000
#define DCACHE_MOUNTED 0x00010000 /* is a mountpoint */
#define DCACHE_NEED_AUTOMOUNT 0x00020000 /* handle automount on this dir */
#define DCACHE_MANAGE_TRANSIT 0x00040000 /* manage transit from this dirent */
#define DCACHE_MANAGED_DENTRY \
(DCACHE_MOUNTED|DCACHE_NEED_AUTOMOUNT|DCACHE_MANAGE_TRANSIT)
#define DCACHE_LRU_LIST 0x00080000
#define DCACHE_ENTRY_TYPE 0x00700000
#define DCACHE_MISS_TYPE 0x00000000 /* Negative dentry (maybe fallthru to nowhere) */
#define DCACHE_WHITEOUT_TYPE 0x00100000 /* Whiteout dentry (stop pathwalk) */
#define DCACHE_DIRECTORY_TYPE 0x00200000 /* Normal directory */
#define DCACHE_AUTODIR_TYPE 0x00300000 /* Lookupless directory (presumed automount) */
#define DCACHE_REGULAR_TYPE 0x00400000 /* Regular file type (or fallthru to such) */
#define DCACHE_SPECIAL_TYPE 0x00500000 /* Other file type (or fallthru to such) */
#define DCACHE_SYMLINK_TYPE 0x00600000 /* Symlink (or fallthru to such) */
#define DCACHE_MAY_FREE 0x00800000
#define DCACHE_FALLTHRU 0x01000000 /* Fall through to lower layer */
#define DCACHE_OP_SELECT_INODE 0x02000000 /* Unioned entry: dcache op selects inode */
extern seqlock_t rename_lock;
/*
* These are the low-level FS interfaces to the dcache..
*/
extern void d_instantiate(struct dentry *, struct inode *);
extern struct dentry * d_instantiate_unique(struct dentry *, struct inode *);
extern int d_instantiate_no_diralias(struct dentry *, struct inode *);
extern void __d_drop(struct dentry *dentry);
extern void d_drop(struct dentry *dentry);
extern void d_delete(struct dentry *);
extern void d_set_d_op(struct dentry *dentry, const struct dentry_operations *op);
/* allocate/de-allocate */
extern struct dentry * d_alloc(struct dentry *, const struct qstr *);
extern struct dentry * d_alloc_pseudo(struct super_block *, const struct qstr *);
extern struct dentry * d_splice_alias(struct inode *, struct dentry *);
extern struct dentry * d_add_ci(struct dentry *, struct inode *, struct qstr *);
extern struct dentry *d_find_any_alias(struct inode *inode);
extern struct dentry * d_obtain_alias(struct inode *);
extern struct dentry * d_obtain_root(struct inode *);
extern void shrink_dcache_sb(struct super_block *);
extern void shrink_dcache_parent(struct dentry *);
extern void shrink_dcache_for_umount(struct super_block *);
extern void d_invalidate(struct dentry *);
/* only used at mount-time */
extern struct dentry * d_make_root(struct inode *);
/* <clickety>-<click> the ramfs-type tree */
extern void d_genocide(struct dentry *);
extern void d_tmpfile(struct dentry *, struct inode *);
extern struct dentry *d_find_alias(struct inode *);
extern void d_prune_aliases(struct inode *);
/* test whether we have any submounts in a subdir tree */
extern int have_submounts(struct dentry *);
/*
* This adds the entry to the hash queues.
*/
extern void d_rehash(struct dentry *);
/**
* d_add - add dentry to hash queues
* @entry: dentry to add
* @inode: The inode to attach to this dentry
*
* This adds the entry to the hash queues and initializes @inode.
* The entry was actually filled in earlier during d_alloc().
*/
static inline void d_add(struct dentry *entry, struct inode *inode)
{
d_instantiate(entry, inode);
d_rehash(entry);
}
/**
* d_add_unique - add dentry to hash queues without aliasing
* @entry: dentry to add
* @inode: The inode to attach to this dentry
*
* This adds the entry to the hash queues and initializes @inode.
* The entry was actually filled in earlier during d_alloc().
*/
static inline struct dentry *d_add_unique(struct dentry *entry, struct inode *inode)
{
struct dentry *res;
res = d_instantiate_unique(entry, inode);
d_rehash(res != NULL ? res : entry);
return res;
}
extern void dentry_update_name_case(struct dentry *, struct qstr *);
/* used for rename() and baskets */
extern void d_move(struct dentry *, struct dentry *);
extern void d_exchange(struct dentry *, struct dentry *);
extern struct dentry *d_ancestor(struct dentry *, struct dentry *);
/* appendix may either be NULL or be used for transname suffixes */
extern struct dentry *d_lookup(const struct dentry *, const struct qstr *);
extern struct dentry *d_hash_and_lookup(struct dentry *, struct qstr *);
extern struct dentry *__d_lookup(const struct dentry *, const struct qstr *);
extern struct dentry *__d_lookup_rcu(const struct dentry *parent,
const struct qstr *name, unsigned *seq);
static inline unsigned d_count(const struct dentry *dentry)
{
return dentry->d_lockref.count;
}
/*
* helper function for dentry_operations.d_dname() members
*/
extern char *dynamic_dname(struct dentry *, char *, int, const char *, ...);
extern char *simple_dname(struct dentry *, char *, int);
extern char *__d_path(const struct path *, const struct path *, char *, int);
extern char *d_absolute_path(const struct path *, char *, int);
extern char *d_path(const struct path *, char *, int);
extern char *dentry_path_raw(struct dentry *, char *, int);
extern char *dentry_path(struct dentry *, char *, int);
/* Allocation counts.. */
/**
* dget, dget_dlock - get a reference to a dentry
* @dentry: dentry to get a reference to
*
* Given a dentry or %NULL pointer increment the reference count
* if appropriate and return the dentry. A dentry will not be
* destroyed when it has references.
*/
static inline struct dentry *dget_dlock(struct dentry *dentry)
{
if (dentry)
dentry->d_lockref.count++;
return dentry;
}
static inline struct dentry *dget(struct dentry *dentry)
{
if (dentry)
lockref_get(&dentry->d_lockref);
return dentry;
}
extern struct dentry *dget_parent(struct dentry *dentry);
/**
* d_unhashed - is dentry hashed
* @dentry: entry to check
*
* Returns true if the dentry passed is not currently hashed.
*/
static inline int d_unhashed(const struct dentry *dentry)
{
return hlist_bl_unhashed(&dentry->d_hash);
}
static inline int d_unlinked(const struct dentry *dentry)
{
return d_unhashed(dentry) && !IS_ROOT(dentry);
}
static inline int cant_mount(const struct dentry *dentry)
{
return (dentry->d_flags & DCACHE_CANT_MOUNT);
}
static inline void dont_mount(struct dentry *dentry)
{
spin_lock(&dentry->d_lock);
dentry->d_flags |= DCACHE_CANT_MOUNT;
spin_unlock(&dentry->d_lock);
}
extern void dput(struct dentry *);
static inline bool d_managed(const struct dentry *dentry)
{
return dentry->d_flags & DCACHE_MANAGED_DENTRY;
}
static inline bool d_mountpoint(const struct dentry *dentry)
{
return dentry->d_flags & DCACHE_MOUNTED;
}
/*
* Directory cache entry type accessor functions.
*/
static inline unsigned __d_entry_type(const struct dentry *dentry)
{
return dentry->d_flags & DCACHE_ENTRY_TYPE;
}
static inline bool d_is_miss(const struct dentry *dentry)
{
return __d_entry_type(dentry) == DCACHE_MISS_TYPE;
}
static inline bool d_is_whiteout(const struct dentry *dentry)
{
return __d_entry_type(dentry) == DCACHE_WHITEOUT_TYPE;
}
static inline bool d_can_lookup(const struct dentry *dentry)
{
return __d_entry_type(dentry) == DCACHE_DIRECTORY_TYPE;
}
static inline bool d_is_autodir(const struct dentry *dentry)
{
return __d_entry_type(dentry) == DCACHE_AUTODIR_TYPE;
}
static inline bool d_is_dir(const struct dentry *dentry)
{
return d_can_lookup(dentry) || d_is_autodir(dentry);
}
static inline bool d_is_symlink(const struct dentry *dentry)
{
return __d_entry_type(dentry) == DCACHE_SYMLINK_TYPE;
}
static inline bool d_is_reg(const struct dentry *dentry)
{
return __d_entry_type(dentry) == DCACHE_REGULAR_TYPE;
}
static inline bool d_is_special(const struct dentry *dentry)
{
return __d_entry_type(dentry) == DCACHE_SPECIAL_TYPE;
}
static inline bool d_is_file(const struct dentry *dentry)
{
return d_is_reg(dentry) || d_is_special(dentry);
}
static inline bool d_is_negative(const struct dentry *dentry)
{
// TODO: check d_is_whiteout(dentry) also.
return d_is_miss(dentry);
}
static inline bool d_is_positive(const struct dentry *dentry)
{
return !d_is_negative(dentry);
}
/**
* d_really_is_negative - Determine if a dentry is really negative (ignoring fallthroughs)
* @dentry: The dentry in question
*
* Returns true if the dentry represents either an absent name or a name that
* doesn't map to an inode (ie. ->d_inode is NULL). The dentry could represent
* a true miss, a whiteout that isn't represented by a 0,0 chardev or a
* fallthrough marker in an opaque directory.
*
* Note! (1) This should be used *only* by a filesystem to examine its own
* dentries. It should not be used to look at some other filesystem's
* dentries. (2) It should also be used in combination with d_inode() to get
* the inode. (3) The dentry may have something attached to ->d_lower and the
* type field of the flags may be set to something other than miss or whiteout.
*/
static inline bool d_really_is_negative(const struct dentry *dentry)
{
return dentry->d_inode == NULL;
}
/**
* d_really_is_positive - Determine if a dentry is really positive (ignoring fallthroughs)
* @dentry: The dentry in question
*
* Returns true if the dentry represents a name that maps to an inode
* (ie. ->d_inode is not NULL). The dentry might still represent a whiteout if
* that is represented on medium as a 0,0 chardev.
*
* Note! (1) This should be used *only* by a filesystem to examine its own
* dentries. It should not be used to look at some other filesystem's
* dentries. (2) It should also be used in combination with d_inode() to get
* the inode.
*/
static inline bool d_really_is_positive(const struct dentry *dentry)
{
return dentry->d_inode != NULL;
}
extern void d_set_fallthru(struct dentry *dentry);
static inline bool d_is_fallthru(const struct dentry *dentry)
{
return dentry->d_flags & DCACHE_FALLTHRU;
}
extern int sysctl_vfs_cache_pressure;
static inline unsigned long vfs_pressure_ratio(unsigned long val)
{
return mult_frac(val, sysctl_vfs_cache_pressure, 100);
}
/**
* d_inode - Get the actual inode of this dentry
* @dentry: The dentry to query
*
* This is the helper normal filesystems should use to get at their own inodes
* in their own dentries and ignore the layering superimposed upon them.
*/
static inline struct inode *d_inode(const struct dentry *dentry)
{
return dentry->d_inode;
}
/**
* d_inode_rcu - Get the actual inode of this dentry with ACCESS_ONCE()
* @dentry: The dentry to query
*
* This is the helper normal filesystems should use to get at their own inodes
* in their own dentries and ignore the layering superimposed upon them.
*/
static inline struct inode *d_inode_rcu(const struct dentry *dentry)
{
return ACCESS_ONCE(dentry->d_inode);
}
/**
* d_backing_inode - Get upper or lower inode we should be using
* @upper: The upper layer
*
* This is the helper that should be used to get at the inode that will be used
* if this dentry were to be opened as a file. The inode may be on the upper
* dentry or it may be on a lower dentry pinned by the upper.
*
* Normal filesystems should not use this to access their own inodes.
*/
static inline struct inode *d_backing_inode(const struct dentry *upper)
{
struct inode *inode = upper->d_inode;
return inode;
}
/**
* d_backing_dentry - Get upper or lower dentry we should be using
* @upper: The upper layer
*
* This is the helper that should be used to get the dentry of the inode that
* will be used if this dentry were opened as a file. It may be the upper
* dentry or it may be a lower dentry pinned by the upper.
*
* Normal filesystems should not use this to access their own dentries.
*/
static inline struct dentry *d_backing_dentry(struct dentry *upper)
{
return upper;
}
#endif /* __LINUX_DCACHE_H */