aboutsummaryrefslogblamecommitdiffstats
blob: 57f3a1c550dc66e59803a2118f377a318ca7e51e (plain) (tree)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15














                                                                           


                            


















                                                         
  

                                                                               
                                                                           





                                                                            
                                                                         
                                                                         




































                                                                                
                                                      


                                                                         
                                                                         
                                                                         
                                                                         
                                                                         
                             




                                                                         
                                                      

                                                                         
                                                                         
                             
      







































                                                                               







                                                                         


                                                                               
                                                                         
                                                                         
                            

                                                                         
                                                                         
                            

  


                                                                              
                                                            

                                                                         
                                                           

  


                                                                   
   
                   

                                                             



                                      
 




                            
  





                                                                           



                                                                   

                                                                         



                                                                         






                                                                           
                                                                         


                                                                         
                                                                         

                                                                         

  




                                                                         

                           




                                                                         



                                          

                        



                                                                         

  
                                                                          

                                                   


                        
                                                           
 



                                                             




                                                                         




                                                                      



                                                                         

           




                                                                         
 



                                                                         

           













                                                                         

                                                                         

                                                                         



                                                                         
                                                                         
                                                                         





























                                                                          
                                                                         
                                                                         


                                                                         






































                                                                         





                                                                           


   


                                                                       
  




                                                                           
   







                                                                                               
                                                                   








                                                                                                       

  

                                                                           
   




                                                                         
 




                                                                         
 


                                                                         
                                                                         
  
 


                                                                         
                                                                         
  
 


                                                                         
                                                                         
  
 




                                                                         
 




                                                                         
 




                                                                         
 



                                                                           
 





                                                                                       

  



                                                                          
   














                                                                                                        


                                                                                     
 
                         
                                 
/*
 * linux/percpu-defs.h - basic definitions for percpu areas
 *
 * DO NOT INCLUDE DIRECTLY OUTSIDE PERCPU IMPLEMENTATION PROPER.
 *
 * This file is separate from linux/percpu.h to avoid cyclic inclusion
 * dependency from arch header files.  Only to be included from
 * asm/percpu.h.
 *
 * This file includes macros necessary to declare percpu sections and
 * variables, and definitions of percpu accessors and operations.  It
 * should provide enough percpu features to arch header files even when
 * they can only include asm/percpu.h to avoid cyclic inclusion dependency.
 */

#ifndef _LINUX_PERCPU_DEFS_H
#define _LINUX_PERCPU_DEFS_H

#ifdef CONFIG_SMP

#ifdef MODULE
#define PER_CPU_SHARED_ALIGNED_SECTION ""
#define PER_CPU_ALIGNED_SECTION ""
#else
#define PER_CPU_SHARED_ALIGNED_SECTION "..shared_aligned"
#define PER_CPU_ALIGNED_SECTION "..shared_aligned"
#endif
#define PER_CPU_FIRST_SECTION "..first"

#else

#define PER_CPU_SHARED_ALIGNED_SECTION ""
#define PER_CPU_ALIGNED_SECTION "..shared_aligned"
#define PER_CPU_FIRST_SECTION ""

#endif

/*
 * Base implementations of per-CPU variable declarations and definitions, where
 * the section in which the variable is to be placed is provided by the
 * 'sec' argument.  This may be used to affect the parameters governing the
 * variable's storage.
 *
 * NOTE!  The sections for the DECLARE and for the DEFINE must match, lest
 * linkage errors occur due the compiler generating the wrong code to access
 * that section.
 */
#define __PCPU_ATTRS(sec)						\
	__percpu __attribute__((section(PER_CPU_BASE_SECTION sec)))	\
	PER_CPU_ATTRIBUTES

#define __PCPU_DUMMY_ATTRS						\
	__attribute__((section(".discard"), unused))

/*
 * s390 and alpha modules require percpu variables to be defined as
 * weak to force the compiler to generate GOT based external
 * references for them.  This is necessary because percpu sections
 * will be located outside of the usually addressable area.
 *
 * This definition puts the following two extra restrictions when
 * defining percpu variables.
 *
 * 1. The symbol must be globally unique, even the static ones.
 * 2. Static percpu variables cannot be defined inside a function.
 *
 * Archs which need weak percpu definitions should define
 * ARCH_NEEDS_WEAK_PER_CPU in asm/percpu.h when necessary.
 *
 * To ensure that the generic code observes the above two
 * restrictions, if CONFIG_DEBUG_FORCE_WEAK_PER_CPU is set weak
 * definition is used for all cases.
 */
#if defined(ARCH_NEEDS_WEAK_PER_CPU) || defined(CONFIG_DEBUG_FORCE_WEAK_PER_CPU)
/*
 * __pcpu_scope_* dummy variable is used to enforce scope.  It
 * receives the static modifier when it's used in front of
 * DEFINE_PER_CPU() and will trigger build failure if
 * DECLARE_PER_CPU() is used for the same variable.
 *
 * __pcpu_unique_* dummy variable is used to enforce symbol uniqueness
 * such that hidden weak symbol collision, which will cause unrelated
 * variables to share the same address, can be detected during build.
 */
#define DECLARE_PER_CPU_SECTION(type, name, sec)			\
	extern __PCPU_DUMMY_ATTRS char __pcpu_scope_##name;		\
	extern __PCPU_ATTRS(sec) __typeof__(type) name

#define DEFINE_PER_CPU_SECTION(type, name, sec)				\
	__PCPU_DUMMY_ATTRS char __pcpu_scope_##name;			\
	extern __PCPU_DUMMY_ATTRS char __pcpu_unique_##name;		\
	__PCPU_DUMMY_ATTRS char __pcpu_unique_##name;			\
	extern __PCPU_ATTRS(sec) __typeof__(type) name;			\
	__PCPU_ATTRS(sec) PER_CPU_DEF_ATTRIBUTES __weak			\
	__typeof__(type) name
#else
/*
 * Normal declaration and definition macros.
 */
#define DECLARE_PER_CPU_SECTION(type, name, sec)			\
	extern __PCPU_ATTRS(sec) __typeof__(type) name

#define DEFINE_PER_CPU_SECTION(type, name, sec)				\
	__PCPU_ATTRS(sec) PER_CPU_DEF_ATTRIBUTES			\
	__typeof__(type) name
#endif

/*
 * Variant on the per-CPU variable declaration/definition theme used for
 * ordinary per-CPU variables.
 */
#define DECLARE_PER_CPU(type, name)					\
	DECLARE_PER_CPU_SECTION(type, name, "")

#define DEFINE_PER_CPU(type, name)					\
	DEFINE_PER_CPU_SECTION(type, name, "")

/*
 * Declaration/definition used for per-CPU variables that must come first in
 * the set of variables.
 */
#define DECLARE_PER_CPU_FIRST(type, name)				\
	DECLARE_PER_CPU_SECTION(type, name, PER_CPU_FIRST_SECTION)

#define DEFINE_PER_CPU_FIRST(type, name)				\
	DEFINE_PER_CPU_SECTION(type, name, PER_CPU_FIRST_SECTION)

/*
 * Declaration/definition used for per-CPU variables that must be cacheline
 * aligned under SMP conditions so that, whilst a particular instance of the
 * data corresponds to a particular CPU, inefficiencies due to direct access by
 * other CPUs are reduced by preventing the data from unnecessarily spanning
 * cachelines.
 *
 * An example of this would be statistical data, where each CPU's set of data
 * is updated by that CPU alone, but the data from across all CPUs is collated
 * by a CPU processing a read from a proc file.
 */
#define DECLARE_PER_CPU_SHARED_ALIGNED(type, name)			\
	DECLARE_PER_CPU_SECTION(type, name, PER_CPU_SHARED_ALIGNED_SECTION) \
	____cacheline_aligned_in_smp

#define DEFINE_PER_CPU_SHARED_ALIGNED(type, name)			\
	DEFINE_PER_CPU_SECTION(type, name, PER_CPU_SHARED_ALIGNED_SECTION) \
	____cacheline_aligned_in_smp

#define DECLARE_PER_CPU_ALIGNED(type, name)				\
	DECLARE_PER_CPU_SECTION(type, name, PER_CPU_ALIGNED_SECTION)	\
	____cacheline_aligned

#define DEFINE_PER_CPU_ALIGNED(type, name)				\
	DEFINE_PER_CPU_SECTION(type, name, PER_CPU_ALIGNED_SECTION)	\
	____cacheline_aligned

/*
 * Declaration/definition used for per-CPU variables that must be page aligned.
 */
#define DECLARE_PER_CPU_PAGE_ALIGNED(type, name)			\
	DECLARE_PER_CPU_SECTION(type, name, "..page_aligned")		\
	__aligned(PAGE_SIZE)

#define DEFINE_PER_CPU_PAGE_ALIGNED(type, name)				\
	DEFINE_PER_CPU_SECTION(type, name, "..page_aligned")		\
	__aligned(PAGE_SIZE)

/*
 * Declaration/definition used for per-CPU variables that must be read mostly.
 */
#define DECLARE_PER_CPU_READ_MOSTLY(type, name)			\
	DECLARE_PER_CPU_SECTION(type, name, "..read_mostly")

#define DEFINE_PER_CPU_READ_MOSTLY(type, name)				\
	DEFINE_PER_CPU_SECTION(type, name, "..read_mostly")

/*
 * Intermodule exports for per-CPU variables.  sparse forgets about
 * address space across EXPORT_SYMBOL(), change EXPORT_SYMBOL() to
 * noop if __CHECKER__.
 */
#ifndef __CHECKER__
#define EXPORT_PER_CPU_SYMBOL(var) EXPORT_SYMBOL(var)
#define EXPORT_PER_CPU_SYMBOL_GPL(var) EXPORT_SYMBOL_GPL(var)
#else
#define EXPORT_PER_CPU_SYMBOL(var)
#define EXPORT_PER_CPU_SYMBOL_GPL(var)
#endif

/*
 * Accessors and operations.
 */
#ifndef __ASSEMBLY__

/*
 * __verify_pcpu_ptr() verifies @ptr is a percpu pointer without evaluating
 * @ptr and is invoked once before a percpu area is accessed by all
 * accessors and operations.  This is performed in the generic part of
 * percpu and arch overrides don't need to worry about it; however, if an
 * arch wants to implement an arch-specific percpu accessor or operation,
 * it may use __verify_pcpu_ptr() to verify the parameters.
 *
 * + 0 is required in order to convert the pointer type from a
 * potential array type to a pointer to a single item of the array.
 */
#define __verify_pcpu_ptr(ptr)						\
do {									\
	const void __percpu *__vpp_verify = (typeof((ptr) + 0))NULL;	\
	(void)__vpp_verify;						\
} while (0)

#ifdef CONFIG_SMP

/*
 * Add an offset to a pointer but keep the pointer as-is.  Use RELOC_HIDE()
 * to prevent the compiler from making incorrect assumptions about the
 * pointer value.  The weird cast keeps both GCC and sparse happy.
 */
#define SHIFT_PERCPU_PTR(__p, __offset)					\
	RELOC_HIDE((typeof(*(__p)) __kernel __force *)(__p), (__offset))

#define per_cpu_ptr(ptr, cpu)						\
({									\
	__verify_pcpu_ptr(ptr);						\
	SHIFT_PERCPU_PTR((ptr), per_cpu_offset((cpu)));			\
})

#define raw_cpu_ptr(ptr)						\
({									\
	__verify_pcpu_ptr(ptr);						\
	arch_raw_cpu_ptr(ptr);						\
})

#ifdef CONFIG_DEBUG_PREEMPT
#define this_cpu_ptr(ptr)						\
({									\
	__verify_pcpu_ptr(ptr);						\
	SHIFT_PERCPU_PTR(ptr, my_cpu_offset);				\
})
#else
#define this_cpu_ptr(ptr) raw_cpu_ptr(ptr)
#endif

#else	/* CONFIG_SMP */

#define VERIFY_PERCPU_PTR(__p)						\
({									\
	__verify_pcpu_ptr(__p);						\
	(typeof(*(__p)) __kernel __force *)(__p);			\
})

#define per_cpu_ptr(ptr, cpu)	({ (void)(cpu); VERIFY_PERCPU_PTR(ptr); })
#define raw_cpu_ptr(ptr)	per_cpu_ptr(ptr, 0)
#define this_cpu_ptr(ptr)	raw_cpu_ptr(ptr)

#endif	/* CONFIG_SMP */

#define per_cpu(var, cpu)	(*per_cpu_ptr(&(var), cpu))

/*
 * Must be an lvalue. Since @var must be a simple identifier,
 * we force a syntax error here if it isn't.
 */
#define get_cpu_var(var)						\
(*({									\
	preempt_disable();						\
	this_cpu_ptr(&var);						\
}))

/*
 * The weird & is necessary because sparse considers (void)(var) to be
 * a direct dereference of percpu variable (var).
 */
#define put_cpu_var(var)						\
do {									\
	(void)&(var);							\
	preempt_enable();						\
} while (0)

#define get_cpu_ptr(var)						\
({									\
	preempt_disable();						\
	this_cpu_ptr(var);						\
})

#define put_cpu_ptr(var)						\
do {									\
	(void)(var);							\
	preempt_enable();						\
} while (0)

/*
 * Branching function to split up a function into a set of functions that
 * are called for different scalar sizes of the objects handled.
 */

extern void __bad_size_call_parameter(void);

#ifdef CONFIG_DEBUG_PREEMPT
extern void __this_cpu_preempt_check(const char *op);
#else
static inline void __this_cpu_preempt_check(const char *op) { }
#endif

#define __pcpu_size_call_return(stem, variable)				\
({									\
	typeof(variable) pscr_ret__;					\
	__verify_pcpu_ptr(&(variable));					\
	switch(sizeof(variable)) {					\
	case 1: pscr_ret__ = stem##1(variable); break;			\
	case 2: pscr_ret__ = stem##2(variable); break;			\
	case 4: pscr_ret__ = stem##4(variable); break;			\
	case 8: pscr_ret__ = stem##8(variable); break;			\
	default:							\
		__bad_size_call_parameter(); break;			\
	}								\
	pscr_ret__;							\
})

#define __pcpu_size_call_return2(stem, variable, ...)			\
({									\
	typeof(variable) pscr2_ret__;					\
	__verify_pcpu_ptr(&(variable));					\
	switch(sizeof(variable)) {					\
	case 1: pscr2_ret__ = stem##1(variable, __VA_ARGS__); break;	\
	case 2: pscr2_ret__ = stem##2(variable, __VA_ARGS__); break;	\
	case 4: pscr2_ret__ = stem##4(variable, __VA_ARGS__); break;	\
	case 8: pscr2_ret__ = stem##8(variable, __VA_ARGS__); break;	\
	default:							\
		__bad_size_call_parameter(); break;			\
	}								\
	pscr2_ret__;							\
})

/*
 * Special handling for cmpxchg_double.  cmpxchg_double is passed two
 * percpu variables.  The first has to be aligned to a double word
 * boundary and the second has to follow directly thereafter.
 * We enforce this on all architectures even if they don't support
 * a double cmpxchg instruction, since it's a cheap requirement, and it
 * avoids breaking the requirement for architectures with the instruction.
 */
#define __pcpu_double_call_return_bool(stem, pcp1, pcp2, ...)		\
({									\
	bool pdcrb_ret__;						\
	__verify_pcpu_ptr(&(pcp1));					\
	BUILD_BUG_ON(sizeof(pcp1) != sizeof(pcp2));			\
	VM_BUG_ON((unsigned long)(&(pcp1)) % (2 * sizeof(pcp1)));	\
	VM_BUG_ON((unsigned long)(&(pcp2)) !=				\
		  (unsigned long)(&(pcp1)) + sizeof(pcp1));		\
	switch(sizeof(pcp1)) {						\
	case 1: pdcrb_ret__ = stem##1(pcp1, pcp2, __VA_ARGS__); break;	\
	case 2: pdcrb_ret__ = stem##2(pcp1, pcp2, __VA_ARGS__); break;	\
	case 4: pdcrb_ret__ = stem##4(pcp1, pcp2, __VA_ARGS__); break;	\
	case 8: pdcrb_ret__ = stem##8(pcp1, pcp2, __VA_ARGS__); break;	\
	default:							\
		__bad_size_call_parameter(); break;			\
	}								\
	pdcrb_ret__;							\
})

#define __pcpu_size_call(stem, variable, ...)				\
do {									\
	__verify_pcpu_ptr(&(variable));					\
	switch(sizeof(variable)) {					\
		case 1: stem##1(variable, __VA_ARGS__);break;		\
		case 2: stem##2(variable, __VA_ARGS__);break;		\
		case 4: stem##4(variable, __VA_ARGS__);break;		\
		case 8: stem##8(variable, __VA_ARGS__);break;		\
		default: 						\
			__bad_size_call_parameter();break;		\
	}								\
} while (0)

/*
 * this_cpu operations (C) 2008-2013 Christoph Lameter <cl@linux.com>
 *
 * Optimized manipulation for memory allocated through the per cpu
 * allocator or for addresses of per cpu variables.
 *
 * These operation guarantee exclusivity of access for other operations
 * on the *same* processor. The assumption is that per cpu data is only
 * accessed by a single processor instance (the current one).
 *
 * The arch code can provide optimized implementation by defining macros
 * for certain scalar sizes. F.e. provide this_cpu_add_2() to provide per
 * cpu atomic operations for 2 byte sized RMW actions. If arch code does
 * not provide operations for a scalar size then the fallback in the
 * generic code will be used.
 *
 * cmpxchg_double replaces two adjacent scalars at once.  The first two
 * parameters are per cpu variables which have to be of the same size.  A
 * truth value is returned to indicate success or failure (since a double
 * register result is difficult to handle).  There is very limited hardware
 * support for these operations, so only certain sizes may work.
 */

/*
 * Operations for contexts where we do not want to do any checks for
 * preemptions.  Unless strictly necessary, always use [__]this_cpu_*()
 * instead.
 *
 * If there is no other protection through preempt disable and/or disabling
 * interupts then one of these RMW operations can show unexpected behavior
 * because the execution thread was rescheduled on another processor or an
 * interrupt occurred and the same percpu variable was modified from the
 * interrupt context.
 */
#define raw_cpu_read(pcp)		__pcpu_size_call_return(raw_cpu_read_, pcp)
#define raw_cpu_write(pcp, val)		__pcpu_size_call(raw_cpu_write_, pcp, val)
#define raw_cpu_add(pcp, val)		__pcpu_size_call(raw_cpu_add_, pcp, val)
#define raw_cpu_and(pcp, val)		__pcpu_size_call(raw_cpu_and_, pcp, val)
#define raw_cpu_or(pcp, val)		__pcpu_size_call(raw_cpu_or_, pcp, val)
#define raw_cpu_add_return(pcp, val)	__pcpu_size_call_return2(raw_cpu_add_return_, pcp, val)
#define raw_cpu_xchg(pcp, nval)		__pcpu_size_call_return2(raw_cpu_xchg_, pcp, nval)
#define raw_cpu_cmpxchg(pcp, oval, nval) \
	__pcpu_size_call_return2(raw_cpu_cmpxchg_, pcp, oval, nval)
#define raw_cpu_cmpxchg_double(pcp1, pcp2, oval1, oval2, nval1, nval2) \
	__pcpu_double_call_return_bool(raw_cpu_cmpxchg_double_, pcp1, pcp2, oval1, oval2, nval1, nval2)

#define raw_cpu_sub(pcp, val)		raw_cpu_add(pcp, -(val))
#define raw_cpu_inc(pcp)		raw_cpu_add(pcp, 1)
#define raw_cpu_dec(pcp)		raw_cpu_sub(pcp, 1)
#define raw_cpu_sub_return(pcp, val)	raw_cpu_add_return(pcp, -(typeof(pcp))(val))
#define raw_cpu_inc_return(pcp)		raw_cpu_add_return(pcp, 1)
#define raw_cpu_dec_return(pcp)		raw_cpu_add_return(pcp, -1)

/*
 * Operations for contexts that are safe from preemption/interrupts.  These
 * operations verify that preemption is disabled.
 */
#define __this_cpu_read(pcp)						\
({									\
	__this_cpu_preempt_check("read");				\
	raw_cpu_read(pcp);						\
})

#define __this_cpu_write(pcp, val)					\
({									\
	__this_cpu_preempt_check("write");				\
	raw_cpu_write(pcp, val);					\
})

#define __this_cpu_add(pcp, val)					\
({									\
	__this_cpu_preempt_check("add");				\
	raw_cpu_add(pcp, val);						\
})

#define __this_cpu_and(pcp, val)					\
({									\
	__this_cpu_preempt_check("and");				\
	raw_cpu_and(pcp, val);						\
})

#define __this_cpu_or(pcp, val)						\
({									\
	__this_cpu_preempt_check("or");					\
	raw_cpu_or(pcp, val);						\
})

#define __this_cpu_add_return(pcp, val)					\
({									\
	__this_cpu_preempt_check("add_return");				\
	raw_cpu_add_return(pcp, val);					\
})

#define __this_cpu_xchg(pcp, nval)					\
({									\
	__this_cpu_preempt_check("xchg");				\
	raw_cpu_xchg(pcp, nval);					\
})

#define __this_cpu_cmpxchg(pcp, oval, nval)				\
({									\
	__this_cpu_preempt_check("cmpxchg");				\
	raw_cpu_cmpxchg(pcp, oval, nval);				\
})

#define __this_cpu_cmpxchg_double(pcp1, pcp2, oval1, oval2, nval1, nval2) \
({	__this_cpu_preempt_check("cmpxchg_double");			\
	raw_cpu_cmpxchg_double(pcp1, pcp2, oval1, oval2, nval1, nval2);	\
})

#define __this_cpu_sub(pcp, val)	__this_cpu_add(pcp, -(typeof(pcp))(val))
#define __this_cpu_inc(pcp)		__this_cpu_add(pcp, 1)
#define __this_cpu_dec(pcp)		__this_cpu_sub(pcp, 1)
#define __this_cpu_sub_return(pcp, val)	__this_cpu_add_return(pcp, -(typeof(pcp))(val))
#define __this_cpu_inc_return(pcp)	__this_cpu_add_return(pcp, 1)
#define __this_cpu_dec_return(pcp)	__this_cpu_add_return(pcp, -1)

/*
 * Operations with implied preemption protection.  These operations can be
 * used without worrying about preemption.  Note that interrupts may still
 * occur while an operation is in progress and if the interrupt modifies
 * the variable too then RMW actions may not be reliable.
 */
#define this_cpu_read(pcp)		__pcpu_size_call_return(this_cpu_read_, pcp)
#define this_cpu_write(pcp, val)	__pcpu_size_call(this_cpu_write_, pcp, val)
#define this_cpu_add(pcp, val)		__pcpu_size_call(this_cpu_add_, pcp, val)
#define this_cpu_and(pcp, val)		__pcpu_size_call(this_cpu_and_, pcp, val)
#define this_cpu_or(pcp, val)		__pcpu_size_call(this_cpu_or_, pcp, val)
#define this_cpu_add_return(pcp, val)	__pcpu_size_call_return2(this_cpu_add_return_, pcp, val)
#define this_cpu_xchg(pcp, nval)	__pcpu_size_call_return2(this_cpu_xchg_, pcp, nval)
#define this_cpu_cmpxchg(pcp, oval, nval) \
	__pcpu_size_call_return2(this_cpu_cmpxchg_, pcp, oval, nval)
#define this_cpu_cmpxchg_double(pcp1, pcp2, oval1, oval2, nval1, nval2) \
	__pcpu_double_call_return_bool(this_cpu_cmpxchg_double_, pcp1, pcp2, oval1, oval2, nval1, nval2)

#define this_cpu_sub(pcp, val)		this_cpu_add(pcp, -(typeof(pcp))(val))
#define this_cpu_inc(pcp)		this_cpu_add(pcp, 1)
#define this_cpu_dec(pcp)		this_cpu_sub(pcp, 1)
#define this_cpu_sub_return(pcp, val)	this_cpu_add_return(pcp, -(typeof(pcp))(val))
#define this_cpu_inc_return(pcp)	this_cpu_add_return(pcp, 1)
#define this_cpu_dec_return(pcp)	this_cpu_add_return(pcp, -1)

#endif /* __ASSEMBLY__ */
#endif /* _LINUX_PERCPU_DEFS_H */