aboutsummaryrefslogblamecommitdiffstats
blob: fa7bc29925c929a36e0f1e53a3a7efc1a18cc9e6 (plain) (tree)
1
2
3
4
5
6
7
8
9







                                                                 
             
                                                            


                                                              
                                                             


                                                                  


                                                                 


                       
                       
                           
                       
                         
                              
 
                               
                 
               
                      
                        
               
 
                                                           

                                                                           
                                                 
                                                            
                                                 
                                                            
                                                        
                                                                   
                                                         
                                                                    
                                                                
                                                                           
                                                            
                                                                       
                                                          
                                                                     
                                                                          
                                                                         

                                                                   
 

                                                                  

                                                                   
                                                                     









                                                                     
  




                                                                     





                                                                    










                                                                    






                                                                         


                                                     


                                                                            
                     
                                                        
                                                                          
                                    



                     




                                        
                                                               
                             

                       


                                                    

                                  
                                 


                                    
                                         
                                        
                                    
                                  
                               
                              




                                                    
                            

  
                      
                                               
                           


                       


                                                                       
                                                                                   

  


                                                                       

  




                                                       
                                    
                                                
                                                         
 
                                                       
                                                 
                                  
                                                   
                                                 
                                  
                                                              
                                                                                    
                                                                         

                                                                           
 

                                                              
                             


                                             
















                                                                                      
                                    



                                               

                          


                                                                        
                            
/*
 * sysctl.h: General linux system control interface
 *
 * Begun 24 March 1995, Stephen Tweedie
 *
 ****************************************************************
 ****************************************************************
 **
 **  WARNING:
 **  The values in this file are exported to user space via 
 **  the sysctl() binary interface.  Do *NOT* change the
 **  numbering of any existing values here, and do not change
 **  any numbers within any one set of values.  If you have to
 **  redefine an existing interface, use a new number for it.
 **  The kernel will then return -ENOTDIR to any application using
 **  the old binary interface.
 **
 ****************************************************************
 ****************************************************************
 */
#ifndef _LINUX_SYSCTL_H
#define _LINUX_SYSCTL_H

#include <linux/list.h>
#include <linux/rcupdate.h>
#include <linux/wait.h>
#include <linux/rbtree.h>
#include <uapi/linux/sysctl.h>

/* For the /proc/sys support */
struct ctl_table;
struct nsproxy;
struct ctl_table_root;
struct ctl_table_header;
struct ctl_dir;

typedef int proc_handler (struct ctl_table *ctl, int write,
			  void __user *buffer, size_t *lenp, loff_t *ppos);

extern int proc_dostring(struct ctl_table *, int,
			 void __user *, size_t *, loff_t *);
extern int proc_dointvec(struct ctl_table *, int,
			 void __user *, size_t *, loff_t *);
extern int proc_dointvec_minmax(struct ctl_table *, int,
				void __user *, size_t *, loff_t *);
extern int proc_dointvec_jiffies(struct ctl_table *, int,
				 void __user *, size_t *, loff_t *);
extern int proc_dointvec_userhz_jiffies(struct ctl_table *, int,
					void __user *, size_t *, loff_t *);
extern int proc_dointvec_ms_jiffies(struct ctl_table *, int,
				    void __user *, size_t *, loff_t *);
extern int proc_doulongvec_minmax(struct ctl_table *, int,
				  void __user *, size_t *, loff_t *);
extern int proc_doulongvec_ms_jiffies_minmax(struct ctl_table *table, int,
				      void __user *, size_t *, loff_t *);
extern int proc_do_large_bitmap(struct ctl_table *, int,
				void __user *, size_t *, loff_t *);

/*
 * Register a set of sysctl names by calling register_sysctl_table
 * with an initialised array of struct ctl_table's.  An entry with 
 * NULL procname terminates the table.  table->de will be
 * set up by the registration and need not be initialised in advance.
 *
 * sysctl names can be mirrored automatically under /proc/sys.  The
 * procname supplied controls /proc naming.
 *
 * The table's mode will be honoured both for sys_sysctl(2) and
 * proc-fs access.
 *
 * Leaf nodes in the sysctl tree will be represented by a single file
 * under /proc; non-leaf nodes will be represented by directories.  A
 * null procname disables /proc mirroring at this node.
 *
 * sysctl(2) can automatically manage read and write requests through
 * the sysctl table.  The data and maxlen fields of the ctl_table
 * struct enable minimal validation of the values being written to be
 * performed, and the mode field allows minimal authentication.
 * 
 * There must be a proc_handler routine for any terminal nodes
 * mirrored under /proc/sys (non-terminals are handled by a built-in
 * directory handler).  Several default handlers are available to
 * cover common cases.
 */

/* Support for userspace poll() to watch for changes */
struct ctl_table_poll {
	atomic_t event;
	wait_queue_head_t wait;
};

static inline void *proc_sys_poll_event(struct ctl_table_poll *poll)
{
	return (void *)(unsigned long)atomic_read(&poll->event);
}

#define __CTL_TABLE_POLL_INITIALIZER(name) {				\
	.event = ATOMIC_INIT(0),					\
	.wait = __WAIT_QUEUE_HEAD_INITIALIZER(name.wait) }

#define DEFINE_CTL_TABLE_POLL(name)					\
	struct ctl_table_poll name = __CTL_TABLE_POLL_INITIALIZER(name)

/* A sysctl table is an array of struct ctl_table: */
struct ctl_table 
{
	const char *procname;		/* Text ID for /proc/sys, or zero */
	void *data;
	int maxlen;
	umode_t mode;
	struct ctl_table *child;	/* Deprecated */
	proc_handler *proc_handler;	/* Callback for text formatting */
	struct ctl_table_poll *poll;
	void *extra1;
	void *extra2;
};

struct ctl_node {
	struct rb_node node;
	struct ctl_table_header *header;
};

/* struct ctl_table_header is used to maintain dynamic lists of
   struct ctl_table trees. */
struct ctl_table_header
{
	union {
		struct {
			struct ctl_table *ctl_table;
			int used;
			int count;
			int nreg;
		};
		struct rcu_head rcu;
	};
	struct completion *unregistering;
	struct ctl_table *ctl_table_arg;
	struct ctl_table_root *root;
	struct ctl_table_set *set;
	struct ctl_dir *parent;
	struct ctl_node *node;
};

struct ctl_dir {
	/* Header must be at the start of ctl_dir */
	struct ctl_table_header header;
	struct rb_root root;
};

struct ctl_table_set {
	int (*is_seen)(struct ctl_table_set *);
	struct ctl_dir dir;
};

struct ctl_table_root {
	struct ctl_table_set default_set;
	struct ctl_table_set *(*lookup)(struct ctl_table_root *root,
					   struct nsproxy *namespaces);
	int (*permissions)(struct ctl_table_header *head, struct ctl_table *table);
};

/* struct ctl_path describes where in the hierarchy a table is added */
struct ctl_path {
	const char *procname;
};

#ifdef CONFIG_SYSCTL

void proc_sys_poll_notify(struct ctl_table_poll *poll);

extern void setup_sysctl_set(struct ctl_table_set *p,
	struct ctl_table_root *root,
	int (*is_seen)(struct ctl_table_set *));
extern void retire_sysctl_set(struct ctl_table_set *set);

void register_sysctl_root(struct ctl_table_root *root);
struct ctl_table_header *__register_sysctl_table(
	struct ctl_table_set *set,
	const char *path, struct ctl_table *table);
struct ctl_table_header *__register_sysctl_paths(
	struct ctl_table_set *set,
	const struct ctl_path *path, struct ctl_table *table);
struct ctl_table_header *register_sysctl(const char *path, struct ctl_table *table);
struct ctl_table_header *register_sysctl_table(struct ctl_table * table);
struct ctl_table_header *register_sysctl_paths(const struct ctl_path *path,
						struct ctl_table *table);

void unregister_sysctl_table(struct ctl_table_header * table);

extern int sysctl_init(void);

extern struct ctl_table sysctl_mount_point[];

#else /* CONFIG_SYSCTL */
static inline struct ctl_table_header *register_sysctl_table(struct ctl_table * table)
{
	return NULL;
}

static inline struct ctl_table_header *register_sysctl_paths(
			const struct ctl_path *path, struct ctl_table *table)
{
	return NULL;
}

static inline void unregister_sysctl_table(struct ctl_table_header * table)
{
}

static inline void setup_sysctl_set(struct ctl_table_set *p,
	struct ctl_table_root *root,
	int (*is_seen)(struct ctl_table_set *))
{
}

#endif /* CONFIG_SYSCTL */

int sysctl_max_threads(struct ctl_table *table, int write,
		       void __user *buffer, size_t *lenp, loff_t *ppos);

#endif /* _LINUX_SYSCTL_H */