diff options
author | Eric W. Biederman | 2016-12-14 06:24:51 -0600 |
---|---|---|
committer | Sasha Levin | 2016-12-23 07:56:35 -0600 |
commit | 1171afc4a34e2926e6e8e27c896cf328c8825ac3 (patch) | |
tree | 16c6e981770b3e664fcc5c5c1bd341bced63b3e5 | |
parent | 62fa696b7b435e93ed114dd6a23aa0881d7f81b9 (diff) | |
download | ti-linux-kernel-1171afc4a34e2926e6e8e27c896cf328c8825ac3.tar.gz ti-linux-kernel-1171afc4a34e2926e6e8e27c896cf328c8825ac3.tar.xz ti-linux-kernel-1171afc4a34e2926e6e8e27c896cf328c8825ac3.zip |
mnt: Add a per mount namespace limit on the number of mounts
[ Upstream commit d29216842a85c7970c536108e093963f02714498 ]
CAI Qian <caiqian@redhat.com> pointed out that the semantics
of shared subtrees make it possible to create an exponentially
increasing number of mounts in a mount namespace.
mkdir /tmp/1 /tmp/2
mount --make-rshared /
for i in $(seq 1 20) ; do mount --bind /tmp/1 /tmp/2 ; done
Will create create 2^20 or 1048576 mounts, which is a practical problem
as some people have managed to hit this by accident.
As such CVE-2016-6213 was assigned.
Ian Kent <raven@themaw.net> described the situation for autofs users
as follows:
> The number of mounts for direct mount maps is usually not very large because of
> the way they are implemented, large direct mount maps can have performance
> problems. There can be anywhere from a few (likely case a few hundred) to less
> than 10000, plus mounts that have been triggered and not yet expired.
>
> Indirect mounts have one autofs mount at the root plus the number of mounts that
> have been triggered and not yet expired.
>
> The number of autofs indirect map entries can range from a few to the common
> case of several thousand and in rare cases up to between 30000 and 50000. I've
> not heard of people with maps larger than 50000 entries.
>
> The larger the number of map entries the greater the possibility for a large
> number of active mounts so it's not hard to expect cases of a 1000 or somewhat
> more active mounts.
So I am setting the default number of mounts allowed per mount
namespace at 100,000. This is more than enough for any use case I
know of, but small enough to quickly stop an exponential increase
in mounts. Which should be perfect to catch misconfigurations and
malfunctioning programs.
For anyone who needs a higher limit this can be changed by writing
to the new /proc/sys/fs/mount-max sysctl.
Tested-by: CAI Qian <caiqian@redhat.com>
Signed-off-by: "Eric W. Biederman" <ebiederm@xmission.com>
Conflicts:
fs/namespace.c
kernel/sysctl.c
Signed-off-by: Philipp Hahn <hahn@univention.de>
Signed-off-by: Sasha Levin <alexander.levin@verizon.com>
-rw-r--r-- | Documentation/sysctl/fs.txt | 7 | ||||
-rw-r--r-- | fs/mount.h | 2 | ||||
-rw-r--r-- | fs/namespace.c | 49 | ||||
-rw-r--r-- | fs/pnode.c | 2 | ||||
-rw-r--r-- | fs/pnode.h | 1 | ||||
-rw-r--r-- | include/linux/mount.h | 2 | ||||
-rw-r--r-- | kernel/sysctl.c | 9 |
7 files changed, 70 insertions, 2 deletions
diff --git a/Documentation/sysctl/fs.txt b/Documentation/sysctl/fs.txt index 302b5ed616a6..35e17f748ca7 100644 --- a/Documentation/sysctl/fs.txt +++ b/Documentation/sysctl/fs.txt | |||
@@ -265,6 +265,13 @@ aio-nr can grow to. | |||
265 | 265 | ||
266 | ============================================================== | 266 | ============================================================== |
267 | 267 | ||
268 | mount-max: | ||
269 | |||
270 | This denotes the maximum number of mounts that may exist | ||
271 | in a mount namespace. | ||
272 | |||
273 | ============================================================== | ||
274 | |||
268 | 275 | ||
269 | 2. /proc/sys/fs/binfmt_misc | 276 | 2. /proc/sys/fs/binfmt_misc |
270 | ---------------------------------------------------------- | 277 | ---------------------------------------------------------- |
diff --git a/fs/mount.h b/fs/mount.h index 6a61c2b3e385..2152c16ddf74 100644 --- a/fs/mount.h +++ b/fs/mount.h | |||
@@ -13,6 +13,8 @@ struct mnt_namespace { | |||
13 | u64 seq; /* Sequence number to prevent loops */ | 13 | u64 seq; /* Sequence number to prevent loops */ |
14 | wait_queue_head_t poll; | 14 | wait_queue_head_t poll; |
15 | u64 event; | 15 | u64 event; |
16 | unsigned int mounts; /* # of mounts in the namespace */ | ||
17 | unsigned int pending_mounts; | ||
16 | }; | 18 | }; |
17 | 19 | ||
18 | struct mnt_pcp { | 20 | struct mnt_pcp { |
diff --git a/fs/namespace.c b/fs/namespace.c index 556721fb0cf6..f853aaf92ec9 100644 --- a/fs/namespace.c +++ b/fs/namespace.c | |||
@@ -27,6 +27,9 @@ | |||
27 | #include "pnode.h" | 27 | #include "pnode.h" |
28 | #include "internal.h" | 28 | #include "internal.h" |
29 | 29 | ||
30 | /* Maximum number of mounts in a mount namespace */ | ||
31 | unsigned int sysctl_mount_max __read_mostly = 100000; | ||
32 | |||
30 | static unsigned int m_hash_mask __read_mostly; | 33 | static unsigned int m_hash_mask __read_mostly; |
31 | static unsigned int m_hash_shift __read_mostly; | 34 | static unsigned int m_hash_shift __read_mostly; |
32 | static unsigned int mp_hash_mask __read_mostly; | 35 | static unsigned int mp_hash_mask __read_mostly; |
@@ -888,6 +891,9 @@ static void commit_tree(struct mount *mnt, struct mount *shadows) | |||
888 | 891 | ||
889 | list_splice(&head, n->list.prev); | 892 | list_splice(&head, n->list.prev); |
890 | 893 | ||
894 | n->mounts += n->pending_mounts; | ||
895 | n->pending_mounts = 0; | ||
896 | |||
891 | attach_shadowed(mnt, parent, shadows); | 897 | attach_shadowed(mnt, parent, shadows); |
892 | touch_mnt_namespace(n); | 898 | touch_mnt_namespace(n); |
893 | } | 899 | } |
@@ -1408,11 +1414,16 @@ static void umount_tree(struct mount *mnt, enum umount_tree_flags how) | |||
1408 | propagate_umount(&tmp_list); | 1414 | propagate_umount(&tmp_list); |
1409 | 1415 | ||
1410 | while (!list_empty(&tmp_list)) { | 1416 | while (!list_empty(&tmp_list)) { |
1417 | struct mnt_namespace *ns; | ||
1411 | bool disconnect; | 1418 | bool disconnect; |
1412 | p = list_first_entry(&tmp_list, struct mount, mnt_list); | 1419 | p = list_first_entry(&tmp_list, struct mount, mnt_list); |
1413 | list_del_init(&p->mnt_expire); | 1420 | list_del_init(&p->mnt_expire); |
1414 | list_del_init(&p->mnt_list); | 1421 | list_del_init(&p->mnt_list); |
1415 | __touch_mnt_namespace(p->mnt_ns); | 1422 | ns = p->mnt_ns; |
1423 | if (ns) { | ||
1424 | ns->mounts--; | ||
1425 | __touch_mnt_namespace(ns); | ||
1426 | } | ||
1416 | p->mnt_ns = NULL; | 1427 | p->mnt_ns = NULL; |
1417 | if (how & UMOUNT_SYNC) | 1428 | if (how & UMOUNT_SYNC) |
1418 | p->mnt.mnt_flags |= MNT_SYNC_UMOUNT; | 1429 | p->mnt.mnt_flags |= MNT_SYNC_UMOUNT; |
@@ -1821,6 +1832,28 @@ static int invent_group_ids(struct mount *mnt, bool recurse) | |||
1821 | return 0; | 1832 | return 0; |
1822 | } | 1833 | } |
1823 | 1834 | ||
1835 | int count_mounts(struct mnt_namespace *ns, struct mount *mnt) | ||
1836 | { | ||
1837 | unsigned int max = READ_ONCE(sysctl_mount_max); | ||
1838 | unsigned int mounts = 0, old, pending, sum; | ||
1839 | struct mount *p; | ||
1840 | |||
1841 | for (p = mnt; p; p = next_mnt(p, mnt)) | ||
1842 | mounts++; | ||
1843 | |||
1844 | old = ns->mounts; | ||
1845 | pending = ns->pending_mounts; | ||
1846 | sum = old + pending; | ||
1847 | if ((old > sum) || | ||
1848 | (pending > sum) || | ||
1849 | (max < sum) || | ||
1850 | (mounts > (max - sum))) | ||
1851 | return -ENOSPC; | ||
1852 | |||
1853 | ns->pending_mounts = pending + mounts; | ||
1854 | return 0; | ||
1855 | } | ||
1856 | |||
1824 | /* | 1857 | /* |
1825 | * @source_mnt : mount tree to be attached | 1858 | * @source_mnt : mount tree to be attached |
1826 | * @nd : place the mount tree @source_mnt is attached | 1859 | * @nd : place the mount tree @source_mnt is attached |
@@ -1890,10 +1923,18 @@ static int attach_recursive_mnt(struct mount *source_mnt, | |||
1890 | struct path *parent_path) | 1923 | struct path *parent_path) |
1891 | { | 1924 | { |
1892 | HLIST_HEAD(tree_list); | 1925 | HLIST_HEAD(tree_list); |
1926 | struct mnt_namespace *ns = dest_mnt->mnt_ns; | ||
1893 | struct mount *child, *p; | 1927 | struct mount *child, *p; |
1894 | struct hlist_node *n; | 1928 | struct hlist_node *n; |
1895 | int err; | 1929 | int err; |
1896 | 1930 | ||
1931 | /* Is there space to add these mounts to the mount namespace? */ | ||
1932 | if (!parent_path) { | ||
1933 | err = count_mounts(ns, source_mnt); | ||
1934 | if (err) | ||
1935 | goto out; | ||
1936 | } | ||
1937 | |||
1897 | if (IS_MNT_SHARED(dest_mnt)) { | 1938 | if (IS_MNT_SHARED(dest_mnt)) { |
1898 | err = invent_group_ids(source_mnt, true); | 1939 | err = invent_group_ids(source_mnt, true); |
1899 | if (err) | 1940 | if (err) |
@@ -1930,11 +1971,13 @@ static int attach_recursive_mnt(struct mount *source_mnt, | |||
1930 | out_cleanup_ids: | 1971 | out_cleanup_ids: |
1931 | while (!hlist_empty(&tree_list)) { | 1972 | while (!hlist_empty(&tree_list)) { |
1932 | child = hlist_entry(tree_list.first, struct mount, mnt_hash); | 1973 | child = hlist_entry(tree_list.first, struct mount, mnt_hash); |
1974 | child->mnt_parent->mnt_ns->pending_mounts = 0; | ||
1933 | umount_tree(child, UMOUNT_SYNC); | 1975 | umount_tree(child, UMOUNT_SYNC); |
1934 | } | 1976 | } |
1935 | unlock_mount_hash(); | 1977 | unlock_mount_hash(); |
1936 | cleanup_group_ids(source_mnt, NULL); | 1978 | cleanup_group_ids(source_mnt, NULL); |
1937 | out: | 1979 | out: |
1980 | ns->pending_mounts = 0; | ||
1938 | return err; | 1981 | return err; |
1939 | } | 1982 | } |
1940 | 1983 | ||
@@ -2758,6 +2801,8 @@ static struct mnt_namespace *alloc_mnt_ns(struct user_namespace *user_ns) | |||
2758 | init_waitqueue_head(&new_ns->poll); | 2801 | init_waitqueue_head(&new_ns->poll); |
2759 | new_ns->event = 0; | 2802 | new_ns->event = 0; |
2760 | new_ns->user_ns = get_user_ns(user_ns); | 2803 | new_ns->user_ns = get_user_ns(user_ns); |
2804 | new_ns->mounts = 0; | ||
2805 | new_ns->pending_mounts = 0; | ||
2761 | return new_ns; | 2806 | return new_ns; |
2762 | } | 2807 | } |
2763 | 2808 | ||
@@ -2807,6 +2852,7 @@ struct mnt_namespace *copy_mnt_ns(unsigned long flags, struct mnt_namespace *ns, | |||
2807 | q = new; | 2852 | q = new; |
2808 | while (p) { | 2853 | while (p) { |
2809 | q->mnt_ns = new_ns; | 2854 | q->mnt_ns = new_ns; |
2855 | new_ns->mounts++; | ||
2810 | if (new_fs) { | 2856 | if (new_fs) { |
2811 | if (&p->mnt == new_fs->root.mnt) { | 2857 | if (&p->mnt == new_fs->root.mnt) { |
2812 | new_fs->root.mnt = mntget(&q->mnt); | 2858 | new_fs->root.mnt = mntget(&q->mnt); |
@@ -2845,6 +2891,7 @@ static struct mnt_namespace *create_mnt_ns(struct vfsmount *m) | |||
2845 | struct mount *mnt = real_mount(m); | 2891 | struct mount *mnt = real_mount(m); |
2846 | mnt->mnt_ns = new_ns; | 2892 | mnt->mnt_ns = new_ns; |
2847 | new_ns->root = mnt; | 2893 | new_ns->root = mnt; |
2894 | new_ns->mounts++; | ||
2848 | list_add(&mnt->mnt_list, &new_ns->list); | 2895 | list_add(&mnt->mnt_list, &new_ns->list); |
2849 | } else { | 2896 | } else { |
2850 | mntput(m); | 2897 | mntput(m); |
diff --git a/fs/pnode.c b/fs/pnode.c index 99899705b105..234a9ac49958 100644 --- a/fs/pnode.c +++ b/fs/pnode.c | |||
@@ -259,7 +259,7 @@ static int propagate_one(struct mount *m) | |||
259 | read_sequnlock_excl(&mount_lock); | 259 | read_sequnlock_excl(&mount_lock); |
260 | } | 260 | } |
261 | hlist_add_head(&child->mnt_hash, list); | 261 | hlist_add_head(&child->mnt_hash, list); |
262 | return 0; | 262 | return count_mounts(m->mnt_ns, child); |
263 | } | 263 | } |
264 | 264 | ||
265 | /* | 265 | /* |
diff --git a/fs/pnode.h b/fs/pnode.h index 0fcdbe7ca648..550f5a8b4fcf 100644 --- a/fs/pnode.h +++ b/fs/pnode.h | |||
@@ -52,4 +52,5 @@ void mnt_set_mountpoint(struct mount *, struct mountpoint *, | |||
52 | struct mount *copy_tree(struct mount *, struct dentry *, int); | 52 | struct mount *copy_tree(struct mount *, struct dentry *, int); |
53 | bool is_path_reachable(struct mount *, struct dentry *, | 53 | bool is_path_reachable(struct mount *, struct dentry *, |
54 | const struct path *root); | 54 | const struct path *root); |
55 | int count_mounts(struct mnt_namespace *ns, struct mount *mnt); | ||
55 | #endif /* _LINUX_PNODE_H */ | 56 | #endif /* _LINUX_PNODE_H */ |
diff --git a/include/linux/mount.h b/include/linux/mount.h index f822c3c11377..dc6cd800cd5d 100644 --- a/include/linux/mount.h +++ b/include/linux/mount.h | |||
@@ -95,4 +95,6 @@ extern void mark_mounts_for_expiry(struct list_head *mounts); | |||
95 | 95 | ||
96 | extern dev_t name_to_dev_t(const char *name); | 96 | extern dev_t name_to_dev_t(const char *name); |
97 | 97 | ||
98 | extern unsigned int sysctl_mount_max; | ||
99 | |||
98 | #endif /* _LINUX_MOUNT_H */ | 100 | #endif /* _LINUX_MOUNT_H */ |
diff --git a/kernel/sysctl.c b/kernel/sysctl.c index 7d4900404c94..cebbff5f34fe 100644 --- a/kernel/sysctl.c +++ b/kernel/sysctl.c | |||
@@ -64,6 +64,7 @@ | |||
64 | #include <linux/binfmts.h> | 64 | #include <linux/binfmts.h> |
65 | #include <linux/sched/sysctl.h> | 65 | #include <linux/sched/sysctl.h> |
66 | #include <linux/kexec.h> | 66 | #include <linux/kexec.h> |
67 | #include <linux/mount.h> | ||
67 | 68 | ||
68 | #include <asm/uaccess.h> | 69 | #include <asm/uaccess.h> |
69 | #include <asm/processor.h> | 70 | #include <asm/processor.h> |
@@ -1709,6 +1710,14 @@ static struct ctl_table fs_table[] = { | |||
1709 | .mode = 0644, | 1710 | .mode = 0644, |
1710 | .proc_handler = proc_doulongvec_minmax, | 1711 | .proc_handler = proc_doulongvec_minmax, |
1711 | }, | 1712 | }, |
1713 | { | ||
1714 | .procname = "mount-max", | ||
1715 | .data = &sysctl_mount_max, | ||
1716 | .maxlen = sizeof(unsigned int), | ||
1717 | .mode = 0644, | ||
1718 | .proc_handler = proc_dointvec_minmax, | ||
1719 | .extra1 = &one, | ||
1720 | }, | ||
1712 | { } | 1721 | { } |
1713 | }; | 1722 | }; |
1714 | 1723 | ||