diff options
author | Jan Kara | 2017-07-30 22:33:01 -0500 |
---|---|---|
committer | Greg Kroah-Hartman | 2017-10-12 04:27:35 -0500 |
commit | 4f22f0793ccedb43a8fd47c20943a777228b2265 (patch) | |
tree | 7aa7c0fea6d948a3ee84731a2654d506460b8f35 | |
parent | 40c00e5fac3abbd5e6fa08e93fa99b3e632ece16 (diff) | |
download | ti-linux-kernel-4f22f0793ccedb43a8fd47c20943a777228b2265.tar.gz ti-linux-kernel-4f22f0793ccedb43a8fd47c20943a777228b2265.tar.xz ti-linux-kernel-4f22f0793ccedb43a8fd47c20943a777228b2265.zip |
ext4: Don't clear SGID when inheriting ACLs
commit a3bb2d5587521eea6dab2d05326abb0afb460abd upstream.
When new directory 'DIR1' is created in a directory 'DIR0' with SGID bit
set, DIR1 is expected to have SGID bit set (and owning group equal to
the owning group of 'DIR0'). However when 'DIR0' also has some default
ACLs that 'DIR1' inherits, setting these ACLs will result in SGID bit on
'DIR1' to get cleared if user is not member of the owning group.
Fix the problem by moving posix_acl_update_mode() out of
__ext4_set_acl() into ext4_set_acl(). That way the function will not be
called when inheriting ACLs which is what we want as it prevents SGID
bit clearing and the mode has been properly set by posix_acl_create()
anyway.
Fixes: 073931017b49d9458aa351605b43a7e34598caef
Signed-off-by: Theodore Ts'o <tytso@mit.edu>
Signed-off-by: Jan Kara <jack@suse.cz>
Reviewed-by: Andreas Gruenbacher <agruenba@redhat.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
-rw-r--r-- | fs/ext4/acl.c | 22 |
1 files changed, 15 insertions, 7 deletions
diff --git a/fs/ext4/acl.c b/fs/ext4/acl.c index c3fe1e323951..ea2ef0eac0c4 100644 --- a/fs/ext4/acl.c +++ b/fs/ext4/acl.c | |||
@@ -195,13 +195,6 @@ __ext4_set_acl(handle_t *handle, struct inode *inode, int type, | |||
195 | switch (type) { | 195 | switch (type) { |
196 | case ACL_TYPE_ACCESS: | 196 | case ACL_TYPE_ACCESS: |
197 | name_index = EXT4_XATTR_INDEX_POSIX_ACL_ACCESS; | 197 | name_index = EXT4_XATTR_INDEX_POSIX_ACL_ACCESS; |
198 | if (acl) { | ||
199 | error = posix_acl_update_mode(inode, &inode->i_mode, &acl); | ||
200 | if (error) | ||
201 | return error; | ||
202 | inode->i_ctime = ext4_current_time(inode); | ||
203 | ext4_mark_inode_dirty(handle, inode); | ||
204 | } | ||
205 | break; | 198 | break; |
206 | 199 | ||
207 | case ACL_TYPE_DEFAULT: | 200 | case ACL_TYPE_DEFAULT: |
@@ -234,6 +227,8 @@ ext4_set_acl(struct inode *inode, struct posix_acl *acl, int type) | |||
234 | { | 227 | { |
235 | handle_t *handle; | 228 | handle_t *handle; |
236 | int error, retries = 0; | 229 | int error, retries = 0; |
230 | umode_t mode = inode->i_mode; | ||
231 | int update_mode = 0; | ||
237 | 232 | ||
238 | retry: | 233 | retry: |
239 | handle = ext4_journal_start(inode, EXT4_HT_XATTR, | 234 | handle = ext4_journal_start(inode, EXT4_HT_XATTR, |
@@ -241,7 +236,20 @@ retry: | |||
241 | if (IS_ERR(handle)) | 236 | if (IS_ERR(handle)) |
242 | return PTR_ERR(handle); | 237 | return PTR_ERR(handle); |
243 | 238 | ||
239 | if ((type == ACL_TYPE_ACCESS) && acl) { | ||
240 | error = posix_acl_update_mode(inode, &mode, &acl); | ||
241 | if (error) | ||
242 | goto out_stop; | ||
243 | update_mode = 1; | ||
244 | } | ||
245 | |||
244 | error = __ext4_set_acl(handle, inode, type, acl); | 246 | error = __ext4_set_acl(handle, inode, type, acl); |
247 | if (!error && update_mode) { | ||
248 | inode->i_mode = mode; | ||
249 | inode->i_ctime = ext4_current_time(inode); | ||
250 | ext4_mark_inode_dirty(handle, inode); | ||
251 | } | ||
252 | out_stop: | ||
245 | ext4_journal_stop(handle); | 253 | ext4_journal_stop(handle); |
246 | if (error == -ENOSPC && ext4_should_retry_alloc(inode->i_sb, &retries)) | 254 | if (error == -ENOSPC && ext4_should_retry_alloc(inode->i_sb, &retries)) |
247 | goto retry; | 255 | goto retry; |