diff options
author | Linus Torvalds | 2015-11-10 20:11:41 -0600 |
---|---|---|
committer | Linus Torvalds | 2015-11-10 20:11:41 -0600 |
commit | 2df4ee78d042ee3d17cbebd51e31b300286549dc (patch) | |
tree | 7c723c99569e1f1a81490d7b31e5d6af27b6d169 /Documentation/devicetree | |
parent | 3419b45039c6b799c974a8019361c045e7ca232c (diff) | |
parent | 8a921265e2cd31e61a0c2eda582af54c5bfef897 (diff) | |
download | ti-linux-kernel-2df4ee78d042ee3d17cbebd51e31b300286549dc.tar.gz ti-linux-kernel-2df4ee78d042ee3d17cbebd51e31b300286549dc.tar.xz ti-linux-kernel-2df4ee78d042ee3d17cbebd51e31b300286549dc.zip |
Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net
Pull networking fixes from David Miller:
1) Fix null deref in xt_TEE netfilter module, from Eric Dumazet.
2) Several spots need to get to the original listner for SYN-ACK
packets, most spots got this ok but some were not. Whilst covering
the remaining cases, create a helper to do this. From Eric Dumazet.
3) Missiing check of return value from alloc_netdev() in CAIF SPI code,
from Rasmus Villemoes.
4) Don't sleep while != TASK_RUNNING in macvtap, from Vlad Yasevich.
5) Use after free in mvneta driver, from Justin Maggard.
6) Fix race on dst->flags access in dst_release(), from Eric Dumazet.
7) Add missing ZLIB_INFLATE dependency for new qed driver. From Arnd
Bergmann.
8) Fix multicast getsockopt deadlock, from WANG Cong.
9) Fix deadlock in btusb, from Kuba Pawlak.
10) Some ipv6_add_dev() failure paths were not cleaning up the SNMP6
counter state. From Sabrina Dubroca.
11) Fix packet_bind() race, which can cause lost notifications, from
Francesco Ruggeri.
12) Fix MAC restoration in qlcnic driver during bonding mode changes,
from Jarod Wilson.
13) Revert bridging forward delay change which broke libvirt and other
userspace things, from Vlad Yasevich.
* git://git.kernel.org/pub/scm/linux/kernel/git/davem/net: (65 commits)
Revert "bridge: Allow forward delay to be cfgd when STP enabled"
bpf_trace: Make dependent on PERF_EVENTS
qed: select ZLIB_INFLATE
net: fix a race in dst_release()
net: mvneta: Fix memory use after free.
net: Documentation: Fix default value tcp_limit_output_bytes
macvtap: Resolve possible __might_sleep warning in macvtap_do_read()
mvneta: add FIXED_PHY dependency
net: caif: check return value of alloc_netdev
net: hisilicon: NET_VENDOR_HISILICON should depend on HAS_DMA
drivers: net: xgene: fix RGMII 10/100Mb mode
netfilter: nft_meta: use skb_to_full_sk() helper
net_sched: em_meta: use skb_to_full_sk() helper
sched: cls_flow: use skb_to_full_sk() helper
netfilter: xt_owner: use skb_to_full_sk() helper
smack: use skb_to_full_sk() helper
net: add skb_to_full_sk() helper and use it in selinux_netlbl_skbuff_setsid()
bpf: doc: correct arch list for supported eBPF JIT
dwc_eth_qos: Delete an unnecessary check before the function call "of_node_put"
bonding: fix panic on non-ARPHRD_ETHER enslave failure
...
Diffstat (limited to 'Documentation/devicetree')
-rw-r--r-- | Documentation/devicetree/bindings/net/cpsw.txt | 5 |
1 files changed, 5 insertions, 0 deletions
diff --git a/Documentation/devicetree/bindings/net/cpsw.txt b/Documentation/devicetree/bindings/net/cpsw.txt index 4efca560adda..9853f8e70966 100644 --- a/Documentation/devicetree/bindings/net/cpsw.txt +++ b/Documentation/devicetree/bindings/net/cpsw.txt | |||
@@ -48,6 +48,11 @@ Optional properties: | |||
48 | - mac-address : See ethernet.txt file in the same directory | 48 | - mac-address : See ethernet.txt file in the same directory |
49 | - phy-handle : See ethernet.txt file in the same directory | 49 | - phy-handle : See ethernet.txt file in the same directory |
50 | 50 | ||
51 | Slave sub-nodes: | ||
52 | - fixed-link : See fixed-link.txt file in the same directory | ||
53 | Either the properties phy_id and phy-mode, | ||
54 | or the sub-node fixed-link can be specified | ||
55 | |||
51 | Note: "ti,hwmods" field is used to fetch the base address and irq | 56 | Note: "ti,hwmods" field is used to fetch the base address and irq |
52 | resources from TI, omap hwmod data base during device registration. | 57 | resources from TI, omap hwmod data base during device registration. |
53 | Future plan is to migrate hwmod data base contents into device tree | 58 | Future plan is to migrate hwmod data base contents into device tree |