diff options
Diffstat (limited to 'fs/utimes.c')
-rw-r--r-- | fs/utimes.c | 4 |
1 files changed, 2 insertions, 2 deletions
diff --git a/fs/utimes.c b/fs/utimes.c index aa138d64560a..61abc3051377 100644 --- a/fs/utimes.c +++ b/fs/utimes.c | |||
@@ -81,7 +81,7 @@ static int utimes_common(struct path *path, struct timespec *times) | |||
81 | newattrs.ia_valid |= ATTR_MTIME_SET; | 81 | newattrs.ia_valid |= ATTR_MTIME_SET; |
82 | } | 82 | } |
83 | /* | 83 | /* |
84 | * Tell inode_change_ok(), that this is an explicit time | 84 | * Tell setattr_prepare(), that this is an explicit time |
85 | * update, even if neither ATTR_ATIME_SET nor ATTR_MTIME_SET | 85 | * update, even if neither ATTR_ATIME_SET nor ATTR_MTIME_SET |
86 | * were used. | 86 | * were used. |
87 | */ | 87 | */ |
@@ -90,7 +90,7 @@ static int utimes_common(struct path *path, struct timespec *times) | |||
90 | /* | 90 | /* |
91 | * If times is NULL (or both times are UTIME_NOW), | 91 | * If times is NULL (or both times are UTIME_NOW), |
92 | * then we need to check permissions, because | 92 | * then we need to check permissions, because |
93 | * inode_change_ok() won't do it. | 93 | * setattr_prepare() won't do it. |
94 | */ | 94 | */ |
95 | error = -EACCES; | 95 | error = -EACCES; |
96 | if (IS_IMMUTABLE(inode)) | 96 | if (IS_IMMUTABLE(inode)) |