aboutsummaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* Linux 5.10.215v5.10.215linux-5.10.yGreg Kroah-Hartman3 days1-1/+1
* x86/head/64: Re-enable stack protectionMichael Roth3 days4-14/+21
* x86/retpoline: Add NOENDBR annotation to the SRSO dummy return thunkBorislav Petkov (AMD)3 days1-0/+1
* scsi: sd: Fix wrong zone_write_granularity value during revalidateShin'ichiro Kawasaki3 days2-9/+6
* kbuild: dummy-tools: adjust to stricter stackprotector checkMichal Kubecek3 days1-1/+5
* VMCI: Fix possible memcpy() run-time warning in vmci_datagram_invoke_guest_ha...Vasiliy Kovalev3 days1-1/+2
* Bluetooth: btintel: Fixe build regressionLuiz Augusto von Dentz3 days1-2/+2
* drm/i915/gt: Reset queue_priority_hint on parkingChris Wilson3 days2-3/+3
* x86/mm/pat: fix VM_PAT handling in COW mappingsDavid Hildenbrand3 days2-14/+40
* virtio: reenable config if freezing device failedDavid Hildenbrand3 days1-2/+8
* tty: n_gsm: require CAP_NET_ADMIN to attach N_GSM0710 ldiscThadeu Lima de Souza Cascardo3 days1-0/+3
* netfilter: nf_tables: discard table flag update with pending basechain deletionPablo Neira Ayuso3 days1-1/+19
* netfilter: nf_tables: release mutex after nft_gc_seq_end from abort pathPablo Neira Ayuso3 days1-5/+8
* netfilter: nf_tables: release batch on table validation from abort pathPablo Neira Ayuso3 days1-4/+10
* fbmon: prevent division by zero in fb_videomode_from_videomode()Roman Smirnov3 days1-3/+4
* drivers/nvme: Add quirks for device 126f:2262Jiawei Fu (iBug)3 days1-0/+3
* fbdev: viafb: fix typo in hw_bitblt_1 and hw_bitblt_2Aleksandr Burakov3 days1-2/+2
* usb: sl811-hcd: only defined function checkdone if QUIRK2 is definedColin Ian King3 days1-0/+2
* usb: typec: tcpci: add generic tcpci fallback compatibleMarco Felsch3 days1-0/+1
* tools: iio: replace seekdir() in iio_generic_bufferPetre Rodan3 days1-1/+1
* ring-buffer: use READ_ONCE() to read cpu_buffer->commit_page in concurrent en...linke li3 days1-1/+1
* ktest: force $buildonly = 1 for 'make_warnings_file' test typeRicardo B. Marliere3 days1-0/+1
* platform/x86: touchscreen_dmi: Add an extra entry for a variant of the Chuwi ...Alban Boyé3 days1-0/+9
* Input: allocate keycode for Display refresh rate toggleGergo Koteles3 days1-0/+1
* RDMA/cm: add timeout to cm_destroy_id waitManjunath Patil3 days1-1/+19
* block: prevent division by zero in blk_rq_stat_sum()Roman Smirnov3 days1-1/+1
* libperf evlist: Avoid out-of-bounds accessIan Rogers3 days2-8/+14
* Revert "ACPI: PM: Block ASUS B1400CEAE from suspend to idle by default"Daniel Drake3 days1-12/+0
* SUNRPC: increase size of rpc_wait_queue.qlen from unsigned short to unsigned intDai Ngo3 days1-1/+1
* drm/amd/display: Fix nanosec stat overflowAric Cyr3 days1-2/+2
* ext4: forbid commit inconsistent quota data when errors=remount-roYe Bin3 days1-0/+12
* ext4: add a hint for block bitmap corrupt state in mb_groupsZhang Yi3 days1-1/+4
* media: sta2x11: fix irq handler castArnd Bergmann3 days1-5/+4
* isofs: handle CDs with bad root inode but good Joliet root directoryAlex Henrie3 days1-2/+16
* scsi: lpfc: Fix possible memory leak in lpfc_rcv_padisc()Justin Tee3 days1-2/+4
* sysv: don't call sb_bread() with pointers_lock heldTetsuo Handa3 days1-6/+4
* pinctrl: renesas: checker: Limit cfg reg enum checks to provided IDsGeert Uytterhoeven3 days1-1/+3
* Input: synaptics-rmi4 - fail probing if memory allocation for "phys" failsKunwu Chan3 days1-1/+5
* Bluetooth: btintel: Fix null ptr deref in btintel_read_versionEdward Adam Davis3 days1-1/+1
* net/smc: reduce rtnl pressure in smc_pnet_create_pnetids_list()Eric Dumazet3 days1-0/+10
* btrfs: send: handle path ref underflow in header iterate_inode_ref()David Sterba3 days1-1/+9
* btrfs: export: handle invalid inode or root reference in btrfs_get_parent()David Sterba3 days1-1/+8
* btrfs: handle chunk tree lookup error in btrfs_relocate_sys_chunks()David Sterba3 days1-1/+11
* tools/power x86_energy_perf_policy: Fix file leak in get_pkg_num()Samasth Norway Ananda3 days1-0/+1
* pstore/zone: Add a null pointer check to the psz_kmsg_readKunwu Chan3 days1-0/+2
* ionic: set adminq irq affinityShannon Nelson3 days1-1/+4
* arm64: dts: rockchip: fix rk3399 hdmi ports nodeJohan Jonker3 days1-2/+10
* arm64: dts: rockchip: fix rk3328 hdmi ports nodeJohan Jonker3 days1-1/+10
* panic: Flush kernel log buffer at the endJohn Ogness3 days1-0/+8
* VMCI: Fix memcpy() run-time warning in dg_dispatch_as_host()Harshit Mogalapalli3 days1-1/+2