aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* Linux 4.4.93HEADv4.4.93masterGreg Kroah-Hartman2017-10-181-1/+1
|
* x86/alternatives: Fix alt_max_short macro to really be a max()Mathias Krause2017-10-182-4/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 6b32c126d33d5cb379bca280ab8acedc1ca978ff upstream. The alt_max_short() macro in asm/alternative.h does not work as intended, leading to nasty bugs. E.g. alt_max_short("1", "3") evaluates to 3, but alt_max_short("3", "1") evaluates to 1 -- not exactly the maximum of 1 and 3. In fact, I had to learn it the hard way by crashing my kernel in not so funny ways by attempting to make use of the ALTENATIVE_2 macro with alternatives where the first one was larger than the second one. According to [1] and commit dbe4058a6a44 ("x86/alternatives: Fix ALTERNATIVE_2 padding generation properly") the right handed side should read "-(-(a < b))" not "-(-(a - b))". Fix that, to make the macro work as intended. While at it, fix up the comments regarding the additional "-", too. It's not about gas' usage of s32 but brain dead logic of having a "true" value of -1 for the < operator ... *sigh* Btw., the one in asm/alternative-asm.h is correct. And, apparently, all current users of ALTERNATIVE_2() pass same sized alternatives, avoiding to hit the bug. [1] http://graphics.stanford.edu/~seander/bithacks.html#IntegerMinOrMax Reviewed-and-tested-by: Borislav Petkov <bp@suse.de> Fixes: dbe4058a6a44 ("x86/alternatives: Fix ALTERNATIVE_2 padding generation properly") Signed-off-by: Mathias Krause <minipli@googlemail.com> Signed-off-by: Thomas Gleixner <tglx@linutronix.de> Cc: Borislav Petkov <bp@suse.de> Link: https://lkml.kernel.org/r/1507228213-13095-1-git-send-email-minipli@googlemail.com Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: serial: console: fix use-after-free after failed setupJohan Hovold2017-10-181-0/+1
| | | | | | | | | | | | | | commit 299d7572e46f98534033a9e65973f13ad1ce9047 upstream. Make sure to reset the USB-console port pointer when console setup fails in order to avoid having the struct usb_serial be prematurely freed by the console code when the device is later disconnected. Fixes: 73e487fdb75f ("[PATCH] USB console: fix disconnection issues") Acked-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org> Signed-off-by: Johan Hovold <johan@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: serial: qcserial: add Dell DW5818, DW5819Shrirang Bagul2017-10-181-0/+4
| | | | | | | | | | | | | commit f5d9644c5fca7d8e8972268598bb516a7eae17f9 upstream. Dell Wireless 5819/5818 devices are re-branded Sierra Wireless MC74 series which will by default boot with vid 0x413c and pid's 0x81cf, 0x81d0, 0x81d1, 0x81d2. Signed-off-by: Shrirang Bagul <shrirang.bagul@canonical.com> Signed-off-by: Johan Hovold <johan@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: serial: option: add support for TP-Link LTE moduleHenryk Heisig2017-10-181-0/+2
| | | | | | | | | | | | commit 837ddc4793a69b256ac5e781a5e729b448a8d983 upstream. This commit adds support for TP-Link LTE mPCIe module is used in in TP-Link MR200v1, MR6400v1 and v2 routers. Signed-off-by: Henryk Heisig <hyniu@o2.pl> Signed-off-by: Johan Hovold <johan@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: serial: cp210x: add support for ELV TFD500Andreas Engel2017-10-181-0/+1
| | | | | | | | | | | commit c496ad835c31ad639b6865714270b3003df031f6 upstream. Add the USB device id for the ELV TFD500 data logger. Signed-off-by: Andreas Engel <anen-nospam@gmx.net> Signed-off-by: Johan Hovold <johan@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: serial: ftdi_sio: add id for Cypress WICED dev boardJeffrey Chu2017-10-182-0/+9
| | | | | | | | | | | | commit a6c215e21b0dc5fe9416dce90f9acc2ea53c4502 upstream. Add CYPRESS_VID vid and CYPRESS_WICED_BT_USB and CYPRESS_WICED_WL_USB device IDs to ftdi_sio driver. Signed-off-by: Jeffrey Chu <jeffrey.chu@cypress.com> Signed-off-by: Johan Hovold <johan@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* fix unbalanced page refcounting in bio_map_user_iovVitaly Mayatskikh2017-10-181-0/+8
| | | | | | | | | | | | | | commit 95d78c28b5a85bacbc29b8dba7c04babb9b0d467 upstream. bio_map_user_iov and bio_unmap_user do unbalanced pages refcounting if IO vector has small consecutive buffers belonging to the same page. bio_add_pc_page merges them into one, but the page reference is never dropped. Signed-off-by: Vitaly Mayatskikh <v.mayatskih@gmail.com> Signed-off-by: Al Viro <viro@zeniv.linux.org.uk> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* direct-io: Prevent NULL pointer access in submit_page_sectionAndreas Gruenbacher2017-10-181-1/+2
| | | | | | | | | | | | | | | | | commit 899f0429c7d3eed886406cd72182bee3b96aa1f9 upstream. In the code added to function submit_page_section by commit b1058b981, sdio->bio can currently be NULL when calling dio_bio_submit. This then leads to a NULL pointer access in dio_bio_submit, so check for a NULL bio in submit_page_section before trying to submit it instead. Fixes xfstest generic/250 on gfs2. Signed-off-by: Andreas Gruenbacher <agruenba@redhat.com> Reviewed-by: Jan Kara <jack@suse.cz> Signed-off-by: Al Viro <viro@zeniv.linux.org.uk> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* usb: gadget: composite: Fix use-after-free in usb_composite_overwrite_optionsAndrew Gabbasov2017-10-181-0/+5
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit aec17e1e249567e82b26dafbb86de7d07fde8729 upstream. KASAN enabled configuration reports an error BUG: KASAN: use-after-free in usb_composite_overwrite_options+... [libcomposite] at addr ... Read of size 1 by task ... when some driver is un-bound and then bound again. For example, this happens with FunctionFS driver when "ffs-test" test application is run several times in a row. If the driver has empty manufacturer ID string in initial static data, it is then replaced with generated string. After driver unbinding the generated string is freed, but the driver data still keep that pointer. And if the driver is then bound again, that pointer is re-used for string emptiness check. The fix is to clean up the driver string data upon its unbinding to drop the pointer to freed memory. Fixes: cc2683c318a5 ("usb: gadget: Provide a default implementation of default manufacturer string") Signed-off-by: Andrew Gabbasov <andrew_gabbasov@mentor.com> Signed-off-by: Felipe Balbi <felipe.balbi@linux.intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ALSA: line6: Fix leftover URB at error-path during probeTakashi Iwai2017-10-181-3/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit c95072b3d88fac4be295815f2b67df366c0c297f upstream. While line6_probe() may kick off URB for a control MIDI endpoint, the function doesn't clean up it properly at its error path. This results in a leftover URB action that is eventually triggered later and causes an Oops like: general protection fault: 0000 [#1] PREEMPT SMP KASAN CPU: 1 PID: 0 Comm: swapper/1 Not tainted RIP: 0010:usb_fill_bulk_urb ./include/linux/usb.h:1619 RIP: 0010:line6_start_listen+0x3fe/0x9e0 sound/usb/line6/driver.c:76 Call Trace: <IRQ> line6_data_received+0x1f7/0x470 sound/usb/line6/driver.c:326 __usb_hcd_giveback_urb+0x2e0/0x650 drivers/usb/core/hcd.c:1779 usb_hcd_giveback_urb+0x337/0x420 drivers/usb/core/hcd.c:1845 dummy_timer+0xba9/0x39f0 drivers/usb/gadget/udc/dummy_hcd.c:1965 call_timer_fn+0x2a2/0x940 kernel/time/timer.c:1281 .... Since the whole clean-up procedure is done in line6_disconnect() callback, we can simply call it in the error path instead of open-coding the whole again. It'll fix such an issue automagically. The bug was spotted by syzkaller. Fixes: eedd0e95d355 ("ALSA: line6: Don't forget to call driver's destructor at error path") Reported-by: Andrey Konovalov <andreyknvl@google.com> Tested-by: Andrey Konovalov <andreyknvl@google.com> Signed-off-by: Takashi Iwai <tiwai@suse.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ALSA: caiaq: Fix stray URB at probe error pathTakashi Iwai2017-10-181-3/+9
| | | | | | | | | | | | | | commit 99fee508245825765ff60155fed43f970ff83a8f upstream. caiaq driver doesn't kill the URB properly at its error path during the probe, which may lead to a use-after-free error later. This patch addresses it. Reported-by: Johan Hovold <johan@kernel.org> Reviewed-by: Johan Hovold <johan@kernel.org> Signed-off-by: Takashi Iwai <tiwai@suse.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ALSA: seq: Fix copy_from_user() call inside lockTakashi Iwai2017-10-182-8/+20
| | | | | | | | | | | | | | | | | | | | | | | | commit 5803b023881857db32ffefa0d269c90280a67ee0 upstream. The event handler in the virmidi sequencer code takes a read-lock for the linked list traverse, while it's calling snd_seq_dump_var_event() in the loop. The latter function may expand the user-space data depending on the event type. It eventually invokes copy_from_user(), which might be a potential dead-lock. The sequencer core guarantees that the user-space data is passed only with atomic=0 argument, but snd_virmidi_dev_receive_event() ignores it and always takes read-lock(). For avoiding the problem above, this patch introduces rwsem for non-atomic case, while keeping rwlock for atomic case. Also while we're at it: the superfluous irq flags is dropped in snd_virmidi_input_open(). Reported-by: Jia-Ju Bai <baijiaju1990@163.com> Signed-off-by: Takashi Iwai <tiwai@suse.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ALSA: seq: Fix use-after-free at creating a portTakashi Iwai2017-10-182-3/+10
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 71105998845fb012937332fe2e806d443c09e026 upstream. There is a potential race window opened at creating and deleting a port via ioctl, as spotted by fuzzing. snd_seq_create_port() creates a port object and returns its pointer, but it doesn't take the refcount, thus it can be deleted immediately by another thread. Meanwhile, snd_seq_ioctl_create_port() still calls the function snd_seq_system_client_ev_port_start() with the created port object that is being deleted, and this triggers use-after-free like: BUG: KASAN: use-after-free in snd_seq_ioctl_create_port+0x504/0x630 [snd_seq] at addr ffff8801f2241cb1 ============================================================================= BUG kmalloc-512 (Tainted: G B ): kasan: bad access detected ----------------------------------------------------------------------------- INFO: Allocated in snd_seq_create_port+0x94/0x9b0 [snd_seq] age=1 cpu=3 pid=4511 ___slab_alloc+0x425/0x460 __slab_alloc+0x20/0x40 kmem_cache_alloc_trace+0x150/0x190 snd_seq_create_port+0x94/0x9b0 [snd_seq] snd_seq_ioctl_create_port+0xd1/0x630 [snd_seq] snd_seq_do_ioctl+0x11c/0x190 [snd_seq] snd_seq_ioctl+0x40/0x80 [snd_seq] do_vfs_ioctl+0x54b/0xda0 SyS_ioctl+0x79/0x90 entry_SYSCALL_64_fastpath+0x16/0x75 INFO: Freed in port_delete+0x136/0x1a0 [snd_seq] age=1 cpu=2 pid=4717 __slab_free+0x204/0x310 kfree+0x15f/0x180 port_delete+0x136/0x1a0 [snd_seq] snd_seq_delete_port+0x235/0x350 [snd_seq] snd_seq_ioctl_delete_port+0xc8/0x180 [snd_seq] snd_seq_do_ioctl+0x11c/0x190 [snd_seq] snd_seq_ioctl+0x40/0x80 [snd_seq] do_vfs_ioctl+0x54b/0xda0 SyS_ioctl+0x79/0x90 entry_SYSCALL_64_fastpath+0x16/0x75 Call Trace: [<ffffffff81b03781>] dump_stack+0x63/0x82 [<ffffffff81531b3b>] print_trailer+0xfb/0x160 [<ffffffff81536db4>] object_err+0x34/0x40 [<ffffffff815392d3>] kasan_report.part.2+0x223/0x520 [<ffffffffa07aadf4>] ? snd_seq_ioctl_create_port+0x504/0x630 [snd_seq] [<ffffffff815395fe>] __asan_report_load1_noabort+0x2e/0x30 [<ffffffffa07aadf4>] snd_seq_ioctl_create_port+0x504/0x630 [snd_seq] [<ffffffffa07aa8f0>] ? snd_seq_ioctl_delete_port+0x180/0x180 [snd_seq] [<ffffffff8136be50>] ? taskstats_exit+0xbc0/0xbc0 [<ffffffffa07abc5c>] snd_seq_do_ioctl+0x11c/0x190 [snd_seq] [<ffffffffa07abd10>] snd_seq_ioctl+0x40/0x80 [snd_seq] [<ffffffff8136d433>] ? acct_account_cputime+0x63/0x80 [<ffffffff815b515b>] do_vfs_ioctl+0x54b/0xda0 ..... We may fix this in a few different ways, and in this patch, it's fixed simply by taking the refcount properly at snd_seq_create_port() and letting the caller unref the object after use. Also, there is another potential use-after-free by sprintf() call in snd_seq_create_port(), and this is moved inside the lock. This fix covers CVE-2017-15265. Reported-and-tested-by: Michael23 Yu <ycqzsy@gmail.com> Suggested-by: Linus Torvalds <torvalds@linux-foundation.org> Signed-off-by: Takashi Iwai <tiwai@suse.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ALSA: usb-audio: Kill stray URB at exitingTakashi Iwai2017-10-182-2/+12
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 124751d5e63c823092060074bd0abaae61aaa9c4 upstream. USB-audio driver may leave a stray URB for the mixer interrupt when it exits by some error during probe. This leads to a use-after-free error as spotted by syzkaller like: ================================================================== BUG: KASAN: use-after-free in snd_usb_mixer_interrupt+0x604/0x6f0 Call Trace: <IRQ> __dump_stack lib/dump_stack.c:16 dump_stack+0x292/0x395 lib/dump_stack.c:52 print_address_description+0x78/0x280 mm/kasan/report.c:252 kasan_report_error mm/kasan/report.c:351 kasan_report+0x23d/0x350 mm/kasan/report.c:409 __asan_report_load8_noabort+0x19/0x20 mm/kasan/report.c:430 snd_usb_mixer_interrupt+0x604/0x6f0 sound/usb/mixer.c:2490 __usb_hcd_giveback_urb+0x2e0/0x650 drivers/usb/core/hcd.c:1779 .... Allocated by task 1484: save_stack_trace+0x1b/0x20 arch/x86/kernel/stacktrace.c:59 save_stack+0x43/0xd0 mm/kasan/kasan.c:447 set_track mm/kasan/kasan.c:459 kasan_kmalloc+0xad/0xe0 mm/kasan/kasan.c:551 kmem_cache_alloc_trace+0x11e/0x2d0 mm/slub.c:2772 kmalloc ./include/linux/slab.h:493 kzalloc ./include/linux/slab.h:666 snd_usb_create_mixer+0x145/0x1010 sound/usb/mixer.c:2540 create_standard_mixer_quirk+0x58/0x80 sound/usb/quirks.c:516 snd_usb_create_quirk+0x92/0x100 sound/usb/quirks.c:560 create_composite_quirk+0x1c4/0x3e0 sound/usb/quirks.c:59 snd_usb_create_quirk+0x92/0x100 sound/usb/quirks.c:560 usb_audio_probe+0x1040/0x2c10 sound/usb/card.c:618 .... Freed by task 1484: save_stack_trace+0x1b/0x20 arch/x86/kernel/stacktrace.c:59 save_stack+0x43/0xd0 mm/kasan/kasan.c:447 set_track mm/kasan/kasan.c:459 kasan_slab_free+0x72/0xc0 mm/kasan/kasan.c:524 slab_free_hook mm/slub.c:1390 slab_free_freelist_hook mm/slub.c:1412 slab_free mm/slub.c:2988 kfree+0xf6/0x2f0 mm/slub.c:3919 snd_usb_mixer_free+0x11a/0x160 sound/usb/mixer.c:2244 snd_usb_mixer_dev_free+0x36/0x50 sound/usb/mixer.c:2250 __snd_device_free+0x1ff/0x380 sound/core/device.c:91 snd_device_free_all+0x8f/0xe0 sound/core/device.c:244 snd_card_do_free sound/core/init.c:461 release_card_device+0x47/0x170 sound/core/init.c:181 device_release+0x13f/0x210 drivers/base/core.c:814 .... Actually such a URB is killed properly at disconnection when the device gets probed successfully, and what we need is to apply it for the error-path, too. In this patch, we apply snd_usb_mixer_disconnect() at releasing. Also introduce a new flag, disconnected, to struct usb_mixer_interface for not performing the disconnection procedure twice. Reported-by: Andrey Konovalov <andreyknvl@google.com> Tested-by: Andrey Konovalov <andreyknvl@google.com> Signed-off-by: Takashi Iwai <tiwai@suse.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iommu/amd: Finish TLB flush in amd_iommu_unmap()Joerg Roedel2017-10-181-0/+1
| | | | | | | | | | | | | commit ce76353f169a6471542d999baf3d29b121dce9c0 upstream. The function only sends the flush command to the IOMMU(s), but does not wait for its completion when it returns. Fix that. Fixes: 601367d76bd1 ('x86/amd-iommu: Remove iommu_flush_domain function') Signed-off-by: Joerg Roedel <jroedel@suse.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* usb: renesas_usbhs: Fix DMAC sequence for receiving zero-length packetKazuya Mizuguchi2017-10-181-1/+1
| | | | | | | | | | | | | | | | | | | commit 29c7f3e68eec4ae94d85ad7b5dfdafdb8089f513 upstream. The DREQE bit of the DnFIFOSEL should be set to 1 after the DE bit of USB-DMAC on R-Car SoCs is set to 1 after the USB-DMAC received a zero-length packet. Otherwise, a transfer completion interruption of USB-DMAC doesn't happen. Even if the driver changes the sequence, normal operations (transmit/receive without zero-length packet) will not cause any side-effects. So, this patch fixes the sequence anyway. Signed-off-by: Kazuya Mizuguchi <kazuya.mizuguchi.ks@renesas.com> [shimoda: revise the commit log] Fixes: e73a9891b3a1 ("usb: renesas_usbhs: add DMAEngine support") Signed-off-by: Yoshihiro Shimoda <yoshihiro.shimoda.uh@renesas.com> Signed-off-by: Felipe Balbi <felipe.balbi@linux.intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* KVM: nVMX: fix guest CR4 loading when emulating L2 to L1 exitHaozhong Zhang2017-10-181-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 8eb3f87d903168bdbd1222776a6b1e281f50513e upstream. When KVM emulates an exit from L2 to L1, it loads L1 CR4 into the guest CR4. Before this CR4 loading, the guest CR4 refers to L2 CR4. Because these two CR4's are in different levels of guest, we should vmx_set_cr4() rather than kvm_set_cr4() here. The latter, which is used to handle guest writes to its CR4, checks the guest change to CR4 and may fail if the change is invalid. The failure may cause trouble. Consider we start a L1 guest with non-zero L1 PCID in use, (i.e. L1 CR4.PCIDE == 1 && L1 CR3.PCID != 0) and a L2 guest with L2 PCID disabled, (i.e. L2 CR4.PCIDE == 0) and following events may happen: 1. If kvm_set_cr4() is used in load_vmcs12_host_state() to load L1 CR4 into guest CR4 (in VMCS01) for L2 to L1 exit, it will fail because of PCID check. As a result, the guest CR4 recorded in L0 KVM (i.e. vcpu->arch.cr4) is left to the value of L2 CR4. 2. Later, if L1 attempts to change its CR4, e.g., clearing VMXE bit, kvm_set_cr4() in L0 KVM will think L1 also wants to enable PCID, because the wrong L2 CR4 is used by L0 KVM as L1 CR4. As L1 CR3.PCID != 0, L0 KVM will inject GP to L1 guest. Fixes: 4704d0befb072 ("KVM: nVMX: Exiting from L2 to L1") Cc: qemu-stable@nongnu.org Signed-off-by: Haozhong Zhang <haozhong.zhang@intel.com> Signed-off-by: Paolo Bonzini <pbonzini@redhat.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* crypto: shash - Fix zero-length shash ahash digest crashHerbert Xu2017-10-181-3/+5
| | | | | | | | | | | | | | | | commit b61907bb42409adf9b3120f741af7c57dd7e3db2 upstream. The shash ahash digest adaptor function may crash if given a zero-length input together with a null SG list. This is because it tries to read the SG list before looking at the length. This patch fixes it by checking the length first. Reported-by: Stephan Müller<smueller@chronox.de> Signed-off-by: Herbert Xu <herbert@gondor.apana.org.au> Tested-by: Stephan Müller <smueller@chronox.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* HID: usbhid: fix out-of-bounds bugJaejoong Kim2017-10-181-1/+11
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit f043bfc98c193c284e2cd768fefabe18ac2fed9b upstream. The hid descriptor identifies the length and type of subordinate descriptors for a device. If the received hid descriptor is smaller than the size of the struct hid_descriptor, it is possible to cause out-of-bounds. In addition, if bNumDescriptors of the hid descriptor have an incorrect value, this can also cause out-of-bounds while approaching hdesc->desc[n]. So check the size of hid descriptor and bNumDescriptors. BUG: KASAN: slab-out-of-bounds in usbhid_parse+0x9b1/0xa20 Read of size 1 at addr ffff88006c5f8edf by task kworker/1:2/1261 CPU: 1 PID: 1261 Comm: kworker/1:2 Not tainted 4.14.0-rc1-42251-gebb2c2437d80 #169 Hardware name: QEMU Standard PC (i440FX + PIIX, 1996), BIOS Bochs 01/01/2011 Workqueue: usb_hub_wq hub_event Call Trace: __dump_stack lib/dump_stack.c:16 dump_stack+0x292/0x395 lib/dump_stack.c:52 print_address_description+0x78/0x280 mm/kasan/report.c:252 kasan_report_error mm/kasan/report.c:351 kasan_report+0x22f/0x340 mm/kasan/report.c:409 __asan_report_load1_noabort+0x19/0x20 mm/kasan/report.c:427 usbhid_parse+0x9b1/0xa20 drivers/hid/usbhid/hid-core.c:1004 hid_add_device+0x16b/0xb30 drivers/hid/hid-core.c:2944 usbhid_probe+0xc28/0x1100 drivers/hid/usbhid/hid-core.c:1369 usb_probe_interface+0x35d/0x8e0 drivers/usb/core/driver.c:361 really_probe drivers/base/dd.c:413 driver_probe_device+0x610/0xa00 drivers/base/dd.c:557 __device_attach_driver+0x230/0x290 drivers/base/dd.c:653 bus_for_each_drv+0x161/0x210 drivers/base/bus.c:463 __device_attach+0x26e/0x3d0 drivers/base/dd.c:710 device_initial_probe+0x1f/0x30 drivers/base/dd.c:757 bus_probe_device+0x1eb/0x290 drivers/base/bus.c:523 device_add+0xd0b/0x1660 drivers/base/core.c:1835 usb_set_configuration+0x104e/0x1870 drivers/usb/core/message.c:1932 generic_probe+0x73/0xe0 drivers/usb/core/generic.c:174 usb_probe_device+0xaf/0xe0 drivers/usb/core/driver.c:266 really_probe drivers/base/dd.c:413 driver_probe_device+0x610/0xa00 drivers/base/dd.c:557 __device_attach_driver+0x230/0x290 drivers/base/dd.c:653 bus_for_each_drv+0x161/0x210 drivers/base/bus.c:463 __device_attach+0x26e/0x3d0 drivers/base/dd.c:710 device_initial_probe+0x1f/0x30 drivers/base/dd.c:757 bus_probe_device+0x1eb/0x290 drivers/base/bus.c:523 device_add+0xd0b/0x1660 drivers/base/core.c:1835 usb_new_device+0x7b8/0x1020 drivers/usb/core/hub.c:2457 hub_port_connect drivers/usb/core/hub.c:4903 hub_port_connect_change drivers/usb/core/hub.c:5009 port_event drivers/usb/core/hub.c:5115 hub_event+0x194d/0x3740 drivers/usb/core/hub.c:5195 process_one_work+0xc7f/0x1db0 kernel/workqueue.c:2119 worker_thread+0x221/0x1850 kernel/workqueue.c:2253 kthread+0x3a1/0x470 kernel/kthread.c:231 ret_from_fork+0x2a/0x40 arch/x86/entry/entry_64.S:431 Reported-by: Andrey Konovalov <andreyknvl@google.com> Signed-off-by: Jaejoong Kim <climbbb.kim@gmail.com> Tested-by: Andrey Konovalov <andreyknvl@google.com> Acked-by: Alan Stern <stern@rowland.harvard.edu> Signed-off-by: Jiri Kosina <jkosina@suse.cz> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* dmaengine: edma: Align the memcpy acnt array size with the transferPeter Ujfalusi2017-10-181-3/+16
| | | | | | | | | | | | | | | | | | | | | | | commit 87a2f622cc6446c7d09ac655b7b9b04886f16a4c upstream. Memory to Memory transfers does not have any special alignment needs regarding to acnt array size, but if one of the areas are in memory mapped regions (like PCIe memory), we need to make sure that the acnt array size is aligned with the mem copy parameters. Before "dmaengine: edma: Optimize memcpy operation" change the memcpy was set up in a different way: acnt == number of bytes in a word based on __ffs((src | dest | len), bcnt and ccnt for looping the necessary number of words to comlete the trasnfer. Instead of reverting the commit we can fix it to make sure that the ACNT size is aligned to the traswnfer. Fixes: df6694f80365a (dmaengine: edma: Optimize memcpy operation) Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com> Signed-off-by: Vinod Koul <vinod.koul@intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* MIPS: math-emu: Remove pr_err() calls from fpu_emu()Paul Burton2017-10-181-2/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | commit ca8eb05b5f332a9e1ab3e2ece498d49f4d683470 upstream. The FPU emulator includes 2 calls to pr_err() which are triggered by invalid instruction encodings for MIPSr6 cmp.cond.fmt instructions. These cases are not kernel errors, merely invalid instructions which are already handled by delivering a SIGILL which will provide notification that something failed in cases where that makes sense. In cases where that SIGILL is somewhat expected & being handled, for example when crashme happens to generate one of the affected bad encodings, the message is printed with no useful context about what triggered it & spams the kernel log for no good reason. Remove the pr_err() calls to make crashme run silently & treat the bad encodings the same way we do others, with a SIGILL & no further kernel log output. Signed-off-by: Paul Burton <paul.burton@imgtec.com> Fixes: f8c3c6717a71 ("MIPS: math-emu: Add support for the CMP.condn.fmt R6 instruction") Cc: linux-mips@linux-mips.org Patchwork: https://patchwork.linux-mips.org/patch/17253/ Signed-off-by: Ralf Baechle <ralf@linux-mips.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: dummy-hcd: Fix deadlock caused by disconnect detectionAlan Stern2017-10-181-3/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit ab219221a5064abfff9f78c323c4a257b16cdb81 upstream. The dummy-hcd driver calls the gadget driver's disconnect callback under the wrong conditions. It should invoke the callback when Vbus power is turned off, but instead it does so when the D+ pullup is turned off. This can cause a deadlock in the composite core when a gadget driver is unregistered: [ 88.361471] ============================================ [ 88.362014] WARNING: possible recursive locking detected [ 88.362580] 4.14.0-rc2+ #9 Not tainted [ 88.363010] -------------------------------------------- [ 88.363561] v4l_id/526 is trying to acquire lock: [ 88.364062] (&(&cdev->lock)->rlock){....}, at: [<ffffffffa0547e03>] composite_disconnect+0x43/0x100 [libcomposite] [ 88.365051] [ 88.365051] but task is already holding lock: [ 88.365826] (&(&cdev->lock)->rlock){....}, at: [<ffffffffa0547b09>] usb_function_deactivate+0x29/0x80 [libcomposite] [ 88.366858] [ 88.366858] other info that might help us debug this: [ 88.368301] Possible unsafe locking scenario: [ 88.368301] [ 88.369304] CPU0 [ 88.369701] ---- [ 88.370101] lock(&(&cdev->lock)->rlock); [ 88.370623] lock(&(&cdev->lock)->rlock); [ 88.371145] [ 88.371145] *** DEADLOCK *** [ 88.371145] [ 88.372211] May be due to missing lock nesting notation [ 88.372211] [ 88.373191] 2 locks held by v4l_id/526: [ 88.373715] #0: (&(&cdev->lock)->rlock){....}, at: [<ffffffffa0547b09>] usb_function_deactivate+0x29/0x80 [libcomposite] [ 88.374814] #1: (&(&dum_hcd->dum->lock)->rlock){....}, at: [<ffffffffa05bd48d>] dummy_pullup+0x7d/0xf0 [dummy_hcd] [ 88.376289] [ 88.376289] stack backtrace: [ 88.377726] CPU: 0 PID: 526 Comm: v4l_id Not tainted 4.14.0-rc2+ #9 [ 88.378557] Hardware name: QEMU Standard PC (i440FX + PIIX, 1996), BIOS 1.10.2-1 04/01/2014 [ 88.379504] Call Trace: [ 88.380019] dump_stack+0x86/0xc7 [ 88.380605] __lock_acquire+0x841/0x1120 [ 88.381252] lock_acquire+0xd5/0x1c0 [ 88.381865] ? composite_disconnect+0x43/0x100 [libcomposite] [ 88.382668] _raw_spin_lock_irqsave+0x40/0x54 [ 88.383357] ? composite_disconnect+0x43/0x100 [libcomposite] [ 88.384290] composite_disconnect+0x43/0x100 [libcomposite] [ 88.385490] set_link_state+0x2d4/0x3c0 [dummy_hcd] [ 88.386436] dummy_pullup+0xa7/0xf0 [dummy_hcd] [ 88.387195] usb_gadget_disconnect+0xd8/0x160 [udc_core] [ 88.387990] usb_gadget_deactivate+0xd3/0x160 [udc_core] [ 88.388793] usb_function_deactivate+0x64/0x80 [libcomposite] [ 88.389628] uvc_function_disconnect+0x1e/0x40 [usb_f_uvc] This patch changes the code to test the port-power status bit rather than the port-connect status bit when deciding whether to isue the callback. Signed-off-by: Alan Stern <stern@rowland.harvard.edu> Reported-by: David Tulloh <david@tulloh.id.au> Signed-off-by: Felipe Balbi <felipe.balbi@linux.intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* rcu: Allow for page faults in NMI handlersPaul E. McKenney2017-10-181-0/+12
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 28585a832602747cbfa88ad8934013177a3aae38 upstream. A number of architecture invoke rcu_irq_enter() on exception entry in order to allow RCU read-side critical sections in the exception handler when the exception is from an idle or nohz_full CPU. This works, at least unless the exception happens in an NMI handler. In that case, rcu_nmi_enter() would already have exited the extended quiescent state, which would mean that rcu_irq_enter() would (incorrectly) cause RCU to think that it is again in an extended quiescent state. This will in turn result in lockdep splats in response to later RCU read-side critical sections. This commit therefore causes rcu_irq_enter() and rcu_irq_exit() to take no action if there is an rcu_nmi_enter() in effect, thus avoiding the unscheduled return to RCU quiescent state. This in turn should make the kernel safe for on-demand RCU voyeurism. Link: http://lkml.kernel.org/r/20170922211022.GA18084@linux.vnet.ibm.com Cc: stable@vger.kernel.org Fixes: 0be964be0 ("module: Sanitize RCU usage and locking") Reported-by: Steven Rostedt <rostedt@goodmis.org> Signed-off-by: Paul E. McKenney <paulmck@linux.vnet.ibm.com> Signed-off-by: Steven Rostedt (VMware) <rostedt@goodmis.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iwlwifi: mvm: use IWL_HCMD_NOCOPY for MCAST_FILTER_CMDLuca Coelho2017-10-181-1/+9
| | | | | | | | | | | | | | | | | | commit 97bce57bd7f96e1218751996f549a6e61f18cc8c upstream. The MCAST_FILTER_CMD can get quite large when we have many mcast addresses to set (we support up to 255). So the command should be send as NOCOPY to prevent a warning caused by too-long commands: WARNING: CPU: 0 PID: 9700 at /root/iwlwifi/stack-dev/drivers/net/wireless/intel/iwlwifi/pcie/tx.c:1550 iwl_pcie_enqueue_hcmd+0x8c7/0xb40 [iwlwifi] Command MCAST_FILTER_CMD (0x1d0) is too large (328 bytes) This fixes: https://bugzilla.kernel.org/show_bug.cgi?id=196743 Signed-off-by: Luca Coelho <luciano.coelho@intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* nl80211: Define policy for packet pattern attributesPeng Xu2017-10-181-2/+10
| | | | | | | | | | | | | | | | | | | | | | | | | commit ad670233c9e1d5feb365d870e30083ef1b889177 upstream. Define a policy for packet pattern attributes in order to fix a potential read over the end of the buffer during nla_get_u32() of the NL80211_PKTPAT_OFFSET attribute. Note that the data there can always be read due to SKB allocation (with alignment and struct skb_shared_info at the end), but the data might be uninitialized. This could be used to leak some data from uninitialized vmalloc() memory, but most drivers don't allow an offset (so you'd just get -EINVAL if the data is non-zero) or just allow it with a fixed value - 100 or 128 bytes, so anything above that would get -EINVAL. With brcmfmac the limit is 1500 so (at least) one byte could be obtained. Cc: stable@kernel.org Signed-off-by: Peng Xu <pxu@qti.qualcomm.com> Signed-off-by: Jouni Malinen <jouni@qca.qualcomm.com> [rewrite description based on SKB allocation knowledge] Signed-off-by: Johannes Berg <johannes.berg@intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* CIFS: Reconnect expired SMB sessionsPavel Shilovsky2017-10-184-0/+32
| | | | | | | | | | | | | | | | commit 511c54a2f69195b28afb9dd119f03787b1625bb4 upstream. According to the MS-SMB2 spec (3.2.5.1.6) once the client receives STATUS_NETWORK_SESSION_EXPIRED error code from a server it should reconnect the current SMB session. Currently the client doesn't do that. This can result in subsequent client requests failing by the server. The patch adds an additional logic to the demultiplex thread to identify expired sessions and reconnect them. Signed-off-by: Pavel Shilovsky <pshilov@microsoft.com> Signed-off-by: Steve French <smfrench@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ext4: in ext4_seek_{hole,data}, return -ENXIO for negative offsetsDarrick J. Wong2017-10-181-2/+2
| | | | | | | | | | | | | | commit 1bd8d6cd3e413d64e543ec3e69ff43e75a1cf1ea upstream. In the ext4 implementations of SEEK_HOLE and SEEK_DATA, make sure we return -ENXIO for negative offsets instead of banging around inside the extent code and returning -EFSCORRUPTED. Reported-by: Mateusz S <muttdini@gmail.com> Signed-off-by: Darrick J. Wong <darrick.wong@oracle.com> Signed-off-by: Theodore Ts'o <tytso@mit.edu> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* brcmfmac: add length check in brcmf_cfg80211_escan_handler()Arend Van Spriel2017-10-181-3/+15
| | | | | | | | | | | | | | | | | commit 17df6453d4be17910456e99c5a85025aa1b7a246 upstream. Upon handling the firmware notification for scans the length was checked properly and may result in corrupting kernel heap memory due to buffer overruns. This fix addresses CVE-2017-0786. Cc: Kevin Cernekee <cernekee@chromium.org> Reviewed-by: Hante Meuleman <hante.meuleman@broadcom.com> Reviewed-by: Pieter-Paul Giesberts <pieter-paul.giesberts@broadcom.com> Reviewed-by: Franky Lin <franky.lin@broadcom.com> Signed-off-by: Arend van Spriel <arend.vanspriel@broadcom.com> Signed-off-by: Kalle Valo <kvalo@codeaurora.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* Linux 4.4.92v4.4.92Greg Kroah-Hartman2017-10-121-1/+1
|
* ext4: don't allow encrypted operations without keysTheodore Ts'o2017-10-121-0/+12
| | | | | | | | | | | | | | | | | | | commit 173b8439e1ba362007315868928bf9d26e5cc5a6 upstream. While we allow deletes without the key, the following should not be permitted: # cd /vdc/encrypted-dir-without-key # ls -l total 4 -rw-r--r-- 1 root root 0 Dec 27 22:35 6,LKNRJsp209FbXoSvJWzB -rw-r--r-- 1 root root 286 Dec 27 22:35 uRJ5vJh9gE7vcomYMqTAyD # mv uRJ5vJh9gE7vcomYMqTAyD 6,LKNRJsp209FbXoSvJWzB Signed-off-by: Theodore Ts'o <tytso@mit.edu> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ext4: Don't clear SGID when inheriting ACLsJan Kara2017-10-121-7/+15
| | | | | | | | | | | | | | | | | | | | | | | commit a3bb2d5587521eea6dab2d05326abb0afb460abd upstream. When new directory 'DIR1' is created in a directory 'DIR0' with SGID bit set, DIR1 is expected to have SGID bit set (and owning group equal to the owning group of 'DIR0'). However when 'DIR0' also has some default ACLs that 'DIR1' inherits, setting these ACLs will result in SGID bit on 'DIR1' to get cleared if user is not member of the owning group. Fix the problem by moving posix_acl_update_mode() out of __ext4_set_acl() into ext4_set_acl(). That way the function will not be called when inheriting ACLs which is what we want as it prevents SGID bit clearing and the mode has been properly set by posix_acl_create() anyway. Fixes: 073931017b49d9458aa351605b43a7e34598caef Signed-off-by: Theodore Ts'o <tytso@mit.edu> Signed-off-by: Jan Kara <jack@suse.cz> Reviewed-by: Andreas Gruenbacher <agruenba@redhat.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ext4: fix data corruption for mmap writesJan Kara2017-10-121-5/+19
| | | | | | | | | | | | | | | | | | | | commit a056bdaae7a181f7dcc876cfab2f94538e508709 upstream. mpage_submit_page() can race with another process growing i_size and writing data via mmap to the written-back page. As mpage_submit_page() samples i_size too early, it may happen that ext4_bio_write_page() zeroes out too large tail of the page and thus corrupts user data. Fix the problem by sampling i_size only after the page has been write-protected in page tables by clear_page_dirty_for_io() call. Reported-by: Michael Zimmer <michael@swarm64.com> CC: stable@vger.kernel.org Fixes: cb20d5188366f04d96d2e07b1240cc92170ade40 Signed-off-by: Jan Kara <jack@suse.cz> Signed-off-by: Theodore Ts'o <tytso@mit.edu> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* sched/cpuset/pm: Fix cpuset vs. suspend-resume bugsPeter Zijlstra2017-10-124-6/+28
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 50e76632339d4655859523a39249dd95ee5e93e7 upstream. Cpusets vs. suspend-resume is _completely_ broken. And it got noticed because it now resulted in non-cpuset usage breaking too. On suspend cpuset_cpu_inactive() doesn't call into cpuset_update_active_cpus() because it doesn't want to move tasks about, there is no need, all tasks are frozen and won't run again until after we've resumed everything. But this means that when we finally do call into cpuset_update_active_cpus() after resuming the last frozen cpu in cpuset_cpu_active(), the top_cpuset will not have any difference with the cpu_active_mask and this it will not in fact do _anything_. So the cpuset configuration will not be restored. This was largely hidden because we would unconditionally create identity domains and mobile users would not in fact use cpusets much. And servers what do use cpusets tend to not suspend-resume much. An addition problem is that we'd not in fact wait for the cpuset work to finish before resuming the tasks, allowing spurious migrations outside of the specified domains. Fix the rebuild by introducing cpuset_force_rebuild() and fix the ordering with cpuset_wait_for_hotplug(). Reported-by: Andy Lutomirski <luto@kernel.org> Signed-off-by: Peter Zijlstra (Intel) <peterz@infradead.org> Cc: <stable@vger.kernel.org> Cc: Andy Lutomirski <luto@amacapital.net> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Mike Galbraith <efault@gmx.de> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Rafael J. Wysocki <rjw@rjwysocki.net> Cc: Tejun Heo <tj@kernel.org> Cc: Thomas Gleixner <tglx@linutronix.de> Fixes: deb7aa308ea2 ("cpuset: reorganize CPU / memory hotplug handling") Link: http://lkml.kernel.org/r/20170907091338.orwxrqkbfkki3c24@hirez.programming.kicks-ass.net Signed-off-by: Ingo Molnar <mingo@kernel.org> Signed-off-by: Mike Galbraith <efault@gmx.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* nvme: protect against simultaneous shutdown invocationsKeith Busch2017-10-122-0/+5
| | | | | | | | | | | | | | | | | | commit 77bf25ea70200cddf083f74b7f617e5f07fac8bd upstream. [Back-ported to 4.4. The difference is the file location of the struct definition that's adding the mutex. This fixes reported kernel panics in 4.4-stable from simultaneous controller resets that was never supposed to be allowed to happen.] Signed-off-by: Keith Busch <keith.busch@intel.com> [hch: split from a larger patch] Signed-off-by: Christoph Hellwig <hch@lst.de> Signed-off-by: Jens Axboe <axboe@fb.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* drm/i915/bios: ignore HDMI on port AJani Nikula2017-10-121-0/+7
| | | | | | | | | | | | | | | | | | | | | commit 2ba7d7e0437127314864238f8bfcb8369d81075c upstream. The hardware state readout oopses after several warnings when trying to use HDMI on port A, if such a combination is configured in VBT. Filter the combo out already at the VBT parsing phase. v2: also ignore DVI (Ville) Bugzilla: https://bugs.freedesktop.org/show_bug.cgi?id=102889 Cc: Imre Deak <imre.deak@intel.com> Reviewed-by: Ville Syrjälä <ville.syrjala@linux.intel.com> Tested-by: Daniel Drake <dan@reactivated.net> Signed-off-by: Jani Nikula <jani.nikula@intel.com> Link: https://patchwork.freedesktop.org/patch/msgid/20170921141920.18172-1-jani.nikula@intel.com (cherry picked from commit d27ffc1d00327c29b3aa97f941b42f0949f9e99f) Signed-off-by: Rodrigo Vivi <rodrigo.vivi@intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* brcmfmac: setup passive scan if requested by user-spaceArend Van Spriel2017-10-122-15/+9
| | | | | | | | | | | | | | | | | | commit 35f62727df0ed8e5e4857e162d94fd46d861f1cf upstream. The driver was not properly configuring firmware with regard to the type of scan. It always performed an active scan even when user-space was requesting for passive scan, ie. the scan request was done without any SSIDs specified. Reported-by: Huang, Jiangyang <Jiangyang.Huang@itron.com> Reviewed-by: Hante Meuleman <hante.meuleman@broadcom.com> Reviewed-by: Pieter-Paul Giesberts <pieter-paul.giesberts@broadcom.com> Reviewed-by: Franky Lin <franky.lin@broadcom.com> Signed-off-by: Arend van Spriel <arend.vanspriel@broadcom.com> Signed-off-by: Kalle Valo <kvalo@codeaurora.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* uwb: ensure that endpoint is interruptAndrey Konovalov2017-10-121-0/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 70e743e4cec3733dc13559f6184b35d358b9ef3f upstream. hwarc_neep_init() assumes that endpoint 0 is interrupt, but there's no check for that, which results in a WARNING in USB core code, when a bad USB descriptor is provided from a device: usb 1-1: BOGUS urb xfer, pipe 1 != type 3 ------------[ cut here ]------------ WARNING: CPU: 0 PID: 3 at drivers/usb/core/urb.c:449 usb_submit_urb+0xf8a/0x11d0 Modules linked in: CPU: 0 PID: 3 Comm: kworker/0:0 Not tainted 4.13.0+ #111 Hardware name: QEMU Standard PC (i440FX + PIIX, 1996), BIOS Bochs 01/01/2011 Workqueue: usb_hub_wq hub_event task: ffff88006bdc1a00 task.stack: ffff88006bde8000 RIP: 0010:usb_submit_urb+0xf8a/0x11d0 drivers/usb/core/urb.c:448 RSP: 0018:ffff88006bdee3c0 EFLAGS: 00010282 RAX: 0000000000000029 RBX: ffff8800672a7200 RCX: 0000000000000000 RDX: 0000000000000029 RSI: ffff88006c815c78 RDI: ffffed000d7bdc6a RBP: ffff88006bdee4c0 R08: fffffbfff0fe00ff R09: fffffbfff0fe00ff R10: 0000000000000018 R11: fffffbfff0fe00fe R12: 1ffff1000d7bdc7f R13: 0000000000000003 R14: 0000000000000001 R15: ffff88006b02cc90 FS: 0000000000000000(0000) GS:ffff88006c800000(0000) knlGS:0000000000000000 CS: 0010 DS: 0000 ES: 0000 CR0: 0000000080050033 CR2: 00007fe4daddf000 CR3: 000000006add6000 CR4: 00000000000006f0 Call Trace: hwarc_neep_init+0x4ce/0x9c0 drivers/uwb/hwa-rc.c:710 uwb_rc_add+0x2fb/0x730 drivers/uwb/lc-rc.c:361 hwarc_probe+0x34e/0x9b0 drivers/uwb/hwa-rc.c:858 usb_probe_interface+0x351/0x8d0 drivers/usb/core/driver.c:361 really_probe drivers/base/dd.c:385 driver_probe_device+0x610/0xa00 drivers/base/dd.c:529 __device_attach_driver+0x230/0x290 drivers/base/dd.c:625 bus_for_each_drv+0x15e/0x210 drivers/base/bus.c:463 __device_attach+0x269/0x3c0 drivers/base/dd.c:682 device_initial_probe+0x1f/0x30 drivers/base/dd.c:729 bus_probe_device+0x1da/0x280 drivers/base/bus.c:523 device_add+0xcf9/0x1640 drivers/base/core.c:1703 usb_set_configuration+0x1064/0x1890 drivers/usb/core/message.c:1932 generic_probe+0x73/0xe0 drivers/usb/core/generic.c:174 usb_probe_device+0xaf/0xe0 drivers/usb/core/driver.c:266 really_probe drivers/base/dd.c:385 driver_probe_device+0x610/0xa00 drivers/base/dd.c:529 __device_attach_driver+0x230/0x290 drivers/base/dd.c:625 bus_for_each_drv+0x15e/0x210 drivers/base/bus.c:463 __device_attach+0x269/0x3c0 drivers/base/dd.c:682 device_initial_probe+0x1f/0x30 drivers/base/dd.c:729 bus_probe_device+0x1da/0x280 drivers/base/bus.c:523 device_add+0xcf9/0x1640 drivers/base/core.c:1703 usb_new_device+0x7b8/0x1020 drivers/usb/core/hub.c:2457 hub_port_connect drivers/usb/core/hub.c:4890 hub_port_connect_change drivers/usb/core/hub.c:4996 port_event drivers/usb/core/hub.c:5102 hub_event+0x23c8/0x37c0 drivers/usb/core/hub.c:5182 process_one_work+0x9fb/0x1570 kernel/workqueue.c:2097 worker_thread+0x1e4/0x1350 kernel/workqueue.c:2231 kthread+0x324/0x3f0 kernel/kthread.c:231 ret_from_fork+0x25/0x30 arch/x86/entry/entry_64.S:425 Code: 48 8b 85 30 ff ff ff 48 8d b8 98 00 00 00 e8 8e 93 07 ff 45 89 e8 44 89 f1 4c 89 fa 48 89 c6 48 c7 c7 a0 e5 55 86 e8 20 08 8f fd <0f> ff e9 9b f7 ff ff e8 4a 04 d6 fd e9 80 f7 ff ff e8 60 11 a6 ---[ end trace 55d741234124cfc3 ]--- Check that endpoint is interrupt. Found by syzkaller. Signed-off-by: Andrey Konovalov <andreyknvl@google.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* uwb: properly check kthread_run return valueAndrey Konovalov2017-10-121-4/+8
| | | | | | | | | | | | | | | | commit bbf26183b7a6236ba602f4d6a2f7cade35bba043 upstream. uwbd_start() calls kthread_run() and checks that the return value is not NULL. But the return value is not NULL in case kthread_run() fails, it takes the form of ERR_PTR(-EINTR). Use IS_ERR() instead. Also add a check to uwbd_stop(). Signed-off-by: Andrey Konovalov <andreyknvl@google.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: adc: mcp320x: Fix oops on module unloadLukas Wunner2017-10-121-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | commit 0964e40947a630a2a6f724e968246992f97bcf1c upstream. The driver calls spi_get_drvdata() in its ->remove hook even though it has never called spi_set_drvdata(). Stack trace for posterity: Unable to handle kernel NULL pointer dereference at virtual address 00000220 Internal error: Oops: 5 [#1] SMP ARM [<8072f564>] (mutex_lock) from [<7f1400d0>] (iio_device_unregister+0x24/0x7c [industrialio]) [<7f1400d0>] (iio_device_unregister [industrialio]) from [<7f15e020>] (mcp320x_remove+0x20/0x30 [mcp320x]) [<7f15e020>] (mcp320x_remove [mcp320x]) from [<8055a8cc>] (spi_drv_remove+0x2c/0x44) [<8055a8cc>] (spi_drv_remove) from [<805087bc>] (__device_release_driver+0x98/0x134) [<805087bc>] (__device_release_driver) from [<80509180>] (driver_detach+0xdc/0xe0) [<80509180>] (driver_detach) from [<8050823c>] (bus_remove_driver+0x5c/0xb0) [<8050823c>] (bus_remove_driver) from [<80509ab0>] (driver_unregister+0x38/0x58) [<80509ab0>] (driver_unregister) from [<7f15e69c>] (mcp320x_driver_exit+0x14/0x1c [mcp320x]) [<7f15e69c>] (mcp320x_driver_exit [mcp320x]) from [<801a78d0>] (SyS_delete_module+0x184/0x1d0) [<801a78d0>] (SyS_delete_module) from [<80108100>] (ret_fast_syscall+0x0/0x1c) Fixes: f5ce4a7a9291 ("iio: adc: add driver for MCP3204/08 12-bit ADC") Cc: Oskar Andero <oskar.andero@gmail.com> Signed-off-by: Lukas Wunner <lukas@wunner.de> Signed-off-by: Jonathan Cameron <Jonathan.Cameron@huawei.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: adc: mcp320x: Fix readout of negative voltagesLukas Wunner2017-10-121-9/+15
| | | | | | | | | | | | | | | | | | | | commit e6f4794371ee7cce1339e7ca9542f1e703c5f84a upstream. Commit f686a36b4b79 ("iio: adc: mcp320x: Add support for mcp3301") returns a signed voltage from mcp320x_adc_conversion() but neglects that the caller interprets a negative return value as failure. Only mcp3301 (and the upcoming mcp3550/1/3) is affected as the other chips are incapable of measuring negative voltages. Fix and while at it, add mcp3301 to the list of supported chips at the top of the file. Fixes: f686a36b4b79 ("iio: adc: mcp320x: Add support for mcp3301") Cc: Andrea Galbusera <gizero@gmail.com> Signed-off-by: Lukas Wunner <lukas@wunner.de> Signed-off-by: Jonathan Cameron <Jonathan.Cameron@huawei.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: ad7793: Fix the serial interface resetDragos Bogdan2017-10-121-2/+2
| | | | | | | | | | | | | | | | commit 7ee3b7ebcb74714df6d94c8f500f307e1ee5dda5 upstream. The serial interface can be reset by writing 32 consecutive 1s to the device. 'ret' was initialized correctly but its value was overwritten when ad7793_check_platform_data() was called. Since a dedicated reset function is present now, it should be used instead. Fixes: 2edb769d246e ("iio:ad7793: Add support for the ad7798 and ad7799") Signed-off-by: Dragos Bogdan <dragos.bogdan@analog.com> Acked-by: Lars-Peter Clausen <lars@metafoo.de> Signed-off-by: Jonathan Cameron <Jonathan.Cameron@huawei.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: core: Return error for failed read_regMatt Fornero2017-10-121-1/+3
| | | | | | | | | | | | | | | commit 3d62c78a6eb9a7d67bace9622b66ad51e81c5f9b upstream. If an IIO device returns an error code for a read access via debugfs, it is currently ignored by the IIO core (other than emitting an error message). Instead, return this error code to user space, so upper layers can detect it correctly. Signed-off-by: Matt Fornero <matt.fornero@mathworks.com> Signed-off-by: Lars-Peter Clausen <lars@metafoo.de> Signed-off-by: Jonathan Cameron <Jonathan.Cameron@huawei.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* staging: iio: ad7192: Fix - use the dedicated reset function avoiding dma ↵Stefan Popa2017-10-121-3/+1
| | | | | | | | | | | | | | | | | | | | from stack. commit f790923f146140a261ad211e5baf75d169f16fb2 upstream. Depends on: 691c4b95d1 ("iio: ad_sigma_delta: Implement a dedicated reset function") SPI host drivers can use DMA to transfer data, so the buffer should be properly allocated. Keeping it on the stack could cause an undefined behavior. The dedicated reset function solves this issue. Signed-off-by: Stefan Popa <stefan.popa@analog.com> Acked-by: Lars-Peter Clausen <lars@metafoo.de> Acked-by: Michael Hennerich <michael.hennerich@analog.com> Signed-off-by: Jonathan Cameron <Jonathan.Cameron@huawei.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: ad_sigma_delta: Implement a dedicated reset functionDragos Bogdan2017-10-122-0/+31
| | | | | | | | | | | | | | | commit 7fc10de8d49a748c476532c9d8e8fe19e548dd67 upstream. Since most of the SD ADCs have the option of reseting the serial interface by sending a number of SCLKs with CS = 0 and DIN = 1, a dedicated function that can do this is usefull. Needed for the patch: iio: ad7793: Fix the serial interface reset Signed-off-by: Dragos Bogdan <dragos.bogdan@analog.com> Acked-by: Lars-Peter Clausen <lars@metafoo.de> Signed-off-by: Jonathan Cameron <Jonathan.Cameron@huawei.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: adc: twl4030: Disable the vusb3v1 rugulator in the error handling path ↵Christophe JAILLET2017-10-121-1/+3
| | | | | | | | | | | | | | | | | | | of 'twl4030_madc_probe()' commit 7f70be6e4025db0551e6863e7eb9cca07122695c upstream. Commit 7cc97d77ee8a has introduced a call to 'regulator_disable()' in the .remove function. So we should also have such a call in the .probe function in case of error after a successful 'regulator_enable()' call. Add a new label for that and use it. Fixes: 7cc97d77ee8a ("iio: adc: twl4030: Fix ADC[3:6] readings") Signed-off-by: Christophe JAILLET <christophe.jaillet@wanadoo.fr> Signed-off-by: Jonathan Cameron <Jonathan.Cameron@huawei.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: adc: twl4030: Fix an error handling path in 'twl4030_madc_probe()'Christophe JAILLET2017-10-121-2/+4
| | | | | | | | | | | | | | commit 245a396a9b1a67ac5c3228737c261b3e48708a2a upstream. If 'devm_regulator_get()' fails, we should go through the existing error handling path instead of returning directly, as done is all the other error handling paths in this function. Fixes: 7cc97d77ee8a ("iio: adc: twl4030: Fix ADC[3:6] readings") Signed-off-by: Christophe JAILLET <christophe.jaillet@wanadoo.fr> Signed-off-by: Jonathan Cameron <Jonathan.Cameron@huawei.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* xhci: fix finding correct bus_state structure for USB 3.1 hostsMathias Nyman2017-10-121-1/+1
| | | | | | | | | | | | | | | commit 5a838a13c9b4e5dd188b7a6eaeb894e9358ead0c upstream. xhci driver keeps a bus_state structure for each hcd (usb2 and usb3) The structure is picked based on hcd speed, but driver only compared for HCD_USB3 speed, returning the wrong bus_state for HCD_USB31 hosts. This caused null pointer dereference errors in bus_resume function. Signed-off-by: Mathias Nyman <mathias.nyman@linux.intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: fix out-of-bounds in usb_set_configurationGreg Kroah-Hartman2017-10-122-3/+12
| | | | | | | | | | | | | | | | | | | commit bd7a3fe770ebd8391d1c7d072ff88e9e76d063eb upstream. Andrey Konovalov reported a possible out-of-bounds problem for a USB interface association descriptor. He writes: It seems there's no proper size check of a USB_DT_INTERFACE_ASSOCIATION descriptor. It's only checked that the size is >= 2 in usb_parse_configuration(), so find_iad() might do out-of-bounds access to intf_assoc->bInterfaceCount. And he's right, we don't check for crazy descriptors of this type very well, so resolve this problem. Yet another issue found by syzkaller... Reported-by: Andrey Konovalov <andreyknvl@google.com> Tested-by: Andrey Konovalov <andreyknvl@google.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* usb: Increase quirk delay for USB devicesDmitry Fleytman2017-10-122-2/+2
| | | | | | | | | | | | | | | | | | | | | commit b2a542bbb3081dbd64acc8929c140d196664c406 upstream. Commit e0429362ab15 ("usb: Add device quirk for Logitech HD Pro Webcams C920 and C930e") introduced quirk to workaround an issue with some Logitech webcams. The workaround is introducing delay for some USB operations. According to our testing, delay introduced by original commit is not long enough and in rare cases we still see issues described by the aforementioned commit. This patch increases delays introduced by original commit. Having this patch applied we do not see those problems anymore. Signed-off-by: Dmitry Fleytman <dmitry@daynix.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>