aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* Documentation: DT bindings: add more Tegra chip compatible stringsPaul Walmsley2015-02-031-1/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Align compatible strings for several IP blocks present on Tegra chips with the latest doctrine from the DT maintainers: http://marc.info/?l=devicetree&m=142255654213019&w=2 The primary objective here is to avoid checkpatch warnings, per: http://marc.info/?l=linux-tegra&m=142201349727836&w=2 DT binding text files have been updated for the following IP blocks: - PCIe - SOR - SoC timers - AHB "gizmo" - APB_MISC - pinmux control - UART - PWM - I2C - SPI - RTC - PMC - eFuse - AHCI - HDA - XUSB_PADCTRL - SDHCI - SOC_THERM - AHUB - I2S - EHCI - USB PHY N.B. The nvidia,tegra20-timer compatible string is removed from the nvidia,tegra30-timer.txt documentation file because it's already mentioned in the nvidia,tegra20-timer.txt documentation file. This second version takes into account the following requests from Rob Herring <robherring2@gmail.com>: - Per-IP block patches have been combined into a single patch - Explicit documentation about which compatible strings are actually matched by the driver has been removed. In its place is implicit documentation that loosely follows Rob's prescribed format: "Must contain '"nvidia,<chip>-pcie", "nvidia,tegra20-pcie"' where <chip> is tegra30, tegra132, ..." [...] "You should attempt to document known values of <chip> if you use it" Signed-off-by: Paul Walmsley <paul@pwsan.com> Cc: Alexandre Courbot <gnurou@gmail.com> Cc: Dylan Reid <dgreid@chromium.org> Cc: Greg Kroah-Hartman <gregkh@linuxfoundation.org> Cc: Hans de Goede <hdegoede@redhat.com> Cc: Ian Campbell <ijc+devicetree@hellion.org.uk> Cc: Jingchang Lu <jingchang.lu@freescale.com> Cc: John Crispin <blogic@openwrt.org> Cc: Kumar Gala <galak@codeaurora.org> Cc: Linus Walleij <linus.walleij@linaro.org> Cc: Mark Rutland <mark.rutland@arm.com> Cc: Mikko Perttunen <mperttunen@nvidia.com> Cc: Murali Karicheri <m-karicheri2@ti.com> Cc: Paul Walmsley <pwalmsley@nvidia.com> Cc: Pawel Moll <pawel.moll@arm.com> Cc: Peter De Schrijver <pdeschrijver@nvidia.com> Cc: Peter Hurley <peter@hurleysoftware.com> Cc: Sean Paul <seanpaul@chromium.org> Cc: Stephen Warren <swarren@wwwdotorg.org> Cc: Takashi Iwai <tiwai@suse.de> Cc: Tejun Heo <tj@kernel.org> Cc: "Terje Bergström" <tbergstrom@nvidia.com> Cc: Thierry Reding <thierry.reding@gmail.com> Cc: Tuomas Tynkkynen <ttynkkynen@nvidia.com> Cc: Wolfram Sang <wsa@the-dreams.de> Cc: Zhang Rui <rui.zhang@intel.com> Cc: dri-devel@lists.freedesktop.org Cc: linux-i2c@vger.kernel.org Cc: linux-kernel@vger.kernel.org Cc: linux-pci@vger.kernel.org Cc: linux-pm@vger.kernel.org Cc: linux-pwm@vger.kernel.org Cc: linux-tegra@vger.kernel.org Acked-by: Eduardo Valentin <edubezval@gmail.com> Signed-off-by: Rob Herring <robh@kernel.org>
* ARM: tegra: document reset properties in DT bindingsStephen Warren2013-12-111-0/+6
| | | | | | | | | | | | | | Update all the Tegra DT bindings to require resets/reset-names properties where the HW module has reset inputs. Remove any entries from clocks or clock-names that were only required to identify reset inputs, rather than referring to real clocks. This is a DT-ABI-incompatible change. It is the first of two changes required for me to consider the Tegra DT bindings as stable, the other being conversion to the common DMA DT bindings. Signed-off-by: Stephen Warren <swarren@nvidia.com> Acked-By: Terje Bergstrom <tbergstrom@nvidia.com>
* ARM: tegra: add missing clock documentation to DT bindingsStephen Warren2013-12-111-1/+4
| | | | | | | | | | | | | Many of the Tegra DT binding documents say nothing about the clocks or clock-names properties, yet those are present and required in DT files. This patch simply updates the documentation file to match the implicit definition of the binding, based on real-world DT content. All Tegra bindings that mention clocks are updated to have consistent wording and formatting of the clock-related properties. Signed-off-by: Stephen Warren <swarren@nvidia.com> Acked-By: Terje Bergstrom <tbergstrom@nvidia.com>
* ASoC: tegra: add tegra30-i2s driverStephen Warren2012-04-131-0/+15
This provides an ASoC DAI interface for Tegra 30's I2S controller. Includes a squashed bugfix from Sumit Bhattacharya <sumitb@nvidia.com> Signed-off-by: Stephen Warren <swarren@nvidia.com> Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>